Post Go back to editing

64-bit build of Kuiper Linux with IndustrialIO for Raspberry Pi 4B

Thread Summary

The user asked if IIO works with the ADIS16475 series of IMUs on 64-bit Linux and if 64-bit builds of Kuiper Linux are available for the Raspberry Pi 4B. The final answer confirmed that libiio and iiod work on 64-bit systems, and provided the Kuiper build process. The user needed to update the device tree overlay parameters to include 'dtparam=device="adi,adis16465-2"' and 'dtparam=drdy_gpio25' to correctly load the ADIS16465 IMU.
AI Generated Content
Category: Software
Product Number: ADIS16475, ADIS16465, EVAL-ADISIMU1-RPIZ

Does IIO work with the ADIS16475 series of IMUs on 64-bit Linux? Are there 64-bit builds of Kuiper Linux that run on the Raspberry Pi 4B available yet (or coming soon)? Ultimately I hope to build a custom 64-bit image with a recent kernel using the IIO support which ADIS has upstreamed. My earlier attempts haven't worked (see  Problem starting iiod with the ADIS16465 on a custom Linux build ) so I'd like to try again with the most recent Kuiper build. How should I set up a Kuiper build environment for this experiment?

Parents Reply
  • Thanks for the details, that helps a lot. I had tried setting it to adis16465 and tried strings from the driver like "adis16465-2", which also didn't work. But since the working image showed "adi,adis16477-1" I used a value like that and now I have an iio device.

    In case anyone else needs it, this is exactly what I added to /boot/config.txt for Kuiper built with a 5.10.63 kernel:

    dtoverlay=adis16475
    dtparam=device="adi,adis16465-2"
    dtparam=drdy_gpio25

    The output from vcdbg log mesg was also really useful for seeing what dtparam value was applied.

Children
No Data