Post Go back to editing

Failure in building ZCU102-ADRV9009 Project

Category: Software

Hello All

I am trying to configure ADRV9009 connected to ZCU102 by following the links

1. https://wiki.analog.com/resources/eval/user-guides/adrv9002/quickstart/zynqmp

2. https://github.com/analogdevicesinc/meta-adi/tree/2019_R2/meta-adi-xilinx#adding-a-new-devicetree

3. github.com/.../2019_R2

for Vivado 2019.1 version. This project is was executed and the images were created successfully last year However, when I am trying to build a new  project , I am the receiving the error that system-conf.dtsi file is not available. The screenshot for the same is attached.  I am observing this error after commenting the line sed -i '/&qspi/,/^$/d; /&axi_ethernet/,/^$/d' "${DT_FILES_PATH}/system-conf.dtsi" by following this link :  Build petalinux 2019.1 + meta-adi

It is observed that components/plnx-workspace/device-tree is not created where the system-conf.dtsi is saved.

Requesting to help me in resolving this issue.

     

  • Hi,

    It seems like that you need to add a new devicetree to meta-adi? Or do you want to do a plain build of the supported project? I will do a build on my side to see if it works for me.

    Did you already tried to do a clean build?

    I am observing this error after commenting the line sed -i '/&qspi/,/^$/d; /&axi_ethernet/,/^$/d' "${DT_FILES_PATH}/system-conf.dtsi" by following this link

    You should not really need to comment this one as... Are you using petalinux? On the link you posted, yocto was being used...

    - Nuno Sá

  • Hello Nuno Sá

    Thanks for response.

    I want to do a plain build of the supported project without adding a new devicetree to meta-adi. 

    I didn't perform clean build, I will perform that.

    I had to comment this line : sed -i '/&qspi/,/^$/d; /&axi_ethernet/,/^$/d' "${DT_FILES_PATH}/system-conf.dtsi because I was receiving error similar to one posted in  Build petalinux 2019.1 + meta-adi  while using yocto.

    Requesting your suggestions.

    -Deepika