Post Go back to editing

Linux Kernel defconfig for ADRV9364-Z7020 + ADVR1CC-BoB

Hardware: ADRV9364-Z7020 + ADVR1CC-BoB

Question: From this link in the 'Configure the Kernel' section it is required to follow this step;

dave@hal9000:~/github-linux-build/linux$ make zynq_xcomm_adv7511_defconfig

My question is - does the above defconfig apply to any Analog Devices SDR card with a Zynq based carrier such as the combination that I have (see in title and beginning of this post)
I looked in the directory arch/arm/configs/ of the Linux Kernel git repo and could not find any other relevant defconfig and was confused because my hardware is not the adv5711

Or should I be using some other defconfig file?

Follow up question: How does this recommended Kernel config differ from the 'xilinx_zynq_defconfig' configuration?



Thank you