Post Go back to editing

QEC INIT

Thread Summary

The user needed to disable TX_QEC_INIT in the AD9371 driver and encountered errors due to incorrect clock settings. The solution involved modifying the device tree to use a VCO divider of 1 (instead of 1.5) and ensuring the VCO frequency did not exceed 9.216 GHz. The final configuration included setting adi,clocks-clk-pll-vco-div to 1 and adi,clocks-clk-pll-vco-freq_khz to 9600000, while maintaining the device clock at 80000 kHz.
AI Generated Content

hello i need to disable TX_QEC_init i dont understand how to do it?

in ug-992 Rev. B | Page 73 i see TX_QEC_INIT it turns out it is disabled by default in git repo r2019_2?

uint32_t initCalMask = TX_BB_FILTER | ADC_TUNER | TIA_3DB_CORNER | DC_OFFSET | TX_ATTENUATION_DELAY | RX_GAIN_DELAY | FLASH_CAL | PATH_DELAY | TX_LO_LEAKAGE_INTERNAL | TX_QEC_INIT | LOOPBACK_RX_LO_DELAY | LOOPBACK_RX_RX_QEC_INIT | RX_LO_DELAY | RX_QEC_INIT; 

original question ez.analog.com/.../changing-the-vcxo-80-mhz-ad9375

Parents
  • Hi,

    TX_QEC_INIT is always run by default.

    You need to modify the source code if you need to skip it.

    When using the jesd204-fsm implementation, these is the place where you need to clear the flag from the mask. 

    https://github.com/analogdevicesinc/linux/blob/master/drivers/iio/adc/adrv9009.c#L6563

    In case you still use the old/deprecated mode, you need to modify the mask here: 

    https://github.com/analogdevicesinc/linux/blob/master/drivers/iio/adc/adrv9009.c#L529

    -Michael

  • Hello, I tried to disable it, but the error still appears.(ez.analog.com/.../ad9375-zc706)

    axi_sysid 45000000.axi-sysid-0: [adrv9371x] on [zc706] git <43cdc6263baf3edb166a3def6fab15bc81c4c729> clean [2022-02-17 11:38:05] UTC
    fpga_manager fpga0: Xilinx Zynq FPGA Manager registered
    usbcore: registered new interface driver snd-usb-audio
    NET: Registered protocol family 10
    Segment Routing with IPv6
    sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    NET: Registered protocol family 17
    NET: Registered protocol family 36
    Registering SWP/SWPB emulation handler
    [drm] Cannot find any crtc or sizes
    [drm] Initialized axi_hdmi_drm 1.0.0 20120930 for 70e00000.axi_hdmi on minor 0
    ad9371 spi0.1: ad9371_probe : enter
    axi_adxcvr 44a60000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.01.a) using CPLL on GTX2 at 0x44A60000. Number of lanes: 2.
    axi_adxcvr 44a50000.axi-adxcvr-rx-os: AXI-ADXCVR-RX (17.01.a) using CPLL on GTX2 at 0x44A50000. Number of lanes: 2.
    axi_adxcvr 44a80000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.01.a) using QPLL on GTX2 at 0x44A80000. Number of lanes: 4.
    asoc-simple-card adv7511_hdmi_snd: spdif-hifi <-> 75c00000.axi-spdif-tx mapping ok
    ad9371 spi0.1: ad9371_probe : enter
    [drm] Cannot find any crtc or sizes
    ERROR: 364: MYKONOS_waitArmCmdStatus() exited due to ARM error for the desired ARM opcode
    ERROR: 282: Unknown error was encountered.
    ad9371 spi0.1: calsDoneLifetime 0x47, calsDoneLastRun 0x47, calsMinimum 0x4F, initErrCal 0x3, initErrCode 0x1
    ad9371 spi0.1: initCalsCompleted 0x47
    ad9371 spi0.1: errorWord 0x2, statusWord 0x0
    ad9371 spi0.1: ArmCmdStatusByte 0xE
    ad9371 spi0.1: deframerStatus (0x60)
    WARNING: 136: Mismatch detected in MYKONOS_jesd204bIlasCheck()
    ad9371 spi0.1: ILAS mismatch: c7f8
    ad9371 spi0.1: ILAS lanes per converter did not match
    ad9371 spi0.1: ILAS scrambling did not match
    ad9371 spi0.1: ILAS octets per frame did not match
    ad9371 spi0.1: ILAS frames per multiframe did not match
    ad9371 spi0.1: ILAS number of converters did not match
    ad9371 spi0.1: ILAS sample resolution did not match
    ad9371 spi0.1: ILAS control bits per sample did not match
    ad9371 spi0.1: ILAS bits per sample did not match
    ad9371 spi0.1: ILAS checksum did not match
    ERROR: 258: Device not in radioOff/IDLE state. Error in MYKONOS_enableTrackingCals()
    ad9371 spi0.1: Device not in radioOff/IDLE state. Error in MYKONOS_enableTrackingCals()
    (258)
    random: crng init done
    ERROR: 364: MYKONOS_waitArmCmdStatus() exited due to ARM error for the desired ARM opcode
    ERROR: 282: Unknown error was encountered.
    ad9371 spi0.1: calsDoneLifetime 0x47, calsDoneLastRun 0x47, calsMinimum 0x4F, initErrCal 0x3, initErrCode 0x1
    ad9371 spi0.1: initCalsCompleted 0x47
    ad9371 spi0.1: errorWord 0x2, statusWord 0x0
    ad9371 spi0.1: ArmCmdStatusByte 0xE
    ad9371 spi0.1: deframerStatus (0x61)
    WARNING: 136: Mismatch detected in MYKONOS_jesd204bIlasCheck()
    ad9371 spi0.1: ILAS mismatch: c7f8
    ad9371 spi0.1: ILAS lanes per converter did not match
    ad9371 spi0.1: ILAS scrambling did not match
    ad9371 spi0.1: ILAS octets per frame did not match
    ad9371 spi0.1: ILAS frames per multiframe did not match
    ad9371 spi0.1: ILAS number of converters did not match
    ad9371 spi0.1: ILAS sample resolution did not match
    ad9371 spi0.1: ILAS control bits per sample did not match
    ad9371 spi0.1: ILAS bits per sample did not match
    ad9371 spi0.1: ILAS checksum did not match
    ERROR: 258: Device not in radioOff/IDLE state. Error in MYKONOS_enableTrackingCals()
    ad9371 spi0.1: Device not in radioOff/IDLE state. Error in MYKONOS_enableTrackingCals()
    (258)
    ad9371: probe of spi0.1 failed with error -14
    input: gpio_keys as /devices/soc0/gpio_keys/input/input0
    rtc-pcf8563 5-0051: setting system clock to 2022-02-28 05:38:15 UTC (1646026695)
    clk: Not disabling unused clocks
    ALSA device list:
    #0: HDMI monitor
    EXT4-fs warning (device mmcblk0p2): ext4_clear_journal_err:4946: Filesystem error recorded from previous mount: IO failure
    EXT4-fs warning (device mmcblk0p2): ext4_clear_journal_err:4947: Marking fs in need of filesystem check.
    EXT4-fs (mmcblk0p2): warning: mounting fs with errors, running e2fsck is recommended
    EXT4-fs (mmcblk0p2): recovery complete
    EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    VFS: Mounted root (ext4 filesystem) on device 179:2.
    devtmpfs: mounted
    Freeing unused kernel memory: 1024K
    Run /sbin/init as init process
    systemd[1]: Failed to lookup module alias 'autofs4': Function not implemented
    systemd[1]: systemd 241 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD -IDN2 +IDN -PCRE2 default-hierarchy=hybrid)
    systemd[1]: Detected architecture arm.

    Welcome to Kuiper GNU/Linux 10 (buster)!

  • what am I doing wrong with my device tree?

  • Can you please add your modifications, into this file and then provide a git diff.

    https://github.com/analogdevicesinc/linux/blob/master/arch/arm/boot/dts/adi-adrv9371.dtsi

    Please also provide your filter wizard profile.

    -Michael

  • 19c19
    < 		adi,vcxo-freq = <80000000>;
    ---
    > 		adi,vcxo-freq = <122880000>;
    27,28c27,28
    < 		//adi,pll1-feedback-div = <4>;
    < 		//adi,pll1-charge-pump-current-nA = <5000>;
    ---
    > 		adi,pll1-feedback-div = <4>;
    > 		adi,pll1-charge-pump-current-nA = <5000>;
    32,35c32,34
    < 		//adi,pll2-vco-div-m1 = <3>; /* use 5 for 184320000 output device clock */
    < 		//adi,pll2-n2-div = <10>; /* N / M1 */
    < 		//adi,pll2-r1-div = <1>;
    < 		adi,pll2-m1-frequency = <1280000000>;
    ---
    > 		adi,pll2-vco-div-m1 = <3>; /* use 5 for 184320000 output device clock */
    > 		adi,pll2-n2-div = <10>; /* N / M1 */
    > 		adi,pll2-r1-div = <1>;
    58c57
    < 			adi,channel-divider = <16>;
    ---
    > 			adi,channel-divider = <10>;
    67c66
    < 			adi,channel-divider = <16>;
    ---
    > 			adi,channel-divider = <10>;
    76c75
    < 			adi,channel-divider = <16>;
    ---
    > 			adi,channel-divider = <10>;
    85c84
    < 			adi,channel-divider = <16>;
    ---
    > 			adi,channel-divider = <10>;
    110,111c109,110
    < 		adi,clocks-clk-pll-vco-freq_khz = <9600000>;
    < 		adi,clocks-device-clock_khz = <80000>;
    ---
    > 		adi,clocks-clk-pll-vco-freq_khz = <9830400>;
    > 		adi,clocks-device-clock_khz = <122880>;
    113c112
    < 		adi,clocks-clk-pll-vco-div = <3>;
    ---
    > 		adi,clocks-clk-pll-vco-div = <2>;
    119,122c118,121
    < 		adi,rx-profile-iq-rate_khz = <40000>;
    < 		adi,rx-profile-rf-bandwidth_hz = <20000000>;
    < 		adi,rx-profile-rhb1-decimation = <2>;
    < 		adi,rx-profile-rx-bbf-3db-corner_khz = <20000>;
    ---
    > 		adi,rx-profile-iq-rate_khz = <122880>;
    > 		adi,rx-profile-rf-bandwidth_hz = <100000000>;
    > 		adi,rx-profile-rhb1-decimation = <1>;
    > 		adi,rx-profile-rx-bbf-3db-corner_khz = <100000>;
    124,126c123
    < 		adi,rx-profile-rx-fir-decimation = <4>;
    < 
    < 		adi,obs-settings-obs-rx-channels-enable = <3>; /* Disable Sniffer Profile */
    ---
    > 		adi,rx-profile-rx-fir-decimation = <2>;
    129,132c126,129
    < 		adi,rx-profile-rx-fir-num-fir-coefs = <72>;
    < 		adi,rx-profile-rx-fir-coefs = /bits/ 16 <(-1) (-1) (0) (3) (5) (4) (0) (-7) (-9) (-4) (4) (6) (-7) (-28) (-32) (9) (92) (168) (147) (-30) (-324) (-562) (-507) (-17) (781) (1457) (1442) (382) (-1524) (-3406) (-4000) (-2241) (2096) (8083) (13870) (17424) (17424) (13870) (8083) (2096) (-2241) (-4000) (-3406) (-1524) (382) (1442) (1457) (781) (-17) (-507) (-562) (-324) (-30) (147) (168) (92) (9) (-32) (-28) (-7) (6) (4) (-4) (-9) (-7) (0) (4) (5) (3) (0) (-1) (-1)>;
    < 				
    < 		adi,rx-profile-custom-adc-profile = /bits/ 16  <(460) (273) (182) (98) (1280) (112) (1505) (53) (1574) (25) (1069) (40) (48) (48) (31) (184)>;
    ---
    > 		adi,rx-profile-rx-fir-num-fir-coefs = <48>;
    > 		adi,rx-profile-rx-fir-coefs = /bits/ 16 <(-5) (-26) (32) (51) (-67) (-116) (140) (212) (-252) (-367) (429) (595) (-688) (-931) (1072) (1427) (-1650) (-2188) (2612) (3496) (-4802) (-7591) (9656) (32317) (32317) (9656) (-7591) (-4802) (3496) (2612) (-2188) (-1650) (1427) (1072) (-931) (-688) (595) (429) (-367) (-252) (212) (140) (-116) (-67) (51) (32) (-26) (-5)>;
    > 
    > 		adi,rx-profile-custom-adc-profile = /bits/ 16  <534 386 201 98 1280 491 1591 279 1306 104 792 28 48 39 23 187>;
    136,139c133,136
    < 		adi,obs-profile-iq-rate_khz = <80000>;
    < 		adi,obs-profile-rf-bandwidth_hz = <60000000>;
    < 		adi,obs-profile-rhb1-decimation = <2>;
    < 		adi,obs-profile-rx-bbf-3db-corner_khz = <30000>;
    ---
    > 		adi,obs-profile-iq-rate_khz = <245760>;
    > 		adi,obs-profile-rf-bandwidth_hz = <200000000>;
    > 		adi,obs-profile-rhb1-decimation = <1>;
    > 		adi,obs-profile-rx-bbf-3db-corner_khz = <100000>;
    141c138
    < 		adi,obs-profile-rx-fir-decimation = <2>;
    ---
    > 		adi,obs-profile-rx-fir-decimation = <1>;
    143,145c140,142
    < 		adi,obs-profile-rx-fir-gain_db = <0>;
    < 		adi,obs-profile-rx-fir-num-fir-coefs = <72>;
    < 		adi,obs-profile-rx-fir-coefs = /bits/ 16 <(0) (1) (-1) (-2) (2) (6) (-4) (-14) (5) (30) (-3) (-56) (-8) (93) (36) (-143) (-92) (202) (189) (-260) (-343) (301) (571) (-300) (-889) (216) (1320) (13) (-1905) (-508) (2731) (1576) (-4111) (-4817) (5434) (17585) (17585) (5434) (-4817) (-4111) (1576) (2731) (-508) (-1905) (13) (1320) (216) (-889) (-300) (571) (301) (-343) (-260) (189) (202) (-92) (-143) (36) (93) (-8) (-56) (-3) (30) (5) (-14) (-4) (6) (2) (-2) (-1) (1) (0)>;
    ---
    > 		adi,obs-profile-rx-fir-gain_db = <6>;
    > 		adi,obs-profile-rx-fir-num-fir-coefs = <24>;
    > 		adi,obs-profile-rx-fir-coefs = /bits/ 16 <(-289) (81) (-23) (-86) (229) (-354) (397) (-233) (-657) (1699) (-4172) (23010) (-4172) (1699) (-657) (-233) (397) (-354) (229) (-86) (-23) (81) (-289) (0)>;
    147,148c144,145
    < 		adi,obs-profile-custom-adc-profile = /bits/ 16  <(459) (273) (182) (98) (1280) (115) (1506) (54) (1575) (25) (1069) (40) (48) (48) (31) (184)>;
    < 		adi,obs-settings-custom-loopback-adc-profile = /bits/ 16  <(460) (273) (182) (98) (1280) (112) (1505) (53) (1574) (25) (1069) (40) (48) (48) (31) (184)>;
    ---
    > 		adi,obs-profile-custom-adc-profile = /bits/ 16  <450 349 201 98 1280 730 1626 818 1476 732 834 20 41 36 24 200>;
    > 		adi,obs-settings-custom-loopback-adc-profile = /bits/ 16  <569 369 201 98 1280 291 1541 149 1320 58 807 34 48 40 23 189>;
    151,153c148,150
    < 		adi,tx-profile-iq-rate_khz = <80000>;
    < 		adi,tx-profile-primary-sig-bandwidth_hz = <20000000>;
    < 		adi,tx-profile-rf-bandwidth_hz = <60000000>;
    ---
    > 		adi,tx-profile-iq-rate_khz = <245760>;
    > 		adi,tx-profile-primary-sig-bandwidth_hz = <75000000>;
    > 		adi,tx-profile-rf-bandwidth_hz = <200000000>;
    155,158c152,155
    < 		adi,tx-profile-thb2-interpolation = <2>;
    < 		adi,tx-profile-tx-bbf-3db-corner_khz = <30000>;
    < 		adi,tx-profile-tx-dac-3db-corner_khz = <92000>;
    < 		adi,tx-profile-tx-fir-interpolation = <2>;
    ---
    > 		adi,tx-profile-thb2-interpolation = <1>;
    > 		adi,tx-profile-tx-bbf-3db-corner_khz = <100000>;
    > 		adi,tx-profile-tx-dac-3db-corner_khz = <187000>;
    > 		adi,tx-profile-tx-fir-interpolation = <1>;
    161,164c158,161
    < 		adi,tx-profile-tx-fir-gain_db = <0>;
    < 		adi,tx-profile-tx-fir-num-fir-coefs = <32>;
    < 		adi,tx-profile-tx-fir-coefs = /bits/ 16 <(-42) (-49) (135) (153) (-313) (-386) (619) (819) (-1108) (-1646) (1799) (3288) (-2375) (-6142) (3518) (18087) (18087) (3518) (-6142) (-2375) (3288) (1799) (-1646) (-1108) (819) (619) (-386) (-313) (153) (135) (-49) (-42)>;
    < 		/*
    ---
    > 		adi,tx-profile-tx-fir-gain_db = <6>;
    > 		adi,tx-profile-tx-fir-num-fir-coefs = <16>;
    > 		adi,tx-profile-tx-fir-coefs = /bits/ 16 <(6) (-270) (203) (-168) (-84) (983) (-3222) (21143) (-3222) (983) (-84) (-168) (203) (-270) (6) (0)>;
    > 
    167c164
    < 		adi,sniffer-profile-iq-rate_khz = <40000>;
    ---
    > 		adi,sniffer-profile-iq-rate_khz = <30720>;
    173d169
    < 		*/
    
    <profile AD9371 version=0 name=Rx 20, IQrate 40.000>
     <clocks>
      <deviceClock_kHz=80000>
      <clkPllVcoFreq_kHz=9600000>
      <clkPllVcoDiv=1.5>
      <clkPllHsDiv=4>
     </clocks>
    
     <rx>
      <adcDiv=1>
      <rxFirDecimation=4>
      <rxDec5Decimation=5>
      <enHighRejDec5=1>
      <rhb1Decimation=2>
      <iqRate_kHz=40000>
      <rfBandwidth_Hz=20000000>
      <rxBbf3dBCorner_kHz=20000>
    
      <filter FIR gain=-6 num=72>
      -1
      -1
      0
      3
      5
      4
      0
      -7
      -9
      -4
      4
      6
      -7
      -28
      -32
      9
      92
      168
      147
      -30
      -324
      -562
      -507
      -17
      781
      1457
      1442
      382
      -1524
      -3406
      -4000
      -2241
      2096
      8083
      13870
      17424
      17424
      13870
      8083
      2096
      -2241
      -4000
      -3406
      -1524
      382
      1442
      1457
      781
      -17
      -507
      -562
      -324
      -30
      147
      168
      92
      9
      -32
      -28
      -7
      6
      4
      -4
      -9
      -7
      0
      4
      5
      3
      0
      -1
      -1
      </filter>
    
      <adc-profile num=16>
      460
      273
      182
      98
      1280
      112
      1505
      53
      1574
      25
      1069
      40
      48
      48
      31
      184
      </adc-profile>
     </rx>
    
     <obs>
      <adcDiv=1>
      <rxFirDecimation=2>
      <rxDec5Decimation=5>
      <enHighRejDec5=1>
      <rhb1Decimation=2>
      <iqRate_kHz=80000>
      <rfBandwidth_Hz=60000000>
      <rxBbf3dBCorner_kHz=30000>
    
      <filter FIR gain=0 num=72>
      0
      1
      -1
      -2
      2
      6
      -4
      -14
      5
      30
      -3
      -56
      -8
      93
      36
      -143
      -92
      202
      189
      -260
      -343
      301
      571
      -300
      -889
      216
      1320
      13
      -1905
      -508
      2731
      1576
      -4111
      -4817
      5434
      17585
      17585
      5434
      -4817
      -4111
      1576
      2731
      -508
      -1905
      13
      1320
      216
      -889
      -300
      571
      301
      -343
      -260
      189
      202
      -92
      -143
      36
      93
      -8
      -56
      -3
      30
      5
      -14
      -4
      6
      2
      -2
      -1
      1
      0
      </filter>
    
      <adc-profile num=16>
      459
      273
      182
      98
      1280
      115
      1506
      54
      1575
      25
      1069
      40
      48
      48
      31
      184
      </adc-profile>
    
      <lpbk-adc-profile num=16>
      460
      273
      182
      98
      1280
      112
      1505
      53
      1574
      25
      1069
      40
      48
      48
      31
      184
      </lpbk-adc-profile>
     </obs>
    
     <sniffer>
      <adcDiv=1>
      <rxFirDecimation=4>
      <rxDec5Decimation=5>
      <enHighRejDec5=1>
      <rhb1Decimation=2>
      <iqRate_kHz=40000>
      <rfBandwidth_Hz=20000000>
      <rxBbf3dBCorner_kHz=20000>
    
      <filter FIR gain=-6 num=72>
      -1
      -1
      0
      3
      5
      4
      0
      -7
      -9
      -4
      4
      6
      -7
      -28
      -32
      9
      92
      168
      147
      -30
      -324
      -562
      -507
      -17
      781
      1457
      1442
      382
      -1524
      -3406
      -4000
      -2241
      2096
      8083
      13870
      17424
      17424
      13870
      8083
      2096
      -2241
      -4000
      -3406
      -1524
      382
      1442
      1457
      781
      -17
      -507
      -562
      -324
      -30
      147
      168
      92
      9
      -32
      -28
      -7
      6
      4
      -4
      -9
      -7
      0
      4
      5
      3
      0
      -1
      -1
      </filter>
    
      <adc-profile num=16>
      460
      273
      182
      98
      1280
      112
      1505
      53
      1574
      25
      1069
      40
      48
      48
      31
      184
      </adc-profile>
     </sniffer>
    
     <tx>
      <dacDiv=2.5>
      <txFirInterpolation=2>
      <thb1Interpolation=2>
      <thb2Interpolation=2>
      <txInputHbInterpolation=1>
      <iqRate_kHz=80000>
      <primarySigBandwidth_Hz=20000000>
      <rfBandwidth_Hz=60000000>
      <txDac3dBCorner_kHz=92000>
      <txBbf3dBCorner_kHz=30000>
    
      <filter FIR gain=0 num=32>
      -42
      -49
      135
      153
      -313
      -386
      619
      819
      -1108
      -1646
      1799
      3288
      -2375
      -6142
      3518
      18087
      18087
      3518
      -6142
      -2375
      3288
      1799
      -1646
      -1108
      819
      619
      -386
      -313
      153
      135
      -49
      -42
      </filter>
     </tx>
    </profile>
    

  •   <clkPllVcoDiv=1.5>

    /**
    * \brief Enum of possible VCO divider settings (1x, 1.5x, 2x, 3x)
    */
    typedef enum
    {
    VCODIV_1 = 0,
    VCODIV_1p5 = 1,
    VCODIV_2 = 2,
    VCODIV_3 = 3
    } mykonosVcoDiv_t;

    According to this you need to use:

    adi,clocks-clk-pll-vco-div = <1>; 

    -Michael

  • The forum has already written that the GUI is incorrect value adi, clocks-clk-pll-vco-div = <1>; and you need to put <3>

    ez.analog.com/.../changing-the-vcxo-80-mhz-ad9375

  • even if u substitute 1....

    mmcblk0: p1 p2 p3
    random: fast init done
    jesd204: /amba/spi@e0006000/ad9528-1@0,jesd204:0,parent=spi0.0: Using as SYSREF provider
    axi_adxcvr 44a60000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.01.a) using CPLL on GTX2 at 0x44A60000. Number of lanes: 2.
    axi_adxcvr 44a50000.axi-adxcvr-rx-os: AXI-ADXCVR-RX (17.01.a) using CPLL on GTX2 at 0x44A50000. Number of lanes: 2.
    axi_adxcvr 44a80000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.01.a) using QPLL on GTX2 at 0x44A80000. Number of lanes: 4.
    axi_sysid 45000000.axi-sysid-0: [adrv9371x] on [zc706] git <43cdc6263baf3edb166a3def6fab15bc81c4c729> clean [2022-02-17 11:38:05] UTC
    fpga_manager fpga0: Xilinx Zynq FPGA Manager registered
    usbcore: registered new interface driver snd-usb-audio
    NET: Registered protocol family 10
    Segment Routing with IPv6
    sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    NET: Registered protocol family 17
    NET: Registered protocol family 36
    Registering SWP/SWPB emulation handler
    [drm] Cannot find any crtc or sizes
    [drm] Initialized axi_hdmi_drm 1.0.0 20120930 for 70e00000.axi_hdmi on minor 0
    ad9371 spi0.1: ad9371_probe : enter
    cf_axi_dds 44a04000.axi-ad9371-tx-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x44A04000 mapped to 0x(ptrval), probed DDS AD9371
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition initialized -> probed
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition initialized -> probed
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition initialized -> probed
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition probed -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition probed -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition probed -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition idle -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition idle -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition idle -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition device_init -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition device_init -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition device_init -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_init -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_init -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_init -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_supported -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_supported -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_supported -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_pre_setup -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_pre_setup -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_pre_setup -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage1 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage1 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage1 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage2 -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage2 -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage2 -> clk_sync_stage3
    [drm] Cannot find any crtc or sizes
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage3 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage3 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage3 -> link_setup
    ERROR: 64: CLKPLL VCO frequency exceeded max(9.216Ghz) in VCO divider /1.5 case ()
    ERROR: 64: CLKPLL VCO frequency exceeded max(9.216Ghz) in VCO divider /1.5 case ()
    ad9371 spi0.1: CLKPLL VCO frequency exceeded max(9.216Ghz) in VCO divider /1.5 case ()
    (64)
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] got error from cb: -14
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: Rolling back from 'link_setup', got error -14
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_setup -> opt_setup_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_setup -> opt_setup_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_setup -> opt_setup_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition opt_setup_stage1 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition opt_setup_stage1 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition opt_setup_stage1 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_setup -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_setup -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_setup -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage3 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage3 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage3 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage2 -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage2 -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage2 -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage1 -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage1 -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage1 -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_pre_setup -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_pre_setup -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_pre_setup -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_supported -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_supported -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_supported -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_init -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_init -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_init -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition device_init -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition device_init -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition device_init -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition idle -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition idle -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition idle -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition idle -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition idle -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition idle -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition device_init -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition device_init -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition device_init -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_init -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_init -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_init -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_supported -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_supported -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_supported -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_pre_setup -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_pre_setup -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_pre_setup -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage1 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage1 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage1 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage2 -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage2 -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage2 -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage3 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage3 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage3 -> link_setup
    ERROR: 64: CLKPLL VCO frequency exceeded max(9.216Ghz) in VCO divider /1.5 case ()
    ERROR: 64: CLKPLL VCO frequency exceeded max(9.216Ghz) in VCO divider /1.5 case ()
    ad9371 spi0.1: CLKPLL VCO frequency exceeded max(9.216Ghz) in VCO divider /1.5 case ()
    (64)
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] got error from cb: -14
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: Rolling back from 'link_setup', got error -14
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_setup -> opt_setup_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_setup -> opt_setup_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_setup -> opt_setup_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition opt_setup_stage1 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition opt_setup_stage1 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition opt_setup_stage1 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_setup -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_setup -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_setup -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage3 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage3 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage3 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage2 -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage2 -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage2 -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage1 -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage1 -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage1 -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_pre_setup -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_pre_setup -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_pre_setup -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_supported -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_supported -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_supported -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_init -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_init -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_init -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition device_init -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition device_init -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition device_init -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition idle -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition idle -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition idle -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition idle -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition idle -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition idle -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition device_init -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition device_init -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition device_init -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_init -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_init -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_init -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_supported -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_supported -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_supported -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_pre_setup -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_pre_setup -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_pre_setup -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage1 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage1 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage1 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage2 -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage2 -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage2 -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage3 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage3 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage3 -> link_setup
    ERROR: 64: CLKPLL VCO frequency exceeded max(9.216Ghz) in VCO divider /1.5 case ()
    ERROR: 64: CLKPLL VCO frequency exceeded max(9.216Ghz) in VCO divider /1.5 case ()
    ad9371 spi0.1: CLKPLL VCO frequency exceeded max(9.216Ghz) in VCO divider /1.5 case ()
    (64)
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] got error from cb: -14
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: Rolling back from 'link_setup', got error -14
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_setup -> opt_setup_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_setup -> opt_setup_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_setup -> opt_setup_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition opt_setup_stage1 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition opt_setup_stage1 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition opt_setup_stage1 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_setup -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_setup -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_setup -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage3 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage3 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage3 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage2 -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage2 -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage2 -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage1 -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage1 -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage1 -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_pre_setup -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_pre_setup -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_pre_setup -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_supported -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_supported -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_supported -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_init -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_init -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_init -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition device_init -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition device_init -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition device_init -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition idle -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition idle -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition idle -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition idle -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition idle -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition idle -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition device_init -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition device_init -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition device_init -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_init -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_init -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_init -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_supported -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_supported -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_supported -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_pre_setup -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_pre_setup -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_pre_setup -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage1 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage1 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage1 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage2 -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage2 -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage2 -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage3 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage3 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage3 -> link_setup
    ERROR: 64: CLKPLL VCO frequency exceeded max(9.216Ghz) in VCO divider /1.5 case ()
    ERROR: 64: CLKPLL VCO frequency exceeded max(9.216Ghz) in VCO divider /1.5 case ()
    ad9371 spi0.1: CLKPLL VCO frequency exceeded max(9.216Ghz) in VCO divider /1.5 case ()
    (64)
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] got error from cb: -14
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: Rolling back from 'link_setup', got error -14
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_setup -> opt_setup_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_setup -> opt_setup_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_setup -> opt_setup_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition opt_setup_stage1 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition opt_setup_stage1 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition opt_setup_stage1 -> link_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_setup -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_setup -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_setup -> clk_sync_stage3
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage3 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage3 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage3 -> clk_sync_stage2
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage2 -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage2 -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage2 -> clk_sync_stage1
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage1 -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage1 -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage1 -> link_pre_setup
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_pre_setup -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_pre_setup -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_pre_setup -> link_supported
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_supported -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_supported -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_supported -> link_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_init -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_init -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_init -> device_init
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition device_init -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition device_init -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition device_init -> idle
    jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: FSM completed with error -14
    asoc-simple-card adv7511_hdmi_snd: spdif-hifi <-> 75c00000.axi-spdif-tx mapping ok
    cf_axi_adc 44a00000.axi-ad9371-rx-hpc: ADI AIM (10.01.b) at 0x44A00000 mapped to 0x(ptrval), probed ADC AD9371 as MASTER
    input: gpio_keys as /devices/soc0/gpio_keys/input/input0
    rtc-pcf8563 5-0051: setting system clock to 2022-03-04 11:18:57 UTC (1646392737)

  • Please see here:

     AD9371 custom profile:calibration error 

    Can you try:

    adi,clocks-clk-pll-vco-freq_khz = <6400000>; 

    adi,clocks-clk-pll-hs-div = <4>;

    adi,clocks-clk-pll-vco-div = <0>; /* VCODIV_1 */

    -Michael

  • yes it works! you can pin this on the wiki, it took me a lot of time

    root@analog:~# dmesg | grep ad9
    [ 0.656405] jesd204: created con: id=0, topo=0, link=0, /amba/spi@e0006000/ad9528-1@0 <-> /fpga-axi@0/axi-adxcvr-tx@44a80000
    [ 0.666367] jesd204: created con: id=1, topo=0, link=2, /amba/spi@e0006000/ad9528-1@0 <-> /fpga-axi@0/axi-adxcvr-rx-os@44a50000
    [ 0.676571] jesd204: created con: id=2, topo=0, link=1, /amba/spi@e0006000/ad9528-1@0 <-> /fpga-axi@0/axi-adxcvr-rx@44a60000
    [ 0.718173] jesd204: created con: id=6, topo=0, link=0, /fpga-axi@0/axi-jesd204-tx@44a90000 <-> /fpga-axi@0/axi-ad9371-tx-hpc@44a04000
    [ 0.728990] jesd204: created con: id=7, topo=0, link=1, /fpga-axi@0/axi-jesd204-rx@44aa0000 <-> /amba/spi@e0006000/ad9371-phy@1
    [ 0.739195] jesd204: created con: id=8, topo=0, link=2, /fpga-axi@0/axi-jesd204-rx@44ab0000 <-> /amba/spi@e0006000/ad9371-phy@1
    [ 0.749381] jesd204: created con: id=9, topo=0, link=0, /fpga-axi@0/axi-ad9371-tx-hpc@44a04000 <-> /amba/spi@e0006000/ad9371-phy@1
    [ 0.759848] jesd204: /amba/spi@e0006000/ad9371-phy@1: JESD204[0] transition uninitialized -> initialized
    [ 0.768032] jesd204: /amba/spi@e0006000/ad9371-phy@1: JESD204[1] transition uninitialized -> initialized
    [ 0.776213] jesd204: /amba/spi@e0006000/ad9371-phy@1: JESD204[2] transition uninitialized -> initialized
    [ 2.358268] ad9371 spi0.1: ad9371_probe : enter
    [ 2.370933] ad9528 spi0.0: spi0.0 supply vcc not found, using dummy regulator
    [ 2.377725] ad9528 spi0.0: Linked as a consumer to regulator.0
    [ 2.419576] jesd204: /amba/spi@e0006000/ad9528-1@0,jesd204:0,parent=spi0.0: Using as SYSREF provider
    [ 2.672278] ad9371 spi0.1: ad9371_probe : enter
    [ 2.707074] cf_axi_dds 44a04000.axi-ad9371-tx-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x44A04000 mapped to 0x(ptrval), probed DDS AD9371
    [ 2.721623] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition initialized -> probed
    [ 2.731319] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition initialized -> probed
    [ 2.740986] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition initialized -> probed
    [ 2.750670] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition probed -> idle
    [ 2.759725] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition probed -> idle
    [ 2.768782] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition probed -> idle
    [ 2.777847] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition idle -> device_init
    [ 2.787341] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition idle -> device_init
    [ 2.796831] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition idle -> device_init
    [ 2.806334] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition device_init -> link_init
    [ 2.816256] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition device_init -> link_init
    [ 2.826181] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition device_init -> link_init
    [ 2.836109] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_init -> link_supported
    [ 2.846298] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_init -> link_supported
    [ 2.856477] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_init -> link_supported
    [ 2.866930] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_supported -> link_pre_setup
    [ 2.877551] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_supported -> link_pre_setup
    [ 2.888169] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_supported -> link_pre_setup
    [ 2.898791] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_pre_setup -> clk_sync_stage1
    [ 2.909494] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_pre_setup -> clk_sync_stage1
    [ 2.920195] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_pre_setup -> clk_sync_stage1
    [ 2.930906] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage1 -> clk_sync_stage2
    [ 2.941696] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage1 -> clk_sync_stage2
    [ 2.952484] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage1 -> clk_sync_stage2
    [ 2.963281] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage2 -> clk_sync_stage3
    [ 2.974073] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage2 -> clk_sync_stage3
    [ 2.984869] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage2 -> clk_sync_stage3
    [ 3.839677] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clk_sync_stage3 -> link_setup
    [ 3.850044] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clk_sync_stage3 -> link_setup
    [ 3.860399] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clk_sync_stage3 -> link_setup
    [ 11.329144] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_setup -> opt_setup_stage1
    [ 11.339597] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_setup -> opt_setup_stage1
    [ 11.350041] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_setup -> opt_setup_stage1
    [ 11.360495] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition opt_setup_stage1 -> opt_setup_stage2
    [ 11.371455] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition opt_setup_stage1 -> opt_setup_stage2
    [ 11.382416] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition opt_setup_stage1 -> opt_setup_stage2
    [ 11.393385] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition opt_setup_stage2 -> opt_setup_stage3
    [ 11.404351] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition opt_setup_stage2 -> opt_setup_stage3
    [ 11.415312] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition opt_setup_stage2 -> opt_setup_stage3
    [ 11.426284] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition opt_setup_stage3 -> opt_setup_stage4
    [ 11.437248] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition opt_setup_stage3 -> opt_setup_stage4
    [ 11.448209] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition opt_setup_stage3 -> opt_setup_stage4
    [ 11.459187] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition opt_setup_stage4 -> opt_setup_stage5
    [ 11.470156] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition opt_setup_stage4 -> opt_setup_stage5
    [ 11.481115] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition opt_setup_stage4 -> opt_setup_stage5
    [ 11.494333] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition opt_setup_stage5 -> clocks_enable
    [ 11.505047] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition opt_setup_stage5 -> clocks_enable
    [ 11.515751] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition opt_setup_stage5 -> clocks_enable
    [ 11.526653] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition clocks_enable -> link_enable
    [ 11.536928] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition clocks_enable -> link_enable
    [ 11.547198] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition clocks_enable -> link_enable
    [ 11.559936] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_enable -> link_running
    [ 11.570130] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_enable -> link_running
    [ 11.580312] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_enable -> link_running
    [ 11.767056] ad9371 spi0.1: AD9375 Rev 4, Firmware 5.2.2 API version: 1.5.2.3566 successfully initialized via jesd204-fsm
    [ 11.776639] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[0] transition link_running -> opt_post_running_stage
    [ 11.787775] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[1] transition link_running -> opt_post_running_stage
    [ 11.798909] jesd204: /amba/spi@e0006000/ad9371-phy@1,jesd204:1,parent=spi0.1: JESD204[2] transition link_running -> opt_post_running_stage
    [ 11.841562] cf_axi_adc 44a00000.axi-ad9371-rx-hpc: ADI AIM (10.01.b) at 0x44A00000 mapped to 0x(ptrval), probed ADC AD9371 as MASTER

  • Just changing the adi,clocks-clk-pll-vco-div aka. clkPllVcoDiv and keeping adi,clocks-clk-pll-vco-freq_khz aka. clkPllVcoFreq_kHz at the same rate didn't make much sense to me.

    The profile wizard original solution was:

    <deviceClock_kHz=80000>
    <clkPllVcoFreq_kHz=9600000>
    <clkPllVcoDiv=1.5>
    <clkPllHsDiv=4>

    This violates, and causes this error: 

    ERROR: 64: CLKPLL VCO frequency exceeded max(9.216Ghz) in VCO divider /1.5 case ()

    I think that the math behind these dividers:

    9600000 / (1.5 * 4) = 1600000 

    We need to maintain the 1600000, so:

    6400000 / (1 * 4) = 1600000  

    Is a solution within all operation ranges.

    If you look further to understand where the 1600000 is coming from:

     <adcDiv=1>
    <rxFirDecimation=4>
    <rxDec5Decimation=5>
    <enHighRejDec5=1>
    <rhb1Decimation=2>
    <iqRate_kHz=40000>
    <rfBandwidth_Hz=20000000>
    <rxBbf3dBCorner_kHz=20000> 

    iqRate_kHz  * rhb1Decimation * rxDec5Decimation * rxFirDecimation * adcDiv = 1600000 

    Likewise on TX.

    -Michael

Reply
  • Just changing the adi,clocks-clk-pll-vco-div aka. clkPllVcoDiv and keeping adi,clocks-clk-pll-vco-freq_khz aka. clkPllVcoFreq_kHz at the same rate didn't make much sense to me.

    The profile wizard original solution was:

    <deviceClock_kHz=80000>
    <clkPllVcoFreq_kHz=9600000>
    <clkPllVcoDiv=1.5>
    <clkPllHsDiv=4>

    This violates, and causes this error: 

    ERROR: 64: CLKPLL VCO frequency exceeded max(9.216Ghz) in VCO divider /1.5 case ()

    I think that the math behind these dividers:

    9600000 / (1.5 * 4) = 1600000 

    We need to maintain the 1600000, so:

    6400000 / (1 * 4) = 1600000  

    Is a solution within all operation ranges.

    If you look further to understand where the 1600000 is coming from:

     <adcDiv=1>
    <rxFirDecimation=4>
    <rxDec5Decimation=5>
    <enHighRejDec5=1>
    <rhb1Decimation=2>
    <iqRate_kHz=40000>
    <rfBandwidth_Hz=20000000>
    <rxBbf3dBCorner_kHz=20000> 

    iqRate_kHz  * rhb1Decimation * rxDec5Decimation * rxFirDecimation * adcDiv = 1600000 

    Likewise on TX.

    -Michael

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.