Hi,
I have followed steps given in github.com/.../README.md (commit c40d1a8) to build PetaLinux2021.1 for zynq-zc706-adv7511-fmcdaq3-revC.
HDL used for building was taken from
github.com/.../hdl.git
commit: 4ec8797c7cbb2b551f5930fd56d8f38a8cf3e7e9
I have generated *.xsa and *.bit for daq3 using the above build.
I could boot ZC706 evaluation board+DAQ3 using the files from above build. It was seen in the booting log that JESD failed:
jesd204: found 0 devices and 0 topologies
ad9680 spi0.2: Failed to enable JESD204 link: -517
(booting_log.txt containing full log is attached)
Welcome to minicom 2.7.1 OPTIONS: I18n Compiled on Aug 13 2017, 15:25:34. Port /dev/ttyUSB0, 10:16:24 Press CTRL-A Z for help on special keys U-Boot 2021.01 (Jun 01 2021 - 11:54:06 +0000) CPU: Zynq 7z045 Silicon: v3.1 Model: Xilinx Zynq ZC706 DRAM: ECC disabled 1 GiB Flash: 0 Bytes NAND: 0 MiB MMC: mmc@e0100000: 0 Loading Environment from FAT... *** Warning - bad CRC, using default environment In: serial@e0001000 Out: serial@e0001000 Err: serial@e0001000 Net: ZYNQ GEM: e000b000, mdio bus e000b000, phyaddr 7, interface rgmii-id Warning: ethernet@e000b000 (eth0) using random MAC address - 92:0d:78:1e:1a:a2 eth0: ethernet@e000b000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0 is current device Scanning mmc 0:1... Found U-Boot script /boot.scr 2595 bytes read in 22 ms (114.3 KiB/s) ## Executing script at 03000000 Trying to load boot images from mmc0 407 bytes read in 19 ms (20.5 KiB/s) Importing environment(uEnv.txt) from mmc0... Running uenvcmd ... Copying Linux from SD to RAM... ** No boot file defined ** 23526900 bytes read in 3862 ms (5.8 MiB/s) ## Loading kernel from FIT Image at 10000000 ... Using 'conf-system-top.dtb' configuration Verifying Hash Integrity ... OK Trying 'kernel-1' kernel subimage Description: Linux kernel Type: Kernel Image Compression: uncompressed Data Start: 0x10000100 Data Size: 7201792 Bytes = 6.9 MiB Architecture: ARM OS: Linux Load Address: 0x00200000 Entry Point: 0x00200000 Hash algo: sha256 Hash value: deb6581eb67822eeb4765e9c386683e0263411a1f1ab094dacf021184407b0ac Verifying Hash Integrity ... sha256+ OK ## Loading ramdisk from FIT Image at 10000000 ... Using 'conf-system-top.dtb' configuration Verifying Hash Integrity ... OK Trying 'ramdisk-1' ramdisk subimage Description: petalinux-image-minimal Type: RAMDisk Image Compression: uncompressed Data Start: 0x106e5b94 Data Size: 16293099 Bytes = 15.5 MiB Architecture: ARM OS: Linux Load Address: unavailable Entry Point: unavailable Hash algo: sha256 Hash value: 8b0ecff5547be5d237b1b9013dc7275dd76b57fe6a52614bce7a669233c26d73 Verifying Hash Integrity ... sha256+ OK ## Loading fdt from FIT Image at 10000000 ... Using 'conf-system-top.dtb' configuration Verifying Hash Integrity ... OK Trying 'fdt-system-top.dtb' fdt subimage Description: Flattened Device Tree blob Type: Flat Device Tree Compression: uncompressed Data Start: 0x106de60c Data Size: 29884 Bytes = 29.2 KiB Architecture: ARM Hash algo: sha256 Hash value: 27601d4ccbd26fd2da7ae1fd158f9d4de89a2263a0f9aac20679fbbd822b031c Verifying Hash Integrity ... sha256+ OK Booting using the fdt blob at 0x106de60c Loading Kernel Image Loading Ramdisk to 2f076000, end 2ffffceb ... OK Loading Device Tree to 2f06b000, end 2f0754bb ... OK Starting kernel ... Booting Linux on physical CPU 0x0 Linux version 5.10.0-xilinx-v2021.1 (oe-user@oe-host) (arm-xilinx-linux-gnueabi-gcc (GCC) 10.2.0, GNU ld (GNU Binutils) 2.35.1) #1 S2 CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache OF: fdt: Machine model: Xilinx Zynq ZC706 earlycon: cdns0 at MMIO 0xe0001000 (options '115200n8') printk: bootconsole [cdns0] enabled Memory policy: Data cache writealloc cma: Reserved 128 MiB at 0x38000000 Zone ranges: Normal [mem 0x0000000000000000-0x000000002fffffff] HighMem [mem 0x0000000030000000-0x000000003fffffff] Movable zone start for each node Early memory node ranges node 0: [mem 0x0000000000000000-0x000000003fffffff] Initmem setup node 0 [mem 0x0000000000000000-0x000000003fffffff] percpu: Embedded 15 pages/cpu s30028 r8192 d23220 u61440 Built 1 zonelists, mobility grouping on. Total pages: 260416 Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait clk_ignore_unused cpuidle.off=1 Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear) Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear) mem auto-init: stack:off, heap alloc:off, heap free:off Memory: 870416K/1048576K available (10240K kernel code, 800K rwdata, 7204K rodata, 1024K init, 172K bss, 47088K reserved, 131072K cm) rcu: Preemptible hierarchical RCU implementation. rcu: RCU event tracing is enabled. rcu: RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2. Trampoline variant of Tasks RCU enabled. rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies. rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 efuse mapped to (ptrval) slcr mapped to (ptrval) L2C: platform modifies aux control register: 0x72360000 -> 0x72760000 L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000 L2C-310 erratum 769419 enabled L2C-310 enabling early BRESP for Cortex-A9 L2C-310 full line of zeros enabled for Cortex-A9 L2C-310 ID prefetch enabled, offset 1 lines L2C-310 dynamic clock gating enabled, standby mode enabled L2C-310 cache controller enabled, 8 ways, 512 kB L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001 random: get_random_bytes called from start_kernel+0x33c/0x4e8 with crng_init=0 zynq_clock_init: clkc starts at (ptrval) Zynq clock init sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns Switching to timer-based delay loop, resolution 3ns clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns timer #0 at (ptrval), irq=25 Console: colour dummy device 80x30 Calibrating delay loop (skipped), value calculated using timer frequency.. 666.66 BogoMIPS (lpj=3333333) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear) Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear) CPU: Testing write buffer coherency: ok CPU0: Spectre v2: using BPIALL workaround CPU0: thread -1, cpu 0, socket 0, mpidr 80000000 Setting up static identity map for 0x100000 - 0x100060 rcu: Hierarchical SRCU implementation. smp: Bringing up secondary CPUs ... CPU1: failed to boot: -1 smp: Brought up 1 node, 1 CPU SMP: Total of 1 processors activated (666.66 BogoMIPS). CPU: All CPU(s) started in SVC mode. devtmpfs: initialized VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4 clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns futex hash table entries: 512 (order: 3, 32768 bytes, linear) pinctrl core: initialized pinctrl subsystem NET: Registered protocol family 16 DMA: preallocated 256 KiB pool for atomic coherent allocations thermal_sys: Registered thermal governor 'step_wise' hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers. hw-breakpoint: maximum watchpoint size is 4 bytes. zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0x(ptrval) e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 33, base_baud = 3125000) is a xuartps printk: console [ttyPS0] enabled printk: console [ttyPS0] enabled printk: bootconsole [cdns0] disabled printk: bootconsole [cdns0] disabled SCSI subsystem initialized usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb mc: Linux media interface: v0.10 videodev: Linux video capture interface: v2.00 jesd204: found 0 devices and 0 topologies FPGA manager framework Advanced Linux Sound Architecture Driver Initialized. clocksource: Switched to clocksource arm_global_timer NET: Registered protocol family 2 tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear) TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear) TCP bind hash table entries: 8192 (order: 4, 65536 bytes, linear) TCP: Hash tables configured (established 8192 bind 8192) UDP hash table entries: 512 (order: 2, 16384 bytes, linear) UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear) NET: Registered protocol family 1 Trying to unpack rootfs image as initramfs... Freeing initrd memory: 15912K hw perfevents: no interrupt-affinity property for /pmu@f8891000, guessing. hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available workingset: timestamp_bits=14 max_order=18 bucket_order=4 bounce: pool size: 64 pages io scheduler mq-deadline registered io scheduler kyber registered zynq-pinctrl 700.pinctrl: zynq pinctrl initialized dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330 dma-pl330 f8003000.dmac: DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16 brd: module loaded loop: module loaded Registered mathworks_ip class spi-nor spi1.0: found s25fl128s1, expected n25q128a11 random: fast init done random: crng init done spi-nor spi1.0: trying to lock already unlocked area spi-nor spi1.0: s25fl128s1 (32768 Kbytes) 5 fixed-partitions partitions found on MTD device spi1.0 Creating 5 MTD partitions on "spi1.0": 0x000000000000-0x000000500000 : "boot" 0x000000500000-0x000000520000 : "bootenv" 0x000000520000-0x000000540000 : "config" 0x000000540000-0x000000fc0000 : "image" 0x000000fc0000-0x000002000000 : "spare" MACsec IEEE 802.1AE libphy: Fixed MDIO Bus: probed tun: Universal TUN/TAP device driver, 1.6 libphy: MACB_mii_bus: probed macb e000b000.ethernet eth0: Cadence GEM rev 0x00020118 at 0xe000b000 irq 36 (92:0d:78:1e:1a:a2) usbcore: registered new interface driver asix usbcore: registered new interface driver ax88179_178a usbcore: registered new interface driver cdc_ether usbcore: registered new interface driver net1080 usbcore: registered new interface driver cdc_subset usbcore: registered new interface driver zaurus usbcore: registered new interface driver cdc_ncm ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver usbcore: registered new interface driver uas usbcore: registered new interface driver usb-storage usbcore: registered new interface driver usbserial_generic usbserial: USB Serial support registered for generic usbcore: registered new interface driver ftdi_sio usbserial: USB Serial support registered for FTDI USB Serial Device usbcore: registered new interface driver upd78f0730 usbserial: USB Serial support registered for upd78f0730 ULPI transceiver vendor/product ID 0x0424/0x0007 Found SMSC USB3320 ULPI transceiver. ULPI integrity check: passed. ci_hdrc ci_hdrc.0: EHCI Host Controller ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1 ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00 usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10 usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 usb usb1: Product: EHCI Host Controller usb usb1: Manufacturer: Linux 5.10.0-xilinx-v2021.1 ehci_hcd usb usb1: SerialNumber: ci_hdrc.0 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected i2c /dev entries driver si570 1-005d: registered, current frequency 156250000 Hz i2c i2c-0: Added multiplexed i2c bus 1 adv7511 2-0039: supply avdd not found, using dummy regulator adv7511 2-0039: supply dvdd not found, using dummy regulator adv7511 2-0039: supply pvdd not found, using dummy regulator adv7511 2-0039: supply bgvdd not found, using dummy regulator adv7511 2-0039: supply dvdd-3v not found, using dummy regulator i2c i2c-0: Added multiplexed i2c bus 2 at24 3-0054: supply vcc not found, using dummy regulator at24 3-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write i2c i2c-0: Added multiplexed i2c bus 3 pca953x 4-0021: supply vcc not found, using dummy regulator pca953x 4-0021: using no AI i2c i2c-0: Added multiplexed i2c bus 4 rtc rtc0: invalid alarm value: 2022-01-20T18:68:00 rtc-pcf8563 5-0051: registered as rtc0 rtc-pcf8563 5-0051: setting system clock to 2022-01-20T00:35:05 UTC (1642638905) i2c i2c-0: Added multiplexed i2c bus 5 at24 6-0050: supply vcc not found, using dummy regulator at24 6-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write at24 6-0054: supply vcc not found, using dummy regulator xiic-i2c 41600000.i2c: Timeout waiting at Tx empty xiic-i2c 41600000.i2c: Timeout waiting at Tx empty regulator-dummy: Underflow of regulator enable count i2c i2c-0: Added multiplexed i2c bus 6 i2c i2c-0: Added multiplexed i2c bus 7 i2c i2c-0: Added multiplexed i2c bus 8 pca954x 0-0074: registered 8 multiplexed busses for I2C switch pca9548 usbcore: registered new interface driver uvcvideo USB Video Class driver (1.1.1) gspca_main: v2.14.0 registered cdns-wdt f8005000.watchdog: Xilinx Watchdog Timer with timeout 10s Xilinx Zynq CpuIdle Driver started failed to register cpuidle driver sdhci: Secure Digital Host Controller Interface driver sdhci: Copyright(c) Pierre Ossman sdhci-pltfm: SDHCI platform and OF driver helper ledtrig-cpu: registered to indicate activity on CPUs hid: raw HID events driver (C) Jiri Kosina usbcore: registered new interface driver usbhid usbhid: USB HID core driver ad9528 spi0.0: supply vcc not found, using dummy regulator mmc0: SDHCI controller on e0100000.mmc [e0100000.mmc] using ADMA mmc0: new high speed SDHC card at address e624 mmcblk0: mmc0:e624 SD32G 29.7 GiB mmcblk0: p1 p2 p3 axi_adxcvr 44a50000.axi-adxcvr-rx: adxcvr_enforce_settings: Using QPLL without access, assuming desired Lane rate will be configurede axi_adxcvr 44a50000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.05.a) using QPLL on GTX2 at 0x44A50000. Number of lanes: 4. axi_adxcvr 44a60000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.05.a) using QPLL on GTX2 at 0x44A60000. Number of lanes: 4. axi-jesd204-rx 44aa0000.axi-jesd204-rx: AXI-JESD204-RX (1.07.a) at 0x44AA0000. Encoder 8b10b, width 4/4, lanes 4. axi-jesd204-tx 44a90000.axi-jesd204-tx: AXI-JESD204-TX (1.06.a) at 0x44A90000. Encoder 8b10b, width 4/4, lanes 4. axi_sysid 45000000.axi-sysid-0: AXI System ID core version (1.01.a) found axi_sysid 45000000.axi-sysid-0: [daq3] on [zc706] git branch <master> git <4ec8797c7cbb2b551f5930fd56d8f38a8cf3e7e9> clean [2022-01-C fpga_manager fpga0: Xilinx Zynq FPGA Manager registered usbcore: registered new interface driver snd-usb-audio NET: Registered protocol family 10 Segment Routing with IPv6 sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver NET: Registered protocol family 17 NET: Registered protocol family 36 Registering SWP/SWPB emulation handler [drm] Initialized axi_hdmi_drm 1.0.0 20120930 for 70e00000.axi_hdmi on minor 0 axi-hdmi 70e00000.axi_hdmi: [drm] Cannot find any crtc or sizes ad9680 spi0.2: AD9680 PLL LOCKED axi_adxcvr 44a50000.axi-adxcvr-rx: QPLL RX: Not ready defer probe axi_adxcvr 44a50000.axi-adxcvr-rx: QPLL RX: Not ready defer probe ad9680 spi0.2: Failed to enable JESD204 link: -517 ad9680 spi0.2: AD9680 PLL LOCKED cf_axi_dds 44a04000.axi-ad9152-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x44A04000 mapped to 0x0407967f, probed DDS AD92 cf_axi_adc 44a10000.axi-ad9680-hpc: ADI AIM (10.01.b) at 0x44A10000 mapped to 0x194cb1b3, probed ADC AD9680 as MASTER input: gpio_keys as /devices/soc0/gpio_keys/input/input0 clk: Not disabling unused clocks ALSA device list: #0: HDMI monitor Freeing unused kernel memory: 1024K Run /init as init process INIT: version 2.97 booting Starting udev udevd[82]: starting version 3.2.9 udevd[83]: starting eudev-3.2.9 EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) macb e000b000.ethernet eth0: PHY [e000b000.ethernet-ffffffff:07] driver [Marvell 88E1116R] (irq=POLL) macb e000b000.ethernet eth0: configuring for phy/rgmii-id link mode axi-hdmi 70e00000.axi_hdmi: [drm] Cannot find any crtc or sizes axi-hdmi 70e00000.axi_hdmi: [drm] Cannot find any crtc or sizes Starting tcf-agent: OK root@my_project:~#
For jesd_status command, I received following for ADC
Here the clock configuration seems to be entirely out of place from the expected build.
Can you please help me in resolving the issue?