Post Go back to editing

Need help on fixing Libiio Error.

 After installing the LIBIIO driver using windows 11, I ran the following command:   C:\>iio_info -s,

This resulted in the following message---Compiled with backends: xml ip usb serial.  Unable to create Local IIO context : Function not implemented (40)

1.  Now, I followed the "Getting Started", but I'm not sure if the LIBIIO library is to be installed on my Windows OS 11 machine or on the PLUTOSDR device?. 

  1. Install the libiio Library: 
    OS: Windows78Buster16.0420.04 Type : .exe.zip Version : Windows-setup
     : libiio-0.23.gc14a0f8-Windows-setup.exe

2. What does this error ( Unable to create Local IIO context : Function not implemented (40). ) message mean?

3. How do I fix this error?