Post Go back to editing

Loading custom profile for ADRV9008-2 and ADRV9008-1

Thread Summary

The user is trying to configure ADRV9008-1 and ADRV9008-2 using Linux and wants to load a custom profile at runtime or during boot. The solution involves using the sysfs API or libiio to load the profile at runtime, and converting the profile to device tree parameters for boot-time configuration. The custom profile file should be added to the Petalinux project to ensure it is available at runtime.
AI Generated Content

Hello ADI Team

I am trying to configure ADRV9008-1 and ADRV9008-2 using Linux. I followed the steps that were provided in https://wiki.analog.com/resources/eval/user-guides/adrv9002/quickstart/zynqmp  and created images for ADRV9008-1 and ADRV9008-2. Now, I  need to load custom profile generated using ADI tool so that I can configure the parameters of Transceivers during Run Time. I have observed that custom profile can be loaded in run time using IIO Oscilloscope. How can I enable this IIO Oscilloscope feature in the custom image that is created so that I can load the profile.

Also, can I load the profile while booting using UART console.

I am an amateur in Linux Domain. Any help in this regard would be highly appreciated.

Thanks

Deepika

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.