Hello ADI Team
I am trying to configure ADRV9008-1 and ADRV9008-2 using Linux. I followed the steps that were provided in https://wiki.analog.com/resources/eval/user-guides/adrv9002/quickstart/zynqmp and created images for ADRV9008-1 and ADRV9008-2. Now, I need to load custom profile generated using ADI tool so that I can configure the parameters of Transceivers during Run Time. I have observed that custom profile can be loaded in run time using IIO Oscilloscope. How can I enable this IIO Oscilloscope feature in the custom image that is created so that I can load the profile.
Also, can I load the profile while booting using UART console.
I am an amateur in Linux Domain. Any help in this regard would be highly appreciated.
Thanks
Deepika