Post Go back to editing

Loading custom profile for ADRV9008-2 and ADRV9008-1

Hello ADI Team

I am trying to configure ADRV9008-1 and ADRV9008-2 using Linux. I followed the steps that were provided in https://wiki.analog.com/resources/eval/user-guides/adrv9002/quickstart/zynqmp  and created images for ADRV9008-1 and ADRV9008-2. Now, I  need to load custom profile generated using ADI tool so that I can configure the parameters of Transceivers during Run Time. I have observed that custom profile can be loaded in run time using IIO Oscilloscope. How can I enable this IIO Oscilloscope feature in the custom image that is created so that I can load the profile.

Also, can I load the profile while booting using UART console.

I am an amateur in Linux Domain. Any help in this regard would be highly appreciated.

Thanks

Deepika

Top Replies

  • How can I enable this IIO Oscilloscope feature in the custom image that is created so that I can load the profile.

    You can load a profile via the sysfs API or by using libiio - please see…

Parents Reply Children