Hello,
Previous discussion was locked for some reason : Custom board adrv9009 QPLL not locking with hmc7044 - Q&A - Linux Software Drivers - EngineerZone (analog.com)
Thanks for the reply
- Indeed, forgot to remove clock assignement from JESD FSM device tree. They are well defined in another device tree file
- added jesd204-ignore-errors;
- removed axi clkgen nodes
- spi-max-frequency = <100000>; instead of //spi-max-frequency = <10000000>; inside hmc node
Boot log
U-Boot 2021.01 (Jun 01 2021 - 11:54:06 +0000) CPU: Zynq 7z045 Silicon: v3.1 Model: Xilinx ZC706 board DRAM: ECC disabled 1 GiB Flash: 0 Bytes NAND: 0 MiB MMC: mmc@e0100000: 0 Loading Environment from FAT... *** Warning - bad CRC, using default environment In: serial@e0001000 Out: serial@e0001000 Err: serial@e0001000 Net: ZYNQ GEM: e000b000, mdio bus e000b000, phyaddr 0, interface rgmii-id Warning: ethernet@e000b000 (eth0) using random MAC address - 36:07:34:74:f2:9d eth0: ethernet@e000b000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0 is current device Scanning mmc 0:1... Found U-Boot script /boot.scr 2595 bytes read in 28 ms (89.8 KiB/s) ## Executing script at 03000000 Trying to load boot images from mmc0 43292884 bytes read in 7071 ms (5.8 MiB/s) ## Loading kernel from FIT Image at 10000000 ... Using 'conf-system-top.dtb' configuration Verifying Hash Integrity ... OK Trying 'kernel-1' kernel subimage Description: Linux kernel Type: Kernel Image Compression: uncompressed Data Start: 0x10000100 Data Size: 25175072 Bytes = 24 MiB Architecture: ARM OS: Linux Load Address: 0x00200000 Entry Point: 0x00200000 Hash algo: sha256 Hash value: 53ffb458f6a7d03799f1a1d7a7c78914beef3c9ae808e065981703b049112304 Verifying Hash Integrity ... sha256+ OK ## Loading ramdisk from FIT Image at 10000000 ... Using 'conf-system-top.dtb' configuration Verifying Hash Integrity ... OK Trying 'ramdisk-1' ramdisk subimage Description: petalinux-image-minimal Type: RAMDisk Image Compression: uncompressed Data Start: 0x1180e500 Data Size: 18067040 Bytes = 17.2 MiB Architecture: ARM OS: Linux Load Address: unavailable Entry Point: unavailable Hash algo: sha256 Hash value: 63acd6d7636a2f96572a0cbe74ca4eebc76015c8aa3158fdff260d6071271e5b Verifying Hash Integrity ... sha256+ OK ## Loading fdt from FIT Image at 10000000 ... Using 'conf-system-top.dtb' configuration Verifying Hash Integrity ... OK Trying 'fdt-system-top.dtb' fdt subimage Description: Flattened Device Tree blob Type: Flat Device Tree Compression: uncompressed Data Start: 0x1180262c Data Size: 48648 Bytes = 47.5 KiB Architecture: ARM Hash algo: sha256 Hash value: fc4bf5530c9fc71e931fb17736e586267ccba779fd78705785957cbc5a5309d9 Verifying Hash Integrity ... sha256+ OK Booting using the fdt blob at 0x1180262c Loading Kernel Image Loading Ramdisk to 2eec5000, end 2ffffe60 ... OK Loading Device Tree to 2eeb6000, end 2eec4e07 ... OK Starting kernel ... Booting Linux on physical CPU 0x0 Linux version 5.10.0-xilinx-v2021.1 (oe-user@oe-host) (arm-xilinx-linux-gnueabi-gcc (GCC) 10.2.0, GNU ld (GNU Binutils) 2.35.1) #1 SMP PREEMPT Thu Nov 18 14:55:54 UTC 2021 CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache OF: fdt: Machine model: Xilinx ZC706 board printk: bootconsole [earlycon0] enabled Memory policy: Data cache writealloc INITRD: 0x00800000+0x01000000 overlaps in-use memory region - disabling initrd cma: Reserved 128 MiB at 0x38000000 Zone ranges: Normal [mem 0x0000000000000000-0x000000002fffffff] HighMem [mem 0x0000000030000000-0x000000003fffffff] Movable zone start for each node Early memory node ranges node 0: [mem 0x0000000000000000-0x000000003fffffff] Initmem setup node 0 [mem 0x0000000000000000-0x000000003fffffff] percpu: Embedded 15 pages/cpu s30028 r8192 d23220 u61440 Built 1 zonelists, mobility grouping on. Total pages: 260416 Kernel command line: console=ttyPS0,115200n8 root=/dev/ram rw initrd=0x00800000,16M earlyprintk mtdparts=physmap-flash.0:512K(nor-fsbl),512K(nor-u-boot),5M(nor-linux),9M(nor-user),1M(nor-scratch),-(nor-rootfs) Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear) Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear) mem auto-init: stack:off, heap alloc:off, heap free:off Memory: 825596K/1048576K available (10240K kernel code, 852K rwdata, 7196K rodata, 44032K init, 168K bss, 91908K reserved, 131072K cma-reserved, 131072K highmem) rcu: Preemptible hierarchical RCU implementation. rcu: RCU event tracing is enabled. rcu: RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2. Trampoline variant of Tasks RCU enabled. rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies. rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 efuse mapped to (ptrval) slcr mapped to (ptrval) L2C: platform modifies aux control register: 0x72360000 -> 0x72760000 L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000 L2C-310 erratum 769419 enabled L2C-310 enabling early BRESP for Cortex-A9 L2C-310 full line of zeros enabled for Cortex-A9 L2C-310 ID prefetch enabled, offset 1 lines L2C-310 dynamic clock gating enabled, standby mode enabled L2C-310 cache controller enabled, 8 ways, 512 kB L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001 random: get_random_bytes called from start_kernel+0x33c/0x4e8 with crng_init=0 zynq_clock_init: clkc starts at (ptrval) Zynq clock init ps_clk frequency not specified, using 33 MHz. sched_clock: 64 bits at 399MHz, resolution 2ns, wraps every 4398046511103ns clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x5c4093a7d1, max_idle_ns: 440795210635 ns Switching to timer-based delay loop, resolution 2ns clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 447945978 ns timer #0 at (ptrval), irq=25 Console: colour dummy device 80x30 Calibrating delay loop (skipped), value calculated using timer frequency.. 799.99 BogoMIPS (lpj=3999999) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear) Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear) CPU: Testing write buffer coherency: ok CPU0: Spectre v2: using BPIALL workaround CPU0: thread -1, cpu 0, socket 0, mpidr 80000000 Setting up static identity map for 0x100000 - 0x100060 rcu: Hierarchical SRCU implementation. smp: Bringing up secondary CPUs ... CPU1: thread -1, cpu 1, socket 0, mpidr 80000001 CPU1: Spectre v2: using BPIALL workaround smp: Brought up 1 node, 2 CPUs SMP: Total of 2 processors activated (1599.99 BogoMIPS). CPU: All CPU(s) started in SVC mode. devtmpfs: initialized VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4 clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns futex hash table entries: 512 (order: 3, 32768 bytes, linear) pinctrl core: initialized pinctrl subsystem NET: Registered protocol family 16 DMA: preallocated 256 KiB pool for atomic coherent allocations thermal_sys: Registered thermal governor 'step_wise' cpuidle: using governor ladder hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers. hw-breakpoint: maximum watchpoint size is 4 bytes. zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0x(ptrval) SCSI subsystem initialized usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb mc: Linux media interface: v0.10 videodev: Linux video capture interface: v2.00 jesd204: created con: id=0, topo=0, link=0, /axi/spi@e0006000/hmc7044@2 <-> /fpga-axi@0/axi-adxcvr-tx@44a80000 jesd204: created con: id=1, topo=0, link=1, /axi/spi@e0006000/hmc7044@2 <-> /fpga-axi@0/axi-adxcvr-rx@44a60000 jesd204: created con: id=2, topo=0, link=0, /fpga-axi@0/axi-adxcvr-tx@44a80000 <-> /fpga-axi@0/axi-jesd204-tx@44a90000 jesd204: created con: id=3, topo=0, link=1, /fpga-axi@0/axi-adxcvr-rx@44a60000 <-> /fpga-axi@0/axi-jesd204-rx@44aa0000 jesd204: created con: id=4, topo=0, link=1, /fpga-axi@0/axi-jesd204-rx@44aa0000 <-> /axi/spi@e0006000/adrv9009-phy@0 jesd204: created con: id=5, topo=0, link=0, /fpga-axi@0/axi-jesd204-tx@44a90000 <-> /axi/spi@e0006000/adrv9009-phy@0 jesd204: /axi/spi@e0006000/adrv9009-phy@0: JESD204[0] transition uninitialized -> initialized jesd204: /axi/spi@e0006000/adrv9009-phy@0: JESD204[1] transition uninitialized -> initialized jesd204: found 6 devices and 1 topologies FPGA manager framework Advanced Linux Sound Architecture Driver Initialized. clocksource: Switched to clocksource arm_global_timer NET: Registered protocol family 2 tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear) TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear) TCP bind hash table entries: 8192 (order: 4, 65536 bytes, linear) TCP: Hash tables configured (established 8192 bind 8192) UDP hash table entries: 512 (order: 2, 16384 bytes, linear) UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear) NET: Registered protocol family 1 hw perfevents: no interrupt-affinity property for /pmu@f8891000, guessing. hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available workingset: timestamp_bits=14 max_order=18 bucket_order=4 bounce: pool size: 64 pages io scheduler mq-deadline registered io scheduler kyber registered zynq-pinctrl 700.pinctrl: zynq pinctrl initialized zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330 dma-pl330 f8003000.dmac: DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16 brd: module loaded loop: module loaded Registered mathworks_ip class spi-nor spi0.0: unrecognized JEDEC id bytes: 00 00 00 00 00 00 MACsec IEEE 802.1AE libphy: Fixed MDIO Bus: probed tun: Universal TUN/TAP device driver, 1.6 zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' libphy: MACB_mii_bus: probed macb e000b000.ethernet eth0: Cadence GEM rev 0x00020118 at 0xe000b000 irq 38 (36:07:34:74:f2:9d) usbcore: registered new interface driver asix usbcore: registered new interface driver ax88179_178a usbcore: registered new interface driver cdc_ether usbcore: registered new interface driver net1080 usbcore: registered new interface driver cdc_subset usbcore: registered new interface driver zaurus usbcore: registered new interface driver cdc_ncm ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver usbcore: registered new interface driver uas usbcore: registered new interface driver usb-storage usbcore: registered new interface driver usbserial_generic usbserial: USB Serial support registered for generic usbcore: registered new interface driver ftdi_sio usbserial: USB Serial support registered for FTDI USB Serial Device usbcore: registered new interface driver upd78f0730 usbserial: USB Serial support registered for upd78f0730 zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' udc-core: couldn't find an available UDC - added [g_mass_storage] to list of pending drivers i2c /dev entries driver zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' cdns-i2c e0004000.i2c: 400 kHz mmio e0004000 irq 32 pca954x 0-0074: probe failed usbcore: registered new interface driver uvcvideo USB Video Class driver (1.1.1) gspca_main: v2.14.0 registered cdns-wdt f8005000.watchdog: Xilinx Watchdog Timer with timeout 10s Xilinx Zynq CpuIdle Driver started sdhci: Secure Digital Host Controller Interface driver sdhci: Copyright(c) Pierre Ossman sdhci-pltfm: SDHCI platform and OF driver helper zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' ledtrig-cpu: registered to indicate activity on CPUs zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' hid: raw HID events driver (C) Jiri Kosina zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' usbcore: registered new interface driver usbhid zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' usbhid: USB HID core driver adrv9009 spi1.0: adrv9009_probe : enter mmc0: SDHCI controller on e0100000.mmc [e0100000.mmc] using ADMA hmc7044 spi1.2: PLL1: Holdover, CLKIN1 @ 40000000 Hz, PFD: 320 kHz - PLL2: Locked @ 2949.120000 MHz jesd204: /axi/spi@e0006000/hmc7044@2,jesd204:0,parent=spi1.2: Using as SYSREF provider axi_adxcvr 44a60000.axi-adxcvr-rx: AXI-ADXCVR-RX (16.01.a) using CPLL on GTX2 at 0x44A60000. Number of lanes: 2. axi_adxcvr 44a80000.axi-adxcvr-tx: AXI-ADXCVR-TX (16.01.a) using QPLL on GTX2 at 0x44A80000. Number of lanes: 2. axi-jesd204-rx 44aa0000.axi-jesd204-rx: AXI-JESD204-RX (1.02.a) at 0x44AA0000. Encoder 8b10b, width 4/0, lanes 2, jesd204-fsm. axi-jesd204-tx 44a90000.axi-jesd204-tx: AXI-JESD204-TX (1.01.a) at 0x44A90000. Encoder 8b10b, width 4/0, lanes 2, jesd204-fsm. fpga_manager fpga0: Xilinx Zynq FPGA Manager registered usbcore: registered new interface driver snd-usb-audio NET: Registered protocol family 10 Segment Routing with IPv6 sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver NET: Registered protocol family 17 NET: Registered protocol family 36 Registering SWP/SWPB emulation handler zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 35, base_baud = 3125000) is a xuartps printk: console [ttyPS0] enabled printk: console [ttyPS0] enabled printk: bootconsole [earlycon0] disabled printk: bootconsole [earlycon0] disabled zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' adrv9009 spi1.0: adrv9009_probe : enter jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition initialized -> probed jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition initialized -> probed jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition probed -> idle jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition probed -> idle jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition idle -> device_init jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition idle -> device_init jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition device_init -> link_init jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition device_init -> link_init jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition link_init -> link_supported jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition link_init -> link_supported jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition link_supported -> link_pre_setup jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition link_supported -> link_pre_setup jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition link_pre_setup -> clk_sync_stage1 jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition link_pre_setup -> clk_sync_stage1 jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition clk_sync_stage1 -> clk_sync_stage2 jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition clk_sync_stage1 -> clk_sync_stage2 jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition clk_sync_stage2 -> clk_sync_stage3 jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition clk_sync_stage2 -> clk_sync_stage3 jesd204: /fpga-axi@0/axi-jesd204-rx@44aa0000,jesd204:2,parent=44aa0000.axi-jesd204-rx: Possible instantiation for multiple chips; HDL lanes 2, Link[1] lanes 1 jesd204: /fpga-axi@0/axi-jesd204-tx@44a90000,jesd204:3,parent=44a90000.axi-jesd204-tx: Possible instantiation for multiple chips; HDL lanes 2, Link[0] lanes 1 axi_adxcvr 44a80000.axi-adxcvr-tx: QPLL TX Error: 0 axi_adxcvr 44a80000.axi-adxcvr-tx: QPLL TX Error: 0 axi-jesd204-tx 44a90000.axi-jesd204-tx: axi_jesd204_tx_jesd204_link_setup: Link0 enable lane clock failed (-5) jesd204: /fpga-axi@0/axi-jesd204-tx@44a90000,jesd204:3,parent=44a90000.axi-jesd204-tx: JESD204[0] In link_setup got error from cb: -5 (ignoring!) adrv9009 spi1.0: ADIHAL_resetHw adrv9009 spi1.0: ERROR: 346: TALISE_verifySpiReadWrite(): Cannot read from a low SPI address adrv9009 spi1.0: adrv9009_jesd204_link_setup:5805 (ret 10) jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] In link_setup got error from cb: -14 (ignoring!) jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition clk_sync_stage3 -> link_setup jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition clk_sync_stage3 -> link_setup adrv9009 spi1.0: adrv9009_jesd204_setup_stage1:5861 Unexpected MCS sync status (0x0) jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] In opt_setup_stage1 got error from cb: -14 (ignoring!) jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition link_setup -> opt_setup_stage1 jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition link_setup -> opt_setup_stage1 adrv9009 spi1.0: adrv9009_jesd204_setup_stage2:5891 Unexpected MCS sync status (0x0) jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] In opt_setup_stage2 got error from cb: -14 (ignoring!) jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition opt_setup_stage1 -> opt_setup_stage2 jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition opt_setup_stage1 -> opt_setup_stage2 jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition opt_setup_stage2 -> opt_setup_stage3 jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition opt_setup_stage2 -> opt_setup_stage3 random: fast init done adrv9009 spi1.0: ERROR: 179: ARM Mailbox Busy. Command not executed in TALISE_sendArmCommand() adrv9009 spi1.0: adrv9009_jesd204_setup_stage4:6040 (ret 5) jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] In opt_setup_stage4 got error from cb: -14 (ignoring!) jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition opt_setup_stage3 -> opt_setup_stage4 jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition opt_setup_stage3 -> opt_setup_stage4 jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition opt_setup_stage4 -> opt_setup_stage5 jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition opt_setup_stage4 -> opt_setup_stage5 axi_adxcvr 44a60000.axi-adxcvr-rx: CPLL RX Error: 0 axi_adxcvr 44a60000.axi-adxcvr-rx: CPLL RX Error: 0 axi-jesd204-rx 44aa0000.axi-jesd204-rx: axi_jesd204_rx_jesd204_clks_enable: Link1 enable lane clock failed (-5) jesd204: /fpga-axi@0/axi-jesd204-rx@44aa0000,jesd204:2,parent=44aa0000.axi-jesd204-rx: JESD204[1] In clocks_enable got error from cb: -5 (ignoring!) jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition opt_setup_stage5 -> clocks_enable jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition opt_setup_stage5 -> clocks_enable jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition clocks_enable -> link_enable jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition clocks_enable -> link_enable axi-jesd204-rx 44aa0000.axi-jesd204-rx: axi_jesd204_rx_jesd204_link_running: Link1 status failed (RESET) jesd204: /fpga-axi@0/axi-jesd204-rx@44aa0000,jesd204:2,parent=44aa0000.axi-jesd204-rx: JESD204[1] In link_running got error from cb: -1 (ignoring!) axi-jesd204-tx 44a90000.axi-jesd204-tx: axi_jesd204_tx_jesd204_link_running: Link0 status failed (WAIT) jesd204: /fpga-axi@0/axi-jesd204-tx@44a90000,jesd204:3,parent=44a90000.axi-jesd204-tx: JESD204[0] In link_running got error from cb: -1 (ignoring!) adrv9009 spi1.0: Link0 TAL_DEFRAMER_A deframerStatus 0x8 adrv9009 spi1.0: Link1 TAL_FRAMER_A framerStatus 0x0 jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition link_enable -> link_running jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition link_enable -> link_running adrv9009 spi1.0: ERROR: 180: Device not in radioOff/IDLE state. Error in TALISE_enableTrackingCals() adrv9009 spi1.0: adrv9009_jesd204_post_running_stage:6141 (ret 5) jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] In opt_post_running_stage got error from cb: -14 (ignoring!) adrv9009 spi1.0: ERROR: 32: TALISE_gpIntHandler(): AUXCLK PLL is not locked jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[0] transition link_running -> opt_post_running_stage adrv9009 spi1.0: AUX PLL lock detect reset adrv9009 spi1.0: (null) jesd204: /axi/spi@e0006000/adrv9009-phy@0,jesd204:1,parent=spi1.0: JESD204[1] transition link_running -> opt_post_running_stage adrv9009 spi1.0: (null) adrv9009 spi1.0: (null) adrv9009 spi1.0: (null) adrv9009 spi1.0: GP Interrupt Status 0x5 Action: ERR_RESET_FULL cf_axi_dds 44a14000.axi-adrv9009-tx-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.00.b) at 0x44A14000 mapped to 0x(ptrval), probed DDS AD9371 zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' cf_axi_adc 44a00000.axi-adrv9009-rx-hpc: ADI AIM (10.00.b) at 0x44A00000 mapped to 0x(ptrval), probed ADC ADRV9009 as MASTER zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' zynq-pinctrl 700.pinctrl: unsupported configuration parameter '18' ALSA device list: No soundcards found. Warning: unable to open an initial console. Freeing unused kernel memory: 44032K Run /init as init process udevd[77]: starting version 3.2.9 random: udevd: uninitialized urandom read (16 bytes read) random: udevd: uninitialized urandom read (16 bytes read) random: udevd: uninitialized urandom read (16 bytes read) udevd[78]: starting eudev-3.2.9 urandom_read: 2 callbacks suppressed random: dd: uninitialized urandom read (512 bytes read) samplemodule: loading out-of-tree module taints kernel. <1>Hello module world : DRIVER !! <1>Module parameters were (0xdeadbeef) and "default" <1>Config_of ok. Sorry, registering the character device failed with macb e000b000.ethernet eth0: PHY [e000b000.ethernet-ffffffff:00] driver [Marvell 88E1510] (irq=POLL) macb e000b000.ethernet eth0: configuring for phy/rgmii-id link mode macb e000b000.ethernet eth0: Link is Up - 1Gbps/Full - flow control tx IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready random: dbus-uuidgen: uninitialized urandom read (12 bytes read) random: dbus-uuidgen: uninitialized urandom read (8 bytes read) random: dbus-daemon: uninitialized urandom read (12 bytes read) random: crng init done random: 1 urandom warning(s) missed due to ratelimiting root@ETRX_petalinux:~#
root@ETRX_petalinux:~# cat /sys/kernel/debug/clk/clk_summary enable prepare protect duty clock count count count rate accuracy phase cycle nshot ---------------------------------------------------------------------------------------------------- spi1.0-tx_sampl_clk 1 1 0 61440000 0 0 50000 0 spi1.0-obs_sampl_clk 0 0 0 122880000 0 0 50000 0 spi1.0-rx_sampl_clk 0 0 0 61440000 0 0 50000 0 hmc7044_out9_FPGA_SYSREF_RX_AB 0 0 0 1920000 0 0 50000 0 hmc7044_out8_FPGA_SYSREF_TX_OBS_AB 0 0 0 1920000 0 0 50000 0 hmc7044_out7_CORE_CLK_RX_AB 2 2 0 122880000 0 0 50000 0 hmc7044_out6_CORE_CLK_TX_OBS_AB 1 1 0 122880000 0 0 50000 0 hmc7044_out5_JESD_REFCLK_RX_AB 1 1 0 245760000 0 0 50000 0 rx_out_clk 0 0 0 245760000 0 0 50000 0 rx_gt_clk 0 0 0 4915200 0 0 50000 0 hmc7044_out4_JESD_REFCLK_TX_OBS_AB 1 1 0 245760000 0 0 50000 0 tx_out_clk 0 0 0 245760000 0 0 50000 0 tx_gt_clk 0 0 0 4915200 0 0 50000 0 hmc7044_out3_DEV_SYSREF_B 0 0 0 1920000 0 0 50000 0 hmc7044_out2_DEV_REFCLK_B 0 0 0 245760000 0 0 50000 0 hmc7044_out1_DEV_SYSREF_A 0 0 0 1920000 0 0 50000 0 hmc7044_out0_DEV_REFCLK_A 1 1 0 245760000 0 0 50000 0 adrv9009_ext_refclk 0 0 0 12288000 0 0 50000 0 audio_clock 0 0 0 12288000 0 0 50000 0 ps_clk 3 3 0 33333333 0 0 50000 0 iopll_int 1 1 0 999999990 0 0 50000 0 iopll 9 9 0 999999990 0 0 50000 0 dbg_mux 1 1 0 999999990 0 0 50000 0 dbg_div 1 1 0 66666666 0 0 50000 0 dbg_emio_mux 1 1 0 66666666 0 0 50000 0 dbg_trc 1 1 0 66666666 0 0 50000 0 can_mux 0 0 0 999999990 0 0 50000 0 can_div0 0 0 0 40000000 0 0 50000 0 can_div1 0 0 0 8000000 0 0 50000 0 can1_gate 0 0 0 8000000 0 0 50000 0 can1 0 0 0 8000000 0 0 50000 0 can0_gate 0 0 0 8000000 0 0 50000 0 can0 0 0 0 8000000 0 0 50000 0 gem1_mux 0 0 0 999999990 0 0 50000 0 gem1_div0 0 0 0 16666667 0 0 50000 0 gem1_div1 0 0 0 16666667 0 0 50000 0 gem1_emio_mux 0 0 0 16666667 0 0 50000 0 gem1 0 0 0 16666667 0 0 50000 0 gem0_mux 1 1 0 999999990 0 0 50000 0 gem0_div0 1 1 0 124999999 0 0 50000 0 gem0_div1 1 1 0 124999999 0 0 50000 0 gem0_emio_mux 1 1 0 124999999 0 0 50000 0 gem0 1 1 0 124999999 0 0 50000 0 spi0_mux 0 0 0 999999990 0 0 50000 0 spi0_div 0 0 0 166666665 0 0 50000 0 spi1 0 0 0 166666665 0 0 50000 0 spi0 0 0 0 166666665 0 0 50000 0 uart0_mux 1 1 0 999999990 0 0 50000 0 uart0_div 1 1 0 50000000 0 0 50000 0 uart1 1 1 0 50000000 0 0 50000 0 uart0 0 0 0 50000000 0 0 50000 0 sdio0_mux 1 1 0 999999990 0 0 50000 0 sdio0_div 1 1 0 50000000 0 0 50000 0 sdio1 0 0 0 50000000 0 0 50000 0 sdio0 1 1 0 50000000 0 0 50000 0 pcap_mux 1 1 0 999999990 0 0 50000 0 pcap_div 1 1 0 199999998 0 0 50000 0 pcap 1 2 0 199999998 0 0 50000 0 fclk3_mux 1 1 0 999999990 0 0 50000 0 fclk3_div0 1 1 0 41666667 0 0 50000 0 fclk3_div1 1 1 0 41666667 0 0 50000 0 fclk3 1 1 0 41666667 0 0 50000 0 fclk2_mux 1 1 0 999999990 0 0 50000 0 fclk2_div0 1 1 0 499999995 0 0 50000 0 fclk2_div1 1 1 0 249999998 0 0 50000 0 fclk2 1 1 0 249999998 0 0 50000 0 fclk1_mux 1 1 0 999999990 0 0 50000 0 fclk1_div0 1 1 0 199999998 0 0 50000 0 fclk1_div1 1 1 0 199999998 0 0 50000 0 fclk1 4 4 0 199999998 0 0 50000 0 fclk0_mux 1 1 0 999999990 0 0 50000 0 fclk0_div0 1 1 0 199999998 0 0 50000 0 fclk0_div1 1 1 0 99999999 0 0 50000 0 fclk0 2 2 0 99999999 0 0 50000 0 ddrpll_int 1 1 0 1066666656 0 0 50000 0 ddrpll 3 3 0 1066666656 0 0 50000 0 dci_div0 1 1 0 71111111 0 0 50000 0 dci_div1 1 1 0 10158731 0 0 50000 0 dci 1 1 0 10158731 0 0 50000 0 ddr3x_div 1 1 0 533333328 0 0 50000 0 ddr3x 1 1 0 533333328 0 0 50000 0 ddr2x_div 1 1 0 355555552 0 0 50000 0 ddr2x 1 1 0 355555552 0 0 50000 0 armpll_int 1 1 0 1599999984 0 0 50000 0 armpll 2 2 0 1599999984 0 0 50000 0 smc_mux 0 0 0 1599999984 0 0 50000 0 smc_div 0 0 0 26666667 0 0 50000 0 smc 0 0 0 26666667 0 0 50000 0 lqspi_mux 1 1 0 1599999984 0 0 50000 0 lqspi_div 1 1 0 40000000 0 0 50000 0 lqspi 2 1 0 40000000 0 0 50000 0 cpu_mux 1 1 0 1599999984 0 0 50000 0 cpu_div 3 3 0 799999992 0 0 50000 0 cpu_1x_div 1 1 0 133333332 0 0 50000 0 cpu_1x 9 10 0 133333332 0 0 50000 0 smc_aper 0 0 0 133333332 0 0 50000 0 lqspi_aper 2 1 0 133333332 0 0 50000 0 gpio_aper 1 1 0 133333332 0 0 50000 0 uart1_aper 1 1 0 133333332 0 0 50000 0 uart0_aper 0 0 0 133333332 0 0 50000 0 i2c1_aper 0 0 0 133333332 0 0 50000 0 i2c0_aper 0 1 0 133333332 0 0 50000 0 can1_aper 0 0 0 133333332 0 0 50000 0 can0_aper 0 0 0 133333332 0 0 50000 0 spi1_aper 0 0 0 133333332 0 0 50000 0 spi0_aper 0 0 0 133333332 0 0 50000 0 sdio1_aper 0 0 0 133333332 0 0 50000 0 sdio0_aper 1 1 0 133333332 0 0 50000 0 gem1_aper 0 0 0 133333332 0 0 50000 0 gem0_aper 2 2 0 133333332 0 0 50000 0 usb1_aper 0 0 0 133333332 0 0 50000 0 usb0_aper 0 0 0 133333332 0 0 50000 0 dbg_apb 1 1 0 133333332 0 0 50000 0 swdt 1 1 0 133333332 0 0 50000 0 cpu_2x_div 1 1 0 266666664 0 0 50000 0 cpu_2x 1 2 0 266666664 0 0 50000 0 dma 0 1 0 266666664 0 0 50000 0 cpu_3or2x_div 1 1 0 399999996 0 0 50000 0 cpu_3or2x 2 2 0 399999996 0 0 50000 0 cpu_6or4x 0 0 0 799999992 0 0 50000 0 can1_mio_mux 0 0 0 0 0 0 50000 0 can0_mio_mux 0 0 0 0 0 0 50000 0
Regards,
Salah
Regards
[edited by: fadsalah_etelm at 4:21 PM (GMT -5) on 8 Dec 2021]