Post Go back to editing

Viewing Boot Messages on the USB UART on the ADRV9364+ADRV1CCR-BOB

After finding the windows driver for the CP2103 chip on the USB UART port P14 on the ADRV1CCR-BOB, I can run it through a boot cycle and watch what should be characters stream out over the COM port.  However, the characters are unintelligible jibberish.  Changing things like Baud rate is not helping.  Is there a special encoding I need other than UTF-8 to access the UART port?  Or is there something else I am missing?

Micah