Hi ADI,
we using ssm4567 on linux 3.10, while driver init, write soft_reset(0xff) to 0, return error code -5. other register can read write ok. what's the problem?
attach debug log
[edited by: sarvdo at 1:43 AM (GMT -5) on 10 Nov 2021]
Hi ADI,
we using ssm4567 on linux 3.10, while driver init, write soft_reset(0xff) to 0, return error code -5. other register can read write ok. what's the problem?
Hi ADI,
we using ssm4567 on allwinner A40i platform(Linux 3.10).i2c(0x34) interface can detect and read register value as following,but while insmod the codec driver module which got from github.com,…
Hi,
Sorry but I missed the link to wiki page for amixer. You can find it here: Linux Sound Driver [Analog Devices Wiki]
Unfortunately we don't support that "tinyalsa" lib so you have to figure out by yourself…
if we using alsamix, (not tinymix) pls list the setting cmd.
the driver is download from your web site........
Hi ADI,
we using ssm4567 on allwinner A40i platform(Linux 3.10).i2c(0x34) interface can detect and read register value as following,but while insmod the codec driver module which got from github.com, the Soft_reset(0xff) return -5.(issue #1)
#2 issue, which we are using tinymix cmd, to config the control path, there is no any control path return.
#3. how to config the control path?
Hi ADI:
Thanks a lot for help reply for the audio issue.
Now we has another audio issue:
mount -t debugfs none /sys/kernel/debug/
echo -n "file soc-core.c +p" >/sys/kernel/debug/dynamic_debug/control
insmod /lib/modules/3.10.65/snd-soc-ssm4567.ko
insmod /lib/modules/3.10.65/snd-soc-ssm4567-i2c.ko
tinymix -D 1 3 1
tinymix -D 1 4 1
tinymix -D 1 8 hub_enable
aplay /mnt/ring03.wav -f S16_LE -Dplughw:1,0 -r 44100 //is silent.
aplay /mnt/notify.wav -f S16_LE -Dplughw:1,0 -r 44100 //is ok
aplay /mnt/music.wav -f S32_LE -Dplughw:1,0 -r 44100 //volume very low.
How to debug these issues?
Hi ADI:
Thanks a lot for help reply for the audio issue.
Now we has another audio issue:
mount -t debugfs none /sys/kernel/debug/
echo -n "file soc-core.c +p" >/sys/kernel/debug/dynamic_debug/control
insmod /lib/modules/3.10.65/snd-soc-ssm4567.ko
insmod /lib/modules/3.10.65/snd-soc-ssm4567-i2c.ko
tinymix -D 1 3 1
tinymix -D 1 4 1
tinymix -D 1 8 hub_enable
aplay /mnt/ring03.wav -f S16_LE -Dplughw:1,0 -r 44100 //is silent.
aplay /mnt/notify.wav -f S16_LE -Dplughw:1,0 -r 44100 //is ok
aplay /mnt/music.wav -f S32_LE -Dplughw:1,0 -r 44100 //volume very low.
How to debug these issues?
Dear Robert,
This question is a duplicate of the topic posted here: there-is-no-sound-speaker-is-silent-from-speaker-when-aplay-it-but-play-the-same-fie-with-other-codec-chip-play-it-on-pc-is-ok-some-wav-file-the-volume-is-very-low-the-other-wav-file-is-ok
It was answered there and this topic is marked as "Answered" by the creator so please let's leave this closed and continue on the other topic.
Thank you
Hi the first attach wav file is "ring03.wav" 9seconds which so voice issue.
the second 1 seconds file is "notify" which is ok wav file.
Hello hirobert,
It does look like the discussion is continuing on the new thread.
Dave T