Hello,engineers!
I am using adrv9009 rf board and zcu102 to design. Now, I want to know how to enable 2nd RX channel of adrv9009 . shown as below:

I should modify the code like:
and refill the buffer like:

is it right?
Thanks for your reply!!
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADRV9009
Recommended for New Designs
The ADRV9009 is a highly integrated, radio frequency (RF), agile transceiver offering dual transmitters and receivers, integrated synthesizers, and digital...
Datasheet
ADRV9009 on Analog.com
Hello,engineers!
I am using adrv9009 rf board and zcu102 to design. Now, I want to know how to enable 2nd RX channel of adrv9009 . shown as below:

I should modify the code like:
and refill the buffer like:

is it right?
Thanks for your reply!!
On the adrv9009-ZU11EG Noticing discontinuities/saturation on the data on this set up when writing to disk vs when only one channel is enabled :( I have cma = 1024M set and also using tmpfs for optimal write speeds.
See those artifacts in the time series around 0.01s?
Are you setting out_altvoltage0_TRX_LO_frequency with separate iio_devices? Your code snippets do not reference these calls.
-Travis
Yes frequency is configured before these code snippets.
wanted to see if I’m enabling the channels correctly.
thanks
Child id should be 1 not 2 for secondary RX channels.
-Travis
Im trying to enable adrv9009-phy's primary RX channel and adrv9009-phy-b's primary RX channel.
I.e. the RX1 channel for each ADC, No secondary RX channels.
Then index 0 and 2 are fine.
-Travis
Hi Trav, I'm now using adrv9009zu11EG + fmcomms8. Has the adrv9009 iio streaming been tested for this hardware? CUrrently getting "Could not create RX buffer: Cannot allocate memory" ERROR.
Notice the destination bus width in the hdl is 128Bits.
This is the dts file arch/arm64/boot/dts/xilinx/zynqmp-adrv9009-zu11eg-revb-adrv2crr-fmc-revb-sync-fmcomms8.dts notice it says 256 bits for destination.
Max is 128 bits for HP
This, even when I only enable one channel from adrv9009-phy and not enable ling the other 7 channels.
This, even when I only enable one channel from adrv9009-phy and not enable ling the other 7 channels.
adrv9009-iiostream from libiio/examples works. So I guess its just my code.
Problem resolved?
-Travis