Hello,engineers!
I am using adrv9009 rf board and zcu102 to design. Now, I want to know how to enable 2nd RX channel of adrv9009 . shown as below:

I should modify the code like:
and refill the buffer like:

is it right?
Thanks for your reply!!
ADRV9009
Recommended for New Designs
The ADRV9009 is a highly integrated, radio frequency (RF), agile transceiver offering dual transmitters and receivers, integrated synthesizers, and digital...
Datasheet
ADRV9009 on Analog.com
Hello,engineers!
I am using adrv9009 rf board and zcu102 to design. Now, I want to know how to enable 2nd RX channel of adrv9009 . shown as below:

I should modify the code like:
and refill the buffer like:

is it right?
Thanks for your reply!!
On the adrv9009-ZU11EG Noticing discontinuities/saturation on the data on this set up when writing to disk vs when only one channel is enabled :( I have cma = 1024M set and also using tmpfs for optimal write speeds.
See those artifacts in the time series around 0.01s?
Results when only one channel is enabled. Notice the amplitude in the time series dosent spike up and I ploted a few more miliseconds.
Do you have a perfectly clean environment? Or for example ground the inputs and set the gain to 0?
I've seen similar data from random Wi-Fi or LTE traffic.
-Travis
Hey Trav, How about code to enable RX1A (I and Q) from adrv9009-phy and
RX1B (I and Q) from adrv9009-phy-b from ADRV9009ZU11EG. This is what I've tried.

I'm noticing that I'm configuring the frequency for both devices ( out_altvoltage0_TRX_LO_frequency file is being updated for both adrv9009-phy and adrv9009-phy-b)
I'm noticing that I'm configuring the frequency for both devices ( out_altvoltage0_TRX_LO_frequency file is being updated for both adrv9009-phy and adrv9009-phy-b)
Are you setting out_altvoltage0_TRX_LO_frequency with separate iio_devices? Your code snippets do not reference these calls.
-Travis
Yes frequency is configured before these code snippets.
wanted to see if I’m enabling the channels correctly.
thanks
Child id should be 1 not 2 for secondary RX channels.
-Travis
Im trying to enable adrv9009-phy's primary RX channel and adrv9009-phy-b's primary RX channel.
I.e. the RX1 channel for each ADC, No secondary RX channels.
Then index 0 and 2 are fine.
-Travis
Hi Trav, I'm now using adrv9009zu11EG + fmcomms8. Has the adrv9009 iio streaming been tested for this hardware? CUrrently getting "Could not create RX buffer: Cannot allocate memory" ERROR.
Notice the destination bus width in the hdl is 128Bits.
This is the dts file arch/arm64/boot/dts/xilinx/zynqmp-adrv9009-zu11eg-revb-adrv2crr-fmc-revb-sync-fmcomms8.dts notice it says 256 bits for destination.
Max is 128 bits for HP
This, even when I only enable one channel from adrv9009-phy and not enable ling the other 7 channels.