Post Go back to editing

ZC706+ADRV9002: SPI probe for ADRV9002 failed

Hi ,

We are booting ZC706+ADRV9002 using uImage and devicetree.dtb obtained by building linux-kernel following the AD's steps provided here:

https://wiki.analog.com/resources/tools-software/linux-build/generic/zynq

BOOT.BIN is generated following the steps provided here:

https://wiki.analog.com/resources/tools-software/linux-software/build-the-zynq-boot-image

ZC706+ADRV9002 is getting booted with this set of files. But spi probe for ad9002 is getting failed with the error:

[    1.965192] adrv9002 spi0.0: Invalid gpio number: 0
[    1.968795] adrv9002: probe of spi0.0 failed with error -22

FYI PFA the bootlog .

Please let us know how to resolve this error to get ad9002 probed successfully.

U-Boot 2014.07-dirty (Nov 20 2014 - 17:07:55)

Board:  Xilinx Zynq
I2C:   ready
DRAM:  ECC disabled 1 GiB
MMC:   zynq_sdhci: 0
SF: Detected S25FL128S_64K with page size 512 Bytes, erase size 128 KiB, total 32 MiB
*** Warning - bad CRC, using default environment

In:    serial
Out:   serial
Err:   serial
Net:   Gem.e000b000
Hit any key to stop autoboot:  0 
Device: zynq_sdhci
Manufacturer ID: 3
OEM: 5344
Name: SC16G 
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 14.8 GiB
Bus Width: 4-bit
reading uEnv.txt
442 bytes read in 11 ms (39.1 KiB/s)
Loaded environment from uEnv.txt
Importing environment from SD ...
Running uenvcmd ...
Copying Linux from SD to RAM...
reading uImage
6579160 bytes read in 564 ms (11.1 MiB/s)
reading devicetree.dtb
18517 bytes read in 16 ms (1.1 MiB/s)
reading uramdisk.image.gz
** Unable to read file uramdisk.image.gz **
## Booting kernel from Legacy Image at 03000000 ...
   Image Name:   Linux-5.4.0-00578-gfa9a9de0f7f8
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    6579096 Bytes = 6.3 MiB
   Load Address: 00008000
   Entry Point:  00008000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 02a00000
   Booting using the fdt blob at 0x2a00000
   Loading Kernel Image ... OK
   Loading Device Tree to 1fff8000, end 1ffff854 ... OK

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 5.4.0-00578-gfa9a9de0f7f8 (pavithra@Lekha-LP-132) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 1
CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
OF: fdt: Machine model: Xilinx Zynq ZC706
printk: bootconsole [earlycon0] enabled
Memory policy: Data cache writealloc
cma: Reserved 128 MiB at 0x38000000
percpu: Embedded 15 pages/cpu s29516 r8192 d23732 u61440
Built 1 zonelists, mobility grouping on.  Total pages: 260608
Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait uio_pdrv_genirq.of_id="generic-uio"
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear)
mem auto-init: stack:off, heap alloc:off, heap free:off
Memory: 888448K/1048576K available (9216K kernel code, 753K rwdata, 7096K rodata, 1024K init, 169K bss, 29056K reserved, 131072K cma-reserved)
rcu: Preemptible hierarchical RCU implementation.
rcu:    RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
        Tasks RCU enabled.
rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.
rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
efuse mapped to (ptrval)
slcr mapped to (ptrval)
L2C: platform modifies aux control register: 0x72360000 -> 0x72760000
L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000
L2C-310 erratum 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 1 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 8 ways, 512 kB
L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001
random: get_random_bytes called from start_kernel+0x2c8/0x450 with crng_init=0
zynq_clock_init: clkc starts at (ptrval)
Zynq clock init
sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns
clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns
Switching to timer-based delay loop, resolution 3ns
clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns
timer #0 at (ptrval), irq=17
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 666.66 BogoMIPS (lpj=3333333)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
CPU: Testing write buffer coherency: ok
CPU0: Spectre v2: using BPIALL workaround
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x100000 - 0x100060
rcu: Hierarchical SRCU implementation.
smp: Bringing up secondary CPUs ...
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU1: Spectre v2: using BPIALL workaround
smp: Brought up 1 node, 2 CPUs
SMP: Total of 2 processors activated (1333.33 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
futex hash table entries: 512 (order: 3, 32768 bytes, linear)
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0x(ptrval)
e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 25, base_baud = 3125000) is a xuartps
printk: console [ttyPS0] enabled
printk: console [ttyPS0] enabled
printk: bootconsole [earlycon0] disabled
printk: bootconsole [earlycon0] disabled
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
mc: Linux media interface: v0.10
videodev: Linux video capture interface: v2.00
jesd204: found 0 devices and 0 topologies
FPGA manager framework
Advanced Linux Sound Architecture Driver Initialized.
clocksource: Switched to clocksource arm_global_timer
thermal_sys: Registered thermal governor 'step_wise'
NET: Registered protocol family 2
tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear)
TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes, linear)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
NET: Registered protocol family 1
hw perfevents: no interrupt-affinity property for /pmu@f8891000, guessing.
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
workingset: timestamp_bits=30 max_order=18 bucket_order=0
bounce: pool size: 64 pages
io scheduler mq-deadline registered
io scheduler kyber registered
zynq-pinctrl 700.pinctrl: zynq pinctrl initialized
dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330
dma-pl330 f8003000.dmac:        DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16
brd: module loaded
loop: module loaded
Registered mathworks_ip class
spi-nor spi1.0: found s25fl128s1, expected n25q128a11
random: fast init done
spi-nor spi1.0: s25fl128s1 (32768 Kbytes)
5 fixed-partitions partitions found on MTD device spi1.0
Creating 5 MTD partitions on "spi1.0":
0x000000000000-0x000000500000 : "boot"
0x000000500000-0x000000520000 : "bootenv"
0x000000520000-0x000000540000 : "config"
0x000000540000-0x000000fc0000 : "image"
0x000000fc0000-0x000002000000 : "spare"
MACsec IEEE 802.1AE
libphy: Fixed MDIO Bus: probed
tun: Universal TUN/TAP device driver, 1.6
libphy: MACB_mii_bus: probed
Marvell 88E1116R e000b000.ethernet-ffffffff:07: attached PHY driver [Marvell 88E1116R] (mii_bus:phy_addr=e000b000.ethernet-ffffffff:07, irq=P)
macb e000b000.ethernet eth0: Cadence GEM rev 0x00020118 at 0xe000b000 irq 28 (00:0a:35:00:01:22)
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
usbcore: registered new interface driver uas
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usbserial_generic
usbserial: USB Serial support registered for generic
usbcore: registered new interface driver ftdi_sio
usbserial: USB Serial support registered for FTDI USB Serial Device
usbcore: registered new interface driver upd78f0730
usbserial: USB Serial support registered for upd78f0730
chipidea-usb2 e0002000.usb: e0002000.usb supply vbus not found, using dummy regulator
ULPI transceiver vendor/product ID 0x0424/0x0007
Found SMSC USB3320 ULPI transceiver.
ULPI integrity check: passed.
ci_hdrc ci_hdrc.0: EHCI Host Controller
ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.04
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: EHCI Host Controller
usb usb1: Manufacturer: Linux 5.4.0-00578-gfa9a9de0f7f8 ehci_hcd
usb usb1: SerialNumber: ci_hdrc.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
i2c /dev entries driver
xiic-i2c 41620000.i2c: IRQ index 0 not found
si570: probe of 1-005d failed with error -5
i2c i2c-0: Added multiplexed i2c bus 1
adv7511 2-0039: 2-0039 supply avdd not found, using dummy regulator
adv7511 2-0039: 2-0039 supply dvdd not found, using dummy regulator
adv7511 2-0039: 2-0039 supply pvdd not found, using dummy regulator
adv7511 2-0039: 2-0039 supply bgvdd not found, using dummy regulator
adv7511 2-0039: 2-0039 supply dvdd-3v not found, using dummy regulator
i2c i2c-0: Added multiplexed i2c bus 2
at24 3-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write
i2c i2c-0: Added multiplexed i2c bus 3
pca953x 4-0021: 4-0021 supply vcc not found, using dummy regulator
i2c i2c-0: Added multiplexed i2c bus 4
rtc-pcf8563 5-0051: registered as rtc0
i2c i2c-0: Added multiplexed i2c bus 5
i2c i2c-0: Added multiplexed i2c bus 6
i2c i2c-0: Added multiplexed i2c bus 7
i2c i2c-0: Added multiplexed i2c bus 8
pca954x 0-0074: registered 8 multiplexed busses for I2C switch pca9548
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)
gspca_main: v2.14.0 registered
cdns-wdt f8005000.watchdog: Xilinx Watchdog Timer with timeout 10s
Xilinx Zynq CpuIdle Driver started
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: SDHCI controller on e0100000.mmc [e0100000.mmc] using ADMA
ledtrig-cpu: registered to indicate activity on CPUs
hidraw: raw HID events driver (C) Jiri Kosina
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
adrv9002 spi0.0: Invalid gpio number: 0
adrv9002: probe of spi0.0 failed with error -22
axi_sysid 45000000.axi-sysid-0: AXI System ID core version (1.01.a) found
axi_sysid 45000000.axi-sysid-0: [adrv9001] [CMOS_LVDS_N=1] on [zc706] git branch <master> git <b4c50312725732c50695afb9dff2419c0359ea3c> cleaC
fpga_manager fpga0: Xilinx Zynq FPGA Manager registered
usbcore: registered new interface driver snd-usb-audio
mmc0: new high speed SDHC card at address aaaa
NET: Registered protocol family 10
mmcblk0: mmc0:aaaa SC16G 14.8 GiB 
Segment Routing with IPv6
sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 36
Registering SWP/SWPB emulation handler
[drm] Cannot find any crtc or sizes
 mmcblk0: p1 p2
[drm] Initialized axi_hdmi_drm 1.0.0 20120930 for 70e00000.axi_hdmi on minor 0
asoc-simple-card adv7511_hdmi_snd: spdif-hifi <-> 75c00000.axi-spdif-tx mapping ok
input: gpio_keys as /devices/soc0/gpio_keys/input/input0
rtc-pcf8563 5-0051: setting system clock to 2021-09-28T11:15:28 UTC (1632827728)
ALSA device list:
  #0: HDMI monitor
EXT4-fs (mmcblk0p2): recovery complete
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 1024K
Run /sbin/init as init process
random: systemd: uninitialized urandom read (16 bytes read)

Welcome to Ubuntu 15.04!

random: systemd: uninitialized urandom read (16 bytes read)
random: systemd-cryptse: uninitialized urandom read (16 bytes read)
Cannot add dependency job for unit org.freedesktop.resolve1.busname, ignoring: Unit org.freedesktop.resolve1.busname failed to load: No such .
Cannot add dependency job for unit display-manager.service, ignoring: Unit display-manager.service failed to load: No such file or directory.
[  OK  ] Reached target Encrypted Volumes.
[  OK  ] Created slice Root Slice.
[  OK  ] Listening on Delayed Shutdown Socket.
[  OK  ] Created slice System Slice.
         Starting Increase datagram queue length...
[  OK  ] Created slice system-getty.slice.
[  OK  ] Listening on Journal Socket.
         Mounting Temporary Directory...
         Starting Nameserver information manager...
[  OK  ] Started Read required files in advance.
         Starting Read required files in advance...
[  OK  ] Started Boot Process Profiler.
         Starting Boot Process Profiler...
         Starting Load Kernel Modules...
[  OK  ] Listening on networkd rtnetlink socket.
[  OK  ] Listening on udev Control Socket.
[  OK  ] Listening on udev Kernel Socket.
         Starting udev Coldplug all Devices...
[  OK  ] Reached target Swap.
         Mounting Debug File System...
[  OK  ] Listening on Journal Socket (/dev/log).
[  OK  ] Listening on /dev/initctl Compatibility Named[drm] Cannot find any crtc or sizes
 Pipe.
         Starting Remount Root and Kernel File Systems...
[  OK  ] Reached target Remote File Systems (Pre).
[[drm] Cannot find any crtc or sizes
  OK  ] Created slice User and Session Slice.
[  OK  ] Reached target Slices.
[  OK  ] Created slice system-serial\x2dgetty.slice.
         Starting Create Static Device Nodes in /dev...
[  OK  ] Reached target Paths.
systemd-bootchart.service failed.
[  OK  ] Started Load Kernel Modules.
[  OK  ] Started Increase datagram queue length.
[  OK  ] Mounted Temporary Directory.
ureadahead.service failed.
[  OK  ] Mounted Debug File System.
[  OK  ] Started Remount Root and Kernel File Systems.
[  OK  ] Started Create Static Device Nodes in /dev.
[  OK  ] Started Nameserver information manager.
[  OK  ] Started udev Coldplug all Devices.
         Starting udev Kernel Device Manager...
         Starting Load/Save Random Seed...
[  OK  ] Reached target Local File Systems (Pre).
[  OK  ] Reached target Local File Systems.
[  OK  ] Reached target Remote File Systems.
         Starting Wait for all "auto" /etc/n... up for network-online.target...
[  OK  ] Listening on Syslog Socket.
         Starting Journal Service...
         Starting Apply Kernel Variables...
         Mounting Configuration File System...
[  OK  ] Started Load/Save Random Seed.
[  OK  ] Mounted Configuration File System.
         Starting LSB: Raise network interfaces....
[  OK  ] Started Wait for all "auto" /etc/ne...be up for network-online.target.
[  OK  ] Started Apply Kernel Variables.
[  OK  ] Started udev Kernel Device Manager.
         Starting Copy rules generated while the root was ro...
[  OK  ] Started Copy rules generated while the root was ro.
[  OK  ] Started Journal Service.
         Starting Flush Journal to Persistent Storage...
[  OK  ] Started Flush Journal to Persistent Storage.
         Starting Create Volatile Files and Directories...
[  OK  ] Started Create Volatile Files and Directories.
         Starting Update UTMP about System Boot/Shutdown...
         Starting Network Time Synchronization...
[  OK  ] Started Network Time Synchronization.
[  OK  ] Reached target System Time Synchronized.
[  OK  ] Started Update UTMP about System Boot/Shutdown.
[  OK  ] Found device /dev/ttyPS0.
[  OK  ] Reached target Sound Card.
[  OK  ] Created slice system-ifup.slice.
[  OK  ] Started ifup for eth0.
         Starting ifup for eth0...
[  OK  ] Started LSB: Raise network interfaces..
[  OK  ] Started ifup for sit0.
         Starting ifup for sit0...
[  OK  ] Reached target System Initialization.
[  OK  ] Listening on OpenBSD Secure Shell server socket.
[  OK  ] Reached target Timers.
[  OK  ] Listening on D-Bus System Message Bus Socket.
[  OK  ] Reached target Sockets.
[  OK  ] Reached target Basic System.
[  OK  ] Started Regular background program processing daemon.
         Starting Regular background program processing daemon...
         Starting Provide limited super user privileges to specific users...
         Starting LSB: Xen daemons...
         Starting Initialize hardware monitoring sensors...
         Starting WPA supplicant...
         Starting Network Manager...
         Starting Permit User Sessions...
         Starting System Logging Service...
         Starting Login Service...
         Starting LSB: Platform initscript...
         Starting LSB: Set the CPU Frequency Scaling governor to "ondemand"...
[  OK  ] Reached target Containers.
Running Platform Init
         Starting D-Bus System Message Bus...
         Starting LSB: Load kernel modules needed to enable cpufreq scaling...
[  OK  ] Started System Logging Service.
[  OK  ] Started Provide limited super user privileges to specific users.
[  OK  ] Started LSB: Xen daemons.
[  OK  ] Started Permit User Sessions.
[  OK  ] Started LSB: Set the CPU Frequency Scaling governor to "ondemand".
[  OK  ] Started D-Bus System Message Bus.
[  OK  ] Started WPA supplicant.
[  OK  ] Started LSB: Load kernel modules needed to enable cpufreq scaling.
[  OK  ] Started Initialize hardware monitoring sensors.
[  OK  ] Started Login Service.
         Starting Authenticate and Authorize Users to Run Privileged Tasks...
         Starting LSB: set CPUFreq kernel parameters...
         Starting Network Service...
         Starting LSB: Start/stop secondary xen domains...
[  OK  ] Started LSB: set CPUFreq kernel parameters.
[  OK  ] Started Network Service.
[  OK  ] Started Authenticate and Authorize Users to Run Privileged Tasks.
         Starting Network Name Resolution...
[  OK  ] Started LSB: Start/stop secondary xen domains.
[  OK  ] Started LSB: Platform initscript.
[  OK  ] Started Network Name Resolution.
[  OK  ] Started Network Manager.
         Starting Network Manager Wait Online...
[  OK  ] Reached target Network.
         Starting /etc/rc.local Compatibility...
[  OK  ] Started Network Manager Wait Online.
[  OK  ] Stopped OpenBSD Secure Shell server.
[  OK  ] Started OpenBSD Secure Shell server.
         Starting OpenBSD Secure Shell server...
[  OK  ] Reached target Network is Online.
         Starting LSB: start Samba daemons for the AD DC...
         Starting LSB: start Samba NetBIOS nameserver (nmbd)...
[  OK  ] Stopped LSB: start Samba SMB/CIFS daemon (smbd).
         Starting LSB: start Samba SMB/CIFS daemon (smbd)...
[  OK  ] Closed OpenBSD Secure Shell server socket.
[  OK  ] Stopped OpenBSD Secure Shell server.
[  OK  ] Started OpenBSD Secure Shell server.
         Starting OpenBSD Secure Shell server...
[  OK  ] Started LSB: start Samba daemons for the AD DC.
[  OK  ] Started LSB: start Samba SMB/CIFS daemon (smbd).
[  OK  ] Started LSB: start Samba NetBIOS nameserver (nmbd).
[  OK  ] Started /etc/rc.local Compatibility.
[  OK  ] Started Serial Getty on ttyPS0.
         Starting Serial Getty on ttyPS0...
[  OK  ] Started Getty on tty1.
         Starting Getty on tty1...
[  OK  ] Reached target Login Prompts.
[  OK  ] Reached target Multi-User System.
[  OK  ] Reached target Graphical Interface.
         Starting Update UTMP about System Runlevel Changes...
[  OK  ] Started Update UTMP about System Runlevel Changes.

Ubuntu 15.04 linaro-developer ttyPS0

linaro-developer login: root (automatic login)

Last login: Tue Sep 28 09:58:23 UTC 2021 on ttyPS0
root@linaro-developer:~# 
root@linaro-developer:~# 
root@linaro-developer:~# demsg | grep spi
-bash: demsg: command not found
root@linaro-developer:~# dmesg | grep spi                                                                                                     
[    0.599999] spi-nor spi1.0: found s25fl128s1, expected n25q128a11
[    0.724295] spi-nor spi1.0: s25fl128s1 (32768 Kbytes)
[    0.728070] 5 fixed-partitions partitions found on MTD device spi1.0
[    0.733110] Creating 5 MTD partitions on "spi1.0":
[    1.965192] adrv9002 spi0.0: Invalid gpio number: 0
[    1.968795] adrv9002: probe of spi0.0 failed with error -22

  • Hello Pavithrasyadav,

    I've moved this question to the Linux SW Drivers forum as this place supports setups taking the approach you are. I hope you can find the help you need here!

    Best Regards,
    Oisín.

  • Which FMC slot is the board plugged into?

    Does the system boot without error with the start SD card provided by ADI? https://wiki.analog.com/resources/tools-software/linux-software/adi-kuiper_images

    -Travis

  • Closed due to inactivity - please reopen if required.

  • Hi Travis,

    Sorry for the delayed response.

    Attached the hardware set up and our device details when connected to TES-GUI-0.15

    We have created SD card with AD's Kuiper Images provided here:

     https://swdownloads.analog.com/cse/kuiper/image_2021-07-28-ADI-Kuiper-full.zip

    But there is boot directory specified for zc706_adrv9002 combination.

    We have got ZC706+ADRV9002 prebuilt BOOT.BIN and devicetree.dtb from this link:

    https://swdownloads.analog.com/cse/prebuilt/zynq-zc706-adv7511-adrv9002-master-2021_05_13-08_13_21.zip

    But there is no uImage provided here.

    Using the uImage provided as part of AD's Kuiper Images's zynq-common directory and BOOT.BIN and devicetree.dtb provided by the above link,  we are able to boot the set up , but SPI probe of ADRV-9002 failed with the following error:

    [    8.922457] adrv9002 spi0.0: [ERROR]: Error number  3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/.
    [    8.948441] adrv9002 spi0.0: adrv9002_digital_init, 2238: failed with "Timed out waiting for ARM bootup to happen" (3)
    [   15.600890] adrv9002 spi0.0: [ERROR]: Error number  3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/.
    [   15.626877] adrv9002 spi0.0: adrv9002_digital_init, 2238: failed with "Timed out waiting for ARM bootup to happen" (3)

    Attached the respective bootlog as well.

    Kindly provide us the working boot images to successfully boot and probe ADRV-9002

    U-Boot 2014.07-dirty (Nov 20 2014 - 17:07:55)
    
    Board:  Xilinx Zynq
    I2C:   ready
    DRAM:  ECC disabled 1 GiB
    MMC:   zynq_sdhci: 0
    SF: Detected S25FL128S_64K with page size 512 Bytes, erase size 128 KiB, total 32 MiB
    *** Warning - bad CRC, using default environment
    
    In:    serial
    Out:   serial
    Err:   serial
    Net:   Gem.e000b000
    Hit any key to stop autoboot:  0 
    Device: zynq_sdhci
    Manufacturer ID: 3
    OEM: 5344
    Name: SC16G 
    Tran Speed: 50000000
    Rd Block Len: 512
    SD version 3.0
    High Capacity: Yes
    Capacity: 14.8 GiB
    Bus Width: 4-bit
    reading uEnv.txt
    407 bytes read in 26 ms (14.6 KiB/s)
    Loaded environment from uEnv.txt
    Importing environment from SD ...
    Running uenvcmd ...
    Copying Linux from SD to RAM...
    reading uImage
    6316720 bytes read in 561 ms (10.7 MiB/s)
    reading devicetree.dtb
    18517 bytes read in 35 ms (516.6 KiB/s)
    reading uramdisk.image.gz
    ** Unable to read file uramdisk.image.gz **
    ## Booting kernel from Legacy Image at 03000000 ...
       Image Name:   Linux-4.19.0-g17f4223
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    6316656 Bytes = 6 MiB
       Load Address: 00008000
       Entry Point:  00008000
       Verifying Checksum ... OK
    ## Flattened Device Tree blob at 02a00000
       Booting using the fdt blob at 0x2a00000
       Loading Kernel Image ... OK
       Loading Device Tree to 1fff8000, end 1ffff854 ... OK
    
    Starting kernel ...
    
    Booting Linux on physical CPU 0x0
    Linux version 4.19.0-g17f4223 (jenkins@romlxbuild1.adlk.analog.com) (gcc version 8.2.0 (GCC)) #1848 SMP PREEMPT Tue Jul 27 12:46:50 IST 2021
    CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
    CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    OF: fdt: Machine model: Xilinx Zynq ZC706
    OF: fdt: earlycon: stdout-path /amba@0/uart@E0001000 not found
    Memory policy: Data cache writealloc
    cma: Reserved 128 MiB at 0x38000000
    random: get_random_bytes called from start_kernel+0xa0/0x404 with crng_init=0
    percpu: Embedded 16 pages/cpu @(ptrval) s33548 r8192 d23796 u65536
    Built 1 zonelists, mobility grouping on.  Total pages: 260608
    Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait clk_ignore_unused cpuidle.off=1
    Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
    Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
    Memory: 889460K/1048576K available (9216K kernel code, 759K rwdata, 6760K rodata, 1024K init, 167K bss, 28044K reserved, 131072K cma-reserved,
     131072K highmem)
    Virtual kernel memory layout:
        vector  : 0xffff0000 - 0xffff1000   (   4 kB)
        fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
        vmalloc : 0xf0800000 - 0xff800000   ( 240 MB)
        lowmem  : 0xc0000000 - 0xf0000000   ( 768 MB)
        pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
        modules : 0xbf000000 - 0xbfe00000   (  14 MB)
          .text : 0x(ptrval) - 0x(ptrval)   (10208 kB)
          .init : 0x(ptrval) - 0x(ptrval)   (1024 kB)
          .data : 0x(ptrval) - 0x(ptrval)   ( 760 kB)
           .bss : 0x(ptrval) - 0x(ptrval)   ( 168 kB)
    rcu: Preemptible hierarchical RCU implementation.
    rcu:    RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
            Tasks RCU enabled.
    rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
    NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
    efuse mapped to (ptrval)
    slcr mapped to (ptrval)
    L2C: platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C-310 erratum 769419 enabled
    L2C-310 enabling early BRESP for Cortex-A9
    L2C-310 full line of zeros enabled for Cortex-A9
    L2C-310 ID prefetch enabled, offset 1 lines
    L2C-310 dynamic clock gating enabled, standby mode enabled
    L2C-310 cache controller enabled, 8 ways, 512 kB
    L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001
    zynq_clock_init: clkc starts at (ptrval)
    Zynq clock init
    sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns
    clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns
    Switching to timer-based delay loop, resolution 3ns
    clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns
    timer #0 at (ptrval), irq=17
    Console: colour dummy device 80x30
    Calibrating delay loop (skipped), value calculated using timer frequency.. 666.66 BogoMIPS (lpj=3333333)
    pid_max: default: 32768 minimum: 301
    Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
    Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
    CPU: Testing write buffer coherency: ok
    CPU0: Spectre v2: using BPIALL workaround
    CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    Setting up static identity map for 0x100000 - 0x100060
    rcu: Hierarchical SRCU implementation.
    smp: Bringing up secondary CPUs ...
    CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
    CPU1: Spectre v2: using BPIALL workaround
    smp: Brought up 1 node, 2 CPUs
    SMP: Total of 2 processors activated (1333.33 BogoMIPS).
    CPU: All CPU(s) started in SVC mode.
    devtmpfs: initialized
    VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
    clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    futex hash table entries: 512 (order: 3, 32768 bytes)
    pinctrl core: initialized pinctrl subsystem
    NET: Registered protocol family 16
    DMA: preallocated 256 KiB pool for atomic coherent allocations
    hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
    hw-breakpoint: maximum watchpoint size is 4 bytes.
    zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0x(ptrval)
    zynq-pinctrl 700.pinctrl: zynq pinctrl initialized
    e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 25, base_baud = 3125000) is a xuartps
    console [ttyPS0] enabled
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    media: Linux media interface: v0.10
    videodev: Linux video capture interface: v2.00
    jesd204: found 0 devices and 0 topologies
    FPGA manager framework
    Advanced Linux Sound Architecture Driver Initialized.
    clocksource: Switched to clocksource arm_global_timer
    NET: Registered protocol family 2
    tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes)
    TCP established hash table entries: 8192 (order: 3, 32768 bytes)
    TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
    TCP: Hash tables configured (established 8192 bind 8192)
    UDP hash table entries: 512 (order: 2, 16384 bytes)
    UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
    NET: Registered protocol family 1
    hw perfevents: no interrupt-affinity property for /pmu@f8891000, guessing.
    hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
    workingset: timestamp_bits=30 max_order=18 bucket_order=0
    bounce: pool size: 64 pages
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    io scheduler mq-deadline registered
    io scheduler kyber registered
    dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330
    dma-pl330 f8003000.dmac:        DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16
    brd: module loaded
    loop: module loaded
    Registered mathworks_ip class
    m25p80 spi1.0: found s25fl128s, expected n25q128a11
    m25p80 spi1.0: Programming Error occurred
    m25p80 spi1.0: timeout while writing configuration register
    m25p80 spi1.0: quad mode not supported
    m25p80: probe of spi1.0 failed with error -5
    MACsec IEEE 802.1AE
    libphy: Fixed MDIO Bus: probed
    tun: Universal TUN/TAP device driver, 1.6
    libphy: MACB_mii_bus: probed
    Marvell 88E1116R e000b000.ethernet-ffffffff:07: attached PHY driver [Marvell 88E1116R] (mii_bus:phy_addr=e000b000.ethernet-ffffffff:07, irq=PO
    LL)
    macb e000b000.ethernet eth0: Cadence GEM rev 0x00020118 at 0xe000b000 irq 28 (00:0a:35:00:01:22)
    usbcore: registered new interface driver asix
    usbcore: registered new interface driver ax88179_178a
    usbcore: registered new interface driver cdc_ether
    usbcore: registered new interface driver net1080
    usbcore: registered new interface driver cdc_subset
    usbcore: registered new interface driver zaurus
    usbcore: registered new interface driver cdc_ncm
    ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    usbcore: registered new interface driver uas
    usbcore: registered new interface driver usb-storage
    usbcore: registered new interface driver usbserial_generic
    usbserial: USB Serial support registered for generic
    usbcore: registered new interface driver ftdi_sio
    usbserial: USB Serial support registered for FTDI USB Serial Device
    usbcore: registered new interface driver upd78f0730
    usbserial: USB Serial support registered for upd78f0730
    chipidea-usb2 e0002000.usb: e0002000.usb supply vbus not found, using dummy regulator
    chipidea-usb2 e0002000.usb: Linked as a consumer to regulator.0
    ULPI transceiver vendor/product ID 0x0424/0x0007
    Found SMSC USB3320 ULPI transceiver.
    ULPI integrity check: passed.
    ci_hdrc ci_hdrc.0: EHCI Host Controller
    ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
    ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
    usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
    usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    usb usb1: Product: EHCI Host Controller
    usb usb1: Manufacturer: Linux 4.19.0-g17f4223 ehci_hcd
    usb usb1: SerialNumber: ci_hdrc.0
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 1 port detected
    i2c /dev entries driver
    si570: probe of 1-005d failed with error -5
    i2c i2c-0: Added multiplexed i2c bus 1
    adv7511 2-0039: 2-0039 supply avdd not found, using dummy regulator
    adv7511 2-0039: Linked as a consumer to regulator.0
    adv7511 2-0039: 2-0039 supply dvdd not found, using dummy regulator
    adv7511 2-0039: 2-0039 supply pvdd not found, using dummy regulator
    adv7511 2-0039: 2-0039 supply bgvdd not found, using dummy regulator
    adv7511 2-0039: 2-0039 supply dvdd-3v not found, using dummy regulator
    i2c i2c-0: Added multiplexed i2c bus 2
    at24 3-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write
    i2c i2c-0: Added multiplexed i2c bus 3
    pca953x 4-0021: 4-0021 supply vcc not found, using dummy regulator
    pca953x 4-0021: Linked as a consumer to regulator.0
    i2c i2c-0: Added multiplexed i2c bus 4
    rtc-pcf8563 5-0051: rtc core: registered rtc-pcf8563 as rtc0
    i2c i2c-0: Added multiplexed i2c bus 5
    i2c i2c-0: Added multiplexed i2c bus 6
    i2c i2c-0: Added multiplexed i2c bus 7
    i2c i2c-0: Added multiplexed i2c bus 8
    pca954x 0-0074: registered 8 multiplexed busses for I2C switch pca9548
    usbcore: registered new interface driver uvcvideo
    USB Video Class driver (1.1.1)
    gspca_main: v2.14.0 registered
    cdns-wdt f8005000.watchdog: Xilinx Watchdog Timer with timeout 10s
    Xilinx Zynq CpuIdle Driver started
    failed to register cpuidle driver
    sdhci: Secure Digital Host Controller Interface driver
    sdhci: Copyright(c) Pierre Ossman
    sdhci-pltfm: SDHCI platform and OF driver helper
    mmc0: SDHCI controller on e0100000.mmc [e0100000.mmc] using ADMA
    ledtrig-cpu: registered to indicate activity on CPUs
    hidraw: raw HID events driver (C) Jiri Kosina
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    axi_sysid 45000000.axi-sysid-0: system ID header version mismatch. Expected 1, Reported 2
    fpga_manager fpga0: Xilinx Zynq FPGA Manager registered
    usbcore: registered new interface driver snd-usb-audio
    mmc0: new high speed SDHC card at address aaaa
    NET: Registered protocol family 10
    mmcblk0: mmc0:aaaa SC16G 14.8 GiB 
    Segment Routing with IPv6
    sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    NET: Registered protocol family 17
    NET: Registered protocol family 36
     mmcblk0: p1 p2 p3
    Registering SWP/SWPB emulation handler
    [drm] Cannot find any crtc or sizes
    [drm] Initialized axi_hdmi_drm 1.0.0 20120930 for 70e00000.axi_hdmi on minor 0
    random: fast init done
    [drm] Cannot find any crtc or sizes
    random: crng init done
    adrv9002 spi0.0: [ERROR]: Error number  3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_a
    drv9001_arm.c, in function adi_adrv9001_arm_StartStatus_Check, in line  189, variable name device.Error message Timed out waiting for ARM boot
    up to happen.
    adrv9002 spi0.0: adrv9002_digital_init, 2238: failed with "Timed out waiting for ARM bootup to happen" (3)
    adrv9002 spi0.0: [ERROR]: Error number  3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_a
    drv9001_arm.c, in function adi_adrv9001_arm_StartStatus_Check, in line  189, variable name device.Error message Timed out waiting for ARM boot
    up to happen.
    adrv9002 spi0.0: adrv9002_digital_init, 2238: failed with "Timed out waiting for ARM bootup to happen" (3)
    cf_axi_adc: probe of 44a00000.axi-adrv9002-rx-lpc failed with error -14
    cf_axi_tdd 44a0c800.axi-adrv9002-core-tdd-lpc: Analog Devices CF_AXI_TDD MASTER (1.00.a)
    Division by zero in kernel.
    CPU: 0 PID: 99 Comm: kworker/0:1 Not tainted 4.19.0-g17f4223 #1848
    Hardware name: Xilinx Zynq Platform
    Workqueue: events deferred_probe_work_func
    [<c010fa50>] (unwind_backtrace) from [<c010bd5c>] (show_stack+0x10/0x14)
    [<c010bd5c>] (show_stack) from [<c08fbfac>] (dump_stack+0x8c/0xa0)
    [<c08fbfac>] (dump_stack) from [<c08f9854>] (Ldiv0_64+0x8/0x18)
    [<c08f9854>] (Ldiv0_64) from [<c03219ec>] (div64_u64+0xcc/0xf0)
    [<c03219ec>] (div64_u64) from [<c074c040>] (cf_axi_dds_default_setup+0x38/0xe0)
    [<c074c040>] (cf_axi_dds_default_setup) from [<c074d764>] (cf_axi_dds_probe+0x8e0/0xb28)
    [<c074d764>] (cf_axi_dds_probe) from [<c03eb4ac>] (platform_drv_probe+0x48/0x98)
    [<c03eb4ac>] (platform_drv_probe) from [<c03e983c>] (really_probe+0x1f4/0x2b8)
    [<c03e983c>] (really_probe) from [<c03e9a64>] (driver_probe_device+0x60/0x164)
    [<c03e9a64>] (driver_probe_device) from [<c03e7c4c>] (bus_for_each_drv+0x80/0xc4)
    [<c03e7c4c>] (bus_for_each_drv) from [<c03e95d8>] (__device_attach+0xd0/0x138)
    [<c03e95d8>] (__device_attach) from [<c03e8a48>] (bus_probe_device+0x84/0x8c)
    [<c03e8a48>] (bus_probe_device) from [<c03e8ee0>] (deferred_probe_work_func+0x60/0x8c)
    [<c03e8ee0>] (deferred_probe_work_func) from [<c0135a30>] (process_one_work+0x1f0/0x3fc)
    [<c0135a30>] (process_one_work) from [<c01369a4>] (worker_thread+0x294/0x584)
    [<c01369a4>] (worker_thread) from [<c013b680>] (kthread+0x148/0x150)
    [<c013b680>] (kthread) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
    Exception stack(0xef25bfb0 to 0xef25bff8)
    bfa0:                                     00000000 00000000 00000000 00000000
    bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
    Division by zero in kernel.
    CPU: 0 PID: 99 Comm: kworker/0:1 Not tainted 4.19.0-g17f4223 #1848
    Hardware name: Xilinx Zynq Platform
    Workqueue: events deferred_probe_work_func
    [<c010fa50>] (unwind_backtrace) from [<c010bd5c>] (show_stack+0x10/0x14)
    [<c010bd5c>] (show_stack) from [<c08fbfac>] (dump_stack+0x8c/0xa0)
    [<c08fbfac>] (dump_stack) from [<c08f9854>] (Ldiv0_64+0x8/0x18)
    [<c08f9854>] (Ldiv0_64) from [<c03219ec>] (div64_u64+0xcc/0xf0)
    [<c03219ec>] (div64_u64) from [<c074c040>] (cf_axi_dds_default_setup+0x38/0xe0)
    [<c074c040>] (cf_axi_dds_default_setup) from [<c074d784>] (cf_axi_dds_probe+0x900/0xb28)
    [<c074d784>] (cf_axi_dds_probe) from [<c03eb4ac>] (platform_drv_probe+0x48/0x98)
    [<c03eb4ac>] (platform_drv_probe) from [<c03e983c>] (really_probe+0x1f4/0x2b8)
    [<c03e983c>] (really_probe) from [<c03e9a64>] (driver_probe_device+0x60/0x164)
    [<c03e9a64>] (driver_probe_device) from [<c03e7c4c>] (bus_for_each_drv+0x80/0xc4)
    [<c03e7c4c>] (bus_for_each_drv) from [<c03e95d8>] (__device_attach+0xd0/0x138)
    [<c03e95d8>] (__device_attach) from [<c03e8a48>] (bus_probe_device+0x84/0x8c)
    [<c03e8a48>] (bus_probe_device) from [<c03e8ee0>] (deferred_probe_work_func+0x60/0x8c)
    [<c03e8ee0>] (deferred_probe_work_func) from [<c0135a30>] (process_one_work+0x1f0/0x3fc)
    [<c0135a30>] (process_one_work) from [<c01369a4>] (worker_thread+0x294/0x584)
    [<c01369a4>] (worker_thread) from [<c013b680>] (kthread+0x148/0x150)
    [<c013b680>] (kthread) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
    Exception stack(0xef25bfb0 to 0xef25bff8)
    bfa0:                                     00000000 00000000 00000000 00000000
    bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
    Division by zero in kernel.
    CPU: 0 PID: 99 Comm: kworker/0:1 Not tainted 4.19.0-g17f4223 #1848
    Hardware name: Xilinx Zynq Platform
    Workqueue: events deferred_probe_work_func
    [<c010fa50>] (unwind_backtrace) from [<c010bd5c>] (show_stack+0x10/0x14)
    [<c010bd5c>] (show_stack) from [<c08fbfac>] (dump_stack+0x8c/0xa0)
    [<c08fbfac>] (dump_stack) from [<c08f9854>] (Ldiv0_64+0x8/0x18)
    [<c08f9854>] (Ldiv0_64) from [<c03219ec>] (div64_u64+0xcc/0xf0)
    [<c03219ec>] (div64_u64) from [<c074c040>] (cf_axi_dds_default_setup+0x38/0xe0)
    [<c074c040>] (cf_axi_dds_default_setup) from [<c074d764>] (cf_axi_dds_probe+0x8e0/0xb28)
    [<c074d764>] (cf_axi_dds_probe) from [<c03eb4ac>] (platform_drv_probe+0x48/0x98)
    [<c03eb4ac>] (platform_drv_probe) from [<c03e983c>] (really_probe+0x1f4/0x2b8)
    [<c03e983c>] (really_probe) from [<c03e9a64>] (driver_probe_device+0x60/0x164)
    [<c03e9a64>] (driver_probe_device) from [<c03e7c4c>] (bus_for_each_drv+0x80/0xc4)
    [<c03e7c4c>] (bus_for_each_drv) from [<c03e95d8>] (__device_attach+0xd0/0x138)
    [<c03e95d8>] (__device_attach) from [<c03e8a48>] (bus_probe_device+0x84/0x8c)
    [<c03e8a48>] (bus_probe_device) from [<c03e8ee0>] (deferred_probe_work_func+0x60/0x8c)
    [<c03e8ee0>] (deferred_probe_work_func) from [<c0135a30>] (process_one_work+0x1f0/0x3fc)
    [<c0135a30>] (process_one_work) from [<c01369a4>] (worker_thread+0x294/0x584)
    [<c01369a4>] (worker_thread) from [<c013b680>] (kthread+0x148/0x150)
    [<c013b680>] (kthread) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
    Exception stack(0xef25bfb0 to 0xef25bff8)
    bfa0:                                     00000000 00000000 00000000 00000000
    bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
    Division by zero in kernel.
    CPU: 0 PID: 99 Comm: kworker/0:1 Not tainted 4.19.0-g17f4223 #1848
    Hardware name: Xilinx Zynq Platform
    Workqueue: events deferred_probe_work_func
    [<c010fa50>] (unwind_backtrace) from [<c010bd5c>] (show_stack+0x10/0x14)
    [<c010bd5c>] (show_stack) from [<c08fbfac>] (dump_stack+0x8c/0xa0)
    [<c08fbfac>] (dump_stack) from [<c08f9854>] (Ldiv0_64+0x8/0x18)
    [<c08f9854>] (Ldiv0_64) from [<c03219ec>] (div64_u64+0xcc/0xf0)
    [<c03219ec>] (div64_u64) from [<c074c040>] (cf_axi_dds_default_setup+0x38/0xe0)
    [<c074c040>] (cf_axi_dds_default_setup) from [<c074d784>] (cf_axi_dds_probe+0x900/0xb28)
    [<c074d784>] (cf_axi_dds_probe) from [<c03eb4ac>] (platform_drv_probe+0x48/0x98)
    [<c03eb4ac>] (platform_drv_probe) from [<c03e983c>] (really_probe+0x1f4/0x2b8)
    [<c03e983c>] (really_probe) from [<c03e9a64>] (driver_probe_device+0x60/0x164)
    [<c03e9a64>] (driver_probe_device) from [<c03e7c4c>] (bus_for_each_drv+0x80/0xc4)
    [<c03e7c4c>] (bus_for_each_drv) from [<c03e95d8>] (__device_attach+0xd0/0x138)
    [<c03e95d8>] (__device_attach) from [<c03e8a48>] (bus_probe_device+0x84/0x8c)
    [<c03e8a48>] (bus_probe_device) from [<c03e8ee0>] (deferred_probe_work_func+0x60/0x8c)
    [<c03e8ee0>] (deferred_probe_work_func) from [<c0135a30>] (process_one_work+0x1f0/0x3fc)
    [<c0135a30>] (process_one_work) from [<c01369a4>] (worker_thread+0x294/0x584)
    [<c01369a4>] (worker_thread) from [<c013b680>] (kthread+0x148/0x150)
    [<c013b680>] (kthread) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
    Exception stack(0xef25bfb0 to 0xef25bff8)
    bfa0:                                     00000000 00000000 00000000 00000000
    bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
    Division by zero in kernel.
    CPU: 0 PID: 99 Comm: kworker/0:1 Not tainted 4.19.0-g17f4223 #1848
    Hardware name: Xilinx Zynq Platform
    Workqueue: events deferred_probe_work_func
    [<c010fa50>] (unwind_backtrace) from [<c010bd5c>] (show_stack+0x10/0x14)
    [<c010bd5c>] (show_stack) from [<c08fbfac>] (dump_stack+0x8c/0xa0)
    [<c08fbfac>] (dump_stack) from [<c08f9854>] (Ldiv0_64+0x8/0x18)
    [<c08f9854>] (Ldiv0_64) from [<c03219ec>] (div64_u64+0xcc/0xf0)
    [<c03219ec>] (div64_u64) from [<c074c040>] (cf_axi_dds_default_setup+0x38/0xe0)
    [<c074c040>] (cf_axi_dds_default_setup) from [<c074d764>] (cf_axi_dds_probe+0x8e0/0xb28)
    [<c074d764>] (cf_axi_dds_probe) from [<c03eb4ac>] (platform_drv_probe+0x48/0x98)
    [<c03eb4ac>] (platform_drv_probe) from [<c03e983c>] (really_probe+0x1f4/0x2b8)
    [<c03e983c>] (really_probe) from [<c03e9a64>] (driver_probe_device+0x60/0x164)
    [<c03e9a64>] (driver_probe_device) from [<c03e7c4c>] (bus_for_each_drv+0x80/0xc4)
    [<c03e7c4c>] (bus_for_each_drv) from [<c03e95d8>] (__device_attach+0xd0/0x138)
    [<c03e95d8>] (__device_attach) from [<c03e8a48>] (bus_probe_device+0x84/0x8c)
    [<c03e8a48>] (bus_probe_device) from [<c03e8ee0>] (deferred_probe_work_func+0x60/0x8c)
    [<c03e8ee0>] (deferred_probe_work_func) from [<c0135a30>] (process_one_work+0x1f0/0x3fc)
    [<c0135a30>] (process_one_work) from [<c01369a4>] (worker_thread+0x294/0x584)
    [<c01369a4>] (worker_thread) from [<c013b680>] (kthread+0x148/0x150)
    [<c013b680>] (kthread) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
    Exception stack(0xef25bfb0 to 0xef25bff8)
    bfa0:                                     00000000 00000000 00000000 00000000
    bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
    Division by zero in kernel.
    CPU: 0 PID: 99 Comm: kworker/0:1 Not tainted 4.19.0-g17f4223 #1848
    Hardware name: Xilinx Zynq Platform
    Workqueue: events deferred_probe_work_func
    [<c010fa50>] (unwind_backtrace) from [<c010bd5c>] (show_stack+0x10/0x14)
    [<c010bd5c>] (show_stack) from [<c08fbfac>] (dump_stack+0x8c/0xa0)
    [<c08fbfac>] (dump_stack) from [<c08f9854>] (Ldiv0_64+0x8/0x18)
    [<c08f9854>] (Ldiv0_64) from [<c03219ec>] (div64_u64+0xcc/0xf0)
    [<c03219ec>] (div64_u64) from [<c074c040>] (cf_axi_dds_default_setup+0x38/0xe0)
    [<c074c040>] (cf_axi_dds_default_setup) from [<c074d784>] (cf_axi_dds_probe+0x900/0xb28)
    [<c074d784>] (cf_axi_dds_probe) from [<c03eb4ac>] (platform_drv_probe+0x48/0x98)
    [<c03eb4ac>] (platform_drv_probe) from [<c03e983c>] (really_probe+0x1f4/0x2b8)
    [<c03e983c>] (really_probe) from [<c03e9a64>] (driver_probe_device+0x60/0x164)
    [<c03e9a64>] (driver_probe_device) from [<c03e7c4c>] (bus_for_each_drv+0x80/0xc4)
    [<c03e7c4c>] (bus_for_each_drv) from [<c03e95d8>] (__device_attach+0xd0/0x138)
    [<c03e95d8>] (__device_attach) from [<c03e8a48>] (bus_probe_device+0x84/0x8c)
    [<c03e8a48>] (bus_probe_device) from [<c03e8ee0>] (deferred_probe_work_func+0x60/0x8c)
    [<c03e8ee0>] (deferred_probe_work_func) from [<c0135a30>] (process_one_work+0x1f0/0x3fc)
    [<c0135a30>] (process_one_work) from [<c01369a4>] (worker_thread+0x294/0x584)
    [<c01369a4>] (worker_thread) from [<c013b680>] (kthread+0x148/0x150)
    [<c013b680>] (kthread) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
    Exception stack(0xef25bfb0 to 0xef25bff8)
    bfa0:                                     00000000 00000000 00000000 00000000
    bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
    Division by zero in kernel.
    CPU: 0 PID: 99 Comm: kworker/0:1 Not tainted 4.19.0-g17f4223 #1848
    Hardware name: Xilinx Zynq Platform
    Workqueue: events deferred_probe_work_func
    [<c010fa50>] (unwind_backtrace) from [<c010bd5c>] (show_stack+0x10/0x14)
    [<c010bd5c>] (show_stack) from [<c08fbfac>] (dump_stack+0x8c/0xa0)
    [<c08fbfac>] (dump_stack) from [<c08f9854>] (Ldiv0_64+0x8/0x18)
    [<c08f9854>] (Ldiv0_64) from [<c03219ec>] (div64_u64+0xcc/0xf0)
    [<c03219ec>] (div64_u64) from [<c074c040>] (cf_axi_dds_default_setup+0x38/0xe0)
    [<c074c040>] (cf_axi_dds_default_setup) from [<c074d764>] (cf_axi_dds_probe+0x8e0/0xb28)
    [<c074d764>] (cf_axi_dds_probe) from [<c03eb4ac>] (platform_drv_probe+0x48/0x98)
    [<c03eb4ac>] (platform_drv_probe) from [<c03e983c>] (really_probe+0x1f4/0x2b8)
    [<c03e983c>] (really_probe) from [<c03e9a64>] (driver_probe_device+0x60/0x164)
    [<c03e9a64>] (driver_probe_device) from [<c03e7c4c>] (bus_for_each_drv+0x80/0xc4)
    [<c03e7c4c>] (bus_for_each_drv) from [<c03e95d8>] (__device_attach+0xd0/0x138)
    [<c03e95d8>] (__device_attach) from [<c03e8a48>] (bus_probe_device+0x84/0x8c)
    [<c03e8a48>] (bus_probe_device) from [<c03e8ee0>] (deferred_probe_work_func+0x60/0x8c)
    [<c03e8ee0>] (deferred_probe_work_func) from [<c0135a30>] (process_one_work+0x1f0/0x3fc)
    [<c0135a30>] (process_one_work) from [<c01369a4>] (worker_thread+0x294/0x584)
    [<c01369a4>] (worker_thread) from [<c013b680>] (kthread+0x148/0x150)
    [<c013b680>] (kthread) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
    Exception stack(0xef25bfb0 to 0xef25bff8)
    bfa0:                                     00000000 00000000 00000000 00000000
    bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
    Division by zero in kernel.
    CPU: 0 PID: 99 Comm: kworker/0:1 Not tainted 4.19.0-g17f4223 #1848
    Hardware name: Xilinx Zynq Platform
    Workqueue: events deferred_probe_work_func
    [<c010fa50>] (unwind_backtrace) from [<c010bd5c>] (show_stack+0x10/0x14)
    [<c010bd5c>] (show_stack) from [<c08fbfac>] (dump_stack+0x8c/0xa0)
    [<c08fbfac>] (dump_stack) from [<c08f9854>] (Ldiv0_64+0x8/0x18)
    [<c08f9854>] (Ldiv0_64) from [<c03219ec>] (div64_u64+0xcc/0xf0)
    [<c03219ec>] (div64_u64) from [<c074c040>] (cf_axi_dds_default_setup+0x38/0xe0)
    [<c074c040>] (cf_axi_dds_default_setup) from [<c074d784>] (cf_axi_dds_probe+0x900/0xb28)
    [<c074d784>] (cf_axi_dds_probe) from [<c03eb4ac>] (platform_drv_probe+0x48/0x98)
    [<c03eb4ac>] (platform_drv_probe) from [<c03e983c>] (really_probe+0x1f4/0x2b8)
    [<c03e983c>] (really_probe) from [<c03e9a64>] (driver_probe_device+0x60/0x164)
    [<c03e9a64>] (driver_probe_device) from [<c03e7c4c>] (bus_for_each_drv+0x80/0xc4)
    [<c03e7c4c>] (bus_for_each_drv) from [<c03e95d8>] (__device_attach+0xd0/0x138)
    [<c03e95d8>] (__device_attach) from [<c03e8a48>] (bus_probe_device+0x84/0x8c)
    [<c03e8a48>] (bus_probe_device) from [<c03e8ee0>] (deferred_probe_work_func+0x60/0x8c)
    [<c03e8ee0>] (deferred_probe_work_func) from [<c0135a30>] (process_one_work+0x1f0/0x3fc)
    [<c0135a30>] (process_one_work) from [<c01369a4>] (worker_thread+0x294/0x584)
    [<c01369a4>] (worker_thread) from [<c013b680>] (kthread+0x148/0x150)
    [<c013b680>] (kthread) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
    Exception stack(0xef25bfb0 to 0xef25bff8)
    bfa0:                                     00000000 00000000 00000000 00000000
    bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    bfe0: 00000000 00000000 00000000 00000000 00000013 00000000
    cf_axi_dds 44a0a000.axi-adrv9002-tx-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x44A0A000 mapped to 0x1e48246d, probed DDS ADRV9002
    asoc-simple-card adv7511_hdmi_snd: spdif-hifi <-> 75c00000.axi-spdif-tx mapping ok
    input: gpio_keys as /devices/soc0/gpio_keys/input/input0
    rtc-pcf8563 5-0051: setting system clock to 2022-02-25 09:39:06 UTC (1645781946)
    clk: Not disabling unused clocks
    ALSA device list:
      #0: HDMI monitor
    EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    VFS: Mounted root (ext4 filesystem) on device 179:2.
    devtmpfs: mounted
    Freeing unused kernel memory: 1024K
    Run /sbin/init as init process
    systemd[1]: Failed to lookup module alias 'autofs4': Function not implemented
    systemd[1]: systemd 241 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +AC
    L +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD -IDN2 +IDN -PCRE2 default-hierarchy=hybrid)
    systemd[1]: Detected architecture arm.
    
    Welcome to Kuiper GNU/Linux 10 (buster)!
    
    systemd[1]: Set hostname to <analog>.
    systemd[1]: File /lib/systemd/system/systemd-journald.service:12 configures an IP firewall (IPAddressDeny=any), but the local system does not 
    support BPF/cgroup based firewalling.
    systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
    systemd[1]: /etc/systemd/system/tof-server.service:1: Assignment outside of section. Ignoring.
    systemd[1]: /etc/systemd/system/tof-server.service:2: Assignment outside of section. Ignoring.
    systemd[1]: Created slice system-serial\x2dgetty.slice.
    [  OK  ] Created slice system-serial\x2dgetty.slice.
    systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    systemd[1]: Created slice User and Session Slice.
    [  OK  ] Created slice User and Session Slice.
    [  OK  ] Started Forward Password R��…uests to Wall Directory Watch.
    [  OK  ] Listening on Syslog Socket.
    [  OK  ] Created slice system-getty.slice.
    [  OK  ] Listening on udev Kernel Socket.
    [  OK  ] Listening on fsck to fsckd communication Socket.
    [  OK  ] Listening on initctl Compatibility Named Pipe.
    [  OK  ] Listening on Journal Socket (/dev/log).
    [  OK  ] Created slice system-systemd\x2dfsck.slice.
    [  OK  ] Reached target Swap.
    [  OK  ] Listening on Journal Socket.
             Mounting RPC Pipe File System...
             Mounting Kernel Debug File System...
             Starting Set the console keyboard layout...
             Starting Load Kernel Modules...
             Starting Restore / save the current clock...
             Starting udev Coldplug all Devices...
    [  OK  ] Reached target Slices.
             Starting Journal Service...
    [FAILED] Failed to mount RPC Pipe File System.
    See 'systemctl status run-rpc_pipefs.mount' for details.
    [DEPEND] Dependency failed for RPC ��…ice for NFS client and server.
    [DEPEND] Dependency failed for RPC ��…curity service for NFS server.
    [  OK  ] Mounted Kernel Debug File System.
    [FAILED] Failed to start Load Kernel Modules.
    See 'systemctl status systemd-modules-load.service' for details.
    [  OK  ] Started Restore / save the current clock.
             Starting Remount Root and Kernel File Systems...
             Starting Apply Kernel Variables...
             Mounting Kernel Configuration File System...
    [  OK  ] Reached target NFS client services.
    [  OK  ] Reached target Remote File Systems (Pre).
    [  OK  ] Reached target Remote File Systems.
    [  OK  ] Started Journal Service.
    [  OK  ] Started Set the console keyboard layout.
    [  OK  ] Started Apply Kernel Variables.
    [  OK  ] Mounted Kernel Configuration File System.
    [  OK  ] Started Remount Root and Kernel File Systems.
             Starting Load/Save Random Seed...
             Starting Flush Journal to Persistent Storage...
             Starting Create System Users...
    [  OK  ] Started udev Coldplug all Devices.
    [  OK  ] Started Load/Save Random Seed.
    [  OK  ] Started Create System Users.
             Starting Create Static Device Nodes in /dev...
             Starting Helper to synchronize boot up for ifupdown...
    [  OK  ] Started Helper to synchronize boot up for ifupdown.
    [  OK  ] Started Create Static Device Nodes in /dev.
    [  OK  ] Reached target Local File Systems (Pre).
             Starting udev Kernel Device Manager...
    [  OK  ] Started Flush Journal to Persistent Storage.
    [  OK  ] Started udev Kernel Device Manager.
             Starting Show Plymouth Boot Screen...
    [  OK  ] Started Show Plymouth Boot Screen.
    [  OK  ] Started Forward Password R��…s to Plymouth Directory Watch.
    [  OK  ] Reached target Local Encrypted Volumes.
    [  OK  ] Found device /dev/ttyPS0.
             Starting Load Kernel Modules...
    [FAILED] Failed to start Load Kernel Modules.
    See 'systemctl status systemd-modules-load.service' for details.
    [  OK  ] Found device /dev/disk/by-partuuid/004ba301-01.
             Starting File System Check��…isk/by-partuuid/004ba301-01...
    [  OK  ] Started File System Check Daemon to report status.
    [  OK  ] Started File System Check ��…/disk/by-partuuid/004ba301-01.
             Mounting /boot...
    [  OK  ] Mounted /boot.
    [  OK  ] Reached target Local File Systems.
             Starting Tell Plymouth To Write Out Runtime Data...
             Starting Set console font and keymap...
             Starting Raise network interfaces...
             Starting Create Volatile Files and Directories...
             Starting Preprocess NFS configuration...
    [  OK  ] Started Tell Plymouth To Write Out Runtime Data.
    [  OK  ] Started Set console font and keymap.
    [  OK  ] Started Preprocess NFS configuration.
    [  OK  ] Started Create Volatile Files and Directories.
             Starting Update UTMP about System Boot/Shutdown...
             Starting Network Time Synchronization...
    [  OK  ] Started Update UTMP about System Boot/Shutdown.
             Starting Load Kernel Modules...
             Starting Tell Plymouth To Write Out Runtime Data...
    [  OK  ] Started Tell Plymouth To Write Out Runtime Data.
    [  OK  ] Started Raise network interfaces.
    [FAILED] Failed to start Load Kernel Modules.
    See 'systemctl status systemd-modules-load.service' for details.
    [  OK  ] Started Network Time Synchronization.
    [  OK  ] Reached target System Initialization.
    [  OK  ] Listening on GPS (Global P��…ioning System) Daemon Sockets.
    [  OK  ] Listening on D-Bus System Message Bus Socket.
    [  OK  ] Listening on CUPS Scheduler.
    [  OK  ] Listening on triggerhappy.socket.
    [  OK  ] Started CUPS Scheduler.
    [  OK  ] Reached target Paths.
    [  OK  ] Started Daily Cleanup of Temporary Directories.
    [  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
    [  OK  ] Reached target Sockets.
    [  OK  ] Reached target Basic System.
             Starting rng-tools.service...
             Starting triggerhappy global hotkey daemon...
    [  OK  ] Started CUPS Scheduler.
    [  OK  ] Started Manage Sound Card State (restore and store).
             Starting Modem Manager...
             Starting dphys-swapfile - ��…unt, and delete a swap file...
             Starting dhcpcd on all interfaces...
             Starting Save/Restore Sound Card State...
    [  OK  ] Started Regular background program processing daemon.
             Starting Disk Manager...
             Starting Avahi mDNS/DNS-SD Stack...
             Starting Check for Raspberry Pi EEPROM updates...
             Starting System Logging Service...
             Starting LSB: Switch to on��…nless shift key is pressed)...
    [  OK  ] Started tof-server.service.
    [  OK  ] Started D-Bus System Message Bus.
             Starting WPA supplicant...
             Starting Login Service...
    [  OK  ] Reached target System Time Synchronized.
    [  OK  ] Started Daily man-db regeneration.
    [  OK  ] Started Daily rotation of log files.
    [  OK  ] Started Daily apt download activities.
    [  OK  ] Started Daily apt upgrade and clean activities.
    [  OK  ] Reached target Timers.
    [  OK  ] Started triggerhappy global hotkey daemon.
    [FAILED] Failed to start rng-tools.service.
    See 'systemctl status rng-tools.service' for details.
    [  OK  ] Started Save/Restore Sound Card State.
    [  OK  ] Started Check for Raspberry Pi EEPROM updates.
    [  OK  ] Reached target Sound Card.
    [  OK  ] Started System Logging Service.
    [  OK  ] Started Login Service.
    [  OK  ] Started dhcpcd on all interfaces.
    [  OK  ] Started Avahi mDNS/DNS-SD Stack.
    [  OK  ] Started WPA supplicant.
    [  OK  ] Started Make remote CUPS printers available locally.
    [  OK  ] Reached target Network.
             Starting Permit User Sessions...
    [  OK  ] Reached target Network is Online.
             Starting /etc/rc.local Compatibility...
             Starting Internet superserver...
             Starting HTTP based time synchronization tool...
    [  OK  ] Started IIO Daemon.
             Starting OpenBSD Secure Shell server...
    [  OK  ] Started Internet superserver.
    [  OK  ] Started /etc/rc.local Compatibility.
             Starting Authorization Manager...
    [  OK  ] Started Permit User Sessions.
    [  OK  ] Started HTTP based time synchronization tool.
             Starting Hold until boot process finishes up...
             Starting Light Display Manager...
    [  OK  ] Started dphys-swapfile - s��…mount, and delete a swap file.
    [  OK  ] Started LSB: Switch to ond��…(unless shift key is pressed).
    [  OK  ] Started OpenBSD Secure Shell server.
    [  OK  ] Started Authorization Manager.
    
    Raspbian GNU/Linux 10 analog ttyPS0
    
    analog login: root (automatic login)
    
    Last login: Fri Feb 25 09:37:31 GMT 2022 on ttyPS0
    Linux analog 4.19.0-g17f4223 #1848 SMP PREEMPT Tue Jul 27 12:46:50 IST 2021 armv7l
    
    The programs included with the Debian GNU/Linux system are free software;
    the exact distribution terms for each program are described in the
    individual files in /usr/share/doc/*/copyright.
    
    Debian GNU/Linux comes with ABSOLUTELY NO WARRANTY, to the extent
    permitted by applicable law.
    root@analog:~# 
    
    
    with ZC706.

  • Hi travis,

    Can you please provide documentation on differentiating B0 and C0 versions silicon of navassa-adrv9002.

    Following the link you have provided, the prebuilt images provided here:http://swdownloads.analog.com/cse/tmp/B0_2019_r2_pre_release_zcu102.zip are specific to zcu102+adrv9002. Can you please guide us to the point where prebuilt images for ZC706+ADRV9002 are provided and are tested to be working.

    Thanks and Regards

    Pavithra

  • Please see the link that I posted above.

    B0 is no longer supported and is not available in our supported release branches.

    -Travis