Post Go back to editing

ADRV9361-Z7035 USB-Serial not enumerating after trying previous solution

Hello, I am running a ADRV9361-Z7035 with the BOB carrier. I am trying to get a FTDI or CP2012 based USB to Serial device to enumerate with the 2021-07-28 ADI Kuiper full image. I found the following link for instructions and tried it.

https://ez.analog.com/linux-software-drivers/f/q-a/87886/breakout-carrier-how-to-use-second-microusb-interface-to-control-a-serial-device

Even after make menuconfig and copying the uImage, after boot and adding the devices I still get the following output from dmesg.  I ran the build_zynq_kernel_image.sh instructions and let it successfully build once. Then I went into the linux-adi subfolder and did make menuconfig there and ensured the linked instructions were selected. Then I rebuilt the kernel image and copied it into the BOOT partition and rebooted. I think I am doing everything correctly, but still am unable to enumerate the device. Any help would be greatly appreciated. I don't necessarily need the USB to work, I just want a second Serial port on the device that I can bind a server program to and take instructions from an external source. Thank you.

[ 63.142355] usb 1-1: new full-speed USB device number 2 using ci_hdrc
[ 63.382351] usb 1-1: device descriptor read/64, error -71
[ 63.742347] usb 1-1: device descriptor read/64, error -71
[ 64.012347] usb 1-1: new full-speed USB device number 3 using ci_hdrc
[ 64.252346] usb 1-1: device descriptor read/64, error -71
[ 64.612346] usb 1-1: device descriptor read/64, error -71
[ 64.732390] usb usb1-port1: attempt power cycle
[ 65.442377] usb 1-1: new full-speed USB device number 4 using ci_hdrc
[ 65.942351] usb 1-1: device not accepting address 4, error -71
[ 66.092355] usb 1-1: new full-speed USB device number 5 using ci_hdrc
[ 66.592347] usb 1-1: device not accepting address 5, error -71
[ 66.592402] usb usb1-port1: unable to enumerate USB device

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.