[ 7%] Building C object CMakeFiles/osc.dir/fru.c.o
/home/erwin/iio-oscilloscope/iio_utils.c: In function ‘get_iio_device_label_or_name’:
/home/erwin/iio-oscilloscope/iio_utils.c:148:7: error: implicit declaration of function ‘iio_device_get_label’; did you mean ‘iio_device_get_name’? [-Werror=implicit-function-declaration]
id = iio_device_get_label(dev);
^~~~~~~~~~~~~~~~~~~~
iio_device_get_name
/home/erwin/iio-oscilloscope/iio_utils.c:148:5: error: assignment makes pointer from integer without a cast [-Werror=int-conversion]
id = iio_device_get_label(dev);
^
cc1: all warnings being treated as errors
CMakeFiles/osc.dir/build.make:158: recipe for target 'CMakeFiles/osc.dir/iio_utils.c.o' failed
make[2]: *** [CMakeFiles/osc.dir/iio_utils.c.o] Error 1
make[2]: *** Waiting for unfinished jobs....
CMakeFiles/Makefile2:104: recipe for target 'CMakeFiles/osc.dir/all' failed
make[1]: *** [CMakeFiles/osc.dir/all] Error 2
Makefile:129: recipe for target 'all' failed
make: *** [all] Error 2
Did anybody see the same? What could be the reason and a solution?
Thanks
Erwin
Hi Erwin,
If you are building iio-oscilloscope from git master, make sure that you are also using libiio from git master. The iio_device_get_label function it fails to see was added to libiio after the 0.21 release, and will be available in the 0.22 release.
Cheers,
-Paul
That did not help a lot. I freshly built libiio from source, also built libad9361-iio again after make clean. I have a IIO-oscilloscope icon in my list of installed applications. A click results in nothing.
Rebuilding libiio killed a working CubicSDR that now opens and closes in a flash.
URH and GNU-radio still work with the Pluto.
Which branches of libiio and IIO-Scope are you using?
-Travis
I am strictly following the wiki documentation :
https://wiki.analog.com/resources/tools-software/linux-software/iio_oscilloscope
on Oracle VirtualBox / Ubuntu 1804
I am just starting a new build on a clean Ubuntu 2004 to see if this gives different results
BUT with this libiio
Install the libiio Library: OS: ubuntu Type : .deb Version : ubuntu-20.04-amd64 : libiio-0.21.g565bf68-ubuntu-20.04-amd64.deb
As that is where the pluto html page brings me before doing anything else
If that fails again I will start fresh and do a complete build libiio from the iio-oscilloscope page reference to the instructions for libiio
I am strictly following the wiki documentation :
https://wiki.analog.com/resources/tools-software/linux-software/iio_oscilloscope
on Oracle VirtualBox / Ubuntu 1804
I am just starting a new build on a clean Ubuntu 2004 to see if this gives different results
BUT with this libiio
Install the libiio Library: OS: ubuntu Type : .deb Version : ubuntu-20.04-amd64 : libiio-0.21.g565bf68-ubuntu-20.04-amd64.deb
As that is where the pluto html page brings me before doing anything else
If that fails again I will start fresh and do a complete build libiio from the iio-oscilloscope page reference to the instructions for libiio
Where this instruction appears to be a bit wrong:
and run `make` and `make install`. If you did not do a make install of the libiio, the libiio install location needs to be set in your path ie: (PATH=/usr/lib:$PATH“) or else an error “Package libiio not found..” will occur.
rgetz@pinky:~/iio-oscilloscope$ mkdir build && cd build
rgetz@pinky:~/iio-oscilloscope$ cmake ../ && make -j $(nproc)
rgetz@pinky:~/iio-oscilloscope$ sudo make install
As for the last 2 steps we are in ../build as the first step brought us there via cd build
Done both, both fail, differently.
The first with the libiio from the base instructions throws the same error.
When doing the second by building libiio from git the Oscilloscope icon is there, clicking it requests su authorisation and then nothing start and you rest with an still empty screen.
The green line below is not correct, I made a mistake in using ./osc instead of osc to start IIO_Oscilloscope
Conclusion: there is no way to build IIO-Oscilloscope currently based on the instructions and available libiio releases or git versions
The first with the libiio from the base instructions throws the same error.
As Paul mentioned you must install libiio from source if you want to use the master branch of IIO-Scope. Using the deb from the release is not the git master.
When doing the second by building libiio from git the Oscilloscope icon is there, clicking it requests su authorisation and then nothing start and you rest with an still empty screen.
Please launch IIO-Scope directly from the command line. Typing osc from the command line will launch it.
-Travis
I set aside my troubles with IIO-Oscilloscope and started to build GNURADIO 3.8 from source to get to the gr-iio blocks for the Pluto (as on 20.04 gnuradio 3.9 is pre-installed which does not work with the gr-iio blocks)
That process did not work well so far BUT I can now start IIO Oscilloscope with the icon!
As if a part of the gnuradio install or its dependencies solved an issue with my setup.
Still, I can NOT start it with ./osc from within the iio-oscilloscope directory. (EDIT: no because I should use osc and not ./osc)
The ABOUT tells me I am using libiio version 0.22-5587c8e
and the osc is HEAD-g1cc52ea
Also in the check for updates pop up window :
This software is newer than the latest release
Latest version: IIO_Oscilloscope - v0.14-master
Starting with osc shows some errors (even though the IIO-Oscilloscope windows open) :
erwin@UBU2004:~/iio-oscilloscope$ osc
(osc:3692): Gtk-WARNING **: 11:01:53.572: Could not load image 'osc128.png': Failed to open file “./glade/osc128.png”: No such file or directory
(osc:3692): Gtk-WARNING **: 11:01:53.590: Could not load image 'IIOlogo.png': Failed to open file “./glade/IIOlogo.png”: No such file or directory
(osc:3692): Gtk-WARNING **: 11:01:53.591: Could not load image 'ADIlogo.png': Failed to open file “./glade/ADIlogo.png”: No such file or directory
ERROR: Unable to claim interface 1:2:5: Device or resource busy (16)
ERROR: Unable to create Avahi DNS-SD browser: Invalid host name
ERROR: Unable to create Avahi DNS-SD browser: Invalid host name
ERROR: Unable to claim interface 1:2:5: Device or resource busy (16)
ERROR: Unable to create Avahi DNS-SD browser: Invalid host name
ERROR: Unable to create Avahi DNS-SD browser: Invalid host name
ERROR: Unable to claim interface 1:2:5: Device or resource busy (16)
ERROR: Unable to create Avahi DNS-SD browser: Invalid host name
ERROR: Unable to create Avahi DNS-SD browser: Invalid host name
(osc:3692): Gtk-WARNING **: 11:03:42.403: Could not load image 'ADIlogo.png': Failed to open file “./glade/ADIlogo.png”: No such file or directory
And see what happens when doing osc from my home directory, and IIO-Oscilloscope windows open
erwin@UBU2004:~$ osc
Found plugin: CN0540
Could not find expected iio devices
Found plugin: ad9739a
Found plugin: CN0511
Found plugin: Debug
Found plugin: FMComms6
Found plugin: DAC Data Manager
Found plugin: AD936X
Found plugin: AD9371
Found plugin: AD9371 Advanced
Found plugin: AD6676
Found plugin: AD7303
Found plugin: CN0357
Found plugin: AD936X Advanced
Found plugin: AD5628-1
Found plugin: DMM
Found plugin: ADRV9009
Found plugin: FMCOMMS11
Found plugin: CN0508
Found plugin: DAQ1/2/3
Found plugin: FMComms1
Found plugin: Spectrum Analyzer
Found plugin: FMComms5
Found plugin: Partial Reconfiguration
Found plugin: LIDAR
Found plugin: FMCADC3
Found plugin: SCPI
Found plugin: Motor Control
Loaded plugin: Debug
Updating widgets...
Updating FIR filter...
Loaded plugin: AD936X
Loaded plugin: AD936X Advanced
Loaded plugin: DMM
Loaded plugin: Spectrum Analyzer
set to peak
error parsing /home/erwin/.osc_profile.ini file: Could not find AD936X
error parsing /home/erwin/.osc_profile.ini file: Could not find AD936X
error parsing /home/erwin/.osc_profile.ini file: Could not find AD936X Advanced
Closing plugin: Debug
Closing plugin: AD936X
Closing plugin: AD936X Advanced
Closing plugin: DMM
Closing plugin: Spectrum Analyzer
erwin@UBU2004:~$
Hi,
To run the iio-oscilloscope that you just built, in the ~/iio-oscilloscope folder, run "./osc" and not "osc", otherwise you are actually running the version that's installed system-wide along with the new plugins and that won't work.
-Paul
I do not understand your comment Paul.
How can there be a version that's installed system-wide along with the new plugins on a clean Ubuntu?
When I built it, there would be only one version?
For me ./osc does not work, nowhere,
erwin@UBU2004:~$ ./osc
bash: ./osc: No such file or directory
erwin@UBU2004:~$ cd iio-oscilloscope
erwin@UBU2004:~/iio-oscilloscope$ ./osc
bash: ./osc: No such file or directory
And with both tries of osc, both start iio-oscilloscope, just with 2 different reactions in the terminal, but both the same version and both the same version of libiio.
The generated binary "osc" will be within the folder you use to build the project. Running "./osc" within that folder will run that version. Running "osc" without the "./" will run the global one in your cache. You can force cache/link updates by running "sudo ldconfig"
The two different outputs you see when running IIO-Scope are related to state that existed from a previous session. IIO-Scope will place a file (~/.osc_profile.ini) in your home directory. This will keep track of old sessions so things will auto-connect when re-launch IIO-Scope. It looks like the first time it was looking for a USB device like Pluto but you never connected to it. Session 2 looks like you did attach to the device.
It is possible you have a corrupt .osc_profile.ini file if the IIO-Scope installs were broken or incomplete. I would recommend just deleting that file from your home folder.
-Travis
[IIO Oscilloscope]
window_x_pos=735
window_y_pos=196
tooltips_enable=1
startup_version_check=1
uri=0456:b673 104000323198000ffbff3300d0d1024a0e
initial contents of .osc_profile.ini
Deleted - Restarted machine
erwin@UBU2004:~$ cd iio-oscilloscope
erwin@UBU2004:~/iio-oscilloscope$ ./osc
bash: ./osc: No such file or directory
erwin@UBU2004:~/iio-oscilloscope$
Still. A simple osc works and starts the program
The profile is now a lot more complete showing 223 lines including debug messages.
sudo ldconfig makes no difference
The states shown are not in parallel to each other but after each other as you can not start a second osc when the Adalm Pluto is already occupied/connected to the first
erwin@UBU2004:~$ cd iio-oscilloscope
erwin@UBU2004:~/iio-oscilloscope$ ./osc
bash: ./osc: No such file or directory
erwin@UBU2004:~/iio-oscilloscope$
But my main point remains : for me ./osc NEVER works where osc always works. On Ubuntu 1804 and on 2004. Both with same versions of libiio and iio-oscilloscope.
Another point:
Plot Type has no Spectrum Mode choice although the Settings Spectrum Analyzer window works (I do have a Spectrum Mode as Plot Type when Start Sweep was activated on the IIO-Oscilloscope install on my UBU1804 laptop created in the same way as the one on the UBU2004 Oracle Virtual Box machine.). I can not do Start Sweep on 2004. When Start Sweep has been active and Spectrum Mode is highlighted I loose my Start and Stop buttons to acquire other types of plots. I have to Start New plot to get back the Capture/Stop green arrow. It looks as if the Sweep only works with the Rev.C and not with the Rev.B HW?
When switching these I now have Ubuntu2004 doing a sweep and showing Spectrum Mode with the Rev.C hardware.
erwin@UBU2004:~$ cd iio-oscilloscope
erwin@UBU2004:~/iio-oscilloscope$ ./osc
bash: ./osc: No such file or directory
erwin@UBU2004:~/iio-oscilloscope$
This pathing assumes you built the library in the same place as the source. In the exact same folder. Now if you built it in say a subfolder named build you would have to run:
cd iio-oscilloscope
cd build
./osc
The states shown are not in parallel to each other but after each other as you can not start a second osc when the Adalm Pluto is already occupied/connected to the first
This is expected if you are using the USB contexts to connect to Pluto. Only one can be used at a time. Using the IP address will allow multiple connections to the same device.
It looks as if the Sweep only works with the Rev.C and not with the Rev.B HW?
You likely have different versions of IIO-Scope between the two machines. Rev B vs Rev C makes no difference. IIO-Scope does not treat them any differently. There is a known bug with the spectrum analyzer sweeper that might be related to the different versions: https://github.com/analogdevicesinc/iio-oscilloscope/issues/315
We usually recommend the users stick with the standard capture window and Frequency Domain plot. The sweeper tab only works well when run on the device itself, when you have low latency access to the fastlock profile selection. Not over USB or Ethernet. This would apply to something like a FMComms3+ZC706 or ADRV9361-Z7035.
-Travis