Post Go back to editing

Running RFSOM-BOX-GUI in PackRF with 2019_R2 Image

Recently I received a pair of PackRFs. When I ran with 2016_R1 image, the RFSOM-BOX-GUI showed up immediately.

However, when I ran with 2019_R2 image, the Linux penguin showed first and then the Linux desktop showed up. The screen is so small that I could not find the application tab and run the RFSOM-BOX-GUI, let alone finding the IP address of the PackRF.

Is there a way to start the RFSOM-BOX-GUI by using the click wheel and button only?

Thanks a lot in advance.

Parents
  • Do you have terminal access to the packrf ? It looks like the OS does not identify the box as RFSOM-BOX. If you have access, can you do "cat /sys/firmware/devicetree/base/model " and post the result ? 

  • The only way I can do is to connect both mouse and keyboard to the USB OTG port, use mouse to open the terminal and them keyboard to type ifconfig to find the IP address. Then I connect the PackRF from my Windows desktop using PuTTY with the known IP address.

    After typing "cat /sys/firmware/devicetree/base/model", the result is 

    AnalogDevicesADRV9361-Z7035RFSOM-BOX(Z7035/AD9361)

Reply
  • The only way I can do is to connect both mouse and keyboard to the USB OTG port, use mouse to open the terminal and them keyboard to type ifconfig to find the IP address. Then I connect the PackRF from my Windows desktop using PuTTY with the known IP address.

    After typing "cat /sys/firmware/devicetree/base/model", the result is 

    AnalogDevicesADRV9361-Z7035RFSOM-BOX(Z7035/AD9361)

Children
No Data