Post Go back to editing

AD9988-FMCB-EBZ and ZCU102

Hello,

I have a question from our customer about AD9988.
A ZynqMP / MPSoC Linux kernel is prepared for  AD9081 and AD9082.
It is introduced on the bellow page.
 wiki.analog.com/.../zynqmp

Our customer wants to use  zynqmp-zcu102-rev10-ad9081-m8-l4.zip (2019_R2 pre) for AD9988-FMCB-EBZ in place of AD9081-FMCCA-EBZ with Xilinx ZCU102.
Will the above zcu102 image( zynqmp-zcu102-rev10-ad9081-m8-l4.zip) work with the AD9988-FMCB-EBZ if I use only the same features as the AD9081?

Best regards,

y_suzuki

Top Replies