Hello Everyone,
I hope you are all doing great!
I am new to AD evaluation platforms and will first time use the Linux image on the following setup:
HW: A10SoC+AD9163-FMCC-EBZ (Eval-AD916x)
HDL: AD-DAC-FMC-EBZ
config.tcl: AD9163 mode:08 (set params(AD9163,08) {2 8 2 1 1 16 16})
I would like to send out patterns read out from DMA (from DDR4) patterns
My first question is :
Which Linux image should I use for this purpose?
Then What is the easiest way to feed the desired patterns over the DDR4 - DMA path to the DAC and get the maximum speed in the end as possible with this 8 lane configuration.
Best Regards,
Ömer.