Unable to read file uImage SD CARD

Hello

I'm trying to evaluate the linux enviroment in zedboard (Zynq 7000 AD9467) following the steps described in:

wiki.analog.com/.../zynq_images

after create the image with win32diskimage (windows 10) and extract the files
from zynq-zed-adv7511-ad9467-fmc-250ebz folder (I have FMC connected)

-boot.bin
-uEnv.txt
-uImage
-devicetree.dtb
-bootgen_sysfiles.tgz


I run the boot commands:

env default -a
saveenv
setenv ethaddr AA:BB:CC:DD:EE:FF
save reset

I get the serial output:

## Resetting to default environment
zynq-uboot> saveenv
Saving Environment to SPI Flash...
SF: Detected S25FL256S_64K with page size 256 Bytes, erase size 64 KiB, total 32 MiB
Erasing SPI flash...Writing to SPI flash...done
zynq-uboot> setenv ethaddr 7C:B0:C2:B7:A2:87
zynq-uboot> save
Saving Environment to SPI Flash...
Erasing SPI flash...Writing to SPI flash...done
zynq-uboot> reset
resetting ...
U-Boot 2014.07-dirty (Nov 20 2014 - 17:05:21)

Board: Xilinx Zynq
I2C: ready
DRAM: ECC disabled 512 MiB
MMC: zynq_sdhci: 0
SF: Detected S25FL256S_64K with page size 256 Bytes, erase size 64 KiB, total 32 MiB
In: serial
Out: serial
Err: serial
Net: Gem.e000b000
Hit any key to stop autoboot: 0
Device: zynq_sdhci
Manufacturer ID: 27
OEM: 5048
Name: SD32G
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 28.9 GiB
Bus Width: 4-bit
reading uEnv.txt
378 bytes read in 8 ms (45.9 KiB/s)
Loaded environment from uEnv.txt
Importing environment from SD ...
Running uenvcmd ...
Copying Linux from SD to RAM...
reading uImage
** Unable to read file uImage **
Copying Linux from SD to RAM...
reading uImage
** Unable to read file uImage **

Can't read file uImage.

I apreciate any help 

thanks

Jael R

Top Replies

    •  Analog Employees 
    Jun 23, 2021 in reply to Jhael +1 verified
    inet 169.254.216.194 netmask 255.255.0.0 broadcast 169.254.255.255

    This means it cannot get an IP address. Make sure your DHCP server is accessible to the device.

    -Travis