ADRV9009-ZU11EG Multi-SOM: 3 SOMs delayed from other 3

I'm running 6 SOMs (without FMCOMMS8) simultaneously, following the multi-SOM guide here.

I'm finding that when I run multi.rx, the second, third, and fifth SOMs are all delayed by approximately 138ns.  So what I have is one set of 3 that are in sync, and another set of 3 that are in sync but delayed.

I've tried adding adding a coarse digital delay in the devicetree and that seemed to make no difference.

I've also tried using the multi.hmc7044_ext_output_delay() function within my python script, which also seems to make no difference.

Noting that my VCO frequency is 122.88 MHz, the 138ns delay I'm seeing would appear to be 17 cycles, which leads me to believe this is related to the coarse digital delay.

Here's the portion of my primary device tree that pertains to hmc7044-ext:

			hmc7044-ext@4 {
				#address-cells = < 0x01 >;
				#size-cells = < 0x00 >;
				#clock-cells = < 0x01 >;
				compatible = "adi,hmc7044";
				reg = < 0x04 >;
				spi-max-frequency = < 0xf4240 >;
				adi,pll1-clkin-frequencies = < 0x00 0x1d4c000 0x00 0x00 >;
				adi,pll1-loop-bandwidth-hz = < 0xc8 >;
				adi,pfd1-maximum-limit-frequency-hz = < 0x3a9800 >;
				adi,vcxo-frequency = < 0x7530000 >;
				adi,pll2-output-frequency = < 0xafc80000 >;
				adi,sysref-timer-divider = < 0xf00 >;
				adi,pulse-generator-mode = < 0x01 >;
				adi,oscin-buffer-mode = < 0x15 >;
				adi,clkin1-buffer-mode = < 0x07 >;
				adi,sync-pin-mode = < 0x01 >;
				adi,gpi-controls = < 0x00 0x00 0x00 0x00 >;
				adi,gpo-controls = < 0x1f 0x2b 0x00 0x00 >;
				clock-output-names = "hmc7044_e_out0_REFCLK_OUT0\0hmc7044_e_out1_SYNC_OUT0\0hmc7044_e_out2_REFCLK_OUT1\0hmc7044_e_out3_SYNC_OUT1\0hmc7044_e_out4_REFCLK_OUT2\0hmc7044_e_out5_SYNC_OUT2\0hmc7044_e_out6_REFCLK_OUT3\0hmc7044_e_out7_SYNC_OUT3\0hmc7044_e_out8_REFCLK_OUT4\0hmc7044_e_out9_SYNC_OUT4\0hmc7044_e_out10_REFCLK_OUT5\0hmc7044_e_out11_SYNC_OUT5\0hmc7044_e_out12_REFCLK_OUT6\0hmc7044_e_out13_SYNC_OUT6";
				jesd204-device;
				#jesd204-cells = < 0x02 >;
				jesd204-sysref-provider;
				adi,hmc-two-level-tree-sync-en;
				phandle = < 0x25 >;

				channel@0 {
					reg = < 0x00 >;
					adi,extended-name = "REFCLK_OUT0";
					adi,divider = < 0x60 >;
					adi,driver-mode = < 0x01 >;
					phandle = < 0x95 >;
				};

				channel@2 {
					reg = < 0x02 >;
					adi,extended-name = "REFCLK_OUT1";
					adi,divider = < 0x60 >;
					adi,driver-mode = < 0x01 >;
					phandle = < 0x96 >;
				};

				channel@5 {
					reg = < 0x05 >;
					adi,extended-name = "SYNC_OUT2";
					adi,divider = < 0xf00 >;
					adi,driver-mode = < 0x03 >;
					adi,startup-mode-dynamic-enable;
					adi,high-performance-mode-disable;
					adi,driver-impedance-mode = < 0x03 >;
					phandle = < 0x97 >;
				};

				channel@6 {
					reg = < 0x06 >;
					adi,extended-name = "REFCLK_OUT3";
					adi,divider = < 0x60 >;
					adi,driver-mode = < 0x01 >;
					phandle = < 0x98 >;
				};

				channel@11 {
					reg = < 0x0b >;
					adi,extended-name = "SYNC_OUT5";
					adi,divider = < 0xf00 >;
					adi,driver-mode = < 0x03 >;
					adi,startup-mode-dynamic-enable;
					adi,high-performance-mode-disable;
					adi,driver-impedance-mode = < 0x03 >;
					phandle = < 0x99 >;
				};

				channel@1 {
					reg = < 0x01 >;
					adi,extended-name = "SYNC_OUT0";
					adi,divider = < 0xf00 >;
					adi,driver-mode = < 0x03 >;
					adi,startup-mode-dynamic-enable;
					adi,high-performance-mode-disable;
					adi,driver-impedance-mode = < 0x03 >;
					phandle = < 0x9a >;
				};

				channel@3 {
					reg = < 0x03 >;
					adi,extended-name = "SYNC_OUT1";
					adi,divider = < 0xf00 >;
					adi,driver-mode = < 0x03 >;
					adi,startup-mode-dynamic-enable;
					adi,high-performance-mode-disable;
					adi,driver-impedance-mode = < 0x03 >;
					phandle = < 0x9b >;
				};

				channel@4 {
					reg = < 0x04 >;
					adi,extended-name = "REFCLK_OUT2";
					adi,divider = < 0x60 >;
					adi,driver-mode = < 0x01 >;
					phandle = < 0x9c >;
				};

				channel@7 {
					reg = < 0x07 >;
					adi,extended-name = "SYNC_OUT3";
					adi,divider = < 0xf00 >;
					adi,driver-mode = < 0x03 >;
					adi,startup-mode-dynamic-enable;
					adi,high-performance-mode-disable;
					adi,driver-impedance-mode = < 0x03 >;
					phandle = < 0x9d >;
				};

				channel@8 {
					reg = < 0x08 >;
					adi,extended-name = "REFCLK_OUT4";
					adi,divider = < 0x60 >;
					adi,driver-mode = < 0x01 >;
					phandle = < 0x9e >;
				};

				channel@9 {
					reg = < 0x09 >;
					adi,extended-name = "SYNC_OUT4";
					adi,divider = < 0xf00 >;
					adi,driver-mode = < 0x03 >;
					adi,startup-mode-dynamic-enable;
					adi,high-performance-mode-disable;
					adi,driver-impedance-mode = < 0x03 >;
					phandle = < 0x9f >;
				};

				channel@10 {
					reg = < 0x0a >;
					adi,extended-name = "REFCLK_OUT5";
					adi,divider = < 0x60 >;
					adi,driver-mode = < 0x01 >;
					phandle = < 0xa0 >;
				};

				channel@12 {
					reg = < 0x0c >;
					adi,extended-name = "REFCLK_OUT6";
					adi,divider = < 0x60 >;
					adi,driver-mode = < 0x01 >;
					phandle = < 0xa1 >;
				};

				channel@13 {
					reg = < 0x0d >;
					adi,extended-name = "SYNC_OUT6";
					adi,divider = < 0xf00 >;
					adi,driver-mode = < 0x03 >;
					adi,startup-mode-dynamic-enable;
					adi,high-performance-mode-disable;
					adi,driver-impedance-mode = < 0x03 >;
					phandle = < 0xa2 >;
				};
			};
		};

Any suggestions?

Parents
  • An update: I have probed the SYNC lines on the clock board, and it appears that the signal is inverted on the ports that exhibit the delay.

    The rising clock edges are 138ns apart so I feel pretty certain that this is the cause.

    Is there a setting that has inverted 3 of my SYNC lines?  Which of the two is the proper SYNC signal?

  • 0
    •  Analog Employees 
    on Apr 29, 2021 6:53 AM in reply to mstone

    Hmm - I'm a bit confused now.

    HMC7044 SYNC signal should be CMOS this looks differential.

    In your device tree you correctly use:

    adi,driver-mode = <3>;

    The output buffers seem to activate/deactivate in sync, like you say they are just inverted.

    Wondering if you probe on one board OUTCLKx_P and on the other OUTCLKx_N?   

  • After implementing the patch to primary and all secondary images, the time delay is unimproved.

    The other main change I have made within the device tree is to add support for the AD9545 clock chip:

    				i2c@1 {
    					#address-cells = <0x1>;
    					#size-cells = <0x0>;
    					reg = <0x1>;
    
    					ad9545@4A {
    						compatible = "adi,ad9545";
    						reg = <0x4a>;
    						#address-cells = <0x1>;
    						#size-cells = <0x0>;
    						adi,ref-crystal;
    						adi,ref-frequency-hz = <0x2ee0000>;
    						#clock-cells = <0x2>;
    						assigned-clocks = <0x18 0x2 0x0 0x18 0x1 0x1 0x18 0x0 0x6 0x18 0x0 0x8>;
    						assigned-clock-rates = <0x2710 0x6fc23ac0 0x9502f90 0x9502f90>;
    						assigned-clock-phases = <0x0 0x0 0x0 0xb4>;
    						phandle = <0x18>;
    
    						aux-nco-clk@0 {
    							reg = <0x0>;
    							adi,freq-lock-threshold-ps = <0xf42400>;
    							adi,phase-lock-threshold-ps = <0xf42400>;
    						};
    
    						pll-clk@1 {
    							reg = <0x1>;
    							#address-cells = <0x1>;
    							#size-cells = <0x0>;
    							phandle = <0x75>;
    
    							profile@0 {
    								reg = <0x0>;
    								adi,pll-source = <0x4>;
    								adi,profile-priority = <0x0>;
    								adi,pll-loop-bandwidth-uhz = <0xbebc200>;
    							};
    						};
    
    						output-clk@6 {
    							reg = <0x6>;
    							adi,output-mode = <0x0>;
    							adi,current-source-microamp = <0x3a98>;
    						};
    
    						output-clk@8 {
    							reg = <0x8>;
    							adi,output-mode = <0x0>;
    							adi,current-source-microamp = <0x3a98>;
    						};
    					};
    				};
    

    I don't think it likely, but is there any way this could be impacting the way the hmc7044-ext device is behaving?

  • 0
    •  Analog Employees 
    on May 3, 2021 1:13 PM in reply to mstone

    Hmm - assuming the HMC7044 on the carrier does reference switching and uses CLKIN0 instead of CLKIN1, then of course the SYNC pulse from the external HMC7044 is no longer synced with the clocks.

    For your multi-SoM syncing you want to make sure that you use the reference clocks from the external HMC7044.

    Can you check:

    root@analog:~# iio_attr -D hmc7044-car
    dev 'hmc7044-car', debug attr 'status', value :'--- PLL1 ---
    Status: Locked
    Using:  CLKIN1 @ 30720000 Hz
    PFD:    7680 kHz
    --- PLL2 ---
    Status: Locked (Synchronized)
    Frequency:      2949120000 Hz (Autocal cap bank value: 14)
    SYSREF Status:  Valid & Locked
    SYNC Status:    Synchronized
    Lock Status:    PLL1 & PLL2 Locked'
    dev 'hmc7044-car', debug attr 'direct_reg_access', value :'0xE'
    root@analog:~# 

    -Michael

  • I ran this sequence of commands on the primary SOM:

    root@analog:~# iio_attr -D hmc7044-car
    dev 'hmc7044-car', debug attr 'status', value :'--- PLL1 ---
    Status:	Locked
    Using:	CLKIN1 @ 30720000 Hz
    PFD:	7680 kHz
    --- PLL2 ---
    Status:	Locked (Unsynchronized)
    Frequency:	2949120000 Hz (Autocal cap bank value: 13)
    SYSREF Status:	Invalid
    SYNC Status:	Unsynchronized
    Lock Status:	PLL1 & PLL2 Locked'
    dev 'hmc7044-car', debug attr 'direct_reg_access', value :'0x0'
    
    root@analog:~# iio_attr -d hmc7044-car reset_dividers_request 1
    0
    
    root@analog:~# iio_attr -d hmc7044-car reseed_request 1
    0
    
    root@analog:~# iio_attr -D hmc7044-car
    dev 'hmc7044-car', debug attr 'status', value :'--- PLL1 ---
    Status:	Locked
    Using:	CLKIN1 @ 30720000 Hz
    PFD:	7680 kHz
    --- PLL2 ---
    Status:	Locked (Synchronized)
    Frequency:	2949120000 Hz (Autocal cap bank value: 13)
    SYSREF Status:	Valid & Locked
    SYNC Status:	Synchronized
    Lock Status:	PLL1 & PLL2 Locked'
    dev 'hmc7044-car', debug attr 'direct_reg_access', value :'0x0'
    

    But I'm still stuck with the inverted SYNC lines on my HMC7044-ext board, which I think is the crux of the problem.

    Do you know which of the two signals in the oscilloscope screengrab above is the correct polarity?

  • 0
    •  Analog Employees 
    on May 4, 2021 7:15 PM in reply to mstone

    The one I'm seeing is the blue one. However with the patch I provided I would be happier with the yellow one, since it wouldn't have the show the dynamic driver enable behavior.

    I'm still confused about that you're seeing Yellow and Blue both on the _P outputs...

    We need to check this on the EVAL board where we have access to both pairs.

    -Michael

  • +1
    •  Analog Employees 
    on May 5, 2021 3:18 PM in reply to mhennerich

    Probed all the outputs on the eval board and it appears CLKOUT1,2,4,7,8,11,12 are 180deg out of phase from CLKOUT0,3,5,6,9,10,13 in CMOS mode. Please use only the following outputs as SYNC: CLKOUT0,3,5,6,9,10 and 13

     Added a note about this issue here.

    Thanks,

    Mihai

Reply Children