AD9265: Unrecognized CHIP_ID 0x64

I am trying to get the AD9265 to work. But I get following linux error message:

ad9467 spi1.0: Unrecognized CHIP_ID 0x64

Branch: 2018_r2:https://github.com/analogdevicesinc/linux/blob/2018_R2/drivers/iio/adc/ad9467.c

This is the dtb configuration:

&axi_quad_spi_0 {
	//reg = <0x80060000 0x10000>;		
	adc_ad9265: ad9265@0 { 
		compatible = "ad9467"; 
		reg = <0>; 
		spi-max-frequency = <10000000>; 
		clock-names = "ext_spi_clk", "s_axi_aclk";
		clocks = <&clk 71>, <&clk 71>;
		adi,spi-3wire-enable; 
	}; 
};

&fpga_axi {
	ad9265_dma: axi_dmac@80005000 {
		clock-names = "s_axi_aclk", "m_dest_axi_aclk", "fifo_wr_clk";
		clocks = <&clk 71>, <&clk 71>, <&misc_clk_0>;
		compatible = "xlnx,axi-dmac-1.0";
		interrupt-names = "irq";
		interrupt-parent = <&gic>;
		interrupts = <0 93 4>;
		reg = <0x80005000 0x1000>;
		#dma-cells = <1>;

		adi,channels {
			#size-cells = <0>;
			#address-cells = <1>;

			dma-channel@0 {
				reg = <0>;
				adi,source-bus-width = <16>;
				adi,source-bus-type = <2>;
				adi,destination-bus-width = <64>;
				adi,destination-bus-type = <0>;
			};
		};
	};

	cf_ad9467_core_0: cf-ad9467-core-lpc@80010000 {
		compatible = "xlnx,cf-ad9467-core-1.00.a";
		reg = <80010000 0x10000>;
		dmas = <&ad9265_dma 0>;
		dma-names = "rx";

		spibus-connected = <&adc_ad9265>;
	};	
}; 

Probably I need to set somewhere that I am using the AD9265 instead of the ad9467. But I don't know where.

Thanks for the assistance.

Best regards,

Jan