zcu102 adrv9002 ADI linux image creation using petalinux

Hi,

I am trying to bring up the ADI linux image in zcu102 BOARD using petalinux method as mentioned below

https://wiki.analog.com/resources/tools-software/linux-build/generic/petalinux

petalinux branch: 2019_R1

META-ADI-BRANCH : 2019_r2

bUILD IS SUCCESSFUL. But got ADRV9002 SPI configuration is failed.

when i do dmesg | grep "spi"

 5.246139] m25p80 spi0.0: found n25q512a, expected m25p80
[    5.251820] m25p80 spi0.0: n25q512a (131072 Kbytes)
[    5.256714] 4 fixed-partitions partitions found on MTD device spi0.0
[    5.263061] Creating 4 MTD partitions on "spi0.0":
[    5.267848] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
[    5.274064] 0x000000100000-0x000000600000 : "qspi-linux"
[    5.279764] 0x000000600000-0x000000620000 : "qspi-device-tree"
[    5.285982] 0x000000620000-0x000000c00000 : "qspi-rootfs"


[   12.522911] adrv9002 spi1.0: [ERROR]: Error number  3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_arm.c, in function adi_adrv9001_arm_StartStatus_Check, in line  183, variable name device.Error message Timed out waiting for ARM bootup to happen.
[   12.550190] adrv9002 spi1.0: adrv9002_digital_init, 2170: failed with "Timed out waiting for ARM bootup to happen" (3)
[   18.945843] adrv9002 spi1.0: [ERROR]: Error number  3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_arm.c, in function adi_adrv9001_arm_StartStatus_Check, in line  183, variable name device.Error message Timed out waiting for ARM bootup to happen.
[   18.973120] adrv9002 spi1.0: adrv9002_digital_init, 2170: failed with "Timed out waiting for ARM bootup to happen" (3)

can u please help why adrv9002 SPI configuration fail. Do i need to add any files to make it work?