ADRV9009-ZU11EG not booting from newest image (2019_R2)

I noticed a February 23 2021 SD image here and tried to use it on my ADRV9009-ZU11EG SOM.

I am not using an FMCOMMS8, so I copied BOOT.BIN and system.dtb from the "zynqmp-adrv9009-zu11eg-revb-adrv2crr-fmc-revb" folder into the top directory.  I also copied IMAGE from "zynqmp-common" to the top directory, as outlined in the README.txt located there.

However, with this SD in the carrier board, it fails to reach a command prompt.

It stops at approximately the same point during its process each time, but the problem doesn't always manifest at the same step.

Xilinx Zynq MP First Stage Boot Loader
Release 2019.1   Feb 19 2021  -  17:22:27


U-Boot 2018.01-21439-gd244ce5 (Jan 15 2021 - 15:07:45 +0000) Analog Devices Inc. ADR9009-ZU11EG, Build: jenkins-development-build_uboot-6

I2C:   ready
DRAM:  4 GiB
EL Level:       EL2
Chip ID:        zu11eg
MMC:   sdhci@ff170000: 0 (SD)
*** Warning - bad CRC, using default environment

In:    serial@ff010000
Out:   serial@ff010000
Err:   serial@ff010000
Bootmode: LVL_SHFT_SD_MODE1
Net:   ZYNQ GEM: ff0b0000, phyaddr 1, interface sgmii
i2c_mux_set: could not set mux: id: 5 chip: 74 channel: 0
I2C EEPROM MAC address read failed

Warning: ethernet@ff0b0000 (eth1) using random MAC address - 9a:f7:61:60:af:0b
eth1: ethernet@ff0b0000ZYNQ GEM: ff0e0000, phyaddr 0, interface rgmii-id
I2C EEPROM MAC address read failed

Warning: ethernet@ff0e0000 (eth0) using random MAC address - ba:53:4b:da:e7:b1
, eth0: ethernet@ff0e0000
Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc0 is current device
Device: sdhci@ff170000
Manufacturer ID: 3
OEM: 5344
Name: SB16G
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 14.8 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
reading uEnv.txt
376 bytes read in 19 ms (18.6 KiB/s)
Loaded environment from uEnv.txt
Importing environment from SD ...
Running uenvcmd ...
Copying Linux from SD to RAM...
** No boot file defined **
SF: Detected n25q512a with page size 512 Bytes, erase size 128 KiB, total 128 MiB
device 0 offset 0x2000000, size 0x20000
SF: 131072 bytes @ 0x2000000 Read: OK
reading system.dtb
65687 bytes read in 27 ms (2.3 MiB/s)
reading Image
29737472 bytes read in 1885 ms (15 MiB/s)
## Flattened Device Tree blob at 04000000
   Booting using the fdt blob at 0x4000000
   Loading Device Tree to 000000000ffec000, end 000000000ffff096 ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 4.19.0-ga6ef26d (jenkins@romlxbuild1.adlk.analog.com) (gcc version 8.2.0 (GCC)) #1105 SMP Fri Feb 19 16:51:27 GMT 2021
[    0.000000] Machine model: Analog Devices ADRV9009-ZU11EG Rev.B
[    0.000000] earlycon: cdns0 at MMIO 0x00000000ff010000 (options '115200n8')
[    0.000000] bootconsole [cdns0] enabled
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] cma: Reserved 256 MiB at 0x0000000070000000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.1
[    0.000000] random: get_random_bytes called from start_kernel+0x94/0x3f8 with crng_init=0
[    0.000000] percpu: Embedded 22 pages/cpu @(____ptrval____) s52504 r8192 d29416 u90112
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: enabling workaround for ARM erratum 845719
[    0.000000] Speculative Store Bypass Disable mitigation not required
[    0.000000] CPU features: detected: Kernel page table isolation (KPTI)
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1034240
[    0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait
[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
[    0.000000] software IO TLB: mapped [mem 0x6bfff000-0x6ffff000] (64MB)
[    0.000000] Memory: 3772240K/4194304K available (12796K kernel code, 1520K rwdata, 13828K rodata, 832K init, 326K bss, 159920K reserved, 262144K cma-reserved)
[    0.000000] rcu: Hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] arch_timer: cp15 timer(s) running at 33.33MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x7b0074340, max_idle_ns: 440795202884 ns
[    0.000003] sched_clock: 56 bits at 33MHz, resolution 30ns, wraps every 2199023255543ns
[    0.008232] Console: colour dummy device 80x25
[    0.012389] Calibrating delay loop (skipped), value calculated using timer frequency.. 66.66 BogoMIPS (lpj=133332)
[    0.022667] pid_max: default: 32768 minimum: 301
[    0.027349] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
[    0.033921] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
[    0.041633] ASID allocator initialised with 32768 entries
[    0.046413] rcu: Hierarchical SRCU implementation.
[    0.051419] EFI services will not be available.
[    0.055725] smp: Bringing up secondary CPUs ...
[    0.060368] Detected VIPT I-cache on CPU1
[    0.060394] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.060671] Detected VIPT I-cache on CPU2
[    0.060688] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[    0.060947] Detected VIPT I-cache on CPU3
[    0.060964] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[    0.061004] smp: Brought up 1 node, 4 CPUs
[    0.095586] SMP: Total of 4 processors activated.
[    0.100259] CPU features: detected: 32-bit EL0 Support
[    0.106656] CPU: All CPU(s) started at EL2
[    0.109437] alternatives: patching kernel code
[    0.114667] devtmpfs: initialized
[    0.123275] Registered cp15_barrier emulation handler
[    0.123322] Registered setend emulation handler
[    0.127290] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.136882] futex hash table entries: 1024 (order: 4, 65536 bytes)
[    0.148010] xor: measuring software checksum speed
[    0.187078]    8regs     :  2639.000 MB/sec
[    0.227104]    8regs_prefetch:  2280.000 MB/sec
[    0.267130]    32regs    :  3027.000 MB/sec
[    0.307157]    32regs_prefetch:  2565.000 MB/sec
[    0.307196] xor: using function: 32regs (3027.000 MB/sec)
[    0.311499] pinctrl core: initialized pinctrl subsystem
[    0.317229] NET: Registered protocol family 16
[    0.321374] audit: initializing netlink subsys (disabled)
[    0.326517] audit: type=2000 audit(0.272:1): state=initialized audit_enabled=0 res=1
[    0.334194] cpuidle: using governor menu
[    0.338189] vdso: 2 pages (1 code @ (____ptrval____), 1 data @ (____ptrval____))
[    0.345410] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.352756] DMA: preallocated 256 KiB pool for atomic allocations
[    0.369905] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.436894] raid6: int64x1  gen()   494 MB/s
[    0.504894] raid6: int64x1  xor()   501 MB/s
[    0.572959] raid6: int64x2  gen()   754 MB/s
[    0.640938] raid6: int64x2  xor()   666 MB/s
[    0.709007] raid6: int64x4  gen()  1089 MB/s
[    0.777017] raid6: int64x4  xor()   819 MB/s
[    0.845062] raid6: int64x8  gen()  1291 MB/s
[    0.913116] raid6: int64x8  xor()   844 MB/s
[    0.981164] raid6: neonx1   gen()   818 MB/s
[    1.049179] raid6: neonx1   xor()   978 MB/s
[    1.117220] raid6: neonx2   gen()  1255 MB/s
[    1.185277] raid6: neonx2   xor()  1305 MB/s
[    1.253307] raid6: neonx4   gen()  1644 MB/s
[    1.321350] raid6: neonx4   xor()  1577 MB/s
[    1.389413] raid6: neonx8   gen()  1724 MB/s
[    1.457425] raid6: neonx8   xor()  1622 MB/s
[    1.457461] raid6: using algorithm neonx8 gen() 1724 MB/s
[    1.461417] raid6: .... xor() 1622 MB/s, rmw enabled
[    1.466348] raid6: using neon recovery algorithm
[    1.471564] SCSI subsystem initialized
[    1.474803] usbcore: registered new interface driver usbfs
[    1.480131] usbcore: registered new interface driver hub
[    1.485409] usbcore: registered new device driver usb
[    1.490536] media: Linux media interface: v0.10
[    1.494913] videodev: Linux video capture interface: v2.00
[    1.500392] pps_core: LinuxPPS API ver. 1 registered
[    1.505274] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    1.514367] PTP clock support registered
[    1.518262] EDAC MC: Ver: 3.0.0
[    1.521713] zynqmp-ipi-mbox mailbox@ff990400: Probed ZynqMP IPI Mailbox driver.
[    1.529156] jesd204: created con: id=0, topo=0, link=0, /fpga-axi@0/axi-jesd204-tx@84a30000 <-> /fpga-axi@0/axi-adrv9009-tx-hpc@84a04000
[    1.540833] jesd204: created con: id=1, topo=0, link=0, /fpga-axi@0/axi-adxcvr-tx@84a20000 <-> /fpga-axi@0/axi-jesd204-tx@84a30000
[    1.552511] jesd204: created con: id=2, topo=0, link=0, /amba/spi@ff040000/hmc7044@0 <-> /fpga-axi@0/axi-adxcvr-tx@84a20000
[    1.563581] jesd204: created con: id=3, topo=0, link=2, /fpga-axi@0/axi-adxcvr-rx-os@84a60000 <-> /fpga-axi@0/axi-jesd204-rx@84a70000
[    1.575524] jesd204: created con: id=4, topo=0, link=2, /amba/spi@ff040000/hmc7044@0 <-> /fpga-axi@0/axi-adxcvr-rx-os@84a60000
[    1.586850] jesd204: created con: id=5, topo=0, link=1, /fpga-axi@0/axi-adxcvr-rx@84a40000 <-> /fpga-axi@0/axi-jesd204-rx@84a50000
[    1.598527] jesd204: created con: id=6, topo=0, link=1, /amba/spi@ff040000/hmc7044@0 <-> /fpga-axi@0/axi-adxcvr-rx@84a40000
[    1.609604] jesd204: created con: id=7, topo=0, link=1, /amba/spi@ff040000/hmc7044-car@3 <-> /amba/spi@ff040000/hmc7044@0
[    1.620498] jesd204: created con: id=8, topo=0, link=2, /amba/spi@ff040000/hmc7044-car@3 <-> /amba/spi@ff040000/hmc7044@0
[    1.631398] jesd204: created con: id=9, topo=0, link=0, /amba/spi@ff040000/hmc7044-car@3 <-> /amba/spi@ff040000/hmc7044@0
[    1.642313] jesd204: created con: id=10, topo=0, link=1, /fpga-axi@0/axi-jesd204-rx@84a50000 <-> /amba/spi@ff040000/adrv9009-phy-b@0
[    1.654154] jesd204: created con: id=11, topo=0, link=2, /fpga-axi@0/axi-jesd204-rx@84a70000 <-> /amba/spi@ff040000/adrv9009-phy-b@0
[    1.666005] jesd204: created con: id=12, topo=0, link=0, /fpga-axi@0/axi-adrv9009-tx-hpc@84a04000 <-> /amba/spi@ff040000/adrv9009-phy-b@0
[    1.678323] jesd204: created con: id=13, topo=0, link=1, /amba/spi@ff040000/adrv9009-phy-b@0 <-> /amba/spi@ff040000/adrv9009-phy@0
[    1.689979] jesd204: created con: id=14, topo=0, link=2, /amba/spi@ff040000/adrv9009-phy-b@0 <-> /amba/spi@ff040000/adrv9009-phy@0
[    1.701665] jesd204: created con: id=15, topo=0, link=0, /amba/spi@ff040000/adrv9009-phy-b@0 <-> /amba/spi@ff040000/adrv9009-phy@0
[    1.713327] jesd204: /amba/spi@ff040000/adrv9009-phy@0: JESD204[0] transition uninitialized -> initialized
[    1.722911] jesd204: /amba/spi@ff040000/adrv9009-phy@0: JESD204[1] transition uninitialized -> initialized
[    1.732512] jesd204: /amba/spi@ff040000/adrv9009-phy@0: JESD204[2] transition uninitialized -> initialized
[    1.742113] jesd204: found 11 devices and 1 topologies
[    1.747250] FPGA manager framework
[    1.750741] Advanced Linux Sound Architecture Driver Initialized.
[    1.756890] Bluetooth: Core ver 2.22
[    1.760204] NET: Registered protocol family 31
[    1.764604] Bluetooth: HCI device and connection manager initialized
[    1.770921] Bluetooth: HCI socket layer initialized
[    1.775763] Bluetooth: L2CAP socket layer initialized
[    1.780789] Bluetooth: SCO socket layer initialized
[    1.786059] clocksource: Switched to clocksource arch_sys_counter
[    1.791771] VFS: Disk quotas dquot_6.6.0
[    1.795606] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    1.806597] NET: Registered protocol family 2
[    1.807045] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes)
[    1.814555] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
[    1.821874] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
[    1.828631] TCP: Hash tables configured (established 32768 bind 32768)
[    1.834812] UDP hash table entries: 2048 (order: 4, 65536 bytes)
[    1.840788] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
[    1.847264] NET: Registered protocol family 1
[    1.851651] RPC: Registered named UNIX socket transport module.
[    1.857338] RPC: Registered udp transport module.
[    1.862005] RPC: Registered tcp transport module.
[    1.866676] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    1.873694] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[    1.880306] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[    1.888607] Initialise system trusted keyrings
[    1.892335] workingset: timestamp_bits=62 max_order=20 bucket_order=0
[    1.899318] NFS: Registering the id_resolver key type
[    1.903709] Key type id_resolver registered
[    1.907852] Key type id_legacy registered
[    1.911833] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    1.918500] jffs2: version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.
[    2.898856] NET: Registered protocol family 38
[    2.951365] Key type asymmetric registered
[    2.951401] Asymmetric key parser 'x509' registered
[    2.954703] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[    2.962021] io scheduler noop registered
[    2.965911] io scheduler deadline registered
[    2.970165] io scheduler cfq registered (default)
[    2.974821] io scheduler mq-deadline registered
[    2.979318] io scheduler kyber registered
[    3.008099] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[    3.011927] cacheinfo: Unable to detect cache hierarchy for CPU 0
[    3.018542] brd: module loaded
[    3.021987] loop: module loaded
[    3.022193] Registered mathworks_ip class
[    3.025672] mtdoops: mtd device (mtddev=name/number) must be supplied
[    3.032684] libphy: Fixed MDIO Bus: probed
[    3.036584] tun: Universal TUN/TAP device driver, 1.6
[    3.040568] CAN device driver interface
[    3.045141] usbcore: registered new interface driver asix
[    3.049683] usbcore: registered new interface driver ax88179_178a
[    3.055714] usbcore: registered new interface driver cdc_ether
[    3.061506] usbcore: registered new interface driver net1080
[    3.067131] usbcore: registered new interface driver cdc_subset
[    3.073011] usbcore: registered new interface driver zaurus
[    3.078555] usbcore: registered new interface driver cdc_ncm
[    3.084784] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    3.090639] ehci-pci: EHCI PCI platform driver
[    3.095289] usbcore: registered new interface driver uas
[    3.100364] usbcore: registered new interface driver usb-storage
[    3.106345] usbcore: registered new interface driver usbserial_generic
[    3.112798] usbserial: USB Serial support registered for generic
[    3.118768] usbcore: registered new interface driver ftdi_sio
[    3.124476] usbserial: USB Serial support registered for FTDI USB Serial Device
[    3.131744] usbcore: registered new interface driver upd78f0730
[    3.137621] usbserial: USB Serial support registered for upd78f0730
[    3.144861] i2c /dev entries driver
[    3.149006] usbcore: registered new interface driver uvcvideo
[    3.153006] USB Video Class driver (1.1.1)
[    3.157537] axi_fan_control_driver 80000000.axi-fan-control: clk_get failed with -517
[    3.165565] Bluetooth: HCI UART driver ver 2.3
[    3.169276] Bluetooth: HCI UART protocol H4 registered
[    3.174373] Bluetooth: HCI UART protocol BCSP registered
[    3.179665] Bluetooth: HCI UART protocol LL registered
[    3.184750] Bluetooth: HCI UART protocol ATH3K registered
[    3.190128] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    3.196378] Bluetooth: HCI UART protocol Intel registered
[    3.201719] Bluetooth: HCI UART protocol QCA registered
[    3.206931] usbcore: registered new interface driver bcm203x
[    3.212540] usbcore: registered new interface driver bpa10x
[    3.218076] usbcore: registered new interface driver bfusb
[    3.223529] usbcore: registered new interface driver btusb
[    3.228952] Bluetooth: Generic Bluetooth SDIO driver ver 0.1
[    3.234613] usbcore: registered new interface driver ath3k
[    3.240314] EDAC MC0: Giving out device to module 1 controller synps_ddr_controller: DEV synps_edac (INTERRUPT)
[    3.250218] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
[    3.262784] sdhci: Secure Digital Host Controller Interface driver
[    3.268310] sdhci: Copyright(c) Pierre Ossman
[    3.272633] sdhci-pltfm: SDHCI platform and OF driver helper
[    3.278606] ledtrig-cpu: registered to indicate activity on CPUs
[    3.284266] zynqmp_firmware_probe Platform Management API v1.1
[    3.290028] zynqmp_firmware_probe Trustzone version v1.0
[    3.297834] zynqmp-pinctrl firmware:zynqmp-firmware:pinctrl: zynqmp pinctrl initialized
[    3.324173] zynqmp_clk_mux_get_parent() getparent failed for clock: lpd_wdt, ret = -22
[    3.326860] alg: No test for xilinx-zynqmp-aes (zynqmp-aes)
[    3.332049] zynqmp_aes zynqmp_aes: AES Successfully Registered
[    3.332049]
[    3.339499] alg: No test for xilinx-keccak-384 (zynqmp-keccak-384)
[    3.345682] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa)
[    3.351200] usbcore: registered new interface driver usbhid
[    3.356544] usbhid: USB HID core driver
[    3.367788] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
[    3.369040] usbcore: registered new interface driver snd-usb-audio
[    3.376456] pktgen: Packet Generator for packet performance testing. Version: 2.75
[    3.382594] Initializing XFRM netlink socket
[    3.386555] NET: Registered protocol family 10
[    3.391257] Segment Routing with IPv6
[    3.394610] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    3.400728] NET: Registered protocol family 17
[    3.404833] NET: Registered protocol family 15
[    3.409248] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[    3.422508] can: controller area network core (rev 20170425 abi 9)
[    3.428293] NET: Registered protocol family 29
[    3.432680] can: raw protocol (rev 20170425)
[    3.436917] can: broadcast manager protocol (rev 20170425 t)
[    3.442541] can: netlink gateway (rev 20170425) max_hops=1
[    3.448053] Bluetooth: RFCOMM TTY layer initialized
[    3.452839] Bluetooth: RFCOMM socket layer initialized
[    3.457946] Bluetooth: RFCOMM ver 1.11
[    3.461660] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    3.466932] Bluetooth: BNEP filters: protocol multicast
[    3.472124] Bluetooth: BNEP socket layer initialized
[    3.477052] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    3.482936] Bluetooth: HIDP socket layer initialized
[    3.487957] 9pnet: Installing 9P2000 support
[    3.492111] NET: Registered protocol family 36
[    3.496527] Key type dns_resolver registered
[    3.501155] registered taskstats version 1
[    3.504824] Loading compiled-in X.509 certificates
[    3.509863] Btrfs loaded, crc32c=crc32c-generic
[    3.519975] ff010000.serial: ttyPS0 at MMIO 0xff010000 (irq = 23, base_baud = 6249999) is a xuartps
[    3.529068] console [ttyPS0] enabled
[    3.529068] console [ttyPS0] enabled
[    3.532666] bootconsole [cdns0] disabled
[    3.532666] bootconsole [cdns0] disabled
[    3.541042] GPIO line 13 (ulpi-phy-reset) hogged as output/high
[    3.550152] of-fpga-region fpga-full: FPGA Region probed
[    3.557058] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed
[    3.563747] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:8 protocol:4 pll_locked:yes
[    3.573182] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Failed to get required clock freq
[    3.583289] xilinx-dp-snd-codec: probe of fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0 failed with error -22
[    3.593386] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed
[    3.601468] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed
[    3.609535] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered
[    3.619604] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000
[    3.626636] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    3.633241] [drm] No driver support for vblank timestamp query.
[    3.639208] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008dc2e70)
[    4.726044] [drm] Cannot find any crtc or sizes
[    4.730830] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0
[    4.738928] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed
[    4.748426] adrv9009 spi1.0: adrv9009_probe : enter
[    4.754181] adrv9009 spi1.1: adrv9009_probe : enter
[    4.806864] jesd204: /amba/spi@ff040000/hmc7044-car@3,jesd204:3,parent=spi1.3: Using as SYSREF provider
[    4.865722] m25p80 spi0.0: SPI-NOR-UniqueID 104000a877040004f4ff1d00ca44718d15
[    4.874534] m25p80 spi0.0: n25q512a (131072 Kbytes)
[    4.879424] 4 fixed-partitions partitions found on MTD device spi0.0
[    4.885772] Creating 4 MTD partitions on "spi0.0":
[    4.890553] 0x000000000000-0x000002000000 : "qspi-fsbl-uboot"
[    4.896725] 0x000002000000-0x000002020000 : "qspi-uboot-env"
[    4.902723] 0x000002020000-0x000002100000 : "qspi-nvmfs"
[    4.908372] 0x000002100000-0x000007f00000 : "qspi-linux"
[    4.914443] macb ff0b0000.ethernet: Not enabling partial store and forward
[    4.921810] libphy: MACB_mii_bus: probed
[    4.971709] macb ff0e0000.ethernet: Not enabling partial store and forward
[    4.979046] libphy: MACB_mii_bus: probed
[    5.058482] Marvell 88E1510 ff0e0000.ethernet-ffffffff:00: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:00, irq=POLL)
[    5.072387] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 13 (00:e0:22:fe:0b:d5)
[    5.082532] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
[    5.089055] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM
[    5.095598] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM
[    5.102083] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM
[    5.110014] dwc3 fe200000.dwc3: Failed to get clk 'ref': -2
[    5.115871] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:0 protocol:3 pll_locked:yes
[    5.125936] OF: graph: no port node found in /amba/zynqmp_phy@fd400000/lane1
[    5.137131] random: fast init done
[    5.236650] at24 0-002c: 2048 byte 24c16 EEPROM, writable, 1 bytes/write
[    5.243393] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 15
[    5.250713] i2c i2c-1: Added multiplexed i2c bus 3
[    5.255659] i2c i2c-1: Added multiplexed i2c bus 4
[    5.260596] i2c i2c-1: Added multiplexed i2c bus 5
[    5.291446] i2c i2c-1: Added multiplexed i2c bus 6
[    5.322141] i2c i2c-1: Added multiplexed i2c bus 7
[    5.354137] i2c i2c-1: Added multiplexed i2c bus 8
[    5.359079] i2c i2c-1: Added multiplexed i2c bus 9
[    5.364009] i2c i2c-1: Added multiplexed i2c bus 10
[    5.368879] pca954x 1-0070: registered 8 multiplexed busses for I2C switch pca9548
[    5.376474] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 16
[    5.383006] axi_fan_control_driver 80000000.axi-fan-control: Failed to initialize device
[    5.391131] axi_fan_control_driver: probe of 80000000.axi-fan-control failed with error -22
[    5.399927] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer with timeout 60s
[    5.407416] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 1333333 KHz
[    5.414811] cpu cpu0: dev_pm_opp_set_rate: failed to find current OPP for freq 1333333320 (-34)
[    5.423542] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 1199999 KHz
[    5.432072] cpu cpu0: dev_pm_opp_set_rate: failed to find current OPP for freq 1333333320 (-34)
[    5.470037] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit
[    5.487293] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered
[    5.497469] adrv9009 spi1.0: adrv9009_probe : enter
[    5.503039] adrv9009 spi1.1: adrv9009_probe : enter
[    5.556253] macb ff0b0000.ethernet: Not enabling partial store and forward
[    5.563617] libphy: MACB_mii_bus: probed
[    5.594772] mmc0: new high speed SDHC card at address e624
[    5.600731] mmcblk0: mmc0:e624 SB16G 14.8 GiB
[    5.609118]  mmcblk0: p1 p2 p3
[    5.646450] Marvell 88E1510 ff0e0000.ethernet-ffffffff:01: attached PHY driver [Marvell 88E1510] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:01, irq=POLL)
[    5.660361] macb ff0b0000.ethernet eth1: Cadence GEM rev 0x50070106 at 0xff0b0000 irq 12 (9a:f7:61:60:af:0b)
[    5.672964] axi_adxcvr 84a40000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.01.a) using CPLL on GTH4 at 0x84A40000. Number of lanes: 4.
[    5.686150] axi_adxcvr 84a60000.axi-adxcvr-rx-os: AXI-ADXCVR-RX (17.01.a) using CPLL on GTH4 at 0x84A60000. Number of lanes: 4.
[    5.698427] axi_adxcvr 84a20000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.01.a) using QPLL on GTH4 at 0x84A20000. Number of lanes: 8.
[    5.712023] asoc-simple-card talise_sound: adau-hifi <-> 82000000.axi-i2s-adi mapping ok
[    5.723495] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered
[    5.733678] adrv9009 spi1.0: adrv9009_probe : enter
[    5.743360] adrv9009 spi1.1: adrv9009_probe : enter
[    5.773815] cf_axi_adc 84a00000.axi-adrv9009-rx-hpc: ADI AIM (10.01.b) at 0x84A00000 mapped to 0x(____ptrval____), probed ADC ADRV9009-X2 as MASTER
[    5.806725] cf_axi_dds 84a04000.axi-adrv9009-tx-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x84A04000 mapped to 0x(____ptrval____), probed DDS ADRV9009-X2
[    5.821530] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition initialized -> probed
[    5.832662] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition initialized -> probed
[    5.843783] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition initialized -> probed
[    5.854910] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition probed -> idle
[    5.865422] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition probed -> idle
[    5.875937] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition probed -> idle
[    5.886462] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition idle -> device_init
[    5.897407] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition idle -> device_init
[    5.908353] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition idle -> device_init
[    5.919309] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition device_init -> link_init
[    5.930687] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition device_init -> link_init
[    5.942066] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition device_init -> link_init
[    5.953459] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition link_init -> link_supported
[    5.965104] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition link_init -> link_supported
[    5.976743] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition link_init -> link_supported
[    5.988424] [drm] Cannot find any crtc or sizes
[    5.993361] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition link_supported -> link_pre_setup
[    6.005446] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition link_supported -> link_pre_setup
[    6.017524] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition link_supported -> link_pre_setup
[    6.050042] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition link_pre_setup -> clk_sync_stage1
[    6.062211] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition link_pre_setup -> clk_sync_stage1
[    6.074378] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition link_pre_setup -> clk_sync_stage1
[    6.098045] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition clk_sync_stage1 -> clk_sync_stage2
[    6.110297] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition clk_sync_stage1 -> clk_sync_stage2
[    6.122543] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition clk_sync_stage1 -> clk_sync_stage2
[    6.134871] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition clk_sync_stage2 -> clk_sync_stage3
[    6.147127] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition clk_sync_stage2 -> clk_sync_stage3
[    6.159372] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition clk_sync_stage2 -> clk_sync_stage3
[    6.171625] jesd204: /fpga-axi@0/axi-jesd204-rx@84a50000,jesd204:5,parent=84a50000.axi-jesd204-rx: Possible instantiation for multiple chips; HDL lanes 4, Link[1] lanes 2
[    6.186836] jesd204: /fpga-axi@0/axi-jesd204-rx@84a70000,jesd204:7,parent=84a70000.axi-jesd204-rx: Possible instantiation for multiple chips; HDL lanes 4, Link[2] lanes 2
[    6.202105] jesd204: /fpga-axi@0/axi-jesd204-tx@84a30000,jesd204:9,parent=84a30000.axi-jesd204-tx: Possible instantiation for multiple chips; HDL lanes 8, Link[0] lanes 4
[    6.218482] adrv9009 spi1.1: ADIHAL_resetHw
[    6.541066] adrv9009 spi1.0: ADIHAL_resetHw
[    6.863423] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition clk_sync_stage3 -> link_setup
[    6.875241] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition clk_sync_stage3 -> link_setup
[    6.887059] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition clk_sync_stage3 -> link_setup
[    6.899070] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition link_setup -> opt_setup_stage1
[    6.910974] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition link_setup -> opt_setup_stage1
[    6.922873] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition link_setup -> opt_setup_stage1
[    7.010396] random: crng init done
[    9.964982] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition opt_setup_stage1 -> opt_setup_stage2
[    9.977410] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition opt_setup_stage1 -> opt_setup_stage2
[    9.989835] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition opt_setup_stage1 -> opt_setup_stage2
[   10.002387] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition opt_setup_stage2 -> opt_setup_stage3
[   10.014818] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition opt_setup_stage2 -> opt_setup_stage3
[   10.027246] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition opt_setup_stage2 -> opt_setup_stage3
[   10.039876] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition opt_setup_stage3 -> opt_setup_stage4
[   10.052298] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition opt_setup_stage3 -> opt_setup_stage4
[   10.064718] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition opt_setup_stage3 -> opt_setup_stage4
[   15.278922] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition opt_setup_stage4 -> opt_setup_stage5
[   15.291349] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition opt_setup_stage4 -> opt_setup_stage5
[   15.303775] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition opt_setup_stage4 -> opt_setup_stage5
[   15.319631] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition opt_setup_stage5 -> clocks_enable
[   15.331795] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition opt_setup_stage5 -> clocks_enable
[   15.343954] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition opt_setup_stage5 -> clocks_enable
[   15.356412] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition clocks_enable -> link_enable
[   15.368140] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition clocks_enable -> link_enable
[   15.379873] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition clocks_enable -> link_enable
[   15.392056] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition link_enable -> link_running
[   15.403702] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition link_enable -> link_running
[   15.415348] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition link_enable -> link_running
[   15.528215] adrv9009 spi1.1: adrv9009_info: adrv9009 Rev 192, Firmware 6.0.2 API version: 3.6.0.5 successfully initialized via jesd204-fsm
[   15.641863] adrv9009 spi1.0: adrv9009_info: adrv9009-x2 Rev 192, Firmware 6.0.2 API version: 3.6.0.5 successfully initialized via jesd204-fsm
[   15.654552] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[0] transition link_running -> opt_post_running_stage
[   15.667150] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[1] transition link_running -> opt_post_running_stage
[   15.679746] jesd204: /amba/spi@ff040000/adrv9009-phy@0,jesd204:0,parent=spi1.0: JESD204[2] transition link_running -> opt_post_running_stage
[   15.692742] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered
[   15.702979] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered
[   15.715545] input: gpio_keys as /devices/platform/gpio_keys/input/input0
[   15.722466] hctosys: unable to open rtc device (rtc0)
[   15.727513] of_cfs_init
[   15.729964] of_cfs_init: OK
[   15.732924] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[   15.741034] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: ASoC: CPU DAI (null) not registered
[   15.858728] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[   15.866002] ALSA device list:
[   15.868960]   #0: ADRV9009 ZU11EG ADAU1761
[   15.873390] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[   15.881993] cfg80211: failed to load regulatory.db
[   15.909216] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[   15.917317] VFS: Mounted root (ext4 filesystem) on device 179:2.
[   15.933347] devtmpfs: mounted
[   15.936471] Freeing unused kernel memory: 832K
[   15.942059] Run /sbin/init as init process
[   16.484362] systemd[1]: System time before build time, advancing clock.
[   16.522141] systemd[1]: systemd 241 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD -IDN2 +IDN -PCRE2 default-hierarchy=hybrid)
[   16.543830] systemd[1]: Detected architecture arm64.

Welcome to Kuiper GNU/Linux 10 (buster)!

[   16.566572] systemd[1]: Set hostname to <analog>.
[   16.579183] systemd[1]: Initializing machine ID from random generator.
[   16.786309] systemd[1]: File /lib/systemd/system/systemd-journald.service:12 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
[   16.803355] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
[   16.941603] systemd[1]: /etc/systemd/system/tof-server.service:1: Assignment outside of section. Ignoring.
[   16.951284] systemd[1]: /etc/systemd/system/tof-server.service:2: Assignment outside of section. Ignoring.
[   17.108297] systemd[1]: Listening on udev Kernel Socket.
[  OK  ] Listening on udev Kernel Socket.
[   17.130448] systemd[1]: Created slice User and Session Slice.
[  OK  ] Created slice User and Session Slice.
[  OK  ] Listening on Journal Socket.
         Starting Restore / save the current clock...
         Starting Load Kernel Modules...
         Mounting Huge Pages File System...
[  OK  ] Listening on Journal Socket (/dev/log).
[  OK  ] Created slice system-serial\x2dgetty.slice.
[  OK  ] Listening on initctl Compatibility Named Pipe.
[  OK  ] Started Forward Password R…uests to Wall Directory Watch.
[  OK  ] Created slice system-getty.slice.
[  OK  ] Listening on Journal Audit Socket.
[  OK  ] Reached target Swap.
         Mounting Kernel Debug File System...
         Mounting RPC Pipe File System...
[  OK  ] Listening on udev Control Socket.
         Starting udev Coldplug all Devices...
         Starting Set the console keyboard layout...
[  OK  ] Listening on Syslog Socket.
[  OK  ] Listening on fsck to fsckd communication Socket.
[  OK  ] Reached target Slices.
[  OK  ] Created slice system-systemd\x2dfsck.slice.
         Mounting POSIX Message Queue File System...
         Starting Journal Service...
[  OK  ] Started Restore / save the current clock.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[  OK  ] Mounted Huge Pages File System.
[  OK  ] Mounted Kernel Debug File System.
[  OK  ] Mounted RPC Pipe File System.
[  OK  ] Started Journal Service.
[  OK  ] Mounted POSIX Message Queue File System.
         Starting Apply Kernel Variables...
         Mounting Kernel Configuration File System...
         Starting Remount Root and Kernel File Systems...
[  OK  ] Started Set the console keyboard layout.
[  OK  ] Started Apply Kernel Variables.
[  OK  ] Mounted Kernel Configuration File System.
[  OK  ] Started udev Coldplug all Devices.
         Starting Helper to synchronize boot up for ifupdown...
[  OK  ] Started Helper to synchronize boot up for ifupdown.
[  OK  ] Started Remount Root and Kernel File Systems.
         Starting Flush Journal to Persistent Storage...
         Starting Load/Save Random Seed...
         Starting Create System Users...
[  OK  ] Started Load/Save Random Seed.
[  OK  ] Started Flush Journal to Persistent Storage.
[  OK  ] Started Create System Users.
         Starting Create Static Device Nodes in /dev...
[  OK  ] Started Create Static Device Nodes in /dev.
         Starting udev Kernel Device Manager...
[  OK  ] Reached target Local File Systems (Pre).
[  OK  ] Started udev Kernel Device Manager.
         Starting Show Plymouth Boot Screen...
[  OK  ] Started Show Plymouth Boot Screen.
[  OK  ] Reached target Local Encrypted Volumes.
[  OK  ] Started Forward Password R…s to Plymouth Directory Watch.
[  OK  ] Found device /dev/ttyPS0.
[  OK  ] Found device /dev/disk/by-partuuid/18f1f9d5-01.
         Starting File System Check…isk/by-partuuid/18f1f9d5-01...
         Starting Load Kernel Modules...
[  OK  ] Started File System Check Daemon to report status.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[  OK  ] Found device /dev/ttyS0.
[  OK  ] Started File System Check …/disk/by-partuuid/18f1f9d5-01.
         Mounting /boot...
[  OK  ] Listening on Load/Save RF …itch Status /dev/rfkill Watch.
[  OK  ] Mounted /boot.
[  OK  ] Reached target Local File Systems.
         Starting Preprocess NFS configuration...
         Starting Set console font and keymap...
         Starting Raise network interfaces...
         Starting Create Volatile Files and Directories...
         Starting Tell Plymouth To Write Out Runtime Data...
[  OK  ] Started Preprocess NFS configuration.
[  OK  ] Reached target NFS client services.
[  OK  ] Reached target Remote File Systems (Pre).
[  OK  ] Reached target Remote File Systems.
[  OK  ] Started Tell Plymouth To Write Out Runtime Data.
[  OK  ] Started Set console font and keymap.
[  OK  ] Started Create Volatile Files and Directories.
         Starting Update UTMP about System Boot/Shutdown...
         Starting Network Time Synchronization...
[  OK  ] Started Update UTMP about System Boot/Shutdown.
[  OK  ] Started Network Time Synchronization.
[  OK  ] Reached target System Initialization.
[  OK  ] Listening on CUPS Scheduler.
[  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Started CUPS Scheduler.
[  OK  ] Reached target Paths.
[  OK  ] Listening on triggerhappy.socket.
[  OK  ] Listening on GPS (Global P…ioning System) Daemon Sockets.
[  OK  ] Listening on D-Bus System Message Bus Socket.
[  OK  ] Reached target Sockets.
[  OK  ] Reached target Basic System.
[  OK  ] Started tof-server.service.
         Starting dphys-swapfile - …unt, and delete a swap file...
         Starting triggerhappy global hotkey daemon...
         Starting LSB: Switch to on…nless shift key is pressed)...
         Starting System Logging Service...
[  OK  ] Started CUPS Scheduler.
[  OK  ] Started Regular background program processing daemon.
         Starting Disk Manager...
         Starting LSB: Resize the r…ilesystem to fill partition...
         Starting Check for Raspberry Pi EEPROM updates...
         Starting rng-tools.service...
         Starting Login Service...
[  OK  ] Started Manage Sound Card State (restore and store).
         Starting Save/Restore Sound Card State...
         Starting Modem Manager...
[  OK  ] Started D-Bus System Message Bus.
         Starting WPA supplicant...
         Starting Avahi mDNS/DNS-SD Stack...
         Starting dhcpcd on all interfaces...
         Starting Regenerate SSH host keys...
[  OK  ] Reached target System Time Synchronized.
[  OK  ] Started Daily apt download activities.
[  OK  ] Started Daily rotation of log files.
[  OK  ] Started Daily man-db regeneration.
[  OK  ] Started Daily apt upgrade and clean activities.
[  OK  ] Reached target Timers.
[  OK  ] Started Login Service.
[  OK  ] Started triggerhappy global hotkey daemon.
[  OK  ] Started System Logging Service.
[FAILED] Failed to start Check for Raspberry Pi EEPROM updates.
See 'systemctl status rpi-eeprom-update.service' for details.
[FAILED] Failed to start rng-tools.service.
See 'systemctl status rng-tools.service' for details.
[  OK  ] Started Save/Restore Sound Card State.
[  OK  ] Started dhcpcd on all interfaces.
[  OK  ] Started Avahi mDNS/DNS-SD Stack.
[  OK  ] Started WPA supplicant.
[  OK  ] Reached target Sleep.
         Starting Suspend...
         Starting Authorization Manager...
[  OK  ] Started Make remote CUPS printers available locally.
[  OK  ] Reached target Sound Card.

After this there are no new messages to the terminal.



replaced ambiguous wording
[edited by: mstone at 12:02 AM (GMT -5) on 5 Mar 2021]
Parents Reply Children
No Data