ADRV9002 + ZCU102 boot error

Hi,

I would like to use ADRV9002 evaluation board with ZCU102 FPGA board. My goal is that evaluate modulation/demodulation algorithm due to Matlab and libiio(use Proto typing Platform).

When I setup the evaluation kit, I didn't connect to FPGA from PC.

I attached log file. There are some setup errors...

*********************

[    8.484330] adrv9002 spi1.0: adrv9002_setup, 1911: failed with "Command error" (13313)

[    8.492260] adrv9002: probe of spi1.0 failed with error -14

*********************

It has ethernet connection. But, I didn't connect to evaluation software on FPGA.

I would like to have any advice for setup ADRV9002 + ZCU102.

Best regards,

Jun

5023.adrv9002_log.txt
Xilinx Zynq MP First Stage Boot Loader
Release 2019.1   Jun 12 2020  -  15:24:33
NOTICE:  ATF running on XCZU9EG/silicon v4/RTL5.1 at 0xfffea000
NOTICE:  BL31: Secure code at 0x0
NOTICE:  BL31: Non secure code at 0x8000000
NOTICE:  BL31: v2.0(release):xilinx-v2019.2
NOTICE:  BL31: Built : 10:19:24, Jan 13 2020
PMUFW:  v1.1


U-Boot 2018.01-21436-gbba91bc203 (Jan 13 2020 - 10:50:58 +0200) Xilinx ZynqMP ZCU102 rev1.0, Build: jenkins-development-build_uboot-1

I2C:   ready
DRAM:  4 GiB
EL Level:       EL2
Chip ID:        zu9eg
MMC:   sdhci@ff170000: 0 (SD)
*** Warning - bad CRC, using default environment

In:    serial@ff000000
Out:   serial@ff000000
Err:   serial@ff000000
Bootmode: LVL_SHFT_SD_MODE1
Net:   ZYNQ GEM: ff0e0000, phyaddr c, interface rgmii-id

Warning: ethernet@ff0e0000 (eth0) using random MAC address - 8a:85:2c:76:ce:da
eth0: ethernet@ff0e0000
Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc0 is current device
Device: sdhci@ff170000
Manufacturer ID: 3
OEM: 5344
Name: SC32G
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 29.7 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
reading uEnv.txt
392 bytes read in 11 ms (34.2 KiB/s)
Loaded environment from uEnv.txt
Importing environment from SD ...
Running uenvcmd ...
Copying Linux from SD to RAM...
** No boot file defined **
reading system.dtb
42007 bytes read in 29 ms (1.4 MiB/s)
reading Image
32354816 bytes read in 2139 ms (14.4 MiB/s)
## Flattened Device Tree blob at 04000000
   Booting using the fdt blob at 0x4000000
   Loading Device Tree to 000000000fff2000, end 000000000ffff416 ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 4.19.0-29506-g6374347742fc (nunojsa@nunojsa-N551JK) (gcc version 8.4.0 (Ubuntu/Linaro 8.4.0-3ubuntu1)) #84 SMP Fri Jun 19 14:16:29 CEST 2020
[    0.000000] Machine model: ZynqMP ZCU102 Rev1.0
[    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
[    0.000000] bootconsole [cdns0] enabled
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] cma: Reserved 256 MiB at 0x0000000070000000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.1
[    0.000000] random: get_random_bytes called from start_kernel+0x94/0x3f8 with crng_init=0
[    0.000000] percpu: Embedded 22 pages/cpu @(____ptrval____) s52504 r8192 d29416 u90112
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: enabling workaround for ARM erratum 845719
[    0.000000] Speculative Store Bypass Disable mitigation not required
[    0.000000] CPU features: detected: Kernel page table isolation (KPTI)
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1034240
[    0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlycon rootfstype=ext4 rootwait cpuidle.off=1 root=/dev/mmcblk0p2 rw rootwait
[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
[    0.000000] software IO TLB: mapped [mem 0x6bfff000-0x6ffff000] (64MB)
[    0.000000] Memory: 3769828K/4194304K available (14844K kernel code, 1452K rwdata, 14436K rodata, 832K init, 329K bss, 162332K reserved, 262144K cma-reserved)
[    0.000000] rcu: Hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8de2d3, max_idle_ns: 440795206112 ns
[    0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511101ns
[    0.008263] Console: colour dummy device 80x25
[    0.012391] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.98 BogoMIPS (lpj=399960)
[    0.022756] pid_max: default: 32768 minimum: 301
[    0.027450] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
[    0.034012] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
[    0.041796] ASID allocator initialised with 32768 entries
[    0.046510] rcu: Hierarchical SRCU implementation.
[    0.051548] EFI services will not be available.
[    0.055832] smp: Bringing up secondary CPUs ...
[    0.060488] Detected VIPT I-cache on CPU1
[    0.060518] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.060826] Detected VIPT I-cache on CPU2
[    0.060845] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[    0.061132] Detected VIPT I-cache on CPU3
[    0.061151] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[    0.061194] smp: Brought up 1 node, 4 CPUs
[    0.095682] SMP: Total of 4 processors activated.
[    0.100355] CPU features: detected: 32-bit EL0 Support
[    0.106873] CPU: All CPU(s) started at EL2
[    0.109534] alternatives: patching kernel code
[    0.114850] devtmpfs: initialized
[    0.122351] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.126920] futex hash table entries: 1024 (order: 4, 65536 bytes)
[    0.138632] xor: measuring software checksum speed
[    0.177132]    8regs     :  2374.000 MB/sec
[    0.217161]    8regs_prefetch:  2051.000 MB/sec
[    0.257192]    32regs    :  2724.000 MB/sec
[    0.297222]    32regs_prefetch:  2308.000 MB/sec
[    0.297263] xor: using function: 32regs (2724.000 MB/sec)
[    0.301570] pinctrl core: initialized pinctrl subsystem
[    0.307373] NET: Registered protocol family 16
[    0.311529] audit: initializing netlink subsys (disabled)
[    0.316598] audit: type=2000 audit(0.268:1): state=initialized audit_enabled=0 res=1
[    0.324230] vdso: 2 pages (1 code @ (____ptrval____), 1 data @ (____ptrval____))
[    0.324235] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.338985] DMA: preallocated 256 KiB pool for atomic allocations
[    0.357555] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.426904] raid6: int64x1  gen()   444 MB/s
[    0.494975] raid6: int64x1  xor()   452 MB/s
[    0.563044] raid6: int64x2  gen()   680 MB/s
[    0.631050] raid6: int64x2  xor()   599 MB/s
[    0.699092] raid6: int64x4  gen()   981 MB/s
[    0.767146] raid6: int64x4  xor()   737 MB/s
[    0.835184] raid6: int64x8  gen()  1162 MB/s
[    0.903228] raid6: int64x8  xor()   759 MB/s
[    0.971275] raid6: neonx1   gen()   735 MB/s
[    1.039323] raid6: neonx1   xor()   880 MB/s
[    1.107350] raid6: neonx2   gen()  1128 MB/s
[    1.175422] raid6: neonx2   xor()  1174 MB/s
[    1.243472] raid6: neonx4   gen()  1479 MB/s
[    1.311514] raid6: neonx4   xor()  1419 MB/s
[    1.379569] raid6: neonx8   gen()  1555 MB/s
[    1.447605] raid6: neonx8   xor()  1459 MB/s
[    1.447643] raid6: using algorithm neonx8 gen() 1555 MB/s
[    1.451601] raid6: .... xor() 1459 MB/s, rmw enabled
[    1.456531] raid6: using neon recovery algorithm
[    1.461817] SCSI subsystem initialized
[    1.465007] usbcore: registered new interface driver usbfs
[    1.470317] usbcore: registered new interface driver hub
[    1.475595] usbcore: registered new device driver usb
[    1.480644] media: Linux media interface: v0.10
[    1.485102] videodev: Linux video capture interface: v2.00
[    1.490577] pps_core: LinuxPPS API ver. 1 registered
[    1.495461] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    1.504555] PTP clock support registered
[    1.508453] EDAC MC: Ver: 3.0.0
[    1.511941] zynqmp-ipi-mbox mailbox@ff990400: Probed ZynqMP IPI Mailbox driver.
[    1.519259] jesd204: found 0 devices and 0 topologies
[    1.523868] FPGA manager framework
[    1.527384] Advanced Linux Sound Architecture Driver Initialized.
[    1.533532] Bluetooth: Core ver 2.22
[    1.536829] NET: Registered protocol family 31
[    1.541225] Bluetooth: HCI device and connection manager initialized
[    1.547542] Bluetooth: HCI socket layer initialized
[    1.552385] Bluetooth: L2CAP socket layer initialized
[    1.557413] Bluetooth: SCO socket layer initialized
[    1.562708] clocksource: Switched to clocksource arch_sys_counter
[    1.568388] VFS: Disk quotas dquot_6.6.0
[    1.572234] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    1.583309] NET: Registered protocol family 2
[    1.583700] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes)
[    1.591184] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
[    1.598521] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
[    1.605294] TCP: Hash tables configured (established 32768 bind 32768)
[    1.611445] UDP hash table entries: 2048 (order: 4, 65536 bytes)
[    1.617422] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
[    1.623910] NET: Registered protocol family 1
[    1.628296] RPC: Registered named UNIX socket transport module.
[    1.633974] RPC: Registered udp transport module.
[    1.638633] RPC: Registered tcp transport module.
[    1.643307] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    1.650449] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[    1.656951] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[    1.665327] Initialise system trusted keyrings
[    1.668979] workingset: timestamp_bits=62 max_order=20 bucket_order=0
[    1.676002] NFS: Registering the id_resolver key type
[    1.680343] Key type id_resolver registered
[    1.684483] Key type id_legacy registered
[    1.688468] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    1.695135] jffs2: version 2.2. (NAND) (SUMMARY)  c 2001-2006 Red Hat, Inc.
[    2.782201] NET: Registered protocol family 38
[    2.841098] Key type asymmetric registered
[    2.841135] Asymmetric key parser 'x509' registered
[    2.844429] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[    2.851755] io scheduler noop registered
[    2.855646] io scheduler deadline registered
[    2.859905] io scheduler cfq registered (default)
[    2.864557] io scheduler mq-deadline registered
[    2.869054] io scheduler kyber registered
[    2.900954] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[    2.905185] cacheinfo: Unable to detect cache hierarchy for CPU 0
[    2.912244] brd: module loaded
[    2.916184] loop: module loaded
[    2.916394] Registered mathworks_ip class
[    2.918656] mtdoops: mtd device (mtddev=name/number) must be supplied
[    2.925630] libphy: Fixed MDIO Bus: probed
[    2.929474] tun: Universal TUN/TAP device driver, 1.6
[    2.933453] CAN device driver interface
[    2.938083] usbcore: registered new interface driver asix
[    2.942538] usbcore: registered new interface driver ax88179_178a
[    2.948581] usbcore: registered new interface driver cdc_ether
[    2.954375] usbcore: registered new interface driver net1080
[    2.960000] usbcore: registered new interface driver cdc_subset
[    2.965881] usbcore: registered new interface driver zaurus
[    2.971425] usbcore: registered new interface driver cdc_ncm
[    2.977752] usbcore: registered new interface driver uas
[    2.982329] usbcore: registered new interface driver usb-storage
[    2.988324] usbcore: registered new interface driver upd78f0730
[    2.994164] usbserial: USB Serial support registered for upd78f0730
[    3.001087] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0
[    3.007615] i2c /dev entries driver
[    3.012977] usbcore: registered new interface driver uvcvideo
[    3.016726] USB Video Class driver (1.1.1)
[    3.022136] Bluetooth: HCI UART driver ver 2.3
[    3.025214] Bluetooth: HCI UART protocol H4 registered
[    3.030308] Bluetooth: HCI UART protocol BCSP registered
[    3.035604] Bluetooth: HCI UART protocol LL registered
[    3.040688] Bluetooth: HCI UART protocol ATH3K registered
[    3.046068] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    3.052319] Bluetooth: HCI UART protocol Intel registered
[    3.057661] Bluetooth: HCI UART protocol QCA registered
[    3.062870] usbcore: registered new interface driver bcm203x
[    3.068484] usbcore: registered new interface driver bpa10x
[    3.074020] usbcore: registered new interface driver bfusb
[    3.079472] usbcore: registered new interface driver btusb
[    3.084894] Bluetooth: Generic Bluetooth SDIO driver ver 0.1
[    3.090560] usbcore: registered new interface driver ath3k
[    3.096093] EDAC MC: ECC not enabled
[    3.099771] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
[    3.111962] CPUidle arm: Failed to register cpuidle driver
[    3.117240] sdhci: Secure Digital Host Controller Interface driver
[    3.123217] sdhci: Copyright(c) Pierre Ossman
[    3.127541] sdhci-pltfm: SDHCI platform and OF driver helper
[    3.133550] ledtrig-cpu: registered to indicate activity on CPUs
[    3.139178] zynqmp_firmware_probe Platform Management API v1.1
[    3.144933] zynqmp_firmware_probe Trustzone version v1.0
[    3.153034] zynqmp-pinctrl firmware:zynqmp-firmware:pinctrl: zynqmp pinctrl initialized
[    3.180341] zynqmp_clk_mux_get_parent() getparent failed for clock: lpd_wdt, ret = -22
[    3.183033] alg: No test for xilinx-zynqmp-aes (zynqmp-aes)
[    3.188158] zynqmp_aes zynqmp_aes: AES Successfully Registered
[    3.188158]
[    3.195675] alg: No test for xilinx-keccak-384 (zynqmp-keccak-384)
[    3.201804] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa)
[    3.207378] usbcore: registered new interface driver usbhid
[    3.212714] usbhid: USB HID core driver
[    3.223121] axi_sysid 85000000.axi-sysid-0: [adrv9001] on [zcu102] git <4af529a57af7acda0a2971601e189df3f01628a5> clean [2020-06-12 14:04:04] UTC
[    3.230848] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
[    3.237407] usbcore: registered new interface driver snd-usb-audio
[    3.244792] pktgen: Packet Generator for packet performance testing. Version: 2.75
[    3.250970] Initializing XFRM netlink socket
[    3.254889] NET: Registered protocol family 10
[    3.259585] Segment Routing with IPv6
[    3.262940] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    3.269083] NET: Registered protocol family 17
[    3.273155] NET: Registered protocol family 15
[    3.277569] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[    3.290484] can: controller area network core (rev 20170425 abi 9)
[    3.296680] NET: Registered protocol family 29
[    3.301006] can: raw protocol (rev 20170425)
[    3.305241] can: broadcast manager protocol (rev 20170425 t)
[    3.310865] can: netlink gateway (rev 20170425) max_hops=1
[    3.316419] Bluetooth: RFCOMM TTY layer initialized
[    3.321165] Bluetooth: RFCOMM socket layer initialized
[    3.326300] Bluetooth: RFCOMM ver 1.11
[    3.329987] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    3.335259] Bluetooth: BNEP filters: protocol multicast
[    3.340450] Bluetooth: BNEP socket layer initialized
[    3.345381] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    3.351267] Bluetooth: HIDP socket layer initialized
[    3.356326] 9pnet: Installing 9P2000 support
[    3.360443] NET: Registered protocol family 36
[    3.364858] Key type dns_resolver registered
[    3.369602] registered taskstats version 1
[    3.373152] Loading compiled-in X.509 certificates
[    3.378228] Btrfs loaded, crc32c=crc32c-generic
[    3.388845] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 40, base_baud = 6249999) is a xuartps
[    3.398721] console [ttyPS0] enabled
[    3.398721] console [ttyPS0] enabled
[    3.402314] bootconsole [cdns0] disabled
[    3.402314] bootconsole [cdns0] disabled
[    3.410409] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 41, base_baud = 6249999) is a xuartps
[    3.423527] GPIO line 130 (output_enable) hogged as output/high
[    3.429698] of-fpga-region fpga-full: FPGA Region probed
[    3.435530] nwl-pcie fd0e0000.pcie: Link is DOWN
[    3.440179] nwl-pcie fd0e0000.pcie: host bridge /amba/pcie@fd0e0000 ranges:
[    3.447155] nwl-pcie fd0e0000.pcie:   MEM 0xe0000000..0xefffffff -> 0xe0000000
[    3.454375] nwl-pcie fd0e0000.pcie:   MEM 0x600000000..0x7ffffffff -> 0x600000000
[    3.461964] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00
[    3.468144] pci_bus 0000:00: root bus resource [bus 00-ff]
[    3.473624] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff]
[    3.480491] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref]
[    3.492553] pci 0000:00:00.0: PCI bridge to [bus 01-0c]
[    3.498747] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed
[    3.505322] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success
[    3.512430] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success
[    3.519538] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success
[    3.526636] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success
[    3.533739] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success
[    3.540840] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success
[    3.547944] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success
[    3.555045] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success
[    3.562297] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:8 protocol:4 pll_locked:yes
[    3.573757] zynqmp_clk_divider_set_rate() set divider failed for spi1_ref_div1, ret = -13
[    3.582431] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed
[    3.593202] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed
[    3.601291] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed
[    3.609716] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
[    3.622161] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
[    3.634847] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed
[    3.645028] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000
[    3.652046] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    3.658655] [drm] No driver support for vblank timestamp query.
[    3.664632] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008fc2930)
[    4.750721] [drm] Cannot find any crtc or sizes
[    4.755478] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0
[    4.763586] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed
[    4.772565] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:3 protocol:2 pll_locked:yes
[    4.790506] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode
[    4.799467] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
[    4.809837] scsi host0: ahci-ceva
[    4.813390] scsi host1: ahci-ceva
[    4.816845] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 37
[    4.824759] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 37
[    4.833846] API_LOG:adi_adrv9001_HwReset(...)
[    4.839218] API_LOG:adi_adrv9001_spi_Configure(...)
[    4.844182] API_LOG:adi_adrv9001_spi_Verify(...)
[    4.868734] random: fast init done
[    5.144946] ata2: SATA link down (SStatus 0 SControl 330)
[    5.150365] ata1: SATA link down (SStatus 0 SControl 330)
[    5.858724] [drm] Cannot find any crtc or sizes
[    8.403846] ERROR:Error number  3 (0x00000003), Recovery action -101.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_arm.c, in function adi_adrv9001_arm_CmdStatus_Wait, in line  638, variable name device.Error message ArmCmdStatusWait() failed due to thrown ARM error. Is device in correct state for calling command?.
[    8.403846]
[    8.435505] ERROR:Error number  13313 (0x00003401), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/private/src/adrv9001_arm.c, in function adrv9001_ArmCmdErrorHandler, in line  2582, variable name mailboxErrCode.Error message Command error.
[    8.435505]
[    8.460093] ERROR:Error number  13313 (0x00003401), Recovery action -2.In file drivers/iio/adc/navassa/devices/adrv9001/public/src/adi_adrv9001_cals.c, in function adi_adrv9001_cals_InitCals_Run, in line  104, variable name NULL.Error message Command error.
[    8.460093]
[    8.484330] adrv9002 spi1.0: adrv9002_setup, 1911: failed with "Command error" (13313)
[    8.492260] adrv9002: probe of spi1.0 failed with error -14
[    8.498644] m25p80 spi0.0: found n25q512a, expected m25p80
[    8.504405] m25p80 spi0.0: n25q512a (131072 Kbytes)
[    8.509293] 4 fixed-partitions partitions found on MTD device spi0.0
[    8.515635] Creating 4 MTD partitions on "spi0.0":
[    8.520419] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
[    8.526697] 0x000000100000-0x000000600000 : "qspi-linux"
[    8.532407] 0x000000600000-0x000000620000 : "qspi-device-tree"
[    8.538618] 0x000000620000-0x000000c00000 : "qspi-rootfs"
[    8.546492] macb ff0e0000.ethernet: Not enabling partial store and forward
[    8.553861] libphy: MACB_mii_bus: probed
[    8.557861] mdio_bus ff0e0000.ethernet-ffffffff: MDIO device at address 21 is missing.
[    8.567905] TI DP83867 ff0e0000.ethernet-ffffffff:0c: attached PHY driver [TI DP83867] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:0c, irq=POLL)
[    8.580939] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 22 (8a:85:2c:76:ce:da)
[    8.591065] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
[    8.597594] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM
[    8.604087] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM
[    8.610570] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM
[    8.618535] dwc3 fe200000.dwc3: Failed to get clk 'ref': -2
[    8.624390] xilinx-psgtr fd400000.zynqmp_phy: Lane:2 type:0 protocol:3 pll_locked:yes
[    8.632737] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    8.638230] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[    8.646210] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x0000000202010810
[    8.655620] xhci-hcd xhci-hcd.0.auto: irq 48, io mem 0xfe200000
[    8.661748] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
[    8.670013] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    8.677231] usb usb1: Product: xHCI Host Controller
[    8.682099] usb usb1: Manufacturer: Linux 4.19.0-29506-g6374347742fc xhci-hcd
[    8.689226] usb usb1: SerialNumber: xhci-hcd.0.auto
[    8.694373] hub 1-0:1.0: USB hub found
[    8.698141] hub 1-0:1.0: 1 port detected
[    8.702245] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    8.707738] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[    8.715391] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0  SuperSpeed
[    8.722127] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 4.19
[    8.730387] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    8.737606] usb usb2: Product: xHCI Host Controller
[    8.742475] usb usb2: Manufacturer: Linux 4.19.0-29506-g6374347742fc xhci-hcd
[    8.749601] usb usb2: SerialNumber: xhci-hcd.0.auto
[    8.754719] hub 2-0:1.0: USB hub found
[    8.758477] hub 2-0:1.0: 1 port detected
[    8.763593] pca953x 0-0020: 0-0020 supply vcc not found, using dummy regulator
[    8.770842] pca953x 0-0020: Linked as a consumer to regulator.0
[    8.777631] GPIO line 496 (sel0) hogged as output/low
[    8.783019] GPIO line 497 (sel1) hogged as output/high
[    8.788490] GPIO line 498 (sel2) hogged as output/high
[    8.793960] GPIO line 499 (sel3) hogged as output/high
[    8.799301] pca953x 0-0021: 0-0021 supply vcc not found, using dummy regulator
[    8.806544] pca953x 0-0021: Linked as a consumer to regulator.0
[    8.813995] ina2xx 3-0040: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.820811] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.827634] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.834452] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.841262] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.848084] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.854912] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.861720] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.868544] ina2xx 3-004a: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.875363] ina2xx 3-004b: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.881777] i2c i2c-0: Added multiplexed i2c bus 3
[    8.887269] ina2xx 4-0040: power monitor ina226 (Rshunt = 2000 uOhm)
[    8.894087] ina2xx 4-0041: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.900904] ina2xx 4-0042: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.907713] ina2xx 4-0043: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.914530] ina2xx 4-0044: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.921346] ina2xx 4-0045: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.928157] ina2xx 4-0046: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.934976] ina2xx 4-0047: power monitor ina226 (Rshunt = 5000 uOhm)
[    8.941375] i2c i2c-0: Added multiplexed i2c bus 4
[    8.980390] i2c i2c-0: Added multiplexed i2c bus 5
[    8.985363] i2c i2c-0: Added multiplexed i2c bus 6
[    8.990153] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544
[    8.997505] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 24
[    9.005289] at24 7-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write
[    9.012037] i2c i2c-1: Added multiplexed i2c bus 7
[    9.017160] i2c i2c-1: Added multiplexed i2c bus 8
[    9.024083] si570 9-005d: registered, current frequency 300000000 Hz
[    9.030480] i2c i2c-1: Added multiplexed i2c bus 9
[    9.049308] si570 10-005d: registered, current frequency 148500000 Hz
[    9.055794] i2c i2c-1: Added multiplexed i2c bus 10
[    9.060895] si5324 11-0069: si5328 probed
[    9.122776] si5324 11-0069: si5328 probe successful
[    9.127701] i2c i2c-1: Added multiplexed i2c bus 11
[    9.132736] i2c i2c-1: Added multiplexed i2c bus 12
[    9.137781] i2c i2c-1: Added multiplexed i2c bus 13
[    9.142836] i2c i2c-1: Added multiplexed i2c bus 14
[    9.147713] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548
[    9.155677] i2c i2c-1: Added multiplexed i2c bus 15
[    9.187413] i2c i2c-1: Added multiplexed i2c bus 16
[    9.192470] i2c i2c-1: Added multiplexed i2c bus 17
[    9.197518] i2c i2c-1: Added multiplexed i2c bus 18
[    9.202562] i2c i2c-1: Added multiplexed i2c bus 19
[    9.207605] i2c i2c-1: Added multiplexed i2c bus 20
[    9.212644] i2c i2c-1: Added multiplexed i2c bus 21
[    9.217694] i2c i2c-1: Added multiplexed i2c bus 22
[    9.222565] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548
[    9.230167] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 25
[    9.236530] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer with timeout 60s
[    9.276326] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit
[    9.293466] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[    9.300503] rtc_zynqmp ffa60000.rtc: setting system clock to 2021-02-19 09:07:02 UTC (1613725622)
[    9.309377] of_cfs_init
[    9.311835] of_cfs_init: OK
[    9.314760] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[    9.416476] mmc0: new ultra high speed SDR104 SDHC card at address aaaa
[    9.423597] mmcblk0: mmc0:aaaa SC32G 29.7 GiB
[    9.432251]  mmcblk0: p1 p2 p3
[    9.453967] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[    9.460574] zynqmp_pll_disable() clock disable failed for dpll_int, ret = -13
[    9.468346] ALSA device list:
[    9.471304]   #0: DisplayPort monitor
[    9.475313] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[    9.483923] cfg80211: failed to load regulatory.db
[    9.518828] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    9.526928] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    9.538363] devtmpfs: mounted
[    9.541510] Freeing unused kernel memory: 832K
[    9.546746] Run /sbin/init as init process
Mount failed for selinuxfs on /sys/fs/selinux:  No such file or directory
[    9.694821] random: init: uninitialized urandom read (12 bytes read)
[    9.802931] random: mountall: uninitialized urandom read (12 bytes read)
 * Setting up X socket directories...                                    [ OK ]
 * STARTDISTCC is set to false in /etc/default/distcc
 * /usr/bin/distccd not starting
 * Starting IIO Daemon iiod                                              [ OK ]

Last login: Thu Jan  1 00:00:07 UTC 1970 on tty1
Welcome to Linaro 14.04 (GNU/Linux 4.19.0-29506-g6374347742fc aarch64)

 * Documentation:  https://wiki.analog.com/ https://ez.analog.com/

root@analog:~#