How to add AD9361 driver after making Linux system with Petalinux2017.4 tool

Hello, I am using Zynq7020, and then using the Petalinux2017.4 tool to customize a Linux system. Then I read in wiki.analog.com/.../zynq_2015r2 "Building with Petalinux" -- -- - wiki.analog.com/.../petalinux will ad9361 driver added to my own custom Linux system, but suggest there is an error, according to the tutorial section, I don't know how to add my own device tree where is part a. I would like to know if this is only available on Petalinux2018.3.

Parents Reply Children
  • 0
    •  Analog Employees 
    on Feb 9, 2021 8:43 AM in reply to zhuangzi

    So, are you using petalinux 2018.3 or 2019.1? If you are using 2019.1, then you can use the conf file method.

    Just realized that the README has a slight bug. You need to escape the " for things to work as what you want to have in the file is KERNEL_DTB="zynq-zed-adv7511-ad9361-fmcomm2-3". Hence run the command like this: echo "KERNEL_DTB=\"zynq-zed-adv7511-ad9361-fmcomm2-3\"" >> project-spec/.../petalinuxbsp.conf

    - Nuno Sá

  • Hello, I am using Petalinux2018.3, and there are a lot of errors after using the add method you are providing now.

    Here's what happened, and I'm at a loss. Looking forward to your reply:

    [INFO] building project
    [INFO] sourcing bitbake
    INFO: bitbake petalinux-user-image
    WARNING: /opt/pkg/petalinux/components/yocto/source/arm/layers/meta-xilinx/meta-xilinx-bsp/recipes-bsp/device-tree/device-tree.bb: KERNEL_DTB is not defined. Your build is likely to fail! Make sure to define it in a conf file...
    Parsing recipes: 100% |##########################################| Time: 0:01:33
    Parsing of 2573 .bb files complete (0 cached, 2573 parsed). 3449 targets, 149 skipped, 0 masked, 0 errors.
    WARNING: No recipes available for:
    /home/ry/test1/meta-adi/meta-adi-xilinx/recipes-core/lsb/lsb_5.0.bbappend
    NOTE: Resolving any missing task queue dependencies
    Initialising tasks: 100% |#######################################| Time: 0:00:05
    Checking sstate mirror object availability: 100% |###############| Time: 0:00:35
    NOTE: Executing SetScene Tasks
    NOTE: Executing RunQueue Tasks
    WARNING: KERNEL_DTB is not defined. Your build is likely to fail! Make sure to define it in a conf file...
    WARNING: KERNEL_DTB is not defined. Your build is likely to fail! Make sure to define it in a conf file...
    WARNING: KERNEL_DTB is not defined. Your build is likely to fail! Make sure to define it in a conf file...
    WARNING: KERNEL_DTB is not defined. Your build is likely to fail! Make sure to define it in a conf file...
    WARNING: KERNEL_DTB is not defined. Your build is likely to fail! Make sure to define it in a conf file...
    WARNING: KERNEL_DTB is not defined. Your build is likely to fail! Make sure to define it in a conf file...
    ERROR: linux-xlnx-4.19-adi_master+gitAUTOINC+d13306d80c-r0 do_kernel_version_sanity_check: Package Version (4.19-adi_master+gitAUTOINC+d13306d80c) does not match of kernel being built (5.4). Please update the PV variable to match the kernel source or set KERNEL_VERSION_SANITY_SKIP="1" in your recipe.
    ERROR: linux-xlnx-4.19-adi_master+gitAUTOINC+d13306d80c-r0 do_kernel_version_sanity_check: Function failed: do_kernel_version_sanity_check (log file is located at /home/ry/test1/ax_peta/build/tmp/work/plnx_zynq7-xilinx-linux-gnueabi/linux-xlnx/4.19-adi_master+gitAUTOINC+d13306d80c-r0/temp/log.do_kernel_version_sanity_check.52630)
    ERROR: Logfile of failure stored in: /home/ry/test1/ax_peta/build/tmp/work/plnx_zynq7-xilinx-linux-gnueabi/linux-xlnx/4.19-adi_master+gitAUTOINC+d13306d80c-r0/temp/log.do_kernel_version_sanity_check.52630
    ERROR: Task (/opt/pkg/petalinux/components/yocto/source/arm/layers/meta-xilinx/meta-xilinx-bsp/recipes-kernel/linux/linux-xlnx_2018.3.bb:do_kernel_version_sanity_check) failed with exit code '1'
    NOTE: Tasks Summary: Attempted 2992 tasks of which 2242 didn't need to be rerun and 1 failed.
    Summary: 1 task failed:
    /opt/pkg/petalinux/components/yocto/source/arm/layers/meta-xilinx/meta-xilinx-bsp/recipes-kernel/linux/linux-xlnx_2018.3.bb:do_kernel_version_sanity_check
    Summary: There were 8 WARNING messages shown.
    Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
    ERROR: Failed to build project
    *****************************************************************************
    [INFO] building project
    [INFO] sourcing bitbake
    INFO: bitbake petalinux-user-image
    Parsing recipes: 100% |##########################################| Time: 0:01:05
    Parsing of 2573 .bb files complete (0 cached, 2573 parsed). 3449 targets, 149 skipped, 0 masked, 0 errors.
    WARNING: No recipes available for:
    /home/ry/test1/meta-adi/meta-adi-xilinx/recipes-core/lsb/lsb_5.0.bbappend
    NOTE: Resolving any missing task queue dependencies
    Initialising tasks: 100% |#######################################| Time: 0:00:05
    Checking sstate mirror object availability: 100% |###############| Time: 0:00:26
    NOTE: Executing SetScene Tasks
    NOTE: Executing RunQueue Tasks
    ERROR: linux-xlnx-4.19-adi_master+gitAUTOINC+d13306d80c-r0 do_populate_lic: QA Issue: linux-xlnx: The LIC_FILES_CHKSUM does not match for file://COPYING;md5=d7810fab7487fb0aad327b76f1be7cd7
    linux-xlnx: The new md5 checksum is bbea815ee2795b2f4230826c0c6b8814
    linux-xlnx: Here is the selected license text:
    vvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvvv
    The Linux Kernel is provided under:
    SPDX-License-Identifier: GPL-2.0 WITH Linux-syscall-note
    Being under the terms of the GNU General Public License version 2 only,
    according with:
    LICENSES/preferred/GPL-2.0
    With an explicit syscall exception, as stated at:
    LICENSES/exceptions/Linux-syscall-note
    In addition, other licenses may also apply. Please see:
    Documentation/process/license-rules.rst
    for more details.
    ^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
    linux-xlnx: Check if the license information has changed in /home/ry/test1/ax_peta/build/tmp/work-shared/plnx-zynq7/kernel-source/COPYING to verify that the LICENSE value "GPLv2" remains valid [license-checksum]
    ERROR: linux-xlnx-4.19-adi_master+gitAUTOINC+d13306d80c-r0 do_populate_lic: Fatal QA errors found, failing task.
    ERROR: linux-xlnx-4.19-adi_master+gitAUTOINC+d13306d80c-r0 do_populate_lic: Function failed: populate_lic_qa_checksum
    ERROR: Logfile of failure stored in: /home/ry/test1/ax_peta/build/tmp/work/plnx_zynq7-xilinx-linux-gnueabi/linux-xlnx/4.19-adi_master+gitAUTOINC+d13306d80c-r0/temp/log.do_populate_lic.55905
    ERROR: linux-xlnx-4.19-adi_master+gitAUTOINC+d13306d80c-r0 do_kernel_version_sanity_check: Package Version (4.19-adi_master+gitAUTOINC+d13306d80c) does not match of kernel being built (5.4). Please update the PV variable to match the kernel source or set KERNEL_VERSION_SANITY_SKIP="1" in your recipe.
    ERROR: linux-xlnx-4.19-adi_master+gitAUTOINC+d13306d80c-r0 do_kernel_version_sanity_check: Function failed: do_kernel_version_sanity_check (log file is located at /home/ry/test1/ax_peta/build/tmp/work/plnx_zynq7-xilinx-linux-gnueabi/linux-xlnx/4.19-adi_master+gitAUTOINC+d13306d80c-r0/temp/log.do_kernel_version_sanity_check.55904)
    ERROR: Logfile of failure stored in: /home/ry/test1/ax_peta/build/tmp/work/plnx_zynq7-xilinx-linux-gnueabi/linux-xlnx/4.19-adi_master+gitAUTOINC+d13306d80c-r0/temp/log.do_kernel_version_sanity_check.55904
    ERROR: Task (/opt/pkg/petalinux/components/yocto/source/arm/layers/meta-xilinx/meta-xilinx-bsp/recipes-kernel/linux/linux-xlnx_2018.3.bb:do_kernel_version_sanity_check) failed with exit code '1'
    ERROR: Task (/opt/pkg/petalinux/components/yocto/source/arm/layers/meta-xilinx/meta-xilinx-bsp/recipes-kernel/linux/linux-xlnx_2018.3.bb:do_populate_lic) failed with exit code '1'
    NOTE: Tasks Summary: Attempted 2056 tasks of which 2053 didn't need to be rerun and 2 failed.
    Summary: 2 tasks failed:
    /opt/pkg/petalinux/components/yocto/source/arm/layers/meta-xilinx/meta-xilinx-bsp/recipes-kernel/linux/linux-xlnx_2018.3.bb:do_kernel_version_sanity_check
    /opt/pkg/petalinux/components/yocto/source/arm/layers/meta-xilinx/meta-xilinx-bsp/recipes-kernel/linux/linux-xlnx_2018.3.bb:do_populate_lic
    Summary: There was 1 WARNING message shown.
    Summary: There were 5 ERROR messages shown, returning a non-zero exit code.
    ERROR: Failed to build project

  • 0
    •  Analog Employees 
    on Feb 9, 2021 11:28 AM in reply to zhuangzi

    If you are using petalinux 2018.3, then you need to use meta-adi 2019_r1...

    So, are you using petalinux 2018.3 or 2019.1? If you are using 2019.1, then you can use the conf file method.

    The method I explained does not apply to your petalinux version. Also it looks like that you are using meta-adi master branch and you need to use 2019_R1. Please follow the instructions in this readme file and forget about the conf file method (unless you are willing to upgrade to petalinux 2019.1).

    - Nuno Sá