ADRV9009 custom profile in Matlab

I every one, 

i would like to set the sampling frequency of Rx on the ADRV9009+ZC706 to 245.76MHz. I used the talise configuration wizard to generate custom profile, but  when loading the automatic generated files but i show error. I would like to know how i can set fre Rx sampling frequency correctly with Matlab example code given in the link https://ez.analog.com/wide-band-rf-transceivers/tes-gui-software-support-adrv9009-adrv9008-1-adrv9008-2/f/q-a/540347/setting-adrv9009-sampling-frequency-245-76mhz-in-matlab.

Please help !!!! I've been looking for the solution for months now.

Bellow is the error

Error in adi.common.Attribute/setDeviceAttributeRAW (line 135)
cstatus(obj,status,['Attribute write failed for : ' attr ' with value ' value]);

Error in adi.ADRV9009.Base/writeProfileFile (line 112)
obj.setDeviceAttributeRAW('profile_config',profle_data_str);

Error in adi.ADRV9009.Tx/setupInit (line 183)
writeProfileFile(obj);

Error in adi.common.RxTx/configureChanBuffers (line 214)
setupInit(obj);

Error in matlabshared.libiio.base/setupImpl

Error in adi.common.RxTx/setupImpl (line 116)
setupImpl@matlabshared.libiio.base(obj);

Error in adi.common.Tx/setupImpl (line 23)
setupImpl@adi.common.RxTx(obj);

Error in ADRV9009_DMA_Example (line 17)

Kind regards!