how to use matlab system block which combined to iio oscilloscope proper ?

Hi everyone.

we have  zynq-zc706-adv7511-ad9361-fmcomms2-3 and it includes the SD-card image which provided by analog devices(including the analog devices linux environment and iio oscilloscope/libiio)

we want to simulate in the simulink (stream data not hdl coder) the next matlab system block Airplane

 

the problem with that block that we want to include in the simulation the ad-freqcvt1-ebz down-up converter. we understand that we may need to change the cfg file which for the moment is written like this :

data_in_device = cf-ad9361-dds-core-lpc
data_out_device = cf-ad9361-lpc
ctrl_device = ad9361-phy
channel = RX_LO_FREQ,IN,out_altvoltage0_RX_LO_frequency,
channel = RX_SAMPLING_FREQ,IN,in_voltage_sampling_frequency,
channel = RX_RF_BANDWIDTH,IN,in_voltage_rf_bandwidth,
channel = RX1_GAIN_MODE,IN,in_voltage0_gain_control_mode,
channel = RX1_GAIN,IN,in_voltage0_hardwaregain,
channel = RX1_RSSI,OUT,in_voltage0_rssi,
channel = RX2_GAIN_MODE,IN,in_voltage1_gain_control_mode,
channel = RX2_GAIN,IN,in_voltage1_hardwaregain,
channel = RX2_RSSI,OUT,in_voltage1_rssi,
channel = TX_LO_FREQ,IN,out_altvoltage1_TX_LO_frequency,
channel = TX_SAMPLING_FREQ,IN,out_voltage_sampling_frequency,
channel = TX_RF_BANDWIDTH,IN,out_voltage_rf_bandwidth,


what are the changes that need to be done in order to achieve the required block ? (and how to write them in cfg file Slight smile)
thank for all the answers.

Top Replies

    •  Analog Employees 
    Jan 13, 2021 in reply to darroz +1 verified
    does the ad-freqcvt1-ebz really need some kind of special support from MATLAB  ?

    We maintain custom classes for each device/board in MATLAB. This is the recommended model from MathWorks. If you…

Parents Reply Children