Hello,
I have a brand new Rev. C ADRV9009-ZU11EG SOM board I am trying to bring up using default files (downloaded the ADRV9009-ZU11EG-RevB-07-08-2020.zip HW Rev.B files on the Quick Start guide). I am using a Rev. B carrier board. I have the boot switches as shown in the Quick Start guide for the Rev. B carrier board.
The system turns on (PG_ALL and PG_SOM LEDs light up), but hangs on the first stage boot loader. After ~1-2 minutes, the PS_ERR_OUT LED turns on. I have rebuilt the SD card in case it was corrupted, but same result. I also tried using the ADRV9009-ZU11EG-RevB-10-09-2019.zip HW Rev.B files with the same result. I have booted off of both the carrier SD card and the SOM microSD card with the same result.
Any ideas what could be the cause of this?
Thanks,
-Samual
I've attached some files that were built using the current master branches. They work fine on our side. Can you do a test using those too?
Thanks,Dragos
zynqmp-adrv9009-zu11eg-revb-adrv2crr-fmc-revb…
Dragos,
I received a new Rev C carrier board yesterday, and those reference files worked. I am closing this out and attributing the boot failure to a hardware failure on the Rev B carrier board.
I appreciate…
Hi Samuel,
Did you see any messages on the UART console?
From the software point of view, it shouldn't be any difference between Rev. B and Rev. C of SOM.
Hi Dragos,
The UART outputs only the first stage boot loader message:
Xilinx Zynq MP First Stage Boot Loader Release 2018.3 Jun 14 2019 - 10:06:14
Note, I just copied/pasted that from the Quick Start Wiki. I am using these reference boot files: ADRV9009-ZU11EG-RevB-07-08-2020.zip HW Rev.B. The release date is the only difference in the message.
A minute or two after power up, the PS_ERR_OUT LED comes on.
Best,
zynqmp-adrv9009-zu11eg-revb-adrv2crr-fmc-revb.zip
I just tried those boot files with the Rev. C SOM and Rev. C carrier. Same thing happened, where the first stage boot loader message pops out, but does not progress to kernel log messages. The PS_ERR_OUT LED comes on within the 1st minute after power is switched on.
Message:
Xilinx Zynq MP First Stage Boot Loader Release 2019.1 Jan 7 2021 - 09:51:43
I appreciate the fast response time.
Many thanks,