ADV7511w : what will be the 'dts' file changes for am437x

Hello community,

Myself is using ADV7511W transmitter for HDMI connection. For this I am bit stuck and not able to figure-out to what changes should be done in the dts files to make this work.

Also, myself is using below snippet mentioned as example at path Documentation/devicetree/bindings/display/bridge/adi,adv7511.txt  in kernel-source-tree to which I am getting the error. 

Request your assistance on this

Snippet

adv7511w: hdmi@39 {
compatible = "adi,adv7511w";
reg = <39>;
interrupt-parent = <&gpio3>;
interrupts = <29 IRQ_TYPE_EDGE_FALLING>;

adi,input-depth = <8>;
adi,input-colorspace = "rgb";
adi,input-clock = "1x";
adi,input-style = <1>;
adi,input-justification = "evenly";

ports {
#address-cells = <1>;
#size-cells = <0>;

port@0 {
reg = <0>;
adv7511w_in: endpoint {
remote-endpoint = <&dpi_out>;
};
};

port@1 {
reg = <1>;
adv7511_out: endpoint {
remote-endpoint = <&hdmi_connector_in>;
};
};
};
};