I am trying to use the ADRV9008-2 evaluation board with the ZC706. When I start up IIO Oscilloscope it only has two tabs Debug and DMM. If choose menu items Settings - connect it finds an eeprom and displays part number ADRV9008-2W/PCBZ. Presumably it is reading this from the mezzanine board. Linux version is reported as 4.14.0. IIO devices AD7291, XADC, ad9258-1, null.
I have read the answers to similar questions, but these seem to advise things that I have already done.
I created my software image as follows:
- Downloaded image 2019_R1
- Programmed SD Card
- In windows 10 machine opened drive named boot.
- Followed the instructions in README.txt i.e. From folder zynq-zc706-adv7511-adrv9008-2 copied BOOT.BIN and devicetree.dtb to folder root and from folder zynq-common copied uImage.
- With the SD Card in the ZC706 board, I powered up the system.
- Ran update scripts ADI Update boot (no change required) and ADI Update Tools (rebuilt things for several minutes)
- I rebooted the system.
I have created a diagnostic report and attached it to this question (might have added it twice by accident).