ADRV9009-ZU11EG

Hi,

Is there a way to make the 3.3V GPIO from the ADRV9009 work more quickly from Python and/or the command line?

Does the initialize command always have to be used?  The initialize command takes was too long, just to set the GPIO. 

Here is some python code I'm testing with ... 

sdr._ctrl.debug_attrs["adi,gpio3v3-source-control"].value = "0x333"                        
sdr._ctrl.debug_attrs["adi,gpio3v3-output-enable-mask"].value = "0xFFF"                 #set all A transciever GPIO (GPIO_0, GPIO_1, ...) as output
sdr._ctrl.debug_attrs["adi,gpio3v3-output-level-mask"].value = "0x000"                     #set GPIO_0 to level 0
sdr._ctrl.debug_attrs["initialize"].value = "1"                                         #Initialize
Nathan