I/O pins use in ADRV9361-Z7035/ADRV1CRR-BOB Board

Hello support,

We have a requirement of routing AD9361 Digital interface with bank 35 ( 24 pins which are used as input/output LVDS pins between AD9361 and Z7035 Board) in a evaluation board ADRV9361-Z7035/ ADRV1CRR-BOB to outer headers such as P2, P13, P4-P7 for external use.

As there are I/O pins available in bank 12, bank 13( HR Banks) as well bank 33, Bank 34( HP Banks) which can be used from P2, P13, P4, P5, P6, P7 of ADRV1CRR-BOB Board. Also we have a requirement to convert that routed LVDS pins to LVTTL standard. 

Kindly suggest , which bank may be suitable for the same to route the AD9361 Digital I/O pins from bank 35 to outer header as LVTTL ? 

Waiting for your response.