Hi,
I'm trying to debug a setup with an ad9136 and to help with this, we're trying to build all the drivers associated with this chip as modules.
I was wondering if this has been tried before and if there are things I should be careful about.
At the moment, it looks like I might have an issue with the order in which the modules are loaded.
Thanks for your time,
Liam
With which version was this working before?
lvb said:Also, We're debugging using modules because the kernel seems to hang when accessing some AXI IP cores. Is that something you've seen before?…
Hi aardelean,
aardelean said:Maybe check that the clock is enabled (clk_prepare_enable() called) before reading anything from the IP core.
Thanks for this suggestion, it seems to have fixed my issue! I've…
Hi Liam,
We usually test the drivers by statically linking in the kernel. As you say some issues might arise with the order that you load the drivers. What drivers are you trying as a module and what is your exact order ?
Regards,
Mircea
Hi Mircea,
At the moment, we're trying to boot with all drivers loaded as modules. Since we are using an AD9136-FMC-EBZ, this also includes the drivers for the ad9516-1.
here is a list of the module names:
- ad9517
- ad9144
- cf_axi_dds_drv
- axi_jesd204_tx
- axi_adxcvr_drv
- dma_axi_dmac
As for the loading order, I'm relying on the devicetree to load everything automatically.
Thanks,
Do you have a dmesg log output with the error you are getting ?
Here is a snippet of my latest bootlog:
ad9517 spi0.1: AD9517 successfully initialized ltc2632 spi4.0: ltc2634-l12 device registered, 4 channels axi_adxcvr_drv b0070000.axi_adxcvr: adxcvr_clk_recalc_rate: Parent Rate 184320000 Hz axi_adxcvr_drv b0070000.axi_adxcvr: adxcvr_clk_set_rate: Rate 8847360 Hz Parent Rate 184320000 Hz axi_adxcvr_drv b0070000.axi_adxcvr: adxcvr_clk_recalc_rate: Parent Rate 184320000 Hz axi_adxcvr_drv b0070000.axi_adxcvr: AXI-ADXCVR-TX (17.01.a) using GTH4 at 0xB0070000 mapped to 0xffffff800ee30000. Number of lanes: 8. ad9144 spi0.0: Setting lane rate 7372800 kHz axi_adxcvr_drv b0070000.axi_adxcvr: adxcvr_clk_round_rate: Rate 7372800 Hz Parent Rate 184320000 Hz axi_adxcvr_drv b0070000.axi_adxcvr: adxcvr_clk_set_rate: Rate 7372800 Hz Parent Rate 184320000 Hz axi_adxcvr_drv b0070000.axi_adxcvr: adxcvr_clk_recalc_rate: Parent Rate 184320000 Hz axi_adxcvr_drv b0070000.axi_adxcvr: adxcvr_clk_enable: TX cf_axi_dds b0098000.ad_ip_jesd204_tpl_dac: Device Tree Probing 'ad_ip_jesd204_tpl_dac' cf_axi_dds b0098000.ad_ip_jesd204_tpl_dac: failed to get converter ad9144 spi0.0: DAC-0 calibration successful ad9144 spi0.0: DAC-1 calibration successful ad9144 spi0.0: Probed.
I forgot to mention but I'm working with the kernel based on 2018.2 (6bfe5ed3d71e1f4e0164817e0dcb0d67da8c3a6e).
I've enabled debug in the ad9144, cf_axi_dds_drv and the axi_adxcvr_drv.
I've also added debug in the `cf_axi_dds_drv` and it seems like it fails during probe when getting the converter.
- 6bfe5ed3d7:drivers/iio/frequency/cf_axi_dds.c#L1391
- master:drivers/iio/frequency/cf_axi_dds.c#L2047
looking at the log, it seems like we try to call spi_get_drvdata() in cf_axi_dds.c before it's set in ad9144.c