1. What is the recommended way to leverage the ADRV9009 HDL Reference Design example for a custom board that uses Xilinx Zynq Ultrascale+ FPGA to communicate with the ADRV9009? a. How should the drivers needed for the ADI IPs and libiio be integrated into Petalinux? b. Can someone build a Petalinux OS using the Vivado generated .hdf file from a modified version of the HDL example.
2. Is there a resource on how to create a device tree file for a generic platform interfacing with the ADRV9009? a. Is ADI provided yocto layer (meta-adi) a possibility for an OS solution? It seems tailored for the example designs. Can it be modified to fit a custom platform? b. For example we use HMC7044 ultra low phase noise clock chip instead of ad9528 that is used on the ADRV9009 evaluation board [1].
3. Is the no-os software portable to run on a linux kernel, and does ADI see any issues if we try to run on the no-os software on a linux kernel?
Thanks
Charly
Hello Charly,
So likely we figured it is power issue on our part. But will post more information if not the case
Yes it was a power issue after all!