Hi,
I followed https://wiki.analog.com/resources/tools-software/linux-software/pyadi-iio#support to install pyadi iio.
I did the following on Windows 10:
pip install pyadi-iioInstalled libiio using installer : https://wiki.analog.com/resources/tools-software/linux-software/libiioand trying following code:
import adiimport numpy as npimport systry: import iioexcept: # By default the iio python bindings are not in path sys.path.append('C:/Python3/Lib/site-packages') import iiosdr = adi.ad9361()data = np.arange(1, 10, 3)# Sendsdr.tx(data)# Receivedata_rx = sdr.rx()I also tried :pip install libiio Following is error:C:\WINDOWS\system32>pip install iioCollecting iio Using cached iio-0.0.3.tar.gz (39 kB)Building wheels for collected packages: iio Building wheel for iio (setup.py) ... error ERROR: Command errored out with exit status 1: command: 'c:\python3\python.exe' -u -c 'import sys, setuptools, tokenize; sys.argv[0] = '"'"'C:\\Users\\swaraj\\AppData\\Local\\Temp\\pip-install-a68jgq5p\\iio\\setup.py'"'"'; __file__='"'"'C:\\Users\\swaraj\\AppData\\Local\\Temp\\pip-install-a68jgq5p\\iio\\setup.py'"'"';f=getattr(tokenize, '"'"'open'"'"', open)(__file__);code=f.read().replace('"'"'\r\n'"'"', '"'"'\n'"'"');f.close();exec(compile(code, __file__, '"'"'exec'"'"'))' bdist_wheel -d 'C:\Users\swaraj\AppData\Local\Temp\pip-wheel-9u6snd5n' cwd: C:\Users\swaraj\AppData\Local\Temp\pip-install-a68jgq5p\iio\ Complete output (15 lines): running bdist_wheel running build running build_py creating build creating build\lib.win32-3.8 copying iio.py -> build\lib.win32-3.8 running build_ext building 'libiio' extension creating build\temp.win32-3.8 creating build\temp.win32-3.8\Release creating build\temp.win32-3.8\Release\iio C:\Program Files (x86)\Microsoft Visual Studio\2017\BuildTools\VC\Tools\MSVC\14.16.27023\bin\HostX86\x86\cl.exe /c /nologo /Ox /W3 /GL /DNDEBUG /MD -Iiio -Ic:\python3\include -Ic:\python3\include "-IC:\Program Files (x86)\Microsoft Visual Studio\2017\BuildTools\VC\Tools\MSVC\14.16.27023\include" "-IC:\Program Files (x86)\Windows Kits\10\include\10.0.17134.0\ucrt" "-IC:\Program Files (x86)\Windows Kits\10\include\10.0.17134.0\shared" "-IC:\Program Files (x86)\Windows Kits\10\include\10.0.17134.0\um" "-IC:\Program Files (x86)\Windows Kits\10\include\10.0.17134.0\winrt" "-IC:\Program Files (x86)\Windows Kits\10\include\10.0.17134.0\cppwinrt" /Tciio/iio.c /Fobuild\temp.win32-3.8\Release\iio/iio.obj iio.c iio/iio.c(175): fatal error C1083: Cannot open include file: 'libgen.h': No such file or directory error: command 'C:\\Program Files (x86)\\Microsoft Visual Studio\\2017\\BuildTools\\VC\\Tools\\MSVC\\14.16.27023\\bin\\HostX86\\x86\\cl.exe' failed with exit status 2 ---------------------------------------- ERROR: Failed building wheel for iio Running setup.py clean for iioFailed to build iioInstalling collected packages: iio Running setup.py install for iio ... error ERROR: Command errored out with exit status 1: command: 'c:\python3\python.exe' -u -c 'import sys, setuptools, tokenize; sys.argv[0] = '"'"'C:\\Users\\swaraj\\AppData\\Local\\Temp\\pip-install-a68jgq5p\\iio\\setup.py'"'"'; __file__='"'"'C:\\Users\\swaraj\\AppData\\Local\\Temp\\pip-install-a68jgq5p\\iio\\setup.py'"'"';f=getattr(tokenize, '"'"'open'"'"', open)(__file__);code=f.read().replace('"'"'\r\n'"'"', '"'"'\n'"'"');f.close();exec(compile(code, __file__, '"'"'exec'"'"'))' install --record 'C:\Users\swaraj\AppData\Local\Temp\pip-record-ikux4b2t\install-record.txt' --single-version-externally-managed --compile --install-headers 'c:\python3\Include\iio' cwd: C:\Users\swaraj\AppData\Local\Temp\pip-install-a68jgq5p\iio\ Complete output (15 lines): running install running build running build_py creating build creating build\lib.win32-3.8 copying iio.py -> build\lib.win32-3.8 running build_ext building 'libiio' extension creating build\temp.win32-3.8 creating build\temp.win32-3.8\Release creating build\temp.win32-3.8\Release\iio C:\Program Files (x86)\Microsoft Visual Studio\2017\BuildTools\VC\Tools\MSVC\14.16.27023\bin\HostX86\x86\cl.exe /c /nologo /Ox /W3 /GL /DNDEBUG /MD -Iiio -Ic:\python3\include -Ic:\python3\include "-IC:\Program Files (x86)\Microsoft Visual Studio\2017\BuildTools\VC\Tools\MSVC\14.16.27023\include" "-IC:\Program Files (x86)\Windows Kits\10\include\10.0.17134.0\ucrt" "-IC:\Program Files (x86)\Windows Kits\10\include\10.0.17134.0\shared" "-IC:\Program Files (x86)\Windows Kits\10\include\10.0.17134.0\um" "-IC:\Program Files (x86)\Windows Kits\10\include\10.0.17134.0\winrt" "-IC:\Program Files (x86)\Windows Kits\10\include\10.0.17134.0\cppwinrt" /Tciio/iio.c /Fobuild\temp.win32-3.8\Release\iio/iio.obj iio.c iio/iio.c(175): fatal error C1083: Cannot open include file: 'libgen.h': No such file or directory error: command 'C:\\Program Files (x86)\\Microsoft Visual Studio\\2017\\BuildTools\\VC\\Tools\\MSVC\\14.16.27023\\bin\\HostX86\\x86\\cl.exe' failed with exit status 2 ----------------------------------------ERROR: Command errored out with exit status 1: 'c:\python3\python.exe' -u -c 'import sys, setuptools, tokenize; sys.argv[0] = '"'"'C:\\Users\\swaraj\\AppData\\Local\\Temp\\pip-install-a68jgq5p\\iio\\setup.py'"'"'; __file__='"'"'C:\\Users\\swaraj\\AppData\\Local\\Temp\\pip-install-a68jgq5p\\iio\\setup.py'"'"';f=getattr(tokenize, '"'"'open'"'"', open)(__file__);code=f.read().replace('"'"'\r\n'"'"', '"'"'\n'"'"');f.close();exec(compile(code, __file__, '"'"'exec'"'"'))' install --record 'C:\Users\swaraj\AppData\Local\Temp\pip-record-ikux4b2t\install-record.txt' --single-version-externally-managed --compile --install-headers 'c:\python3\Include\iio' Check the logs for full command output.
The pypi package name iio is not libiio, which is instead pylibiio: https://pypi.org/project/pylibiio/
Note that the bindings require the library to be installed beforehand which sounds like you have already…