ADRV9361-z7035 Network Connexion failed while running adi_update_tools

Hi everybody,

I'm currently working on the AD9361 on the ADRV9361-z7035 with the ADRVCRR-BOB board. I wanted to run the example that is given in the SD card but it's failing when I'm running thadi_update_tools.sh. There is the message that the terminal gives me :

root@analog:~# sudo  adi_update_tools..sh
wget: unable to resolve host address ‘github.comâ€Tm
eth0      Link encap:Ethernet  HWaddr 00:02:b5:01:06:75
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)
          Interrupt:28 Base address:0xb000

lo        Link encap:Local Loopback
          inet addr:127.0.0.1  Mask:255.0.0.0
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:58 errors:0 dropped:0 overruns:0 frame:0
          TX packets:58 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:4260 (4.2 KB)  TX bytes:4260 (4.2 KB)



Network Connection: FAILED

If anyone faced this problem or has an idea about how to solve it it would be really great !

Thanks & Regards !

Paul