The ADRV9009‘s Slicer GPIOs are not working with AGC Mode 2

HI,We use adrv9009 chip with version "adrv9009 Rev 192, Firmware 6.0.2 API version: 3.6.0.5". We  try to use the agc mode 2(Mode 2—Digital Gain Compensation with Slicer GPIO Outputs).

The setting profile is "tx_bw400_ir491p52_rx_bw200_or245p76_orx_bw400_or491p52_dc245p76"

The slicer GPIO outputs are gpio(8,9,10, 12,13,14) of adrv9009. we  use pin mode with api "TALISE_setRadioCtlPinMode(phy->talDevice, TAL_TXRX_PIN_MODE|TAL_ORX_PIN_MODE|TAL_ORX_SEL|TAL_ORX_ENAB_SEL_PIN, TAL_ORX1ORX2_PAIR_45_SEL);"

If we do not use pin mode, the slicer gpios(8,9,10, 12,13,14) of adrv9009 are working good. for example, the gpios(10 9 8) value is 0 0 1 when Rx1 receive radio signal with -5db, and Digital gain  is Compensed.

But if we use the pin mode, the slicer gpios(8,9,10, 12,13,14) of adrv9009 are not working. and the Digital gain is working good. for example,  the gpios(10 9 8) value is 0 0 0 when Rx1 receive radio signal with -5db, and Digital gain  is Compensed.

would you please give me some suguestion about that. Thank you.

Parents Reply Children
No Data