ADRV9009-ZU11EG SPI error when booting with 2019_R1 release

Hello,

I am updating my Linux/HDL design to the 2019_R1 release, and running into some issues. I followed the Zynq & Altera SoC Quick Start Guide to configure an SD card, and I extracted all the necessary files for the ADRV9009-ZU11EG to the root of the BOOT partition of the SD card, I also updated to Linux kernel 4.19 to deal with USB connectivity issues detailed in this post. When I boot up the SOM, I am able to get into the Linux userspace, but the ADRV9009 and related IIO devices aren't found. I then used the master branch files posted by Dragos in the above mentioned post about USB connectivity, and ran into the same issues.

The 2019_R1 dmesg output is included below. One line that stands out to me is:

[    8.414607] adrv9009: probe of spi1.1 failed with error -14

which implies to me that the ADRV9009 isn't getting communicated with by the ARM processor. Could this issue be in the device tree, or something else with my Linux build? I haven't found the location where the error codess are listed.

Any insight is appreciated!

Thanks,

-Samual

dmesg output:

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 4.19.0-ga5f6da0 (jenkins@romlxbuild2.adlk.analog.co                     m) (gcc version 8.2.0 (GCC)) #98 SMP Wed Mar 11 14:14:15 GMT 2020
[    0.000000] Machine model: Analog Devices ADRV9009-ZU11EG Rev.B
[    0.000000] earlycon: cdns0 at MMIO 0x00000000ff010000 (options '115200n8')
[    0.000000] bootconsole [cdns0] enabled
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] cma: Reserved 256 MiB at 0x0000000070000000
[    0.000000] On node 0 totalpages: 1048576
[    0.000000]   DMA32 zone: 7168 pages used for memmap
[    0.000000]   DMA32 zone: 0 pages reserved
[    0.000000]   DMA32 zone: 524288 pages, LIFO batch:63
[    0.000000]   Normal zone: 7168 pages used for memmap
[    0.000000]   Normal zone: 524288 pages, LIFO batch:63
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.1
[    0.000000] random: get_random_bytes called from start_kernel+0x94/0x3f8 with                      crng_init=0
[    0.000000] percpu: Embedded 22 pages/cpu @(____ptrval____) s52504 r8192 d294                     16 u90112
[    0.000000] pcpu-alloc: s52504 r8192 d29416 u90112 alloc=22*4096
[    0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: enabling workaround for ARM erratum 845719
[    0.000000] Speculative Store Bypass Disable mitigation not required
[    0.000000] CPU features: detected: Kernel page table isolation (KPTI)
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1034240
[    0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw                      earlycon rootfstype=ext4 rootwait cpuidle.off=1 root=/dev/mmcblk0p2 rw rootwait
[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes                     )
[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
[    0.000000] software IO TLB: mapped [mem 0x6bfff000-0x6ffff000] (64MB)
[    0.000000] Memory: 3774476K/4194304K available (12156K kernel code, 1380K rw                     data, 12456K rodata, 832K init, 315K bss, 157684K reserved, 262144K cma-reserved                     )
[    0.000000] rcu: Hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] arch_timer: cp15 timer(s) running at 33.33MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles:                      0x7b0074340, max_idle_ns: 440795202884 ns
[    0.000003] sched_clock: 56 bits at 33MHz, resolution 30ns, wraps every 21990                     23255543ns
[    0.008223] Console: colour dummy device 80x25
[    0.012388] Calibrating delay loop (skipped), value calculated using timer fr                     equency.. 66.66 BogoMIPS (lpj=133332)
[    0.022667] pid_max: default: 32768 minimum: 301
[    0.027349] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
[    0.033921] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
[    0.041636] ASID allocator initialised with 32768 entries
[    0.046414] rcu: Hierarchical SRCU implementation.
[    0.051413] EFI services will not be available.
[    0.055725] smp: Bringing up secondary CPUs ...
[    0.060370] Detected VIPT I-cache on CPU1
[    0.060396] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.060675] Detected VIPT I-cache on CPU2
[    0.060692] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[    0.060953] Detected VIPT I-cache on CPU3
[    0.060971] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[    0.061010] smp: Brought up 1 node, 4 CPUs
[    0.095586] SMP: Total of 4 processors activated.
[    0.100259] CPU features: detected: 32-bit EL0 Support
[    0.106578] CPU: All CPU(s) started at EL2
[    0.109436] alternatives: patching kernel code
[    0.114662] devtmpfs: initialized
[    0.123245] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, ma                     x_idle_ns: 7645041785100000 ns
[    0.127332] futex hash table entries: 1024 (order: 4, 65536 bytes)
[    0.138457] xor: measuring software checksum speed
[    0.177529]    8regs     :  2639.000 MB/sec
[    0.217554]    8regs_prefetch:  2280.000 MB/sec
[    0.257580]    32regs    :  3027.000 MB/sec
[    0.297606]    32regs_prefetch:  2565.000 MB/sec
[    0.297634] xor: using function: 32regs (3027.000 MB/sec)
[    0.301948] pinctrl core: initialized pinctrl subsystem
[    0.307700] NET: Registered protocol family 16
[    0.311879] audit: initializing netlink subsys (disabled)
[    0.316967] audit: type=2000 audit(0.268:1): state=initialized audit_enabled=                     0 res=1
[    0.324607] vdso: 2 pages (1 code @ (____ptrval____), 1 data @ (____ptrval___                     _))
[    0.324611] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.339302] DMA: preallocated 256 KiB pool for atomic allocations
[    0.356302] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.423309] raid6: int64x1  gen()   495 MB/s
[    0.491311] raid6: int64x1  xor()   502 MB/s
[    0.559321] raid6: int64x2  gen()   755 MB/s
[    0.627400] raid6: int64x2  xor()   666 MB/s
[    0.695401] raid6: int64x4  gen()  1089 MB/s
[    0.763448] raid6: int64x4  xor()   819 MB/s
[    0.831496] raid6: int64x8  gen()  1291 MB/s
[    0.899540] raid6: int64x8  xor()   844 MB/s
[    0.967579] raid6: neonx1   gen()   817 MB/s
[    1.035620] raid6: neonx1   xor()   978 MB/s
[    1.103678] raid6: neonx2   gen()  1254 MB/s
[    1.171693] raid6: neonx2   xor()  1304 MB/s
[    1.239756] raid6: neonx4   gen()  1644 MB/s
[    1.307774] raid6: neonx4   xor()  1576 MB/s
[    1.375822] raid6: neonx8   gen()  1727 MB/s
[    1.443858] raid6: neonx8   xor()  1621 MB/s
[    1.443884] raid6: using algorithm neonx8 gen() 1727 MB/s
[    1.447854] raid6: .... xor() 1621 MB/s, rmw enabled
[    1.452784] raid6: using neon recovery algorithm
[    1.457981] SCSI subsystem initialized
[    1.461117] libata version 3.00 loaded.
[    1.461250] usbcore: registered new interface driver usbfs
[    1.466568] usbcore: registered new interface driver hub
[    1.471842] usbcore: registered new device driver usb
[    1.476890] media: Linux media interface: v0.10
[    1.481351] videodev: Linux video capture interface: v2.00
[    1.486823] pps_core: LinuxPPS API ver. 1 registered
[    1.491711] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giome                     tti <giometti@linux.it>
[    1.500802] PTP clock support registered
[    1.504701] EDAC MC: Ver: 3.0.0
[    1.508147] zynqmp-ipi-mbox mailbox@ff990400: Probed ZynqMP IPI Mailbox drive                     r.
[    1.515492] jesd204: found 0 devices and 0 topologies
[    1.520113] FPGA manager framework
[    1.523621] Advanced Linux Sound Architecture Driver Initialized.
[    1.529764] Bluetooth: Core ver 2.22
[    1.533074] NET: Registered protocol family 31
[    1.537470] Bluetooth: HCI device and connection manager initialized
[    1.543786] Bluetooth: HCI socket layer initialized
[    1.548629] Bluetooth: L2CAP socket layer initialized
[    1.553655] Bluetooth: SCO socket layer initialized
[    1.558914] clocksource: Switched to clocksource arch_sys_counter
[    1.564621] VFS: Disk quotas dquot_6.6.0
[    1.568473] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    1.579164] NET: Registered protocol family 2
[    1.579900] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 3276                     8 bytes)
[    1.587420] TCP established hash table entries: 32768 (order: 6, 262144 bytes                     )
[    1.594740] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
[    1.601497] TCP: Hash tables configured (established 32768 bind 32768)
[    1.607677] UDP hash table entries: 2048 (order: 4, 65536 bytes)
[    1.613654] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
[    1.620141] NET: Registered protocol family 1
[    1.624508] RPC: Registered named UNIX socket transport module.
[    1.630203] RPC: Registered udp transport module.
[    1.634870] RPC: Registered tcp transport module.
[    1.639541] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    1.646179] PCI: CLS 0 bytes, default 64
[    1.646627] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[    1.653167] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters av                     ailable
[    1.661482] Initialise system trusted keyrings
[    1.665204] workingset: timestamp_bits=62 max_order=20 bucket_order=0
[    1.672172] NFS: Registering the id_resolver key type
[    1.676576] Key type id_resolver registered
[    1.680715] Key type id_legacy registered
[    1.684699] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    1.691365] jffs2: version 2.2. (NAND) (SUMMARY)  \xffffffc2\xffffffa9\xfffff                     fa9 2001-2006 Red Hat, Inc.
[    2.671991] NET: Registered protocol family 38
[    2.729257] Key type asymmetric registered
[    2.729284] Asymmetric key parser 'x509' registered
[    2.732584] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 2                     46)
[    2.739913] io scheduler noop registered
[    2.743802] io scheduler deadline registered
[    2.748060] io scheduler cfq registered (default)
[    2.752713] io scheduler mq-deadline registered
[    2.757209] io scheduler kyber registered
[    2.786240] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[    2.790099] cacheinfo: Unable to detect cache hierarchy for CPU 0
[    2.797012] brd: module loaded
[    2.800528] loop: module loaded
[    2.800710] Registered mathworks_ip class
[    2.803821] mtdoops: mtd device (mtddev=name/number) must be supplied
[    2.810753] libphy: Fixed MDIO Bus: probed
[    2.814648] tun: Universal TUN/TAP device driver, 1.6
[    2.818724] CAN device driver interface
[    2.823272] usbcore: registered new interface driver asix
[    2.827817] usbcore: registered new interface driver ax88179_178a
[    2.833860] usbcore: registered new interface driver cdc_ether
[    2.839649] usbcore: registered new interface driver net1080
[    2.845272] usbcore: registered new interface driver cdc_subset
[    2.851155] usbcore: registered new interface driver zaurus
[    2.856700] usbcore: registered new interface driver cdc_ncm
[    2.862950] usbcore: registered new interface driver uas
[    2.867598] usbcore: registered new interface driver usb-storage
[    2.873590] usbcore: registered new interface driver upd78f0730
[    2.879437] usbserial: USB Serial support registered for upd78f0730
[    2.886084] i2c /dev entries driver
[    2.890811] usbcore: registered new interface driver uvcvideo
[    2.894818] USB Video Class driver (1.1.1)
[    2.899346] axi_fan_control_driver 80000000.axi-fan-control: clk_get failed w                     ith -517
[    2.907428] Bluetooth: HCI UART driver ver 2.3
[    2.911085] Bluetooth: HCI UART protocol H4 registered
[    2.916182] Bluetooth: HCI UART protocol BCSP registered
[    2.921476] Bluetooth: HCI UART protocol LL registered
[    2.926561] Bluetooth: HCI UART protocol ATH3K registered
[    2.931940] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    2.938189] Bluetooth: HCI UART protocol Intel registered
[    2.943531] Bluetooth: HCI UART protocol QCA registered
[    2.948737] usbcore: registered new interface driver bcm203x
[    2.954354] usbcore: registered new interface driver bpa10x
[    2.959891] usbcore: registered new interface driver bfusb
[    2.965338] usbcore: registered new interface driver btusb
[    2.970764] Bluetooth: Generic Bluetooth SDIO driver ver 0.1
[    2.976427] usbcore: registered new interface driver ath3k
[    2.982125] EDAC MC0: Giving out device to module 1 controller synps_ddr_cont                     roller: DEV synps_edac (INTERRUPT)
[    2.992033] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac control                     ler zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
[    3.004247] CPUidle arm: Failed to register cpuidle driver
[    3.009581] sdhci: Secure Digital Host Controller Interface driver
[    3.015571] sdhci: Copyright(c) Pierre Ossman
[    3.019895] sdhci-pltfm: SDHCI platform and OF driver helper
[    3.025856] ledtrig-cpu: registered to indicate activity on CPUs
[    3.031526] zynqmp_firmware_probe Platform Management API v1.1
[    3.037285] zynqmp_firmware_probe Trustzone version v1.0
[    3.045104] zynqmp-pinctrl firmware:zynqmp-firmware:pinctrl: zynqmp pinctrl i                     nitialized
[    3.070767] zynqmp_clk_mux_get_parent() getparent failed for clock: lpd_wdt,                      ret = -22
[    3.073460] alg: No test for xilinx-zynqmp-aes (zynqmp-aes)
[    3.078658] zynqmp_aes zynqmp_aes: AES Successfully Registered
[    3.078658]
[    3.086099] alg: No test for xilinx-keccak-384 (zynqmp-keccak-384)
[    3.092230] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa)
[    3.097786] usbcore: registered new interface driver usbhid
[    3.103138] usbhid: USB HID core driver
[    3.113223] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
[    3.114484] usbcore: registered new interface driver snd-usb-audio
[    3.121899] pktgen: Packet Generator for packet performance testing. Version:                      2.75
[    3.128022] Initializing XFRM netlink socket
[    3.131991] NET: Registered protocol family 10
[    3.136692] Segment Routing with IPv6
[    3.140046] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    3.146167] NET: Registered protocol family 17
[    3.150271] NET: Registered protocol family 15
[    3.154686] bridge: filtering via arp/ip/ip6tables is no longer available by                      default. Update your scripts to load br_netfilter if you need this.
[    3.167595] can: controller area network core (rev 20170425 abi 9)
[    3.173754] NET: Registered protocol family 29
[    3.178116] can: raw protocol (rev 20170425)
[    3.182353] can: broadcast manager protocol (rev 20170425 t)
[    3.187978] can: netlink gateway (rev 20170425) max_hops=1
[    3.193615] Bluetooth: RFCOMM TTY layer initialized
[    3.198276] Bluetooth: RFCOMM socket layer initialized
[    3.203382] Bluetooth: RFCOMM ver 1.11
[    3.207096] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    3.212368] Bluetooth: BNEP filters: protocol multicast
[    3.217560] Bluetooth: BNEP socket layer initialized
[    3.222489] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    3.228373] Bluetooth: HIDP socket layer initialized
[    3.233431] 9pnet: Installing 9P2000 support
[    3.237549] NET: Registered protocol family 36
[    3.241964] Key type dns_resolver registered
[    3.246648] registered taskstats version 1
[    3.250260] Loading compiled-in X.509 certificates
[    3.255329] Btrfs loaded, crc32c=crc32c-generic
[    3.265530] ff010000.serial: ttyPS0 at MMIO 0xff010000 (irq = 22, base_baud =                      6249999) is a xuartps
[    3.274475] console [ttyPS0] enabled
[    3.278063] bootconsole [cdns0] disabled
[    3.286392] GPIO line 13 (ulpi-phy-reset) hogged as output/high
[    3.295566] of-fpga-region fpga-full: FPGA Region probed
[    3.302361] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed
[    3.309054] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:8 protocol:4 pll_lo                     cked:yes
[    3.318237] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0:                      Failed to get required clock freq
[    3.328346] xilinx-dp-snd-codec: probe of fd4a0000.zynqmp-display:zynqmp_dp_s                     nd_codec0 failed with error -22
[    3.338439] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PC                     M probed
[    3.346502] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PC                     M probed
[    3.354566] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: AS                     oC: CPU DAI (null) not registered
[    3.364635] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000
[    3.371680] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    3.378286] [drm] No driver support for vblank timestamp query.
[    3.384255] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8                     008d223d8)
[    4.470924] [drm] Cannot find any crtc or sizes
[    4.475665] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display                      on minor 0
[    4.483763] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsys                     tem driver probed
[    4.493725] adrv9009 spi1.0: adrv9009_probe : enter
[    4.498991] adrv9009 spi1.1: adrv9009_probe : enter
[    4.549472] macb ff0b0000.ethernet: Not enabling partial store and forward
[    4.556840] libphy: MACB_mii_bus: probed
[    4.596546] macb ff0e0000.ethernet: Not enabling partial store and forward
[    4.603898] libphy: MACB_mii_bus: probed
[    4.679356] Marvell 88E1510 ff0e0000.ethernet-ffffffff:00: attached PHY drive                     r [Marvell 88E1510] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:00, irq=POLL)
[    4.693262] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e                     0000 irq 13 (f6:ee:fe:03:87:05)
[    4.703397] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
[    4.709906] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM
[    4.716377] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM
[    4.722850] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM
[    4.730719] dwc3 fe200000.dwc3: Failed to get clk 'ref': -2
[    4.736581] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:0 protocol:3 pll_lo                     cked:yes
[    4.746488] OF: graph: no port node found in /amba/zynqmp_phy@fd400000/lane1
[    4.754825] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    4.760318] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus nu                     mber 1
[    4.769107] at24 0-002c: 2048 byte 24c16 EEPROM, writable, 1 bytes/write
[    4.775856] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 15
[    4.782511] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100                      quirks 0x0000000202010010
[    4.791919] xhci-hcd xhci-hcd.0.auto: irq 38, io mem 0xfe200000
[    4.798603] adau1761 3-003b: Direct firmware load for adau1761.bin failed wit                     h error -2
[    4.806608] adau1761 3-003b: Could not find firmware file: -2
[    4.812409] i2c i2c-1: Added multiplexed i2c bus 3
[    4.817302] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bc                     dDevice= 4.19
[    4.825567] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=                     1
[    4.832782] usb usb1: Product: xHCI Host Controller
[    4.837649] usb usb1: Manufacturer: Linux 4.19.0-ga5f6da0 xhci-hcd
[    4.843824] usb usb1: SerialNumber: xhci-hcd.0.auto
[    4.848897] i2c i2c-1: Added multiplexed i2c bus 4
[    4.853838] i2c i2c-1: Added multiplexed i2c bus 5
[    4.859009] hub 1-0:1.0: USB hub found
[    4.862773] hub 1-0:1.0: 1 port detected
[    4.866879] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    4.872372] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus nu                     mber 2
[    4.880029] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0  SuperSpeed
[    4.886771] i2c i2c-1: Added multiplexed i2c bus 6
[    4.891823] usb usb2: We don't know the algorithms for LPM for this host, dis                     abling LPM.
[    4.900189] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bc                     dDevice= 4.19
[    4.908450] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=                     1
[    4.915669] usb usb2: Product: xHCI Host Controller
[    4.920536] usb usb2: Manufacturer: Linux 4.19.0-ga5f6da0 xhci-hcd
[    4.926707] usb usb2: SerialNumber: xhci-hcd.0.auto
[    4.931774] i2c i2c-1: Added multiplexed i2c bus 7
[    4.936910] hub 2-0:1.0: USB hub found
[    4.940672] hub 2-0:1.0: 1 port detected
[    4.963274] i2c i2c-1: Added multiplexed i2c bus 8
[    4.968219] i2c i2c-1: Added multiplexed i2c bus 9
[    4.973176] i2c i2c-1: Added multiplexed i2c bus 10
[    4.978058] pca954x 1-0070: registered 8 multiplexed busses for I2C switch pc                     a9548
[    4.985659] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 16
[    4.992044] axi_fan_control_driver 80000000.axi-fan-control: Failed to initia                     lize device
[    5.000163] axi_fan_control_driver: probe of 80000000.axi-fan-control failed                      with error -22
[    5.008935] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer at (____ptrval_                     ___) with timeout 60s
[    5.018158] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 1333333                      KHz
[    5.025558] cpu cpu0: dev_pm_opp_set_rate: failed to find current OPP for fre                     q 1333333320 (-34)
[    5.034287] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed                      to: 1199999 KHz
[    5.042817] cpu cpu0: dev_pm_opp_set_rate: failed to find current OPP for fre                     q 1333333320 (-34)
[    5.083475] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA                      64-bit
[    5.099792] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: AS                     oC: CPU DAI (null) not registered
[    5.109950] adrv9009 spi1.0: adrv9009_probe : enter
[    5.115030] adrv9009 spi1.1: adrv9009_probe : enter
[    5.167233] macb ff0b0000.ethernet: Not enabling partial store and forward
[    5.174602] libphy: MACB_mii_bus: probed
[    5.207909] random: fast init done
[    5.211500] mmc0: new high speed SDHC card at address 0001
[    5.217456] mmcblk0: mmc0:0001 EB1QT 29.8 GiB
[    5.222914]  mmcblk0: p1 p2 p3
[    5.255330] Marvell 88E1510 ff0e0000.ethernet-ffffffff:01: attached PHY drive                     r [Marvell 88E1510] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:01, irq=POLL)
[    5.269244] macb ff0b0000.ethernet eth1: Cadence GEM rev 0x50070106 at 0xff0b                     0000 irq 12 (6a:15:2d:15:12:d0)
[    5.281479] axi_adxcvr 84a40000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.01.a) using                      GTH4 at 0x84A40000 mapped to 0x(____ptrval____). Number of lanes: 4.
[    5.296338] axi_adxcvr 84a60000.axi-adxcvr-rx-os: AXI-ADXCVR-RX (17.01.a) usi                     ng GTH4 at 0x84A60000 mapped to 0x(____ptrval____). Number of lanes: 4.
[    5.310302] axi_adxcvr 84a20000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.01.a) using                      GTH4 at 0x84A20000 mapped to 0x(____ptrval____). Number of lanes: 8.
[    5.325717] asoc-simple-card talise_sound: adau-hifi <-> 82000000.axi-i2s-adi                      mapping ok
[    5.337215] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: AS                     oC: CPU DAI (null) not registered
[    5.347381] adrv9009 spi1.0: adrv9009_probe : enter
[    5.354598] adrv9009 spi1.0: ADIHAL_resetHw at index
[    5.618923] [drm] Cannot find any crtc or sizes
[    5.682324] adrv9009 spi1.0: adrv9009_do_setup:662 Unexpected MCS sync status                      (0x0)
[    5.689974] ------------[ cut here ]------------
[    5.694575] jesd_tx_lane_clk already disabled
[    5.698949] WARNING: CPU: 0 PID: 51 at drivers/clk/clk.c:856 clk_core_disable                     +0xa0/0xa8
[    5.706936] Modules linked in:
[    5.709976] CPU: 0 PID: 51 Comm: kworker/0:1 Not tainted 4.19.0-ga5f6da0 #98
[    5.717004] Hardware name: Analog Devices ADRV9009-ZU11EG Rev.B (DT)
[    5.723346] Workqueue: events deferred_probe_work_func
[    5.728473] pstate: 60000085 (nZCv daIf -PAN -UAO)
[    5.733247] pc : clk_core_disable+0xa0/0xa8
[    5.737413] lr : clk_core_disable+0xa0/0xa8
[    5.741578] sp : ffffff8009c3ba30
[    5.744876] x29: ffffff8009c3ba30 x28: 00000000003a9800
[    5.750171] x27: ffffffc87aeaf848 x26: 00000000fffffff2
[    5.755466] x25: 00000000000e5def x24: ffffffc87a127380
[    5.760760] x23: 0000000000000003 x22: 0000000000000004
[    5.766055] x21: 0000000000000002 x20: ffffffc87b38b300
[    5.771350] x19: ffffffc87b38b300 x18: 0000000000000010
[    5.776645] x17: 0000000000000000 x16: 0000000000000000
[    5.781940] x15: ffffffffffffffff x14: ffffff8009968648
[    5.787235] x13: ffffff8089ac15cf x12: ffffff8009ac15d7
[    5.792529] x11: ffffff800997a000 x10: ffffff8009c3b710
[    5.797824] x9 : 00000000ffffffd0 x8 : ffffff80085589b0
[    5.803119] x7 : 656e616c5f78745f x6 : 0000000000000152
[    5.808414] x5 : 000000000000000f x4 : 0000000000000000
[    5.813709] x3 : 0000000000000000 x2 : ffffffffffffffff
[    5.819004] x1 : f496a42279913800 x0 : 0000000000000000
[    5.824299] Call trace:
[    5.826732]  clk_core_disable+0xa0/0xa8
[    5.830551]  clk_core_disable_lock+0x20/0x38
[    5.834804]  clk_disable+0x1c/0x28
[    5.838190]  adrv9009_setup+0x31c/0x1200
[    5.842094]  adrv9009_probe+0x299c/0x2f28
[    5.846088]  spi_drv_probe+0x7c/0xd8
[    5.849646]  really_probe+0x1c8/0x280
[    5.853292]  driver_probe_device+0x54/0xe8
[    5.857371]  __device_attach_driver+0xb8/0xe8
[    5.861711]  bus_for_each_drv+0x78/0xc8
[    5.865531]  __device_attach+0xd4/0x130
[    5.869350]  device_initial_probe+0x10/0x18
[    5.873516]  bus_probe_device+0x90/0x98
[    5.877335]  deferred_probe_work_func+0x6c/0xa0
[    5.881851]  process_one_work+0x1e4/0x340
[    5.885851]  worker_thread+0x248/0x488
[    5.889584]  kthread+0x124/0x128
[    5.892796]  ret_from_fork+0x10/0x18
[    5.896353] ---[ end trace da24355d694791a0 ]---
[    5.900975] ------------[ cut here ]------------
[    5.905586] jesd_tx_lane_clk already unprepared
[    5.910130] WARNING: CPU: 0 PID: 51 at drivers/clk/clk.c:715 clk_core_unprepa                     re+0xdc/0x100
[    5.918373] Modules linked in:
[    5.921414] CPU: 0 PID: 51 Comm: kworker/0:1 Tainted: G        W         4.19                     .0-ga5f6da0 #98
[    5.929831] Hardware name: Analog Devices ADRV9009-ZU11EG Rev.B (DT)
[    5.936170] Workqueue: events deferred_probe_work_func
[    5.941299] pstate: 60000005 (nZCv daif -PAN -UAO)
[    5.946074] pc : clk_core_unprepare+0xdc/0x100
[    5.950501] lr : clk_core_unprepare+0xdc/0x100
[    5.954925] sp : ffffff8009c3ba40
[    5.958224] x29: ffffff8009c3ba40 x28: 00000000003a9800
[    5.963519] x27: ffffffc87aeaf848 x26: 00000000fffffff2
[    5.968813] x25: 00000000000e5def x24: ffffffc87a127380
[    5.974108] x23: 0000000000000003 x22: 0000000000000004
[    5.979403] x21: 0000000000000002 x20: ffffff8009968648
[    5.984698] x19: ffffffc87b38b300 x18: 0000000000000010
[    5.989993] x17: 0000000000000000 x16: 0000000000000000
[    5.995288] x15: ffffffffffffffff x14: ffffff8009968648
[    6.000582] x13: ffffff8089ac15cf x12: ffffff8009ac15d7
[    6.005877] x11: ffffff800997a000 x10: ffffff8009c3b720
[    6.011172] x9 : 00000000ffffffd0 x8 : ffffff80085589b0
[    6.016467] x7 : 726c61206b6c635f x6 : 0000000000000180
[    6.021762] x5 : 000000000000000f x4 : 0000000000000000
[    6.027057] x3 : 0000000000000000 x2 : ffffffffffffffff
[    6.032352] x1 : f496a42279913800 x0 : 0000000000000000
[    6.037646] Call trace:
[    6.040079]  clk_core_unprepare+0xdc/0x100
[    6.044158]  clk_unprepare+0x28/0x40
[    6.047717]  adrv9009_setup+0x324/0x1200
[    6.051623]  adrv9009_probe+0x299c/0x2f28
[    6.055616]  spi_drv_probe+0x7c/0xd8
[    6.059175]  really_probe+0x1c8/0x280
[    6.062820]  driver_probe_device+0x54/0xe8
[    6.066900]  __device_attach_driver+0xb8/0xe8
[    6.071240]  bus_for_each_drv+0x78/0xc8
[    6.075059]  __device_attach+0xd4/0x130
[    6.078879]  device_initial_probe+0x10/0x18
[    6.083045]  bus_probe_device+0x90/0x98
[    6.086864]  deferred_probe_work_func+0x6c/0xa0
[    6.091379]  process_one_work+0x1e4/0x340
[    6.095371]  worker_thread+0x248/0x488
[    6.099103]  kthread+0x124/0x128
[    6.102315]  ret_from_fork+0x10/0x18
[    6.105872] ---[ end trace da24355d694791a1 ]---
[    6.110494] adrv9009 spi1.0: ADIHAL_resetHw at index
[    6.116665] usb 2-1: new SuperSpeed Gen 1 USB device number 2 using xhci-hcd
[    6.382256] usb 2-1: New USB device found, idVendor=2109, idProduct=0812, bcd                     Device=90.91
[    6.390426] usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[    6.397557] usb 2-1: Product: USB3.0 Hub
[    6.402599] usb 2-1: Manufacturer: VIA Labs, Inc.
[    6.438830] hub 2-1:1.0: USB hub found
[    6.442784] hub 2-1:1.0: 4 ports detected
[    6.453574] adrv9009 spi1.0: adrv9009_do_setup:662 Unexpected MCS sync status                      (0x0)
[    6.461225] ------------[ cut here ]------------
[    6.465827] jesd_tx_lane_clk already disabled
[    6.470193] WARNING: CPU: 0 PID: 51 at drivers/clk/clk.c:856 clk_core_disable                     +0xa0/0xa8
[    6.478178] Modules linked in:
[    6.481219] CPU: 0 PID: 51 Comm: kworker/0:1 Tainted: G        W         4.19                     .0-ga5f6da0 #98
[    6.489636] Hardware name: Analog Devices ADRV9009-ZU11EG Rev.B (DT)
[    6.495976] Workqueue: events deferred_probe_work_func
[    6.501104] pstate: 60000085 (nZCv daIf -PAN -UAO)
[    6.505879] pc : clk_core_disable+0xa0/0xa8
[    6.510045] lr : clk_core_disable+0xa0/0xa8
[    6.514209] sp : ffffff8009c3ba30
[    6.517508] x29: ffffff8009c3ba30 x28: 00000000003a9800
[    6.522803] x27: ffffffc87aeaf848 x26: 00000000fffffff2
[    6.528097] x25: 00000000000e5def x24: ffffffc87a127380
[    6.533392] x23: 0000000000000003 x22: 0000000000000004
[    6.538687] x21: 0000000000000002 x20: ffffffc87b38b300
[    6.543982] x19: ffffffc87b38b300 x18: 0000000000000010
[    6.549277] x17: 0000000000000000 x16: 0000000000000000
[    6.554572] x15: ffffffffffffffff x14: ffffff8009968648
[    6.559867] x13: ffffff8089ac15cf x12: ffffff8009ac15d7
[    6.565161] x11: ffffff800997a000 x10: ffffff8009c3b710
[    6.570456] x9 : 00000000ffffffd0 x8 : ffffff80085589b0
[    6.575751] x7 : 6b6c635f656e616c x6 : 00000000000001b6
[    6.581046] x5 : 000000000000000f x4 : 0000000000000000
[    6.586341] x3 : 0000000000000000 x2 : ffffffffffffffff
[    6.591636] x1 : f496a42279913800 x0 : 0000000000000000
[    6.596930] Call trace:
[    6.599364]  clk_core_disable+0xa0/0xa8
[    6.603182]  clk_core_disable_lock+0x20/0x38
[    6.607435]  clk_disable+0x1c/0x28
[    6.610821]  adrv9009_setup+0x31c/0x1200
[    6.614726]  adrv9009_probe+0x2e70/0x2f28
[    6.618719]  spi_drv_probe+0x7c/0xd8
[    6.622278]  really_probe+0x1c8/0x280
[    6.625923]  driver_probe_device+0x54/0xe8
[    6.630003]  __device_attach_driver+0xb8/0xe8
[    6.634343]  bus_for_each_drv+0x78/0xc8
[    6.638162]  __device_attach+0xd4/0x130
[    6.641982]  device_initial_probe+0x10/0x18
[    6.646148]  bus_probe_device+0x90/0x98
[    6.649967]  deferred_probe_work_func+0x6c/0xa0
[    6.654482]  process_one_work+0x1e4/0x340
[    6.658474]  worker_thread+0x248/0x488
[    6.662207]  kthread+0x124/0x128
[    6.665418]  ret_from_fork+0x10/0x18
[    6.668976] ---[ end trace da24355d694791a2 ]---
[    6.673592] ------------[ cut here ]------------
[    6.678199] jesd_tx_lane_clk already unprepared
[    6.682744] WARNING: CPU: 0 PID: 51 at drivers/clk/clk.c:715 clk_core_unprepa                     re+0xdc/0x100
[    6.690987] Modules linked in:
[    6.694028] CPU: 0 PID: 51 Comm: kworker/0:1 Tainted: G        W         4.19                     .0-ga5f6da0 #98
[    6.702446] Hardware name: Analog Devices ADRV9009-ZU11EG Rev.B (DT)
[    6.708784] Workqueue: events deferred_probe_work_func
[    6.713913] pstate: 60000005 (nZCv daif -PAN -UAO)
[    6.718689] pc : clk_core_unprepare+0xdc/0x100
[    6.723115] lr : clk_core_unprepare+0xdc/0x100
[    6.727540] sp : ffffff8009c3ba40
[    6.730838] x29: ffffff8009c3ba40 x28: 00000000003a9800
[    6.736133] x27: ffffffc87aeaf848 x26: 00000000fffffff2
[    6.741428] x25: 00000000000e5def x24: ffffffc87a127380
[    6.746723] x23: 0000000000000003 x22: 0000000000000004
[    6.752017] x21: 0000000000000002 x20: ffffff8009968648
[    6.757312] x19: ffffffc87b38b300 x18: 0000000000000010
[    6.762607] x17: 0000000000000000 x16: 0000000000000000
[    6.767902] x15: ffffffffffffffff x14: ffffff8009968648
[    6.773197] x13: ffffff8089ac15cf x12: ffffff8009ac15d7
[    6.778492] x11: ffffff800997a000 x10: ffffff8009c3b720
[    6.783787] x9 : 00000000ffffffd0 x8 : ffffff80085589b0
[    6.789081] x7 : 79646165726c6120 x6 : 00000000000001e4
[    6.794376] x5 : 000000000000000f x4 : 0000000000000000
[    6.799671] x3 : 0000000000000000 x2 : ffffffffffffffff
[    6.804966] x1 : f496a42279913800 x0 : 0000000000000000
[    6.810261] Call trace:
[    6.812694]  clk_core_unprepare+0xdc/0x100
[    6.816772]  clk_unprepare+0x28/0x40
[    6.820331]  adrv9009_setup+0x324/0x1200
[    6.824237]  adrv9009_probe+0x2e70/0x2f28
[    6.828230]  spi_drv_probe+0x7c/0xd8
[    6.831789]  really_probe+0x1c8/0x280
[    6.835435]  driver_probe_device+0x54/0xe8
[    6.839515]  __device_attach_driver+0xb8/0xe8
[    6.843854]  bus_for_each_drv+0x78/0xc8
[    6.847674]  __device_attach+0xd4/0x130
[    6.851493]  device_initial_probe+0x10/0x18
[    6.855659]  bus_probe_device+0x90/0x98
[    6.859479]  deferred_probe_work_func+0x6c/0xa0
[    6.863993]  process_one_work+0x1e4/0x340
[    6.867986]  worker_thread+0x248/0x488
[    6.871718]  kthread+0x124/0x128
[    6.874929]  ret_from_fork+0x10/0x18
[    6.878487] ---[ end trace da24355d694791a3 ]---
[    6.883118] adrv9009: probe of spi1.0 failed with error -14
[    6.888931] adrv9009 spi1.1: adrv9009_probe : enter
[    6.896005] adrv9009 spi1.1: ADIHAL_resetHw at index
[    6.902016] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[    7.056376] usb 1-1: New USB device found, idVendor=2109, idProduct=2812, bcd                     Device=90.90
[    7.064546] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[    7.071670] usb 1-1: Product: USB2.0 Hub
[    7.076714] usb 1-1: Manufacturer: VIA Labs, Inc.
[    7.126885] hub 1-1:1.0: USB hub found
[    7.130756] hub 1-1:1.0: 4 ports detected
[    7.142952] usb 2-1.4: new SuperSpeed Gen 1 USB device number 3 using xhci-hc                     d
[    7.167425] usb 2-1.4: New USB device found, idVendor=2537, idProduct=1081, b                     cdDevice= 1.00
[    7.175774] usb 2-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber                     =3
[    7.183070] usb 2-1.4: Product: NS1081
[    7.186805] usb 2-1.4: Manufacturer: Norelsys
[    7.191150] usb 2-1.4: SerialNumber: 0123456789ABCDE
[    7.197083] usb-storage 2-1.4:1.0: USB Mass Storage device detected
[    7.203653] scsi host0: usb-storage 2-1.4:1.0
[    7.229093] adrv9009 spi1.1: adrv9009_do_setup:662 Unexpected MCS sync status                      (0x0)
[    7.236739] ------------[ cut here ]------------
[    7.241341] jesd_tx_lane_clk already disabled
[    7.245712] WARNING: CPU: 0 PID: 51 at drivers/clk/clk.c:856 clk_core_disable                     +0xa0/0xa8
[    7.253700] Modules linked in:
[    7.256742] CPU: 0 PID: 51 Comm: kworker/0:1 Tainted: G        W         4.19                     .0-ga5f6da0 #98
[    7.265158] Hardware name: Analog Devices ADRV9009-ZU11EG Rev.B (DT)
[    7.271500] Workqueue: events deferred_probe_work_func
[    7.276627] pstate: 60000085 (nZCv daIf -PAN -UAO)
[    7.281401] pc : clk_core_disable+0xa0/0xa8
[    7.285568] lr : clk_core_disable+0xa0/0xa8
[    7.289732] sp : ffffff8009c3ba30
[    7.293030] x29: ffffff8009c3ba30 x28: 00000000003a9800
[    7.298325] x27: ffffffc87aeaf848 x26: 00000000fffffff2
[    7.303620] x25: 00000000000e5def x24: ffffffc87a127380
[    7.308914] x23: 0000000000000003 x22: 0000000000000004
[    7.314209] x21: 0000000000000002 x20: ffffffc87b38b300
[    7.319504] x19: ffffffc87b38b300 x18: 0000000000000010
[    7.324799] x17: 0000000000000000 x16: 0000000000000000
[    7.330094] x15: ffffffffffffffff x14: ffffff8009968648
[    7.335389] x13: ffffff8089ac15cf x12: ffffff8009ac15d7
[    7.340684] x11: ffffff800997a000 x10: ffffff8009c3b710
[    7.345979] x9 : 00000000ffffffd0 x8 : ffffff80085589b0
[    7.351273] x7 : 6b6c635f656e616c x6 : 0000000000000224
[    7.356568] x5 : 000000000000000f x4 : 0000000000000000
[    7.361863] x3 : 0000000000000000 x2 : ffffffffffffffff
[    7.367158] x1 : f496a42279913800 x0 : 0000000000000000
[    7.372453] Call trace:
[    7.374886]  clk_core_disable+0xa0/0xa8
[    7.378705]  clk_core_disable_lock+0x20/0x38
[    7.382958]  clk_disable+0x1c/0x28
[    7.386343]  adrv9009_setup+0x31c/0x1200
[    7.390248]  adrv9009_probe+0x299c/0x2f28
[    7.394242]  spi_drv_probe+0x7c/0xd8
[    7.397801]  really_probe+0x1c8/0x280
[    7.401446]  driver_probe_device+0x54/0xe8
[    7.405526]  __device_attach_driver+0xb8/0xe8
[    7.409865]  bus_for_each_drv+0x78/0xc8
[    7.413685]  __device_attach+0xd4/0x130
[    7.417504]  device_initial_probe+0x10/0x18
[    7.421670]  bus_probe_device+0x90/0x98
[    7.425490]  deferred_probe_work_func+0x6c/0xa0
[    7.430005]  process_one_work+0x1e4/0x340
[    7.433997]  worker_thread+0x248/0x488
[    7.437729]  kthread+0x124/0x128
[    7.440941]  ret_from_fork+0x10/0x18
[    7.444498] ---[ end trace da24355d694791a4 ]---
[    7.449113] ------------[ cut here ]------------
[    7.453721] jesd_tx_lane_clk already unprepared
[    7.458267] WARNING: CPU: 0 PID: 51 at drivers/clk/clk.c:715 clk_core_unprepa                     re+0xdc/0x100
[    7.466510] Modules linked in:
[    7.469551] CPU: 0 PID: 51 Comm: kworker/0:1 Tainted: G        W         4.19                     .0-ga5f6da0 #98
[    7.477968] Hardware name: Analog Devices ADRV9009-ZU11EG Rev.B (DT)
[    7.484307] Workqueue: events deferred_probe_work_func
[    7.489436] pstate: 60000005 (nZCv daif -PAN -UAO)
[    7.494211] pc : clk_core_unprepare+0xdc/0x100
[    7.498637] lr : clk_core_unprepare+0xdc/0x100
[    7.503062] sp : ffffff8009c3ba40
[    7.506361] x29: ffffff8009c3ba40 x28: 00000000003a9800
[    7.511655] x27: ffffffc87aeaf848 x26: 00000000fffffff2
[    7.516950] x25: 00000000000e5def x24: ffffffc87a127380
[    7.522245] x23: 0000000000000003 x22: 0000000000000004
[    7.527540] x21: 0000000000000002 x20: ffffff8009968648
[    7.532835] x19: ffffffc87b38b300 x18: 0000000000000010
[    7.538130] x17: 0000000000000000 x16: 0000000000000000
[    7.543425] x15: ffffffffffffffff x14: ffffff8009968648
[    7.548719] x13: ffffff8089ac15cf x12: ffffff8009ac15d7
[    7.554014] x11: ffffff800997a000 x10: ffffff8009c3b720
[    7.559309] x9 : 00000000ffffffd0 x8 : ffffff80085589b0
[    7.564604] x7 : 79646165726c6120 x6 : 0000000000000252
[    7.569899] x5 : 000000000000000f x4 : 0000000000000000
[    7.575194] x3 : 0000000000000000 x2 : ffffffffffffffff
[    7.580488] x1 : f496a42279913800 x0 : 0000000000000000
[    7.585783] Call trace:
[    7.588216]  clk_core_unprepare+0xdc/0x100
[    7.592295]  clk_unprepare+0x28/0x40
[    7.595854]  adrv9009_setup+0x324/0x1200
[    7.599760]  adrv9009_probe+0x299c/0x2f28
[    7.603753]  spi_drv_probe+0x7c/0xd8
[    7.607312]  really_probe+0x1c8/0x280
[    7.610957]  driver_probe_device+0x54/0xe8
[    7.615037]  __device_attach_driver+0xb8/0xe8
[    7.619376]  bus_for_each_drv+0x78/0xc8
[    7.623196]  __device_attach+0xd4/0x130
[    7.627015]  device_initial_probe+0x10/0x18
[    7.631182]  bus_probe_device+0x90/0x98
[    7.635001]  deferred_probe_work_func+0x6c/0xa0
[    7.639515]  process_one_work+0x1e4/0x340
[    7.643508]  worker_thread+0x248/0x488
[    7.647240]  kthread+0x124/0x128
[    7.650452]  ret_from_fork+0x10/0x18
[    7.654009] ---[ end trace da24355d694791a5 ]---
[    7.658633] adrv9009 spi1.1: ADIHAL_resetHw at index
[    7.898922] usb 1-1.1: new low-speed USB device number 3 using xhci-hcd
[    7.985066] adrv9009 spi1.1: adrv9009_do_setup:662 Unexpected MCS sync status                      (0x0)
[    7.992713] ------------[ cut here ]------------
[    7.997315] jesd_tx_lane_clk already disabled
[    8.001678] WARNING: CPU: 0 PID: 51 at drivers/clk/clk.c:856 clk_core_disable                     +0xa0/0xa8
[    8.009666] Modules linked in:
[    8.012707] CPU: 0 PID: 51 Comm: kworker/0:1 Tainted: G        W         4.19                     .0-ga5f6da0 #98
[    8.021124] Hardware name: Analog Devices ADRV9009-ZU11EG Rev.B (DT)
[    8.027463] Workqueue: events deferred_probe_work_func
[    8.032592] pstate: 60000085 (nZCv daIf -PAN -UAO)
[    8.037367] pc : clk_core_disable+0xa0/0xa8
[    8.041534] lr : clk_core_disable+0xa0/0xa8
[    8.045698] sp : ffffff8009c3ba30
[    8.048996] x29: ffffff8009c3ba30 x28: 00000000003a9800
[    8.054291] x27: ffffffc87aeaf848 x26: 00000000fffffff2
[    8.059586] x25: 00000000000e5def x24: ffffffc87a127380
[    8.064881] x23: 0000000000000003 x22: 0000000000000004
[    8.070175] x21: 0000000000000002 x20: ffffffc87b38b300
[    8.075470] x19: ffffffc87b38b300 x18: 0000000000000010
[    8.080765] x17: 0000000000000000 x16: 0000000000000000
[    8.086060] x15: ffffffffffffffff x14: ffffff8009968648
[    8.091355] x13: ffffff8089ac15cf x12: ffffff8009ac15d7
[    8.096650] x11: ffffff800997a000 x10: ffffff8009c3b710
[    8.101945] x9 : 00000000ffffffd0 x8 : ffffff80085589b0
[    8.107240] x7 : 726c61206b6c635f x6 : 0000000000000282
[    8.112534] x5 : 000000000000000f x4 : 0000000000000000
[    8.117829] x3 : 0000000000000000 x2 : ffffffffffffffff
[    8.123124] x1 : f496a42279913800 x0 : 0000000000000000
[    8.128419] Call trace:
[    8.130852]  clk_core_disable+0xa0/0xa8
[    8.134671]  clk_core_disable_lock+0x20/0x38
[    8.138924]  clk_disable+0x1c/0x28
[    8.142309]  adrv9009_setup+0x31c/0x1200
[    8.146214]  adrv9009_probe+0x2e70/0x2f28
[    8.150207]  spi_drv_probe+0x7c/0xd8
[    8.153766]  really_probe+0x1c8/0x280
[    8.157412]  driver_probe_device+0x54/0xe8
[    8.161492]  __device_attach_driver+0xb8/0xe8
[    8.165831]  bus_for_each_drv+0x78/0xc8
[    8.169651]  __device_attach+0xd4/0x130
[    8.173470]  device_initial_probe+0x10/0x18
[    8.177637]  bus_probe_device+0x90/0x98
[    8.181456]  deferred_probe_work_func+0x6c/0xa0
[    8.185970]  process_one_work+0x1e4/0x340
[    8.189963]  worker_thread+0x248/0x488
[    8.193695]  kthread+0x124/0x128
[    8.196906]  ret_from_fork+0x10/0x18
[    8.200464] ---[ end trace da24355d694791a6 ]---
[    8.205080] ------------[ cut here ]------------
[    8.209688] jesd_tx_lane_clk already unprepared
[    8.214232] WARNING: CPU: 0 PID: 51 at drivers/clk/clk.c:715 clk_core_unprepa                     re+0xdc/0x100
[    8.222476] Modules linked in:
[    8.225517] CPU: 0 PID: 51 Comm: kworker/0:1 Tainted: G        W         4.19                     .0-ga5f6da0 #98
[    8.233934] Hardware name: Analog Devices ADRV9009-ZU11EG Rev.B (DT)
[    8.240273] Workqueue: events deferred_probe_work_func
[    8.245402] pstate: 60000005 (nZCv daif -PAN -UAO)
[    8.250177] pc : clk_core_unprepare+0xdc/0x100
[    8.254604] lr : clk_core_unprepare+0xdc/0x100
[    8.259028] sp : ffffff8009c3ba40
[    8.262327] x29: ffffff8009c3ba40 x28: 00000000003a9800
[    8.267621] x27: ffffffc87aeaf848 x26: 00000000fffffff2
[    8.272916] x25: 00000000000e5def x24: ffffffc87a127380
[    8.278211] x23: 0000000000000003 x22: 0000000000000004
[    8.283506] x21: 0000000000000002 x20: ffffff8009968648
[    8.288801] x19: ffffffc87b38b300 x18: 0000000000000010
[    8.294096] x17: 0000000000000000 x16: 0000000000000000
[    8.299391] x15: ffffffffffffffff x14: ffffff8009968648
[    8.304685] x13: ffffff8089ac15cf x12: ffffff8009ac15d7
[    8.309980] x11: ffffff800997a000 x10: ffffff8009c3b720
[    8.315275] x9 : 00000000ffffffd0 x8 : ffffff80085589b0
[    8.320570] x7 : 656e616c5f78745f x6 : 00000000000002b0
[    8.325865] x5 : 000000000000000f x4 : 0000000000000000
[    8.331160] x3 : 0000000000000000 x2 : ffffffffffffffff
[    8.336455] x1 : f496a42279913800 x0 : 0000000000000000
[    8.341749] Call trace:
[    8.344182]  clk_core_unprepare+0xdc/0x100
[    8.348261]  clk_unprepare+0x28/0x40
[    8.351820]  adrv9009_setup+0x324/0x1200
[    8.355726]  adrv9009_probe+0x2e70/0x2f28
[    8.359719]  spi_drv_probe+0x7c/0xd8
[    8.363278]  really_probe+0x1c8/0x280
[    8.366923]  driver_probe_device+0x54/0xe8
[    8.371003]  __device_attach_driver+0xb8/0xe8
[    8.375343]  bus_for_each_drv+0x78/0xc8
[    8.379162]  __device_attach+0xd4/0x130
[    8.382981]  device_initial_probe+0x10/0x18
[    8.387148]  bus_probe_device+0x90/0x98
[    8.390967]  deferred_probe_work_func+0x6c/0xa0
[    8.395482]  process_one_work+0x1e4/0x340
[    8.399474]  worker_thread+0x248/0x488
[    8.403206]  kthread+0x124/0x128
[    8.406418]  ret_from_fork+0x10/0x18
[    8.409975] ---[ end trace da24355d694791a7 ]---
[    8.414607] adrv9009: probe of spi1.1 failed with error -14
[    8.421277] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: AS                     oC: CPU DAI (null) not registered
[    8.431987] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: AS                     oC: CPU DAI (null) not registered
[    8.444569] input: gpio_keys as /devices/platform/gpio_keys/input/input0
[    8.451663] hctosys: unable to open rtc device (rtc0)
[    8.456710] of_cfs_init
[    8.459171] of_cfs_init: OK
[    8.462118] cfg80211: Loading compiled-in X.509 certificates for regulatory d                     atabase
[    8.470900] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: AS                     oC: CPU DAI (null) not registered
[    8.484202] usb 1-1.1: New USB device found, idVendor=413c, idProduct=301a, b                     cdDevice= 1.00
[    8.492551] usb 1-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber                     =0
[    8.499847] usb 1-1.1: Product: Dell MS116 USB Optical Mouse
[    8.505497] usb 1-1.1: Manufacturer: PixArt
[    8.568820] input: PixArt Dell MS116 USB Optical Mouse as /devices/platform/a                     mba/ff9d0000.usb0/fe200000.dwc3/xhci-hcd.0.auto/usb1/1-1/1-1.1/1-1.1:1.0/0003:41                     3C:301A.0001/input/input1
[    8.585144] hid-generic 0003:413C:301A.0001: input: USB HID v1.11 Mouse [PixA                     rt Dell MS116 USB Optical Mouse] on usb-xhci-hcd.0.auto-1.1/input0
[    8.589272] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[    8.598992] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: AS                     oC: CPU DAI (null) not registered
[    8.605296] ALSA device list:
[    8.617476]   #0: ADRV9009 ZU11EG ADAU1761
[    8.621856] platform regulatory.0: Direct firmware load for regulatory.db fai                     led with error -2
[    8.630458] cfg80211: failed to load regulatory.db
[    8.645033] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. O                     pts: (null)
[    8.653134] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    8.666314] devtmpfs: mounted
[    8.669439] Freeing unused kernel memory: 832K
[    8.686958] Run /sbin/init as init process
[    8.913732] random: init: uninitialized urandom read (12 bytes read)
[    8.999958] init: hwclock main process (2263) terminated with status 1
[    9.117737] random: mountall: uninitialized urandom read (12 bytes read)
[    9.413782] systemd-udevd[2361]: starting version 204
[    9.547232] random: dbus-daemon: uninitialized urandom read (12 bytes read)
[   10.095163] pps pps0: new PPS source ptp0
[   10.095175] macb ff0e0000.ethernet: gem-ptp-timer ptp clock registered.
[   10.095326] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[   10.242575] urandom_read: 2 callbacks suppressed
[   10.242578] random: avahi-daemon: uninitialized urandom read (4 bytes read)
[   10.456713] init: failsafe main process (3472) killed by TERM signal
[   10.602632] random: dd: uninitialized urandom read (512 bytes read)
[   10.724446] scsi 0:0:0:0: Direct-Access     NORELSYS 1081             0    PQ                     : 0 ANSI: 6
[   10.726297] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: AS                     oC: CPU DAI (null) not registered
[   10.727538] sd 0:0:0:0: [sda] Attached SCSI removable disk
[   11.051084] init: udev-fallback-graphics main process (3695) terminated with                      status 1
[   11.418272] random: samba: uninitialized urandom read (1 bytes read)
[   11.424421] random: smbd: uninitialized urandom read (0 bytes read)
[   11.461893] random: sshd: uninitialized urandom read (32 bytes read)
[   11.776728] init: tty1 main process (3866) killed by TERM signal
[   11.876887] random: crng init done
[   12.000420] pps pps1: new PPS source ptp1
[   12.000432] macb ff0b0000.ethernet: gem-ptp-timer ptp clock registered.
[   12.000539] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[   12.112416] init: samba-ad-dc main process (3793) terminated with status 1
[   13.231291] macb ff0e0000.ethernet eth0: link up (1000/Full)
[   13.231314] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

Device tree is attached as a .txt file.

6366.system.txt

Parents Reply Children