AD9375 + ZC706 manual gain control

Hi,

I am using AD9375 + ZC706 with Matlab 2019b on Windows.

I was able to transmit and receive signals with the attached files (I had to make minor changes to the ORx.m file and to the ad9371.m file).

I am trying to change the observation receiver to work with 'manual' gain control instead of 'automatic' gain control and I am getting the following error:

"Error using matlabshared.libiio.base/cstatus

Attribute harswaregain return value -190, expected 10"

1) Any suggestions about how to fix this?

2) Is it because I am using AD9375 and not AD9371 (I am using the AD9371 files provided by Bogdan)?

2) How do I set the target power for automatic gain control?

Thanks,

Yaniv

8308.zip

Top Replies