ZCU102 rev 1.1 - 05 (new memory) + FMCOMMS2-EBZ Logint Prompt not coming up.

I created Linaro distro from the newest image archives: https://wiki.analog.com/resources/tools-software/linux-software/zynq_images

I copied correct Image, boot.bin and devices files to BOOT.BIN. ZCU102 boots fine but never shows login prompt. I can't point specific problem.

I got worse results with files from https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz/quickstart/zynqmp, it will not boot correctly.

Xilinx Zynq MP First Stage Boot Loader

Release 2018.3   Dec  4 2019  -  23:48:13

NOTICE:  ATF running on XCZU9EG/silicon v4/RTL5.1 at 0xfffea000

NOTICE:  BL31: Secure code at 0x0

NOTICE:  BL31: Non secure code at 0x8000000

NOTICE:  BL31: v1.5(release):xilinx-v2018.3

NOTICE:  BL31: Built : 15:00:47, Mar 18 2019

PMUFW: v1.1

U-Boot 2018.01 (Jun 29 2018 - 13:20:51 +0200) Xilinx ZynqMP ZCU102 rev1.0

I2C:   ready

DRAM:  4 GiB

EL Level: EL2

Chip ID: zu9eg

MMC:   sdhci@ff170000: 0 (SD)

*** Warning - bad CRC, using default environment

In:    serial@ff000000

Out:   serial@ff000000

Err:   serial@ff000000

Bootmode: LVL_SHFT_SD_MODE1

Net:   ZYNQ GEM: ff0e0000, phyaddr c, interface rgmii-id

Warning: ethernet@ff0e0000 using MAC address from ROM

eth0: ethernet@ff0e0000

Hit any key to stop autoboot:  0

switch to partitions #0, OK

mmc0 is current device

Device: sdhci@ff170000

Manufacturer ID: 1b

OEM: 534d

Name: GB1QT

Tran Speed: 50000000

Rd Block Len: 512

SD version 3.0

High Capacity: Yes

Capacity: 29.8 GiB

Bus Width: 4-bit

Erase Group Size: 512 Bytes

reading system.dtb

44219 bytes read in 19 ms (2.2 MiB/s)

reading Image

16361984 bytes read in 1074 ms (14.5 MiB/s)

## Flattened Device Tree blob at 04000000

   Booting using the fdt blob at 0x4000000

   Loading Device Tree to 000000000fff2000, end 000000000ffffcba ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0

[    0.000000] Linux version 4.14.0-g8a57ede (jenkins@romlxbuild1.adlk.analog.com) (gcc version 7.3.1 20180314 (Linaro GCC 7.3-2018.04-rc3)) #653 SMP Mon Feb 3 16:44:50 GMT 2020

[    0.000000] Boot CPU: AArch64 Processor [410fd034]

[    0.000000] Machine model: ZynqMP ZCU102 Rev1.0

[    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')

[    0.000000] bootconsole [cdns0] enabled

[    0.000000] efi: Getting EFI parameters from FDT:

[    0.000000] efi: UEFI not found.

[    0.000000] cma: Reserved 256 MiB at 0x0000000070000000

[    0.000000] psci: probing for conduit method from DT.

[    0.000000] psci: PSCIv1.1 detected in firmware.

[    0.000000] psci: Using standard PSCI v0.2 function IDs

[    0.000000] psci: MIGRATE_INFO_TYPE not supported.

[    0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff61000 s45080 r8192 d32744 u86016

[    0.000000] Detected VIPT I-cache on CPU0

[    0.000000] CPU features: enabling workaround for ARM erratum 845719

[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1034240

[    0.000000] Kernel command line: earlycon clk_ignore_unused root=/dev/mmcblk0p2 rw rootwait

[    0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)

[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)

[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)

[    0.000000] software IO TLB [mem 0x6bfff000-0x6ffff000] (64MB) mapped at [ffffffc06bfff000-ffffffc06fffefff]

[    0.000000] Memory: 3783852K/4194304K available (10236K kernel code, 746K rwdata, 4448K rodata, 512K init, 2154K bss, 148308K reserved, 262144K cma-reserved)

[    0.000000] Virtual kernel memory layout:

[    0.000000]     modules : 0xffffff8000000000 - 0xffffff8008000000   (   128 MB)

[    0.000000]     vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000   (   250 GB)

[    0.000000]       .text : 0xffffff8008080000 - 0xffffff8008a80000   ( 10240 KB)

[    0.000000]     .rodata : 0xffffff8008a80000 - 0xffffff8008ee0000   (  4480 KB)

[    0.000000]       .init : 0xffffff8008ee0000 - 0xffffff8008f60000   (   512 KB)

[    0.000000]       .data : 0xffffff8008f60000 - 0xffffff800901aa00   (   747 KB)

[    0.000000]        .bss : 0xffffff800901aa00 - 0xffffff8009235530   (  2155 KB)

[    0.000000]     fixed   : 0xffffffbefe7fd000 - 0xffffffbefec00000   (  4108 KB)

[    0.000000]     PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000   (    16 MB)

[    0.000000]     vmemmap : 0xffffffbf00000000 - 0xffffffc000000000   (     4 GB maximum)

[    0.000000]               0xffffffbf00000000 - 0xffffffbf1dc00000   (   476 MB actual)

[    0.000000]     memory  : 0xffffffc000000000 - 0xffffffc880000000   ( 34816 MB)

[    0.000000] Hierarchical RCU implementation.

[    0.000000] RCU event tracing is enabled.

[    0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.

[    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4

[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0

[    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000

[    0.000000] GIC: Using split EOI/Deactivate mode

[    0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).

[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8de2d3, max_idle_ns: 440795206112 ns

[    0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511101ns

[    0.008298] Console: colour dummy device 80x25

[    0.012378] console [tty0] enabled

[    0.015744] bootconsole [cdns0] disabled

[    0.000000] Booting Linux on physical CPU 0x0

[    0.000000] Linux version 4.14.0-g8a57ede (jenkins@romlxbuild1.adlk.analog.com) (gcc version 7.3.1 20180314 (Linaro GCC 7.3-2018.04-rc3)) #653 SMP Mon Feb 3 16:44:50 GMT 2020

[    0.000000] Boot CPU: AArch64 Processor [410fd034]

[    0.000000] Machine model: ZynqMP ZCU102 Rev1.0

[    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')

[    0.000000] bootconsole [cdns0] enabled

[    0.000000] efi: Getting EFI parameters from FDT:

[    0.000000] efi: UEFI not found.

[    0.000000] cma: Reserved 256 MiB at 0x0000000070000000

[    0.000000] psci: probing for conduit method from DT.

[    0.000000] psci: PSCIv1.1 detected in firmware.

[    0.000000] psci: Using standard PSCI v0.2 function IDs

[    0.000000] psci: MIGRATE_INFO_TYPE not supported.

[    0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff61000 s45080 r8192 d32744 u86016

[    0.000000] Detected VIPT I-cache on CPU0

[    0.000000] CPU features: enabling workaround for ARM erratum 845719

[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1034240

[    0.000000] Kernel command line: earlycon clk_ignore_unused root=/dev/mmcblk0p2 rw rootwait

[    0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)

[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)

[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)

[    0.000000] software IO TLB [mem 0x6bfff000-0x6ffff000] (64MB) mapped at [ffffffc06bfff000-ffffffc06fffefff]

[    0.000000] Memory: 3783852K/4194304K available (10236K kernel code, 746K rwdata, 4448K rodata, 512K init, 2154K bss, 148308K reserved, 262144K cma-reserved)

[    0.000000] Virtual kernel memory layout:

[    0.000000]     modules : 0xffffff8000000000 - 0xffffff8008000000   (   128 MB)

[    0.000000]     vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000   (   250 GB)

[    0.000000]       .text : 0xffffff8008080000 - 0xffffff8008a80000   ( 10240 KB)

[    0.000000]     .rodata : 0xffffff8008a80000 - 0xffffff8008ee0000   (  4480 KB)

[    0.000000]       .init : 0xffffff8008ee0000 - 0xffffff8008f60000   (   512 KB)

[    0.000000]       .data : 0xffffff8008f60000 - 0xffffff800901aa00   (   747 KB)

[    0.000000]        .bss : 0xffffff800901aa00 - 0xffffff8009235530   (  2155 KB)

[    0.000000]     fixed   : 0xffffffbefe7fd000 - 0xffffffbefec00000   (  4108 KB)

[    0.000000]     PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000   (    16 MB)

[    0.000000]     vmemmap : 0xffffffbf00000000 - 0xffffffc000000000   (     4 GB maximum)

[    0.000000]               0xffffffbf00000000 - 0xffffffbf1dc00000   (   476 MB actual)

[    0.000000]     memory  : 0xffffffc000000000 - 0xffffffc880000000   ( 34816 MB)

[    0.000000] Hierarchical RCU implementation.

[    0.000000] RCU event tracing is enabled.

[    0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.

[    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4

[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0

[    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000

[    0.000000] GIC: Using split EOI/Deactivate mode

[    0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).

[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8de2d3, max_idle_ns: 440795206112 ns

[    0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511101ns

[    0.008298] Console: colour dummy device 80x25

[    0.012378] console [tty0] enabled

[    0.015744] bootconsole [cdns0] disabled

[    0.019654] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.98 BogoMIPS (lpj=399960)

[    0.019667] pid_max: default: 32768 minimum: 301

[    0.019771] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)

[    0.019789] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)

[    0.020368] ASID allocator initialised with 65536 entries

[    0.020415] Hierarchical SRCU implementation.

[    0.020772] EFI services will not be available.

[    0.020805] zynqmp_plat_init Platform Management API v1.1

[    0.020813] zynqmp_plat_init Trustzone version v1.0

[    0.020909] smp: Bringing up secondary CPUs ...

[    0.021157] Detected VIPT I-cache on CPU1

[    0.021185] CPU1: Booted secondary processor [410fd034]

[    0.021455] Detected VIPT I-cache on CPU2

[    0.021473] CPU2: Booted secondary processor [410fd034]

[    0.021728] Detected VIPT I-cache on CPU3

[    0.021746] CPU3: Booted secondary processor [410fd034]

[    0.021789] smp: Brought up 1 node, 4 CPUs

[    0.021819] SMP: Total of 4 processors activated.

[    0.021827] CPU features: detected feature: 32-bit EL0 Support

[    0.021837] CPU: All CPU(s) started at EL2

[    0.021853] alternatives: patching kernel code

[    0.022592] devtmpfs: initialized

[    0.027513] random: get_random_u32 called from bucket_table_alloc+0x108/0x258 with crng_init=0

[    0.027728] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns

[    0.027750] futex hash table entries: 1024 (order: 5, 131072 bytes)

[    0.027910] random: fast init done

[    0.033207] xor: measuring software checksum speed

[    0.071738]    8regs     :  2303.000 MB/sec

[    0.111767]    8regs_prefetch:  2052.000 MB/sec

[    0.151799]    32regs    :  2831.000 MB/sec

[    0.191831]    32regs_prefetch:  2456.000 MB/sec

[    0.191839] xor: using function: 32regs (2831.000 MB/sec)

[    0.191915] pinctrl core: initialized pinctrl subsystem

[    0.192419] NET: Registered protocol family 16

[    0.192998] cpuidle: using governor menu

[    0.193552] vdso: 2 pages (1 code @ ffffff8008a86000, 1 data @ ffffff8008f64000)

[    0.193569] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.

[    0.194035] DMA: preallocated 256 KiB pool for atomic allocations

[    0.216062] zynqmp-pinctrl pinctrl: zynqmp pinctrl initialized

[    0.216856] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed

[    0.217490] ARM CCI_400_r1 PMU driver probed

[    0.227665] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages

[    0.295993] raid6: int64x1  gen()   457 MB/s

[    0.364010] raid6: int64x1  xor()   443 MB/s

[    0.432099] raid6: int64x2  gen()   689 MB/s

[    0.500099] raid6: int64x2  xor()   605 MB/s

[    0.568165] raid6: int64x4  gen()  1043 MB/s

[    0.636212] raid6: int64x4  xor()   765 MB/s

[    0.704269] raid6: int64x8  gen()   982 MB/s

[    0.772298] raid6: int64x8  xor()   751 MB/s

[    0.840349] raid6: neonx1   gen()   726 MB/s

[    0.908407] raid6: neonx1   xor()   852 MB/s

[    0.976442] raid6: neonx2   gen()  1168 MB/s

[    1.044488] raid6: neonx2   xor()  1207 MB/s

[    1.112569] raid6: neonx4   gen()  1505 MB/s

[    1.180579] raid6: neonx4   xor()  1440 MB/s

[    1.248650] raid6: neonx8   gen()  1665 MB/s

[    1.316686] raid6: neonx8   xor()  1533 MB/s

[    1.316694] raid6: using algorithm neonx8 gen() 1665 MB/s

[    1.316701] raid6: .... xor() 1533 MB/s, rmw enabled

[    1.316708] raid6: using neon recovery algorithm

[    1.318077] SCSI subsystem initialized

[    1.318241] usbcore: registered new interface driver usbfs

[    1.318277] usbcore: registered new interface driver hub

[    1.318316] usbcore: registered new device driver usb

[    1.318378] media: Linux media interface: v0.10

[    1.318403] Linux video capture interface: v2.00

[    1.318442] pps_core: LinuxPPS API ver. 1 registered

[    1.318450] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

[    1.318469] PTP clock support registered

[    1.318719] zynqmp-ipi ff9905c0.mailbox: Probed ZynqMP IPI Mailbox driver.

[    1.318853] FPGA manager framework

[    1.318963] fpga-region fpga-full: FPGA Region probed

[    1.319050] Advanced Linux Sound Architecture Driver Initialized.

[    1.319296] Bluetooth: Core ver 2.22

[    1.319321] NET: Registered protocol family 31

[    1.319329] Bluetooth: HCI device and connection manager initialized

[    1.319340] Bluetooth: HCI socket layer initialized

[    1.319349] Bluetooth: L2CAP socket layer initialized

[    1.319372] Bluetooth: SCO socket layer initialized

[    1.319898] clocksource: Switched to clocksource arch_sys_counter

[    1.319975] VFS: Disk quotas dquot_6.6.0

[    1.320017] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)

[    1.323935] NET: Registered protocol family 2

[    1.324230] TCP established hash table entries: 32768 (order: 6, 262144 bytes)

[    1.324440] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)

[    1.324853] TCP: Hash tables configured (established 32768 bind 32768)

[    1.324926] UDP hash table entries: 2048 (order: 4, 65536 bytes)

[    1.325003] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)

[    1.325157] NET: Registered protocol family 1

[    1.325377] RPC: Registered named UNIX socket transport module.

[    1.325387] RPC: Registered udp transport module.

[    1.325394] RPC: Registered tcp transport module.

[    1.325401] RPC: Registered tcp NFSv4.1 backchannel transport module.

[    1.325833] hw perfevents: no interrupt-affinity property for /pmu, guessing.

[    1.325986] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available

[    1.326609] audit: initializing netlink subsys (disabled)

[    1.326967] audit: type=2000 audit(1.308:1): state=initialized audit_enabled=0 res=1

[    1.327010] workingset: timestamp_bits=62 max_order=20 bucket_order=0

[    1.327679] NFS: Registering the id_resolver key type

[    1.327699] Key type id_resolver registered

[    1.327706] Key type id_legacy registered

[    1.327717] nfs4filelayout_init: NFSv4 File Layout Driver Registering...

[    1.327738] jffs2: version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.

[    1.351751] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)

[    1.351770] io scheduler noop registered

[    1.351777] io scheduler deadline registered

[    1.351797] io scheduler cfq registered (default)

[    1.351806] io scheduler mq-deadline registered

[    1.351813] io scheduler kyber registered

[    1.352403] nwl-pcie fd0e0000.pcie: Link is DOWN

[    1.352447] OF: PCI: host bridge /amba/pcie@fd0e0000 ranges:

[    1.352468] OF: PCI:   MEM 0xe0000000..0xefffffff -> 0xe0000000

[    1.352480] OF: PCI:   MEM 0x600000000..0x7ffffffff -> 0x600000000

[    1.352613] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00

[    1.352627] pci_bus 0000:00: root bus resource [bus 00-ff]

[    1.352637] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff]

[    1.352648] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref]

[    1.352910] pci 0000:00:00.0: PCI bridge to [bus 01-0c]

[    1.354158] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed

[    1.354419] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success

[    1.354580] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success

[    1.354740] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success

[    1.354901] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success

[    1.355061] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success

[    1.355222] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success

[    1.355380] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success

[    1.355543] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success

[    1.380446] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled

[    1.382904] cacheinfo: Unable to detect cache hierarchy for CPU 0

[    1.386913] brd: module loaded

[    1.390257] loop: module loaded

[    1.390950] ahci-ceva fd0c0000.ahci: couldn't get PHY in node ahci: -517

[    1.391109] mtdoops: mtd device (mtddev=name/number) must be supplied

[    1.392415] m25p80 spi0.0: SPI-NOR-UniqueID 10440088170200151300240088e2ac8bc0

[    1.392431] m25p80 spi0.0: found n25q512a, expected m25p80

[    1.392599] m25p80 spi0.0: n25q512a (131072 Kbytes)

[    1.392623] 4 ofpart partitions found on MTD device spi0.0

[    1.392631] Creating 4 MTD partitions on "spi0.0":

[    1.392643] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot"

[    1.393072] 0x000000100000-0x000000600000 : "qspi-linux"

[    1.393441] 0x000000600000-0x000000620000 : "qspi-device-tree"

[    1.393806] 0x000000620000-0x000000c00000 : "qspi-rootfs"

[    1.395028] libphy: Fixed MDIO Bus: probed

[    1.396021] tun: Universal TUN/TAP device driver, 1.6

[    1.396155] CAN device driver interface

[    1.398190] macb ff0e0000.ethernet: Not enabling partial store and forward

[    1.398573] libphy: MACB_mii_bus: probed

[    1.399077] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 23 (00:0a:35:05:1a:e6)

[    1.399093] TI DP83867 ff0e0000.ethernet-ffffffff:0c: attached PHY driver [TI DP83867] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:0c, irq=POLL)

[    1.399594] usbcore: registered new interface driver asix

[    1.399644] usbcore: registered new interface driver ax88179_178a

[    1.399677] usbcore: registered new interface driver cdc_ether

[    1.399707] usbcore: registered new interface driver net1080

[    1.399737] usbcore: registered new interface driver cdc_subset

[    1.399766] usbcore: registered new interface driver zaurus

[    1.399805] usbcore: registered new interface driver cdc_ncm

[    1.400129] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM

[    1.401613] usbcore: registered new interface driver uas

[    1.401654] usbcore: registered new interface driver usb-storage

[    1.402131] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0

[    1.402184] i2c /dev entries driver

[    1.403116] IR NEC protocol handler initialized

[    1.403125] IR RC5(x/sz) protocol handler initialized

[    1.403132] IR RC6 protocol handler initialized

[    1.403139] IR JVC protocol handler initialized

[    1.403146] IR Sony protocol handler initialized

[    1.403153] IR SANYO protocol handler initialized

[    1.403159] IR Sharp protocol handler initialized

[    1.403166] IR MCE Keyboard/mouse protocol handler initialized

[    1.403174] IR XMP protocol handler initialized

[    1.403815] usbcore: registered new interface driver uvcvideo

[    1.403823] USB Video Class driver (1.1.1)

[    1.404314] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer at ffffff80092a5000 with timeout 60s

[    1.404479] Bluetooth: HCI UART driver ver 2.3

[    1.404489] Bluetooth: HCI UART protocol H4 registered

[    1.404497] Bluetooth: HCI UART protocol BCSP registered

[    1.404505] Bluetooth: HCI UART protocol ATH3K registered

[    1.404512] Bluetooth: HCI UART protocol Three-wire (H5) registered

[    1.404553] Bluetooth: HCI UART protocol Intel registered

[    1.404561] Bluetooth: HCI UART protocol QCA registered

[    1.404599] usbcore: registered new interface driver bcm203x

[    1.404633] usbcore: registered new interface driver bpa10x

[    1.404665] usbcore: registered new interface driver bfusb

[    1.404699] usbcore: registered new interface driver btusb

[    1.404707] Bluetooth: Generic Bluetooth SDIO driver ver 0.1

[    1.404754] usbcore: registered new interface driver ath3k

[    1.405539] sdhci: Secure Digital Host Controller Interface driver

[    1.405548] sdhci: Copyright(c) Pierre Ossman

[    1.405554] sdhci-pltfm: SDHCI platform and OF driver helper

[    1.406784] ledtrig-cpu: registered to indicate activity on CPUs

[    1.406908] usbcore: registered new interface driver usbhid

[    1.406916] usbhid: USB HID core driver

[    1.407593] ad9361 spi1.0: ad9361_probe : enter (ad9361)

[    1.411889] axi_sysid 85000000.axi-sysid-0: [fmcomms2] on [zcu102] git <2e4ac278eb09c13471e381459b0da790ebad8373> clean [2019-12-04 23:16:58] UTC

[    1.412274] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered

[    1.413022] pktgen: Packet Generator for packet performance testing. Version: 2.75

[    1.413292] Netfilter messages via NETLINK v0.30.

[    1.413409] ip_tables: (C) 2000-2006 Netfilter Core Team

[    1.413544] Initializing XFRM netlink socket

[    1.413603] NET: Registered protocol family 10

[    1.413995] Segment Routing with IPv6

[    1.414041] ip6_tables: (C) 2000-2006 Netfilter Core Team

[    1.414165] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver

[    1.414468] NET: Registered protocol family 17

[    1.414484] NET: Registered protocol family 15

[    1.414501] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.

[    1.414515] Ebtables v2.0 registered

[    1.414598] can: controller area network core (rev 20170425 abi 9)

[    1.414633] NET: Registered protocol family 29

[    1.414647] can: raw protocol (rev 20170425)

[    1.414655] can: broadcast manager protocol (rev 20170425 t)

[    1.414666] can: netlink gateway (rev 20170425) max_hops=1

[    1.414855] Bluetooth: RFCOMM TTY layer initialized

[    1.414867] Bluetooth: RFCOMM socket layer initialized

[    1.414882] Bluetooth: RFCOMM ver 1.11

[    1.414896] Bluetooth: BNEP (Ethernet Emulation) ver 1.3

[    1.414904] Bluetooth: BNEP filters: protocol multicast

[    1.414914] Bluetooth: BNEP socket layer initialized

[    1.414922] Bluetooth: HIDP (Human Interface Emulation) ver 1.2

[    1.414931] Bluetooth: HIDP socket layer initialized

[    1.415035] 9pnet: Installing 9P2000 support

[    1.415054] Key type dns_resolver registered

[    1.415420] registered taskstats version 1

[    1.415729] Btrfs loaded, crc32c=crc32c-generic

[    1.420242] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 40, base_baud = 6249999) is a xuartps

[    2.971671] console [ttyPS0] enabled

[    2.975780] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 41, base_baud = 6249999) is a xuartps

[    2.986398] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:8 protocol:4 pll_locked:yes

[    2.994602] PLL: shutdown

[    2.998912] zynqmp_clk_divider_set_rate() set divider failed for spi1_ref_div1, ret = -13

[    3.007452] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed

[    3.018127] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed

[    3.026165] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed

[    3.034511] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok

[    3.046942] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok

[    3.059617] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed

[    3.069796] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000

[    3.076793] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).

[    3.083406] [drm] No driver support for vblank timestamp query.

[    3.089374] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008b32030)

[    4.175909] [drm] Cannot find any crtc or sizes

[    4.180610] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0

[    4.188718] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed

[    4.197679] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:3 protocol:2 pll_locked:yes

[    4.205566] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode

[    4.214530] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst

[    4.224877] scsi host0: ahci-ceva

[    4.228381] scsi host1: ahci-ceva

[    4.231786] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 37

[    4.239705] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 37

[    4.249431] xilinx-psgtr fd400000.zynqmp_phy: Lane:2 type:0 protocol:3 pll_locked:yes

[    4.257425] dwc3 fe200000.dwc3: stop_host(): INFO: Host already stopped

[    4.264366] dwc3 fe200000.dwc3: stop_peripheral(): INFO: Peripheral already stopped

[    4.308636] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller

[    4.314133] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1

[    4.322004] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x22010810

[    4.330723] xhci-hcd xhci-hcd.0.auto: irq 48, io mem 0xfe200000

[    4.336752] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

[    4.343542] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

[    4.350762] usb usb1: Product: xHCI Host Controller

[    4.355641] usb usb1: Manufacturer: Linux 4.14.0-g8a57ede xhci-hcd

[    4.361821] usb usb1: SerialNumber: xhci-hcd.0.auto

[    4.366975] hub 1-0:1.0: USB hub found

[    4.370739] hub 1-0:1.0: 1 port detected

[    4.374833] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller

[    4.380328] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2

[    4.388095] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003

[    4.394882] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1

[    4.402101] usb usb2: Product: xHCI Host Controller

[    4.406977] usb usb2: Manufacturer: Linux 4.14.0-g8a57ede xhci-hcd

[    4.413158] usb usb2: SerialNumber: xhci-hcd.0.auto

[    4.418260] hub 2-0:1.0: USB hub found

[    4.422023] hub 2-0:1.0: 1 port detected

[    4.427086] pca953x 0-0020: 0-0020 supply vcc not found, using dummy regulator

[    4.437310] GPIO line 496 (sel0) hogged as output/low

[    4.442690] GPIO line 497 (sel1) hogged as output/high

[    4.448166] GPIO line 498 (sel2) hogged as output/high

[    4.453632] GPIO line 499 (sel3) hogged as output/high

[    4.458867] pca953x 0-0020: interrupt support not compiled in

[    4.464705] pca953x 0-0021: 0-0021 supply vcc not found, using dummy regulator

[    4.474650] pca953x 0-0021: interrupt support not compiled in

[    4.481197] ina2xx 3-0040: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.487963] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.494739] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.501514] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.508292] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.515072] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.521847] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.528621] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.531902] xhci-hcd xhci-hcd.0.auto: remove, state 4

[    4.531916] usb usb2: USB disconnect, device number 1

[    4.532297] xhci-hcd xhci-hcd.0.auto: USB bus 2 deregistered

[    4.532307] xhci-hcd xhci-hcd.0.auto: remove, state 4

[    4.532317] usb usb1: USB disconnect, device number 1

[    4.532715] xhci-hcd xhci-hcd.0.auto: USB bus 1 deregistered

[    4.532727] dwc3 fe200000.dwc3: stop_peripheral(): INFO: Peripheral already stopped

[    4.562090] ata2: SATA link down (SStatus 0 SControl 330)

[    4.562113] ata1: SATA link down (SStatus 0 SControl 330)

[    4.585298] ina2xx 3-004a: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.592079] ina2xx 3-004b: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.598463] i2c i2c-0: Added multiplexed i2c bus 3

[    4.603852] ina2xx 4-0040: power monitor ina226 (Rshunt = 2000 uOhm)

[    4.610620] ina2xx 4-0041: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.617401] ina2xx 4-0042: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.624174] ina2xx 4-0043: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.630948] ina2xx 4-0044: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.637719] ina2xx 4-0045: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.644493] ina2xx 4-0046: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.651267] ina2xx 4-0047: power monitor ina226 (Rshunt = 5000 uOhm)

[    4.657654] i2c i2c-0: Added multiplexed i2c bus 4

[    4.703547] i2c i2c-0: Added multiplexed i2c bus 5

[    4.708468] i2c i2c-0: Added multiplexed i2c bus 6

[    4.713259] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544

[    4.720593] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 25

[    4.728168] at24 7-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write

[    4.734904] i2c i2c-1: Added multiplexed i2c bus 7

[    4.739883] i2c i2c-1: Added multiplexed i2c bus 8

[    4.746744] si570 9-005d: registered, current frequency 300000000 Hz

[    4.753125] i2c i2c-1: Added multiplexed i2c bus 9

[    4.771885] si570 10-005d: registered, current frequency 148500000 Hz

[    4.778357] i2c i2c-1: Added multiplexed i2c bus 10

[    4.783434] i2c i2c-1: Added multiplexed i2c bus 11

[    4.788431] i2c i2c-1: Added multiplexed i2c bus 12

[    4.793429] i2c i2c-1: Added multiplexed i2c bus 13

[    4.798419] i2c i2c-1: Added multiplexed i2c bus 14

[    4.803300] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548

[    4.812305] at24 15-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write

[    4.819036] i2c i2c-1: Added multiplexed i2c bus 15

[    4.824040] i2c i2c-1: Added multiplexed i2c bus 16

[    4.829038] i2c i2c-1: Added multiplexed i2c bus 17

[    4.834037] i2c i2c-1: Added multiplexed i2c bus 18

[    4.839040] i2c i2c-1: Added multiplexed i2c bus 19

[    4.844094] i2c i2c-1: Added multiplexed i2c bus 20

[    4.849128] i2c i2c-1: Added multiplexed i2c bus 21

[    4.854134] i2c i2c-1: Added multiplexed i2c bus 22

[    4.859010] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548

[    4.866603] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 26

[    4.915914] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit

[    4.929764] ad9361 spi1.0: ad9361_probe : enter (ad9361)

[    4.975197] mmc0: new SDHC card at address 0001

[    4.979899] mmcblk0: mmc0:0001 GB1QT 29.8 GiB

[    4.985754]  mmcblk0: p1 p2 p3

[    5.163366] ad9361 spi1.0: ad9361_probe : AD936x Rev 2 successfully initialized

[    5.188327] cf_axi_dds 99024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x99024000 mapped to 0xffffff8009435000, probed DDS AD9361

[    5.349323] [drm] Cannot find any crtc or sizes

[    6.397209] cf_axi_adc 99020000.cf-ad9361-lpc: ADI AIM (10.01.b) at 0x99020000 mapped to 0xffffff800cf38000, probed ADC AD9361 as MASTER

[    6.410309] input: gpio-keys as /devices/platform/gpio-keys/input/input0

[    6.417195] rtc_zynqmp ffa60000.rtc: setting system clock to 2019-02-23 02:45:30 UTC (1550889930)

[    6.426185] clk: Not disabling unused clocks

[    6.430702] ALSA device list:

[    6.433662]   #0: DisplayPort monitor

[    6.438775] EXT4-fs (mmcblk0p2): couldn't mount as ext3 due to feature incompatibilities

[    6.743571] EXT4-fs (mmcblk0p2): recovery complete

[    6.751177] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)

[    6.759294] VFS: Mounted root (ext4 filesystem) on device 179:2.

[    6.786040] devtmpfs: mounted

[    6.789119] Freeing unused kernel memory: 512K

Mount failed for selinuxfs on /sys/fs/selinux:  No such file or directory

* Setting up X socket directories...                                    [ OK ]

* STARTDISTCC is set to false in /etc/default/distcc

* /usr/bin/distccd not starting

* Starting IIO Daemon iiod                                              [ OK ]

å