Post Go back to editing

Interfacing AD7606B with Launchpad through SPI

Hi,

My enquiry is regaring thr interfacing of AD7076 with Launchpad F28379D through SPI.

Can the obove interfacing be established.

Adding to the query:

1. Does AD7606D support standalone application (say Ads-mcu-lcd).

2. Is there any code that can establish the transfer of data between the above two or any  launchpads or any MCU from abalog devices? Do suggest me any alternative board that can do the following.

3. Can I achieve the following project using ads7606d with raspberry pi?

P.s: My project is building protection relay, so i need a standalone system which captures the analog waveforms from the transformers and transfer the data to an MCU/DSP to process and control the circuit breaker triggering

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.