ZC706 and AD9375 recommended Matlab version and toolboxes for Windows

Hi,

I am trying to understand what are the recommended tools to work with the ZC706+AD9375 using Matlab on a Windows host.

First, I would like to control the evaluation kit and transmit a signal using Matlab (Later, I would like to design a transmitter using Matlab\Verilog and test it on the evaluation kit).

I read https://wiki.analog.com/resources/eval/user-guides/matlab_bsp and have a few questions:

1) Do you have an example for a Matlab code to control the evaluation kit and transmit a signal on ZC706+AD9375?

2) I have installed the "Communications Toolbox Support Package for Xilinx Zynq-Based Radio" but it seems like it doesn't support AD9375 (only AD936x). Can I use it for AD9375 or do I need a different Toolbox?

3) What is the recommended Matlab version (currently I have 2019b but I can downgrade if it is recommended)?

4) What is the recommended version of Analog Devices BSP Toolbox?

https://github.com/analogdevicesinc/MathWorks_tools/releases

5) What is the recommended version of Analog Devices transceiver Toolbox (and do I need both the BSP toolbox and the  transceiver toolbox)? 

https://github.com/analogdevicesinc/TransceiverToolbox/releases

6) What is the recommended version of libiio?

https://github.com/analogdevicesinc/libiio/releases

7) What is the recommended SD image (e.g. do you recommend to work with Linux-OS or with No-OS)? does it depend on the Matlab version \ Toolboxes version \ libiio version?

8) Do I need additional installations to be able to control the ZC706+AD9375 and transmit a signal using Matlab?

I will be happy to get recommendations.

Thanks,

Yaniv

Parents Reply Children