Hey all, I am a bit stuck on getting my system operational.
OS: Ubuntu 18.04 in a VM, host system is Windows 10
LIBIIO: compiled using the cmake build described by AD in https://wiki.analog.com/resources/eval/user-guides/ad-fmcdaq2-ebz/software/linux/applications/libiio
The pluto is recognized and I can interact with it / SSH is fine
PYADI: installed in python 3 using pip
When trying to import the adi package in python3 I get the following error message. I read some things that it may be caused by the incorrect installation of the python bindings but I'm puzzled on how to proceed.
Who can help?
Thanks
>>> import adiTraceback (most recent call last): File "<stdin>", line 1, in <module> File "<frozen importlib._bootstrap>", line 971, in _find_and_load File "<frozen importlib._bootstrap>", line 955, in _find_and_load_unlocked File "<frozen importlib._bootstrap>", line 656, in _load_unlocked File "<frozen importlib._bootstrap>", line 626, in _load_backward_compatible File "/usr/local/lib/python3.6/dist-packages/pyadi_iio-0.0.5-py3.6.egg/adi/__init__.py", line 34, in <module> File "<frozen importlib._bootstrap>", line 971, in _find_and_load File "<frozen importlib._bootstrap>", line 955, in _find_and_load_unlocked File "<frozen importlib._bootstrap>", line 656, in _load_unlocked File "<frozen importlib._bootstrap>", line 626, in _load_backward_compatible File "/usr/local/lib/python3.6/dist-packages/pyadi_iio-0.0.5-py3.6.egg/adi/ad9361.py", line 34, in <module> File "<frozen importlib._bootstrap>", line 971, in _find_and_load File "<frozen importlib._bootstrap>", line 955, in _find_and_load_unlocked File "<frozen importlib._bootstrap>", line 656, in _load_unlocked File "<frozen importlib._bootstrap>", line 626, in _load_backward_compatible File "/usr/local/lib/python3.6/dist-packages/pyadi_iio-0.0.5-py3.6.egg/adi/context_manager.py", line 34, in <module> File "/home/bert/temp/libiio/bindings/python/iio.py", line 71, in <module> _get_backends_count = _lib.iio_get_backends_count File "/usr/lib/python3.6/ctypes/__init__.py", line 361, in __getattr__ func = self.__getitem__(name) File "/usr/lib/python3.6/ctypes/__init__.py", line 366, in __getitem__ func = self._FuncPtr((name_or_ordinal, self))AttributeError: python3: undefined symbol: iio_get_backends_count
Yeah, there's the problem. Looks like there is a bug from a recent commit in master. I would roll back a bit by running this: git checkout a3a4c0803c51b7b207fec90244fe829a8a4fcc62
Then retry from cmake…
Sorry about that Trevis, I was confused because your link was referring to the pyadi install. The outcome of the make install of libiio is shown below, it installs just fine and I can call the executables as demonstrated above.
I think it has something to do with the binding of the pyadi module to the libiio driver bindings. Referring to https://ez.analog.com/linux-device-drivers/linux-software-drivers/f/q-a/116409/libiio---python-bindings
gives a very similar problem but I have no clue how to implement this in my machine on python 3.
How do install the iio bindings on my file system?
b41dd32c59194e_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/annotated.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__TopLevel_ga55574e54de682499c5c08566c652114a_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga41582140b8e1fe98148e51ae1350b816_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga176d11776f916c8148c6dfa1368cea3c_cgraph.png-- Up-to-date: /lib/udev/rules.d/90-libiio.rules-- Up-to-date: /usr/bin/iio_genxml-- Up-to-date: /usr/bin/iio_info-- Up-to-date: /usr/bin/iio_attr-- Up-to-date: /usr/bin/iio_readdev-- Up-to-date: /usr/bin/iio_reg-- Up-to-date: /usr/bin/iio_writedev-- Up-to-date: /usr/bin/iio_adi_xflow_check-- Up-to-date: /usr/sbin/iiodµ
When you do make install it tells you where it puts the iio.py file. When built with python3 it usually puts them in something similar to (say or 3.6): /usr/lib/python3.6/site-package
Therefore the export command would be:
export PYTHONPATH=$PYTHONPATH:'/usr/lib/python3.6/site-package
One thing I would also mention, pyadi-iio works fine on Windows as well. See the Windows section here about installing the bindings: https://wiki.analog.com/resources/tools-software/linux-software/pyadi-iio#prerequisites
-Travis
Thanks Trevor, in attachment the complete transcript of the make install of libiio. There is no reference to an installation of iio.py?
[ 41%] Built target iio[ 46%] Built target iio_info[ 51%] Built target iio_adi_xflow_check[ 56%] Built target iio_genxml[ 61%] Built target iio_reg[ 66%] Built target iio_attr[ 71%] Built target iio_writedev[ 76%] Built target iio_readdev[100%] Built target iiodInstall the project...-- Install configuration: "RelWithDebInfo"-- Up-to-date: /usr/lib/x86_64-linux-gnu/pkgconfig/libiio.pc-- Up-to-date: /usr/lib/x86_64-linux-gnu/libiio.so.0.18-- Up-to-date: /usr/lib/x86_64-linux-gnu/libiio.so.0-- Up-to-date: /usr/lib/x86_64-linux-gnu/libiio.so-- Up-to-date: /usr/include/iio.h-- Up-to-date: /usr/share/doc/libiio0-doc/html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga5cc6251fbf69e26befccb82d5f5a6625_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga3baae3a4b76956f9a7bc31c2ebb5b682_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/graph_legend.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gafd133e49a1a694e394939b4c5a073cb5_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gacb37ef830dcc100a9908d0592d1ff190_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga3c86ab8607c4ae38e2a36fa8c6bedcfd_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_gab5300f917bbdfc5dafc093a60138f131_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga36c7e7f895c58409dc129b128cc5983a_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/sort_8h_source.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga66bdc45f6b55cd28e76945ead18686ca_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga7b73b6fa484da3af7735cd80b90f3464_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga5cc6251fbf69e26befccb82d5f5a6625_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/tab_h.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__TopLevel_gac261dc30aa66453d1eabed1e88aa8728_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gac43421333d85b03e7aeb31eb60a676fe_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__TopLevel_ga8b5f231e009524ab5be5f918e6f041c3_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/iio_8h.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga3baae3a4b76956f9a7bc31c2ebb5b682_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gacb37ef830dcc100a9908d0592d1ff190_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan_ga279a930b7b597a06f454a30a0e770f85_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga68c8e6c772dbf4bbec921c1dc050ab3e_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga0d9e98519d12fc02a17a3f47011321fb_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga451ca34c6c249a980d85e3ceaa7e3784_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga2013f7206e2dde3aedee31ba01945585_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gaee1f1895db399936d29c5dff34eac21e_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga01b435571a0bd034bc47987295821573_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gace7a0de3e19a58c38f23e2a9b444dfff_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/tabs.css-- Up-to-date: /usr/share/doc/libiio0-doc/html/folderopen.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_gabb89575442d19f28b6557eee97f8fafd_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gaa35f0bbf7f6be8f859adb3fc692c600e_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gaa35f0bbf7f6be8f859adb3fc692c600e_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__TopLevel_gac261dc30aa66453d1eabed1e88aa8728_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga04957021a00fb18689b9d9ae6f95a928_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga451ca34c6c249a980d85e3ceaa7e3784_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga4aafea4c127b872d5214d41ccb4ce8c1_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gabcd0cd25e203976bdc525790b6fe4e23_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga176d11776f916c8148c6dfa1368cea3c_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga5f1aef2258268209b6486e788a1967ec_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga0073a46392fcf6efaa488b75cf8bcb6c_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/splitbar.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga01151f264c7e22fcf8390b5303b51bb3_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/folderclosed.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gacf36dfa2fc04a80ce93db3b131bae099_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__TopLevel_gaaa29e5bac86d00a1cef6e2d00b0ea24c_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga5cea41d7dd9babf48937e939aa0d3c5b_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga18a52045b14205192e3fbbcb4e2ddb58_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/closed.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gae7adad053ab5e2a5f447851f7d34dc04_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga01b435571a0bd034bc47987295821573_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga891aa6ffd6290fc3848e4f14a923d1fb_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga6f587251cdca7cd1983d6e3a2a5e3ae6_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga83e2e2ef3c9fa91561b41dd32c59194e_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga6ecca643c857855e8aa27fee21553337_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gaeb192bd3730c8c65a4e5c29feca62257_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga233b868380bca0578907bda28d3a5480_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gaee333f1061000b0b71298dff59104513_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga823b2e43e8d1bc0122266e83fe81fbc4_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga5f1aef2258268209b6486e788a1967ec_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga28c43d91ddaf8856f2d1a79562072280_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga000d2f4c8b72060db1c38ec905bf4156_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gace7a0de3e19a58c38f23e2a9b444dfff_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga18d5cb8d912b5b888b9b54c6d0c7f92c_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga8c5fc6f7ccee7f9da338833822f799ec_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga0d06dce5819723c3b16c4588eb5f477a_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga638c2f54b187a1b137f9885f34fad338_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/jquery.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/globals_func.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__TopLevel_ga55574e54de682499c5c08566c652114a_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga6ecca643c857855e8aa27fee21553337_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga68819e214490f2d556599ee64799e267_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga1c7689aa48b6789168e266a0e9bfef7e_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gaeb192bd3730c8c65a4e5c29feca62257_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga66bdc45f6b55cd28e76945ead18686ca_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gaabf46f157171dead5bf1f0a3da1aab93_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga5cea41d7dd9babf48937e939aa0d3c5b_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gae7adad053ab5e2a5f447851f7d34dc04_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga81493a122a9da884af36d087cbc80614_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/open.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_gab5300f917bbdfc5dafc093a60138f131_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gaf0a9a659af18b62ffa0520301402eabb_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan_gad40746585b3f8a77e5209301a9ad21cd_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/structiio__channel.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gae3a265d5053a2cac254eb59a8eeda9da_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/globals.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga28c43d91ddaf8856f2d1a79562072280_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga68c8e6c772dbf4bbec921c1dc050ab3e_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/structiio__context__info.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/iio_8h_source.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga000d2f4c8b72060db1c38ec905bf4156_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gac43421333d85b03e7aeb31eb60a676fe_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gacf9fe193b8183df86eab56df7da7361d_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga823b2e43e8d1bc0122266e83fe81fbc4_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan_ga279a930b7b597a06f454a30a0e770f85_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga18d5cb8d912b5b888b9b54c6d0c7f92c_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gac2d887e2f77423596487302d2728c99e_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/doc-- Up-to-date: /usr/share/doc/libiio0-doc/html/doc/codemodel.svg-- Up-to-date: /usr/share/doc/libiio0-doc/html/dynsections.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga1c7689aa48b6789168e266a0e9bfef7e_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_gab5300f917bbdfc5dafc093a60138f131_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga4e5e9abbd5c0129826ab9a623a635c70_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/structiio__data__format.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/functions_vars.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga343be1b2a9b4a23aa1ad6e22b5b334b3_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga7b73b6fa484da3af7735cd80b90f3464_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga30151c105a19b3fc3ad6376046d60bf9_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan_ga649d7821636c744753067e8301a84e6d_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gaeb192bd3730c8c65a4e5c29feca62257_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga4e5e9abbd5c0129826ab9a623a635c70_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga0d43279d1c04a32f06c627fa75ec5d13_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gaf910dce06335badc1ba307526c4112a6_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga68c8e6c772dbf4bbec921c1dc050ab3e_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan_ga4e618c6efb5a62e04a664f53f1b80d99_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan_ga649d7821636c744753067e8301a84e6d_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gab673fa9f0dd70dcc6dd756048593a0fa_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga6caadf077c112ae55a64276aa24ef832_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gae3a265d5053a2cac254eb59a8eeda9da_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__TopLevel_ga8b5f231e009524ab5be5f918e6f041c3_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga01151f264c7e22fcf8390b5303b51bb3_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gaa08ea63cf2ed45b5d47deb14019e12bf_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga0073a46392fcf6efaa488b75cf8bcb6c_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/iio-lock_8h_source.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/menudata.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga18a52045b14205192e3fbbcb4e2ddb58_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga6caadf077c112ae55a64276aa24ef832_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga19f42665351b5a2122c653de801f848b_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gaf64c20583fd66701afcc6c7ba3deb6ea_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga821ace05c0f77bf4f87be7555ae84d52_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gabf4e2755877dedae40a5fbeb54a3829e_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga1d105cd9079c1218c363db75cf504e0d_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga4d8f3a846d5df8ee97c91789014dcb16_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga0073a46392fcf6efaa488b75cf8bcb6c_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga821ace05c0f77bf4f87be7555ae84d52_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gace7a0de3e19a58c38f23e2a9b444dfff_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga8be1b9fa5383746ff8d76cedf1ff0156_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gac43421333d85b03e7aeb31eb60a676fe_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga8c5fc6f7ccee7f9da338833822f799ec_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/structiio__buffer.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gac2d887e2f77423596487302d2728c99e_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga233b868380bca0578907bda28d3a5480_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga33b167ee45641b618f5d45365df969c4_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gabf4e2755877dedae40a5fbeb54a3829e_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gace7a0de3e19a58c38f23e2a9b444dfff_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga2ae0fe2e179de9f6de10900f72fc28be_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gaa35f0bbf7f6be8f859adb3fc692c600e_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__TopLevel.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga36c7e7f895c58409dc129b128cc5983a_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gacf9fe193b8183df86eab56df7da7361d_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/sync_on.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gabf4e2755877dedae40a5fbeb54a3829e_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga4e5e9abbd5c0129826ab9a623a635c70_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga4d8f3a846d5df8ee97c91789014dcb16_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga6caadf077c112ae55a64276aa24ef832_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gafd133e49a1a694e394939b4c5a073cb5_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/globals_enum.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga8be1b9fa5383746ff8d76cedf1ff0156_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga66bdc45f6b55cd28e76945ead18686ca_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga891aa6ffd6290fc3848e4f14a923d1fb_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gaa08ea63cf2ed45b5d47deb14019e12bf_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gaabf46f157171dead5bf1f0a3da1aab93_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga8c5fc6f7ccee7f9da338833822f799ec_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga2013f7206e2dde3aedee31ba01945585_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga5f18bbe6c9e1993f26480f73f92e1ad5_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga41582140b8e1fe98148e51ae1350b816_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga6ecca643c857855e8aa27fee21553337_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga343be1b2a9b4a23aa1ad6e22b5b334b3_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gacb37ef830dcc100a9908d0592d1ff190_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga2ae0fe2e179de9f6de10900f72fc28be_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga451ca34c6c249a980d85e3ceaa7e3784_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gabcd0cd25e203976bdc525790b6fe4e23_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga343be1b2a9b4a23aa1ad6e22b5b334b3_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga638c2f54b187a1b137f9885f34fad338_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga4d8f3a846d5df8ee97c91789014dcb16_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga6f587251cdca7cd1983d6e3a2a5e3ae6_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga33b167ee45641b618f5d45365df969c4_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gaee1f1895db399936d29c5dff34eac21e_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga000d2f4c8b72060db1c38ec905bf4156_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/codemodel.svg-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga83e2e2ef3c9fa91561b41dd32c59194e_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga01151f264c7e22fcf8390b5303b51bb3_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga638c2f54b187a1b137f9885f34fad338_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gacf36dfa2fc04a80ce93db3b131bae099_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__TopLevel_gac261dc30aa66453d1eabed1e88aa8728_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gaee333f1061000b0b71298dff59104513_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga36c7e7f895c58409dc129b128cc5983a_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga0d43279d1c04a32f06c627fa75ec5d13_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga7d4d3e7aec9330c7649cd76df2f29b94_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga3baae3a4b76956f9a7bc31c2ebb5b682_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/iio_8h__incl.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga5cc6251fbf69e26befccb82d5f5a6625_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan_ga649d7821636c744753067e8301a84e6d_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga233b868380bca0578907bda28d3a5480_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/sync_off.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/search-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/enums_0.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/search.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/groups_3.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_4.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_4.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/groups_1.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/groups_0.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_0.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_1.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/files_0.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_7.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/variables_0.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/groups_2.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/variables_5.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/variables_5.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/variables_3.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/classes_0.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/close.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/variables_0.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/searchdata.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/nomatches.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/mag_sel.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/functions_0.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/variables_1.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/search_l.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/groups_0.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/search.css-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/enums_0.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/variables_1.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_8.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/groups_1.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/variables_3.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_5.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_7.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_1.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/search_r.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/groups_3.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_2.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_6.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_0.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/variables_4.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/variables_2.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/files_0.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_9.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/classes_0.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_2.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_8.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/functions_0.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_5.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/groups_2.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/search_m.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/groups_4.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_6.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_3.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/variables_2.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_9.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/groups_4.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/all_3.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/search/variables_4.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga5cea41d7dd9babf48937e939aa0d3c5b_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/iio-config_8h_source.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gaee1f1895db399936d29c5dff34eac21e_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gaf549d2113214add88129493697cb3587_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__TopLevel_ga55574e54de682499c5c08566c652114a_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga821ace05c0f77bf4f87be7555ae84d52_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gaf549d2113214add88129493697cb3587_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga41582140b8e1fe98148e51ae1350b816_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/structiio__device.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga41582140b8e1fe98148e51ae1350b816_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga04957021a00fb18689b9d9ae6f95a928_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gacf9fe193b8183df86eab56df7da7361d_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gac2d887e2f77423596487302d2728c99e_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/menu.js-- Up-to-date: /usr/share/doc/libiio0-doc/html/bdwn.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga4e5e9abbd5c0129826ab9a623a635c70_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gaf64c20583fd66701afcc6c7ba3deb6ea_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/index.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga50a525201c9b29ed1adb3090739d7ff0_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan_ga279a930b7b597a06f454a30a0e770f85_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga18d5cb8d912b5b888b9b54c6d0c7f92c_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga8be1b9fa5383746ff8d76cedf1ff0156_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/nav_g.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga3baae3a4b76956f9a7bc31c2ebb5b682_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gab673fa9f0dd70dcc6dd756048593a0fa_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga0d06dce5819723c3b16c4588eb5f477a_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga68819e214490f2d556599ee64799e267_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga000d2f4c8b72060db1c38ec905bf4156_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga451ca34c6c249a980d85e3ceaa7e3784_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/iio_8h__incl.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan_ga279a930b7b597a06f454a30a0e770f85_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_gabb89575442d19f28b6557eee97f8fafd_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__TopLevel_gaaa29e5bac86d00a1cef6e2d00b0ea24c_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga68c8e6c772dbf4bbec921c1dc050ab3e_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_gabb89575442d19f28b6557eee97f8fafd_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/classes.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga705f8f74e26d872dbec6cf718671c830_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga30151c105a19b3fc3ad6376046d60bf9_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga000d2f4c8b72060db1c38ec905bf4156_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga83e2e2ef3c9fa91561b41dd32c59194e_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan_ga279a930b7b597a06f454a30a0e770f85_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga0d43279d1c04a32f06c627fa75ec5d13_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/doxygen.css-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga5cc6251fbf69e26befccb82d5f5a6625_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/iiod-client_8h_source.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga50a525201c9b29ed1adb3090739d7ff0_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga9f864d556e8089450a3062fd7f184041_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/files.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gaf910dce06335badc1ba307526c4112a6_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/structiio__context.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga8c5fc6f7ccee7f9da338833822f799ec_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga2013f7206e2dde3aedee31ba01945585_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga0430f53a97a6fe7474416d7e2b228421_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gaee333f1061000b0b71298dff59104513_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/nav_h.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga4e5e9abbd5c0129826ab9a623a635c70_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gace7a0de3e19a58c38f23e2a9b444dfff_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga1c7689aa48b6789168e266a0e9bfef7e_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/tab_b.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga5f18bbe6c9e1993f26480f73f92e1ad5_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan_ga4e618c6efb5a62e04a664f53f1b80d99_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gabcd0cd25e203976bdc525790b6fe4e23_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/nav_f.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/tab_a.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga8c5fc6f7ccee7f9da338833822f799ec_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga28c43d91ddaf8856f2d1a79562072280_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga1d105cd9079c1218c363db75cf504e0d_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga19f42665351b5a2122c653de801f848b_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga41582140b8e1fe98148e51ae1350b816_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga9f864d556e8089450a3062fd7f184041_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga0430f53a97a6fe7474416d7e2b228421_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga3c86ab8607c4ae38e2a36fa8c6bedcfd_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga41582140b8e1fe98148e51ae1350b816_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga0d9e98519d12fc02a17a3f47011321fb_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan_ga4e618c6efb5a62e04a664f53f1b80d99_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga7d4d3e7aec9330c7649cd76df2f29b94_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gaf549d2113214add88129493697cb3587_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga83e2e2ef3c9fa91561b41dd32c59194e_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga0d06dce5819723c3b16c4588eb5f477a_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan_ga279a930b7b597a06f454a30a0e770f85_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__TopLevel_gaaa29e5bac86d00a1cef6e2d00b0ea24c_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/modules.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gaf64c20583fd66701afcc6c7ba3deb6ea_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga01151f264c7e22fcf8390b5303b51bb3_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga5f1aef2258268209b6486e788a1967ec_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga5cc6251fbf69e26befccb82d5f5a6625_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga705f8f74e26d872dbec6cf718671c830_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga4aafea4c127b872d5214d41ccb4ce8c1_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gac43421333d85b03e7aeb31eb60a676fe_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga176d11776f916c8148c6dfa1368cea3c_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/doc.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan_gad40746585b3f8a77e5209301a9ad21cd_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga2ae0fe2e179de9f6de10900f72fc28be_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga81493a122a9da884af36d087cbc80614_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gaa08ea63cf2ed45b5d47deb14019e12bf_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_gafd133e49a1a694e394939b4c5a073cb5_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga81493a122a9da884af36d087cbc80614_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga0d9e98519d12fc02a17a3f47011321fb_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga68819e214490f2d556599ee64799e267_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga30151c105a19b3fc3ad6376046d60bf9_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/tab_s.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga8c5fc6f7ccee7f9da338833822f799ec_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga8dd9233a125c95969dac270b4dd5e8b0_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga33b167ee45641b618f5d45365df969c4_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga8dd9233a125c95969dac270b4dd5e8b0_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga68c8e6c772dbf4bbec921c1dc050ab3e_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/graph_legend.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga823b2e43e8d1bc0122266e83fe81fbc4_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gac43421333d85b03e7aeb31eb60a676fe_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gae3a265d5053a2cac254eb59a8eeda9da_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga5f18bbe6c9e1993f26480f73f92e1ad5_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gae7adad053ab5e2a5f447851f7d34dc04_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gace7a0de3e19a58c38f23e2a9b444dfff_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/bc_s.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga000d2f4c8b72060db1c38ec905bf4156_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga50a525201c9b29ed1adb3090739d7ff0_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga06d2d53147ee7e028da0092350efc22c_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga891aa6ffd6290fc3848e4f14a923d1fb_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga4e5e9abbd5c0129826ab9a623a635c70_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/graph_legend.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga83e2e2ef3c9fa91561b41dd32c59194e_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga1d105cd9079c1218c363db75cf504e0d_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga3c86ab8607c4ae38e2a36fa8c6bedcfd_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gac43421333d85b03e7aeb31eb60a676fe_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/iio_8h__incl.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga3baae3a4b76956f9a7bc31c2ebb5b682_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gaabf46f157171dead5bf1f0a3da1aab93_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga5f269befaf97db803d0cfbc1ed122e6d_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga8dd9233a125c95969dac270b4dd5e8b0_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga7b73b6fa484da3af7735cd80b90f3464_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga9f864d556e8089450a3062fd7f184041_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga5cc6251fbf69e26befccb82d5f5a6625_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gaf0a9a659af18b62ffa0520301402eabb_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga5f269befaf97db803d0cfbc1ed122e6d_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga04957021a00fb18689b9d9ae6f95a928_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga01b435571a0bd034bc47987295821573_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer_ga705f8f74e26d872dbec6cf718671c830_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga19f42665351b5a2122c653de801f848b_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga01151f264c7e22fcf8390b5303b51bb3_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga5f269befaf97db803d0cfbc1ed122e6d_cgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gaf0a9a659af18b62ffa0520301402eabb_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga451ca34c6c249a980d85e3ceaa7e3784_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga68c8e6c772dbf4bbec921c1dc050ab3e_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/functions.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gab673fa9f0dd70dcc6dd756048593a0fa_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Buffer.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga451ca34c6c249a980d85e3ceaa7e3784_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga01151f264c7e22fcf8390b5303b51bb3_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Context_ga4aafea4c127b872d5214d41ccb4ce8c1_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga6f587251cdca7cd1983d6e3a2a5e3ae6_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_gaf910dce06335badc1ba307526c4112a6_icgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga7d4d3e7aec9330c7649cd76df2f29b94_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga06d2d53147ee7e028da0092350efc22c_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__TopLevel_ga8b5f231e009524ab5be5f918e6f041c3_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga3baae3a4b76956f9a7bc31c2ebb5b682_cgraph.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_gacf36dfa2fc04a80ce93db3b131bae099_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga06d2d53147ee7e028da0092350efc22c_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Scan_gad40746585b3f8a77e5209301a9ad21cd_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga18a52045b14205192e3fbbcb4e2ddb58_icgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Channel_ga0430f53a97a6fe7474416d7e2b228421_cgraph.map-- Up-to-date: /usr/share/doc/libiio0-doc/html/doxygen.png-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Debug_ga83e2e2ef3c9fa91561b41dd32c59194e_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/annotated.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__TopLevel_ga55574e54de682499c5c08566c652114a_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga41582140b8e1fe98148e51ae1350b816_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga176d11776f916c8148c6dfa1368cea3c_cgraph.png-- Up-to-date: /lib/udev/rules.d/90-libiio.rules-- Up-to-date: /usr/bin/iio_genxml-- Up-to-date: /usr/bin/iio_info-- Up-to-date: /usr/bin/iio_attr-- Up-to-date: /usr/bin/iio_readdev-- Up-to-date: /usr/bin/iio_reg-- Up-to-date: /usr/bin/iio_writedev-- Up-to-date: /usr/bin/iio_adi_xflow_check-- Up-to-date: /usr/sbin/iiod
Can you provide the output of your cmake command?
Here you go. I tried to figure out where to find or make a python configuration file but had no clue.
-- Looking for libusb-1.0 : FoundCMake Warning at bindings/python/CMakeLists.txt:4 (find_package): By not providing "FindPython.cmake" in CMAKE_MODULE_PATH this project has asked CMake to find a package configuration file provided by "Python", but CMake did not find one. Could not find a package configuration file provided by "Python" with any of the following names: PythonConfig.cmake python-config.cmake Add the installation prefix of "Python" to CMAKE_PREFIX_PATH or set "Python_DIR" to a directory containing one of the above files. If "Python" provides a separate development package or SDK, be sure it has been installed.-- Check for case-sensitive file systems-- File system is case-sensitive-- Configuring done-- Generating done-- Build files have been written to: /home/bert/temp/libiio