Linux LIBIIO python bindings

Hey all, I am a bit stuck on getting my system operational.

OS: Ubuntu 18.04 in a VM, host system is Windows 10

LIBIIO: compiled using the cmake build described by AD in https://wiki.analog.com/resources/eval/user-guides/ad-fmcdaq2-ebz/software/linux/applications/libiio

The pluto is recognized and I can interact with it / SSH is fine

PYADI: installed in python 3 using pip

When trying to import the adi package in python3 I get the following error message. I read some things that it may be caused by the incorrect installation of the python bindings but I'm puzzled on how to proceed.

Who can help?

Thanks

>>> import adi
Traceback (most recent call last):
File "<stdin>", line 1, in <module>
File "<frozen importlib._bootstrap>", line 971, in _find_and_load
File "<frozen importlib._bootstrap>", line 955, in _find_and_load_unlocked
File "<frozen importlib._bootstrap>", line 656, in _load_unlocked
File "<frozen importlib._bootstrap>", line 626, in _load_backward_compatible
File "/usr/local/lib/python3.6/dist-packages/pyadi_iio-0.0.5-py3.6.egg/adi/__init__.py", line 34, in <module>
File "<frozen importlib._bootstrap>", line 971, in _find_and_load
File "<frozen importlib._bootstrap>", line 955, in _find_and_load_unlocked
File "<frozen importlib._bootstrap>", line 656, in _load_unlocked
File "<frozen importlib._bootstrap>", line 626, in _load_backward_compatible
File "/usr/local/lib/python3.6/dist-packages/pyadi_iio-0.0.5-py3.6.egg/adi/ad9361.py", line 34, in <module>
File "<frozen importlib._bootstrap>", line 971, in _find_and_load
File "<frozen importlib._bootstrap>", line 955, in _find_and_load_unlocked
File "<frozen importlib._bootstrap>", line 656, in _load_unlocked
File "<frozen importlib._bootstrap>", line 626, in _load_backward_compatible
File "/usr/local/lib/python3.6/dist-packages/pyadi_iio-0.0.5-py3.6.egg/adi/context_manager.py", line 34, in <module>
File "/home/bert/temp/libiio/bindings/python/iio.py", line 71, in <module>
_get_backends_count = _lib.iio_get_backends_count
File "/usr/lib/python3.6/ctypes/__init__.py", line 361, in __getattr__
func = self.__getitem__(name)
File "/usr/lib/python3.6/ctypes/__init__.py", line 366, in __getitem__
func = self._FuncPtr((name_or_ordinal, self))
AttributeError: python3: undefined symbol: iio_get_backends_count