Hey all, I am a bit stuck on getting my system operational.
OS: Ubuntu 18.04 in a VM, host system is Windows 10
LIBIIO: compiled using the cmake build described by AD in https://wiki.analog.com/resources/eval/user-guides/ad-fmcdaq2-ebz/software/linux/applications/libiio
The pluto is recognized and I can interact with it / SSH is fine
PYADI: installed in python 3 using pip
When trying to import the adi package in python3 I get the following error message. I read some things that it may be caused by the incorrect installation of the python bindings but I'm puzzled on how to proceed.
Who can help?
Thanks
>>> import adiTraceback (most recent call last): File "<stdin>", line 1, in <module> File "<frozen importlib._bootstrap>", line 971, in _find_and_load File "<frozen importlib._bootstrap>", line 955, in _find_and_load_unlocked File "<frozen importlib._bootstrap>", line 656, in _load_unlocked File "<frozen importlib._bootstrap>", line 626, in _load_backward_compatible File "/usr/local/lib/python3.6/dist-packages/pyadi_iio-0.0.5-py3.6.egg/adi/__init__.py", line 34, in <module> File "<frozen importlib._bootstrap>", line 971, in _find_and_load File "<frozen importlib._bootstrap>", line 955, in _find_and_load_unlocked File "<frozen importlib._bootstrap>", line 656, in _load_unlocked File "<frozen importlib._bootstrap>", line 626, in _load_backward_compatible File "/usr/local/lib/python3.6/dist-packages/pyadi_iio-0.0.5-py3.6.egg/adi/ad9361.py", line 34, in <module> File "<frozen importlib._bootstrap>", line 971, in _find_and_load File "<frozen importlib._bootstrap>", line 955, in _find_and_load_unlocked File "<frozen importlib._bootstrap>", line 656, in _load_unlocked File "<frozen importlib._bootstrap>", line 626, in _load_backward_compatible File "/usr/local/lib/python3.6/dist-packages/pyadi_iio-0.0.5-py3.6.egg/adi/context_manager.py", line 34, in <module> File "/home/bert/temp/libiio/bindings/python/iio.py", line 71, in <module> _get_backends_count = _lib.iio_get_backends_count File "/usr/lib/python3.6/ctypes/__init__.py", line 361, in __getattr__ func = self.__getitem__(name) File "/usr/lib/python3.6/ctypes/__init__.py", line 366, in __getitem__ func = self._FuncPtr((name_or_ordinal, self))AttributeError: python3: undefined symbol: iio_get_backends_count
Yeah, there's the problem. Looks like there is a bug from a recent commit in master. I would roll back a bit by running this: git checkout a3a4c0803c51b7b207fec90244fe829a8a4fcc62
Then retry from cmake…
It appears as the libiio bindings are installed but not the actual library itself.
Can you run `iio_info -s` from the same directory you are running `import adi` from?
-Travis
Hi Travis, thank you for the fast reply
the command gives me
Library version: 0.18 (git tag: 1036e51)Compiled with backends: local xml ip usb serialAvailable contexts: 0: 0456:b673 (Analog Devices Inc. PlutoSDR (ADALM-PLUTO)), serial=104473ce6991000706000d007e2789c931 [usb:1.4.5]
Additional information: The previous python error shows when running from the /libiio/bindings/python/ directory. When running it from somewhere else the error message is different:
Python 3.6.9 (default, Nov 7 2019, 10:44:02) [GCC 8.3.0] on linuxType "help", "copyright", "credits" or "license" for more information.>>> import adiTraceback (most recent call last): File "<stdin>", line 1, in <module> File "/usr/local/lib/python3.6/dist-packages/pyadi_iio-0.0.5-py3.6.egg/adi/__init__.py", line 34, in <module> File "/usr/local/lib/python3.6/dist-packages/pyadi_iio-0.0.5-py3.6.egg/adi/ad9361.py", line 34, in <module> File "/usr/local/lib/python3.6/dist-packages/pyadi_iio-0.0.5-py3.6.egg/adi/context_manager.py", line 34, in <module>ModuleNotFoundError: No module named 'iio'
That means that the bindings are not on path.
I would recommend installing libiio to the standard location (not custom prefix), which is usually /usr/lib, and making sure the bindings are on path.
There is a note about this in the doc: analogdevicesinc.github.io/.../quick.html
Which is exactly whay I did. I cloned the pyadi-iio github project, and installed the package using
python3 setup.py install.
Here are the last lines from the process. It installed just fine?
removing 'build/bdist.linux-x86_64/egg' (and everything under it)Processing pyadi_iio-0.0.5-py3.6.eggRemoving /usr/local/lib/python3.6/dist-packages/pyadi_iio-0.0.5-py3.6.eggCopying pyadi_iio-0.0.5-py3.6.egg to /usr/local/lib/python3.6/dist-packagespyadi-iio 0.0.5 is already the active version in easy-install.pthInstalled /usr/local/lib/python3.6/dist-packages/pyadi_iio-0.0.5-py3.6.eggProcessing dependencies for pyadi-iio==0.0.5Searching for numpy==1.18.0rc1Best match: numpy 1.18.0rc1Processing numpy-1.18.0rc1-py3.6-linux-x86_64.eggnumpy 1.18.0rc1 is already the active version in easy-install.pth
That is pyadi-iio, not libiio. It looks like libiio is just in the directory "/home/bert/temp/libiio/" and not installed into a system path.
Sorry about that Trevis, I was confused because your link was referring to the pyadi install. The outcome of the make install of libiio is shown below, it installs just fine and I can call the executables as demonstrated above.
I think it has something to do with the binding of the pyadi module to the libiio driver bindings. Referring to https://ez.analog.com/linux-device-drivers/linux-software-drivers/f/q-a/116409/libiio---python-bindings
gives a very similar problem but I have no clue how to implement this in my machine on python 3.
How do install the iio bindings on my file system?
b41dd32c59194e_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/annotated.html-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__TopLevel_ga55574e54de682499c5c08566c652114a_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga41582140b8e1fe98148e51ae1350b816_icgraph.md5-- Up-to-date: /usr/share/doc/libiio0-doc/html/group__Device_ga176d11776f916c8148c6dfa1368cea3c_cgraph.png-- Up-to-date: /lib/udev/rules.d/90-libiio.rules-- Up-to-date: /usr/bin/iio_genxml-- Up-to-date: /usr/bin/iio_info-- Up-to-date: /usr/bin/iio_attr-- Up-to-date: /usr/bin/iio_readdev-- Up-to-date: /usr/bin/iio_reg-- Up-to-date: /usr/bin/iio_writedev-- Up-to-date: /usr/bin/iio_adi_xflow_check-- Up-to-date: /usr/sbin/iiodµ
When you do make install it tells you where it puts the iio.py file. When built with python3 it usually puts them in something similar to (say or 3.6): /usr/lib/python3.6/site-package
Therefore the export command would be:
export PYTHONPATH=$PYTHONPATH:'/usr/lib/python3.6/site-package
One thing I would also mention, pyadi-iio works fine on Windows as well. See the Windows section here about installing the bindings: https://wiki.analog.com/resources/tools-software/linux-software/pyadi-iio#prerequisites