AD5360
Production
The AD5360 / AD5361Â contain sixteen, 16-/14-bit DACs in a single 52-lead LQFP or 56-lead LFCSP package. They provide buffered voltage outputs with a span...
Datasheet
AD5360 on Analog.com
Hi, I'm having some issues trying to compile a raspberry pi kernel to use for my EVAL-AD5370 board.
I've followed the following sites:
https://wiki.analog.com/resources/tools-software/linux-build/generic/raspberrypi
https://linux.ime.usp.br/~marcelosc/2019/09/RaspberryPi-kernel-compilation
I've tried running this script : https://raw.githubusercontent.com/analogdevicesinc/wiki-scripts/master/linux/build_rpi_kernel_image.sh
But it keeps failing.
1. The git checkout rpi-4.19.y fails because that needs to be run from the linux-adi folder. I fixed that.
2. Then the script fails trying to make the adi_bcm2709_defconfig with some gcc-linaro Exec Format Errors and some Kconfig syntax and invalid options errors.
Any help would be greatly appreciated.
Hi,
What arm-toolchain do you use?
Dragos
I have tried both the one the script uses which is the 5.5.0-2017.10 linero.org one and I also tried the latest 2019 version.
Thanks!
I have tried both the one the script uses which is the 5.5.0-2017.10 linero.org one and I also tried the latest 2019 version.
Thanks!