Hi Travis, there are a few questions that I would like to clarify with you with regards to the ADALM Pluto. Below are the questions:
1) How do I activate and use the Digital Half-band Filters (HB1, HB2 and HB3) in AD9363 RF transceiver for both transmit and receive in Python? What are the syntax to do that? What is the purpose of the digital half-band filters in ADALM Pluto?
2) What is the purpose of the firmware in the ADALM Pluto? What does it do and how it is an integral part of the ADALM Pluto?
3) Is there any guide in the Analog Devices wiki page that provides the guide on how to program the FPGA in the Xilinx Zynq processor to control the AD9363 transceiver to transmit and receive signals?
4) Why is the AD9363 RF transceiver chip designed in such a way that both the transmit as well as the receive path have I/Q components(one is 0 degrees and the other is 90 degrees out of phase)? What is the purpose of having the I/Q components in the AD9363 chip?
5) I extended the tuning range of the ADALM Pluto to 70MHz-6GHz from the original specification of 325MHz-3.8GHz. After which, I went on to evaluate the ADALM Pluto's transmit by transmitting a tone at 800MHz into my spectrum analyzer. What I have observed is that, there are quite a number of harmonics and some spurs alongside with the main tone transmitted.
As far as I know, the ADALM Pluto is able to run out of specification and extend the frequency range from 325MHz-3.8GHz to the range of 70MHz-6GHz. Due to the wide tuning range, there is no band specific receive and transmit filters in the ADALM Pluto. Is it because at the extended frequency range, there is no filters to filter off the harmonics and spurs and that is why I am seeing a lot of harmonics and spurs in the spectrum analyzer of the transmitted tone?
6) Currently the design of digital FIR filter is available in MATLAB filter design wizard and in libad9361-iio design using C. Will there be any possibility that a Python binding is provided to design the FIR filter in Python in the future?