I'm porting the FMCOMMS5 to a custom board and every time I build the project I receive the following error:
### ad_ip_instance axi_iic axi_iic_main ### ad_ip_parameter axi_iic_main CONFIG.USE_BOARD_FLOW true ### ad_ip_parameter axi_iic_main CONFIG.IIC_BOARD_INTERFACE {IIC_MAIN} ERROR: [IP_Flow 19-3461] Value 'IIC_MAIN' is out of the range for parameter 'IIC Board Interface(IIC_BOARD_INTERFACE)' for BD Cell 'axi_iic_main' . Valid values are - Custom INFO: [IP_Flow 19-3438] Customization errors found on 'axi_iic_main'. Restoring to previous valid configuration. ERROR: [BD 41-245] set_property error - Value 'IIC_MAIN' is out of the range for parameter 'IIC Board Interface(IIC_BOARD_INTERFACE)' for BD Cell 'axi_iic_main' . Valid values are - Custom Customization errors found on 'axi_iic_main'. Restoring to previous valid configuration. ERROR: [Common 17-39] 'set_property' failed due to earlier errors. while executing "rdi::set_property CONFIG.IIC_BOARD_INTERFACE IIC_MAIN /axi_iic_main" invoked from within "set_property ${i_param} ${i_value} [get_bd_cells ${i_name}]" (procedure "ad_ip_parameter" line 3) invoked from within "ad_ip_parameter axi_iic_main CONFIG.IIC_BOARD_INTERFACE {IIC_MAIN}" (file "/home/nturner/gemini_hdl/projects/common/custom/custom_system_bd.tcl" line 64) while executing "source $ad_hdl_dir/projects/common/custom/custom_system_bd.tcl" (file "system_bd.tcl" line 3) while executing "source system_bd.tcl" (procedure "adi_project_xilinx" line 114) invoked from within "adi_project_xilinx fmcomms5_custom" (file "system_project.tcl" line 6) INFO: [Common 17-206] Exiting Vivado at Wed Jun 26 17:43:14 2019...
The project includes some 3rd party IP that includes the following lines:
<spirit:busInterfaces> <spirit:busInterface> <spirit:name>EMIO_I2C1</spirit:name> <spirit:displayName>EMIO I2C</spirit:displayName> <spirit:description>EMIO I2C connection to SC resources</spirit:description> <spirit:busType spirit:vendor="xilinx.com" spirit:library="interface" spirit:name="iic" spirit:version="1.0"/> <spirit:abstractionType spirit:vendor="xilinx.com" spirit:library="interface" spirit:name="iic_rtl" spirit:version="1.0"/> <spirit:slave/> <spirit:portMaps> <spirit:portMap> <spirit:logicalPort> <spirit:name>SDA_I</spirit:name> </spirit:logicalPort> <spirit:physicalPort> <spirit:name>sda_i</spirit:name> </spirit:physicalPort> </spirit:portMap> <spirit:portMap> <spirit:logicalPort> <spirit:name>SCL_I</spirit:name> </spirit:logicalPort> <spirit:physicalPort> <spirit:name>scl_i</spirit:name> </spirit:physicalPort> </spirit:portMap> <spirit:portMap> <spirit:logicalPort> <spirit:name>SDA_O</spirit:name> </spirit:logicalPort> <spirit:physicalPort> <spirit:name>sda_o</spirit:name> </spirit:physicalPort> </spirit:portMap> <spirit:portMap> <spirit:logicalPort> <spirit:name>SCL_O</spirit:name> </spirit:logicalPort> <spirit:physicalPort> <spirit:name>scl_o</spirit:name> </spirit:physicalPort> </spirit:portMap> <spirit:portMap> <spirit:logicalPort> <spirit:name>SDA_T</spirit:name> </spirit:logicalPort> <spirit:physicalPort> <spirit:name>sda_t</spirit:name> </spirit:physicalPort> </spirit:portMap> <spirit:portMap> <spirit:logicalPort> <spirit:name>SCL_T</spirit:name> </spirit:logicalPort> <spirit:physicalPort> <spirit:name>scl_t</spirit:name> </spirit:physicalPort> </spirit:portMap> </spirit:portMaps> </spirit:busInterface> <spirit:busInterface> <spirit:name>EXT_I2C</spirit:name> <spirit:busType spirit:vendor="xilinx.com" spirit:library="interface" spirit:name="iic" spirit:version="1.0"/> <spirit:abstractionType spirit:vendor="xilinx.com" spirit:library="interface" spirit:name="iic_rtl" spirit:version="1.0"/> <spirit:master/> <spirit:portMaps> <spirit:portMap> <spirit:logicalPort> <spirit:name>SCL_T</spirit:name> </spirit:logicalPort> <spirit:physicalPort> <spirit:name>ext_scl_t</spirit:name> </spirit:physicalPort> </spirit:portMap> <spirit:portMap> <spirit:logicalPort> <spirit:name>SDA_O</spirit:name> </spirit:logicalPort> <spirit:physicalPort> <spirit:name>ext_sda_o</spirit:name> </spirit:physicalPort> </spirit:portMap> <spirit:portMap> <spirit:logicalPort> <spirit:name>SDA_I</spirit:name> </spirit:logicalPort> <spirit:physicalPort> <spirit:name>ext_sda_i</spirit:name> </spirit:physicalPort> </spirit:portMap> <spirit:portMap> <spirit:logicalPort> <spirit:name>SDA_T</spirit:name> </spirit:logicalPort> <spirit:physicalPort> <spirit:name>ext_sda_t</spirit:name> </spirit:physicalPort> </spirit:portMap> <spirit:portMap> <spirit:logicalPort> <spirit:name>SCL_O</spirit:name> </spirit:logicalPort> <spirit:physicalPort> <spirit:name>ext_scl_o</spirit:name> </spirit:physicalPort> </spirit:portMap> <spirit:portMap> <spirit:logicalPort> <spirit:name>SCL_I</spirit:name> </spirit:logicalPort> <spirit:physicalPort> <spirit:name>ext_scl_i</spirit:name> </spirit:physicalPort> </spirit:portMap> </spirit:portMaps> </spirit:busInterface> </spirit:busInterfaces>
Would the way the I2C is implemented in this IP block interfere with how it's implemented in custom_system_bd.tcl? If not is there another reason for this error? Other posts seem to suggest a version mismatch, but I'm using Vivado 2018.2 with the hdl_2018_r2 branch.
Hi,
You will have to add the missing info in your board files or customize your IIC IP instance.Andrei
Hi,This is something new.Can you please start a build of the project from the Vivado GUI.If you kept the ADI build flow, open GUI. In the tcl console enter: cd <your project location> source ./system_project.tclAfter the error occurs, manually remove the AXI_IIC core from the block design and add it back again and take a look at the tcl commands vivado is outputting.
Let me know if it works, and if you see some differences in the tcl commands, comparing with the ones from the _bd.tcl script.Thanks,Andrei
When I manually add the IP core the tcl commands say:
update_compile_order -fileset sources_1 delete_bd_objs [get_bd_cells axi_iic_main] startgroup create_bd_cell -type ip -vlnv xilinx.com:ip:axi_iic:2.0 axi_iic_0 endgroup
Afterwords I get the option to run the automated board connection, which runs successfully, but connects the IIC port on the IP to a new external port I didn't create instead of the iic_main port I would like to use.
Should I use the create_bd_cell command that Vivado uses in place of the ad_ip_instance command from the _bd.tcl script?